![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the integrated NTAG module of MCUXpresso SDK devices.
Data Structures | |
| struct | ntag_config_t |
| NTAG user configuration. More... | |
Macros | |
| #define | RFT1503 |
| FD polling implementation options. More... | |
| #define | NTAG_IRQ NFCTag_IRQn |
| NTAG FD interrupt line. | |
Typedefs | |
| typedef void(* | ntag_field_detect_callback_t )(ntag_field_detect_t fd, void *userData) |
| NTAG Field Detect callback typedef. More... | |
Enumerations | |
| enum | ntag_state_t { kNTAG_StateActive, kNTAG_StateInactive } |
| ntag operating state More... | |
| enum | ntag_field_detect_t { kNTAG_FieldDetectIn, kNTAG_FieldDetectOut } |
| Field Detect line state. More... | |
Functions | |
| void | NTAG_GetDefaultConfig (ntag_config_t *config) |
| Sets the NTAG configuration structure to default values. More... | |
| void | NTAG_Init (const ntag_config_t *config) |
| Initialize the internal NTAG peripheral. More... | |
| ntag_field_detect_t | NTAG_PollFieldDetect (void) |
| Poll state of Field Detect line. More... | |
| void | NTAG_SetState (ntag_state_t state) |
| Configure NTAG operating state. More... | |
| struct ntag_config_t |
Data Fields | |
| ntag_field_detect_callback_t | callback |
| A callback function called at the transfer event. More... | |
| void * | userData |
| A callback parameter passed to the callback function. More... | |
| ntag_field_detect_callback_t ntag_config_t::callback |
| void* ntag_config_t::userData |
| #define RFT1503 |
| typedef void(* ntag_field_detect_callback_t)(ntag_field_detect_t fd, void *userData) |
| enum ntag_state_t |
| enum ntag_field_detect_t |
| void NTAG_GetDefaultConfig | ( | ntag_config_t * | config | ) |
| config | A pointer to the configuration structure. |
| void NTAG_Init | ( | const ntag_config_t * | config | ) |
| config | A pointer to the NTAG configuration structure |
| ntag_field_detect_t NTAG_PollFieldDetect | ( | void | ) |
| void NTAG_SetState | ( | ntag_state_t | state | ) |
| state | NTAG operating state |