MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Power: Power driver

Overview

The MCUXpresso SDK provides a power driver for the MCUXpresso SDK devices.

Function description

Power driver and library provides these functions:

Power enable and disable

Power driver provides two API's POWER_EnablePD() and POWER_DisablePD() to enable or disable the PDRUNCFG bits in SYSCON The PDRUNCFG has an inverted logic i.e. the peripheral is powered on when the bit is cleared and powered off when bit is set. So the API POWER_DisablePD() is used to power on a peripheral and POWER_EnablePD() is used to power off a peripheral. The API's take a parameter of type pd_bit_t which organizes the PDRUNCFG bits. The driver also provides two separate API's to power down and power up Flash, POWER_PowerDownFlash() and POWER_PowerUpFlash()

Files

file  fsl_power.h
 

Data Structures

struct  pm_bod_cfg_t
 BOD config. More...
 
struct  pm_power_config_t
 Power config. More...
 

Macros

#define POWER_BOD_ENABLE   ( 1 << 0 )
 BODVBAT configuration flag.
 
#define POWER_BOD_HIGH   ( 1 << 3 )
 ES2 BOD VBAT only.
 
#define POWER_BOD_LVL_1_75V   9
 BOD trigger level setting. More...
 
#define POWER_BOD_LVL_1_8V   10
 BOD trigger level 1.8V.
 
#define POWER_BOD_LVL_1_9V   11
 BOD trigger level 1.9V.
 
#define POWER_BOD_LVL_2_0V   12
 BOD trigger level 2.0V.
 
#define POWER_BOD_LVL_2_1V   13
 BOD trigger level 2.1V.
 
#define POWER_BOD_LVL_2_2V   14
 BOD trigger level 2.2V.
 
#define POWER_BOD_LVL_2_3V   15
 BOD trigger level 2.3V.
 
#define POWER_BOD_LVL_2_4V   16
 BOD trigger level 2.4V.
 
#define POWER_BOD_LVL_2_5V   17
 BOD trigger level 2.5V.
 
#define POWER_BOD_LVL_2_6V   18
 BOD trigger level 2.6V.
 
#define POWER_BOD_LVL_2_7V   19
 BOD trigger level 2.7V.
 
#define POWER_BOD_LVL_2_8V   20
 BOD trigger level 2.8V.
 
#define POWER_BOD_LVL_2_9V   21
 BOD trigger level 2.9V.
 
#define POWER_BOD_LVL_3_0V   22
 BOD trigger level 3.0V.
 
#define POWER_BOD_LVL_3_1V   23
 BOD trigger level 3.1V.
 
#define POWER_BOD_LVL_3_2V   24
 BOD trigger level 3.2V.
 
#define POWER_BOD_LVL_3_3V   25
 BOD trigger level 3.3V.
 
#define POWER_BOD_HYST_25MV   0
 BOD Hysteresis control setting. More...
 
#define POWER_BOD_HYST_50MV   1
 BOD Hysteresis control 50mV.
 
#define POWER_BOD_HYST_75MV   2
 BOD Hysteresis control 75mV.
 
#define POWER_BOD_HYST_100MV   3
 BOD Hysteresis control 100mV, default at Reset.
 
#define PM_CFG_SRAM_BANK_BIT_BASE   0
 SRAM banks definition list for retention in power down modes !
 
#define PM_CFG_SRAM_BANK0_RET   (1<<0)
 On ES1, this bank shall be kept in retention for Warmstart from power down.
 
#define PM_CFG_SRAM_BANK1_RET   (1<<1)
 Bank 1 shall be kept in retention.
 
#define PM_CFG_SRAM_BANK2_RET   (1<<2)
 Bank 2 shall be kept in retention.
 
#define PM_CFG_SRAM_BANK3_RET   (1<<3)
 Bank 3 shall be kept in retention.
 
#define PM_CFG_SRAM_BANK4_RET   (1<<4)
 Bank 4 shall be kept in retention.
 
#define PM_CFG_SRAM_BANK5_RET   (1<<5)
 Bank 5 shall be kept in retention.
 
#define PM_CFG_SRAM_BANK6_RET   (1<<6)
 Bank 6 shall be kept in retention.
 
#define PM_CFG_SRAM_BANK7_RET   (1<<7)
 On ES2, this bank shall be kept in retention for Warmstart.
 
#define PM_CFG_SRAM_BANK8_RET   (1<<8)
 Bank 8 shall be kept in retention.
 
#define PM_CFG_SRAM_BANK9_RET   (1<<9)
 Bank 9 shall be kept in retention.
 
#define PM_CFG_SRAM_BANK10_RET   (1<<10)
 Bank 10 shall be kept in retention.
 
#define PM_CFG_SRAM_BANK11_RET   (1<<11)
 Bank 11 shall be kept in retention.
 
#define PM_CFG_SRAM_ALL_RETENTION   0xFFF
 All banks shall be kept in retention.
 
#define PM_CFG_KEEP_AO_VOLTAGE   (1<<15)
 keep the same voltage on the Always-on power domain - typical used with FRO32K to avoid timebase drift
 
#define POWER_WAKEUPSRC_SYSTEM   LOWPOWER_WAKEUPSRCINT0_SYSTEM_IRQ
 BOD, Watchdog Timer, Flash controller, [DEEP SLEEP] BODVBAT [POWER_DOWN].
 
#define POWER_WAKEUPSRC_DMA   LOWPOWER_WAKEUPSRCINT0_DMA_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_GINT   LOWPOWER_WAKEUPSRCINT0_GINT_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_IRBLASTER   LOWPOWER_WAKEUPSRCINT0_IRBLASTER_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_PINT0   LOWPOWER_WAKEUPSRCINT0_PINT0_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_PINT1   LOWPOWER_WAKEUPSRCINT0_PINT1_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_PINT2   LOWPOWER_WAKEUPSRCINT0_PINT2_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_PINT3   LOWPOWER_WAKEUPSRCINT0_PINT3_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_SPIFI   LOWPOWER_WAKEUPSRCINT0_SPIFI_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_TIMER0   LOWPOWER_WAKEUPSRCINT0_TIMER0_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_TIMER1   LOWPOWER_WAKEUPSRCINT0_TIMER1_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_USART0   LOWPOWER_WAKEUPSRCINT0_USART0_IRQ
 [DEEP SLEEP, POWER DOWN]
 
#define POWER_WAKEUPSRC_USART1   LOWPOWER_WAKEUPSRCINT0_USART1_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_I2C0   LOWPOWER_WAKEUPSRCINT0_I2C0_IRQ
 [DEEP SLEEP, POWER DOWN]
 
#define POWER_WAKEUPSRC_I2C1   LOWPOWER_WAKEUPSRCINT0_I2C1_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_SPI0   LOWPOWER_WAKEUPSRCINT0_SPI0_IRQ
 [DEEP SLEEP, POWER DOWN]
 
#define POWER_WAKEUPSRC_SPI1   LOWPOWER_WAKEUPSRCINT0_SPI1_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_PWM0   LOWPOWER_WAKEUPSRCINT0_PWM0_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_PWM1   LOWPOWER_WAKEUPSRCINT0_PWM1_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_PWM2   LOWPOWER_WAKEUPSRCINT0_PWM2_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_PWM3   LOWPOWER_WAKEUPSRCINT0_PWM3_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_PWM4   LOWPOWER_WAKEUPSRCINT0_PWM4_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_PWM5   LOWPOWER_WAKEUPSRCINT0_PWM5_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_PWM6   LOWPOWER_WAKEUPSRCINT0_PWM6_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_PWM7   LOWPOWER_WAKEUPSRCINT0_PWM7_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_PWM8   LOWPOWER_WAKEUPSRCINT0_PWM8_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_PWM9   LOWPOWER_WAKEUPSRCINT0_PWM9_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_PWM10   LOWPOWER_WAKEUPSRCINT0_PWM10_IR
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_I2C2   LOWPOWER_WAKEUPSRCINT0_I2C2_IRQ
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_RTC   LOWPOWER_WAKEUPSRCINT0_RTC_IRQ
 [DEEP SLEEP, POWER DOWN]
 
#define POWER_WAKEUPSRC_NFCTAG   LOWPOWER_WAKEUPSRCINT0_NFCTAG_IRQ
 [DEEP SLEEP, POWER DOWN (ES2 Only), DEEP DOWN (ES2 only)]
 
#define POWER_WAKEUPSRC_MAILBOX   LOWPOWER_WAKEUPSRCINT0_MAILBOX_IRQ
 Mailbox, Wake-up from DEEP SLEEP and POWER DOWN low power mode [DEEP SLEEP, POWER DOWN].
 
#define POWER_WAKEUPSRC_ADC_SEQA   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_ADC_SEQA_IRQ << 32)
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_ADC_SEQB   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_ADC_SEQB_IRQ << 32)
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_ADC_THCMP_OVR   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_ADC_THCMP_OVR_IRQ << 32)
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_DMIC   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_DMIC_IRQ << 32)
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_HWVAD   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_HWVAD_IRQ << 32)
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_BLE_DP   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_BLE_DP_IRQ << 32)
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_BLE_DP0   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_BLE_DP0_IRQ << 32)
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_BLE_DP1   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_BLE_DP1_IRQ << 32)
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_BLE_DP2   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_BLE_DP2_IRQ << 32)
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_BLE_LL_ALL   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_BLE_LL_ALL_IRQ << 32)
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_ZIGBEE_MAC   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_ZIGBEE_MAC_IRQ << 32)
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_ZIGBEE_MODEM   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_ZIGBEE_MODEM_IRQ << 32)
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_RFP_TMU   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_RFP_TMU_IRQ << 32)
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_RFP_AGC   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_RFP_AGC_IRQ << 32)
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_ISO7816   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_ISO7816_IRQ << 32)
 [DEEP SLEEP]
 
#define POWER_WAKEUPSRC_ANA_COMP   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_ANA_COMP_IRQ << 32)
 [DEEP SLEEP, POWER DOWN]
 
#define POWER_WAKEUPSRC_WAKE_UP_TIMER0   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_WAKE_UP_TIMER0_IRQ << 32)
 [DEEP SLEEP, POWER DOWN]
 
#define POWER_WAKEUPSRC_WAKE_UP_TIMER1   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_WAKE_UP_TIMER1_IRQ << 32)
 [DEEP SLEEP, POWER DOWN]
 
#define POWER_WAKEUPSRC_BLE_WAKE_TIMER   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_BLE_WAKE_TIMER_IRQ << 32)
 [DEEP SLEEP, POWER DOWN]
 
#define POWER_WAKEUPSRC_BLE_OSC_EN   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_BLE_OSC_EN_IRQ << 32)
 [DEEP SLEEP, POWER DOWN]
 
#define POWER_WAKEUPSRC_IO   ((uint64_t)LOWPOWER_WAKEUPSRCINT1_IO_IRQ << 32)
 [POWER DOWN, DEEP DOWN]
 

Enumerations

enum  pd_bit_t {
  kPDRUNCFG_PD_LDO_ADC_EN = 22,
  kPDRUNCFG_PD_BOD_MEM_EN = 23,
  kPDRUNCFG_PD_BOD_CORE_EN = 24,
  kPDRUNCFG_PD_FRO32K_EN = 25,
  kPDRUNCFG_PD_XTAL32K_EN = 26,
  kPDRUNCFG_PD_BOD_ANA_COMP_EN = 27
}
 PDRUNCFG bits offset. More...
 
enum  pm_power_mode_t {
  PM_POWER_DOWN,
  PM_DEEP_DOWN
}
 Power modes. More...
 
enum  reset_cause_t { ,
  RESET_POR = (1 << 0),
  RESET_EXT_PIN = (1 << 1),
  RESET_BOR = (1 << 2),
  RESET_SYS_REQ = (1 << 3),
  RESET_WDT = (1 << 4),
  RESET_WAKE_DEEP_PD = (1 << 5),
  RESET_WAKE_PD = (1 << 6),
  RESET_SW_REQ = (1 << 7)
}
 Reset Cause definition. More...
 
enum  pm_ldo_volt_t {
  PM_LDO_VOLT_1_1V_DEFAULT,
  PM_LDO_VOLT_1_0V
}
 LDO voltage setting. More...
 

Power Configuration

void POWER_Init (void)
 Initialize the sdk power drivers. More...
 
void POWER_SetTrimDefaultActiveVoltage (void)
 Optimize the LDO voltage for power saving Initialize the power domains. More...
 
void POWER_BodSetUp (void)
 BODMEM and BODCORE setup. More...
 
void POWER_BodActivate (void)
 enable SW reset for the BODCORE More...
 
static void POWER_EnablePD (pd_bit_t en)
 API to enable PDRUNCFG bit in the Syscon. More...
 
static void POWER_DisablePD (pd_bit_t en)
 API to disable PDRUNCFG bit in the Syscon. More...
 
static uint32_t POWER_GetIoWakeStatus (void)
 Get IO and Ntag Field detect Wake-up sources from Power Down and Deep Power Down modes. More...
 
static void POWER_EnterSleep (void)
 Power API to enter sleep mode (Doze mode) More...
 
bool POWER_EnterPowerMode (pm_power_mode_t pm_power_mode, pm_power_config_t *pm_power_config)
 Power Library API to enter different power mode. More...
 
reset_cause_t POWER_GetResetCause (void)
 determine cause of reset More...
 
void POWER_ClearResetCause (void)
 Clear cause of reset.
 
uint32_t POWER_GetLibVersion (void)
 Power Library API to return the library version. More...
 
void POWER_BodVbatGetDefaultConfig (pm_bod_cfg_t *bod_cfg_p)
 Get default Vbat BOD config parameters, level @1.75V, Hysteresis @ 100mV. More...
 
bool POWER_BodVbatConfig (pm_bod_cfg_t *bod_cfg_p)
 Configure the VBAT BOD. More...
 
void POWER_ApplyLdoActiveVoltage (pm_ldo_volt_t ldoVolt)
 Configure the LDO voltage. More...
 
#define POWER_ENTER_SLEEP()   __DSB(); __WFI(); __ISB();
 Power API to enter sleep mode (Doze mode) More...
 

Data Structure Documentation

struct pm_bod_cfg_t

Data Fields

uint8_t bod_level
 BOD trigger level.
 
uint8_t bod_hyst
 BOD Hysteresis control.
 
uint8_t bod_cfg
 BOD config setting.
 
struct pm_power_config_t

Data Fields

pm_wake_source_t pm_wakeup_src
 Wakeup source select.
 
uint32_t pm_wakeup_io
 Wakeup IO.
 
uint32_t pm_config
 Power mode config.
 

Macro Definition Documentation

#define POWER_BOD_LVL_1_75V   9

Default at Reset , 1.7V on ES1

#define POWER_BOD_HYST_25MV   0

BOD Hysteresis control 25mV

#define POWER_ENTER_SLEEP ( )    __DSB(); __WFI(); __ISB();
Note
: The static inline function has not the expecetd effect in -O0. If order to force inline this macro is added
Returns
none

Enumeration Type Documentation

enum pd_bit_t
Enumerator
kPDRUNCFG_PD_LDO_ADC_EN 

Offset is 22, LDO ADC enabled.

kPDRUNCFG_PD_BOD_MEM_EN 

Offset is 23, BOD MEM enabled.

kPDRUNCFG_PD_BOD_CORE_EN 

Offset is 24, BOD CORE enabled.

kPDRUNCFG_PD_FRO32K_EN 

Offset is 25, FRO32K enabled.

kPDRUNCFG_PD_XTAL32K_EN 

Offset is 26, XTAL32K enabled.

kPDRUNCFG_PD_BOD_ANA_COMP_EN 

Offset is 27, Analog Comparator enabled.

Enumerator
PM_POWER_DOWN 

Power down mode.

PM_DEEP_DOWN 

Deep power down mode.

Enumerator
RESET_POR 

The last chip reset was caused by a Power On Reset.

RESET_EXT_PIN 

The last chip reset was caused by a Pad Reset.

RESET_BOR 

The last chip reset was caused by a Brown Out Detector.

RESET_SYS_REQ 

The last chip reset was caused by a System Reset requested by the ARM CPU.

RESET_WDT 

The last chip reset was caused by the Watchdog Timer.

RESET_WAKE_DEEP_PD 

The last chip reset was caused by a Wake-up I/O (GPIO or internal NTAG FD INT).

RESET_WAKE_PD 

The last CPU reset was caused by a Wake-up from Power down (many sources possible: timer, IO, ...).

RESET_SW_REQ 

The last chip reset was caused by a Software.

ES2 Only

Enumerator
PM_LDO_VOLT_1_1V_DEFAULT 

LDO voltage 1.1V.

PM_LDO_VOLT_1_0V 

not safe at system start/wakeup and CPU clock switch to higher frequency

Function Documentation

void POWER_Init ( void  )

Optimize the LDO voltage for power saving Initialize the power domains

Returns
none
void POWER_SetTrimDefaultActiveVoltage ( void  )
Returns
none
void POWER_BodSetUp ( void  )

Enable the BOD core and BOD mem Disable the analog comnparator clock

Returns
none
void POWER_BodActivate ( void  )
Returns
none
static void POWER_EnablePD ( pd_bit_t  en)
inlinestatic

Note that enabling the bit powers down the peripheral

Parameters
enperipheral for which to enable the PDRUNCFG bit
Returns
none
static void POWER_DisablePD ( pd_bit_t  en)
inlinestatic

Note that disabling the bit powers up the peripheral

Parameters
enperipheral for which to disable the PDRUNCFG bit
Returns
none
static uint32_t POWER_GetIoWakeStatus ( void  )
inlinestatic

Allow to identify the wake-up source when waking up from Power-Down modes or Deep Power Down modes. Status is reset by POR, RSTN, WDT. bit in range from 0 to 21 are for DIO0 to DIO21 bit 22 is NTAG field detect wakeup source

Returns
IO and Field detect Wake-up source
static void POWER_EnterSleep ( void  )
inlinestatic
Note
: If the user desires to program a wakeup timer before going to sleep, it needs to use either the fsl_wtimer.h API or use the POWER_SetLowPower() API instead see POWER_ENTER_SLEEP
Returns
none
bool POWER_EnterPowerMode ( pm_power_mode_t  pm_power_mode,
pm_power_config_t pm_power_config 
)

If requested mode is PM_POWER_DOWN, the API will perform the clamping of the DIOs if the PIO register has the bit IO_CLAMPING set: SYSCON->RETENTIONCTRL.IOCLAMP will be set

Parameters
pm_power_modePower modes
See Also
pm_power_mode_t
Parameters
pm_power_configPower config
See Also
pm_power_config_t
Returns
false if chip could not go to sleep. Configuration structure is incorrect
reset_cause_t POWER_GetResetCause ( void  )
Returns
reset_cause
uint32_t POWER_GetLibVersion ( void  )
Parameters
none
Returns
version number of the power library
void POWER_BodVbatGetDefaultConfig ( pm_bod_cfg_t bod_cfg_p)
Parameters
bod_cfg_pBOD config
See Also
pm_bod_cfg_t
Returns
none
bool POWER_BodVbatConfig ( pm_bod_cfg_t bod_cfg_p)
Parameters
bod_cfg_pBOD config
See Also
pm_bod_cfg_t
Returns
false if configuration parameters are incorrect
void POWER_ApplyLdoActiveVoltage ( pm_ldo_volt_t  ldoVolt)
Parameters
ldoVoltLDO voltage setting
See Also
pm_ldo_volt_t
Returns
none