![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
#include <asn1.h>
Data Fields | |
| size_t | len |
| unsigned char | unused_bits |
| unsigned char * | p |
Container for ASN1 bit strings.
| size_t mbedtls_asn1_bitstring::len |
ASN1 length, in octets.
| unsigned char mbedtls_asn1_bitstring::unused_bits |
Number of unused bits at the end of the string
| unsigned char* mbedtls_asn1_bitstring::p |
Raw ASN1 data for the bit string