The MCUXpresso SDK provides a peripheral driver for the OCOTP module of MCUXpresso SDK devices.
This section contains information describing the requirements for the on-chip eFuse OTP controller along with details about the block functionality and implementation.
OCOTP function group
The OCOTP driver support operaing API to allow read and write the fuse map.
Initialization and de-initialization
The funciton OCOTP_Init() is to initialize the OCOTP with peripheral base address and source clock frequency.
The function OCOTP_Deinit() is to de-initialize the OCOTP controller with peripheral base address.
Read and Write operation
The function OCOTP_ReloadShadowRegister() is to reload the value from the fuse map. this API should be called firstly before reading the register.
The OCOTP_ReadFuseShadowRegister() is to read the value from a given address, if operation is success, a known value will be return, othwise, a value of 0xBADABADA will be returned.
The function OCOTP_WriteFuseShadowRegister() will write a specific value to a known address. please check the return status o make sure whether the access to register is success.
OCOTP example
This example shows how to get the controller version using API. Due to the eFuse is One-Time programmable, example will only print the information of OCOTP controller version. If more operations are needed, please using the API to implement the write and read operation.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/ocotp
Note that, these value are used for calcalating the read/write timings. And the values should statisfy below rules:
Tsp_rd=(WAIT+1)/ipg_clk_freq should be >= 150ns; Tsp_pgm=(RELAX+1)/ipg_clk_freq should be >= 100ns; Trd = ((STROBE_READ+1)- 2*(RELAX_READ+1)) /ipg_clk_freq, The Trd is required to be larger than 40 ns. Tpgm = ((STROBE_PROG+1)- 2*(RELAX_PROG+1)) /ipg_clk_freq; The Tpgm should be configured within the range of 9000 ns < Tpgm < 11000 ns;
Data Fields |
| uint32_t | wait |
| | Wait time value to fill in the TIMING register. More...
|
| |
| uint32_t | relax |
| | Relax time value to fill in the TIMING register. More...
|
| |
| uint32_t | strobe_prog |
| | Storbe program time value to fill in the TIMING register. More...
|
| |
| uint32_t | strobe_read |
| | Storbe read time value to fill in the TIMING register. More...
|
| |
| uint32_t ocotp_timing_t::wait |
| uint32_t ocotp_timing_t::relax |
| uint32_t ocotp_timing_t::strobe_prog |
| uint32_t ocotp_timing_t::strobe_read |
| Enumerator |
|---|
| kStatus_OCOTP_AccessError |
eFuse and shadow register access error.
|
| kStatus_OCOTP_CrcFail |
CRC check failed.
|
| void OCOTP_Init |
( |
OCOTP_Type * |
base, |
|
|
uint32_t |
srcClock_Hz |
|
) |
| |
- Parameters
-
| base | OCOTP peripheral base address. |
| srcClock_Hz | source clock frequency in unit of Hz. |
| void OCOTP_Deinit |
( |
OCOTP_Type * |
base | ) |
|
- Return values
-
| kStatus_Success | upon successful execution, error status otherwise. |
| static bool OCOTP_CheckBusyStatus |
( |
OCOTP_Type * |
base | ) |
|
|
inlinestatic |
Checking this BUSY bit will help confirm if the OCOTP controller is ready for access.
- Parameters
-
| base | OCOTP peripheral base address. |
- Return values
-
| true | for bit set and false for cleared. |
| static bool OCOTP_CheckErrorStatus |
( |
OCOTP_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | OCOTP peripheral base address. |
- Return values
-
| true | for bit set and false for cleared. |
| static void OCOTP_ClearErrorStatus |
( |
OCOTP_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | OCOTP peripheral base address. |
| void OCOTP_ReloadShadowRegister |
( |
OCOTP_Type * |
base | ) |
|
This function will help reload the shadow register without reseting the OCOTP module. Please make sure the OCOTP has been initialized before calling this API.
- Parameters
-
| base | OCOTP peripheral base addess. |
| uint32_t OCOTP_ReadFuseShadowRegister |
( |
OCOTP_Type * |
base, |
|
|
uint32_t |
address |
|
) |
| |
- Parameters
-
| base | OCOTP peripheral base address. |
| address | the fuse address to be read from. |
| status_t OCOTP_WriteFuseShadowRegister |
( |
OCOTP_Type * |
base, |
|
|
uint32_t |
address, |
|
|
uint32_t |
data |
|
) |
| |
Please make sure the wrtie address is not locked while calling this API.
- Parameters
-
| base | OCOTP peripheral base address. |
| address | the fuse address to be written. |
| data | the value will be writen to fuse address. |
- Return values
-
| write | status, kStatus_Success for success and kStatus_Fail for failed. |
| static uint32_t OCOTP_GetVersion |
( |
OCOTP_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | OCOTP peripheral base address. |
- Return values
-