![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Initialize structure of TFA9XXX.
#include <fsl_tfa9xxx.h>
Data Fields | |
| tfa9xxx_protocol_t | protocol |
| Audio transfer protocol. | |
| tfa9xxx_audio_format_t | format |
| Audio format. | |
| uint8_t | slaveAddress |
| tfa9xxx device address | |
| codec_i2c_config_t | i2cConfig |
| i2c configuration | |
| uint8_t * | tfaContainer |
| tfa container array | |
| uint8_t | deviceIndex |
| tfa device index, starting from 0, up to TFA9XXX_DEV_NUM - 1 | |