![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Macros | |
#define | USB_DEVICE_CONFIG_SELF_POWER (1U) |
Whether device is self power. More... | |
#define | USB_DEVICE_CONFIG_ENDPOINTS (4U) |
How many endpoints are supported in the stack. More... | |
#define | USB_DEVICE_CONFIG_USE_TASK (0U) |
Whether the device task is enabled. More... | |
#define | USB_DEVICE_CONFIG_MAX_MESSAGES (8U) |
How many the notification message are supported when the device task is enabled. More... | |
#define | USB_DEVICE_CONFIG_USB20_TEST_MODE (0U) |
Whether test mode enabled. More... | |
#define | USB_DEVICE_CONFIG_CV_TEST (0U) |
Whether device CV test is enabled. More... | |
#define | USB_DEVICE_CONFIG_COMPLIANCE_TEST (0U) |
Whether device compliance test is enabled. More... | |
#define | USB_DEVICE_CONFIG_KEEP_ALIVE_MODE (0U) |
Whether the keep alive feature enabled. More... | |
#define | USB_DEVICE_CONFIG_BUFFER_PROPERTY_CACHEABLE (0U) |
Whether the transfer buffer is cache-enabled or not. More... | |
#define | USB_DEVICE_CONFIG_LOW_POWER_MODE (0U) |
Whether the low power mode is enabled or not. More... | |
#define | USB_DEVICE_CONFIG_REMOTE_WAKEUP (0U) |
The device remote wakeup is unsupported. More... | |
#define | USB_DEVICE_CONFIG_DETACH_ENABLE (0U) |
Whether the device detached feature is enabled or not. More... | |
#define | USB_DEVICE_CONFIG_ERROR_HANDLING (0U) |
Whether handle the USB bus error. More... | |
#define | USB_DEVICE_CHARGER_DETECT_ENABLE (0U) |
Whether the device charger detect feature is enabled or not. More... | |
class instance define | |
#define | USB_DEVICE_CONFIG_HID (0U) |
HID instance count. | |
#define | USB_DEVICE_CONFIG_CDC_ACM (1U) |
CDC ACM instance count. | |
#define | USB_DEVICE_CONFIG_MSC (0U) |
MSC instance count. | |
#define | USB_DEVICE_CONFIG_AUDIO (0U) |
Audio instance count. | |
#define | USB_DEVICE_CONFIG_PHDC (0U) |
PHDC instance count. | |
#define | USB_DEVICE_CONFIG_VIDEO (0U) |
Video instance count. | |
#define | USB_DEVICE_CONFIG_CCID (0U) |
CCID instance count. | |
#define | USB_DEVICE_CONFIG_PRINTER (0U) |
Printer instance count. | |
#define | USB_DEVICE_CONFIG_DFU (0U) |
DFU instance count. | |
#define USB_DEVICE_CONFIG_SELF_POWER (1U) |
1U supported, 0U not supported
#define USB_DEVICE_CONFIG_ENDPOINTS (4U) |
#define USB_DEVICE_CONFIG_USE_TASK (0U) |
#define USB_DEVICE_CONFIG_MAX_MESSAGES (8U) |
#define USB_DEVICE_CONFIG_USB20_TEST_MODE (0U) |
#define USB_DEVICE_CONFIG_CV_TEST (0U) |
#define USB_DEVICE_CONFIG_COMPLIANCE_TEST (0U) |
If the macro is enabled, the test mode and CV test macroes will be set.
#define USB_DEVICE_CONFIG_KEEP_ALIVE_MODE (0U) |
#define USB_DEVICE_CONFIG_BUFFER_PROPERTY_CACHEABLE (0U) |
#define USB_DEVICE_CONFIG_LOW_POWER_MODE (0U) |
#define USB_DEVICE_CONFIG_REMOTE_WAKEUP (0U) |
#define USB_DEVICE_CONFIG_DETACH_ENABLE (0U) |
#define USB_DEVICE_CONFIG_ERROR_HANDLING (0U) |
#define USB_DEVICE_CHARGER_DETECT_ENABLE (0U) |