![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Macros | |
| #define | LWIP_NETBIOS_RESPOND_NAME_QUERY 0 |
| #define LWIP_NETBIOS_RESPOND_NAME_QUERY 0 |
NetBIOS name of lwip device This must be uppercase until NETBIOS_STRCMP() is defined to a string comparision function that is case insensitive. If you want to use the netif's hostname, use this (with LWIP_NETIF_HOSTNAME): (ip_current_netif() != NULL ? ip_current_netif()->hostname != NULL ? ip_current_netif()->hostname : "" : "")
If this is not defined, netbiosns_set_name() can be called at runtime to change the name. Respond to NetBIOS name queries Default is disabled