![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Macros | |
| #define | LWIP_TIMERS 1 |
| #define | LWIP_TIMERS_CUSTOM 0 |
| #define LWIP_TIMERS 1 |
LWIP_TIMERS==0: Drop support for sys_timeout and lwip-internal cyclic timers. (the array of lwip-internal cyclic timers is still provided) (check NO_SYS_NO_TIMERS for compatibility to old versions)
| #define LWIP_TIMERS_CUSTOM 0 |
LWIP_TIMERS_CUSTOM==1: Provide your own timer implementation. Function prototypes in timeouts.h and the array of lwip-internal cyclic timers are still included, but the implementation is not. The following functions will be required: sys_timeouts_init(), sys_timeout(), sys_untimeout(), sys_timeouts_mbox_fetch()