![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Macros | |
| #define | LWIP_MPU_COMPATIBLE 0 |
| #define | LWIP_TCPIP_CORE_LOCKING 1 |
| #define | LWIP_TCPIP_CORE_LOCKING_INPUT 0 |
| #define | SYS_LIGHTWEIGHT_PROT 1 |
| #define | LWIP_ASSERT_CORE_LOCKED() |
| #define | LWIP_MARK_TCPIP_THREAD() |
| #define LWIP_MPU_COMPATIBLE 0 |
LWIP_MPU_COMPATIBLE: enables special memory management mechanism which makes lwip able to work on MPU (Memory Protection Unit) system by not passing stack-pointers to other threads (this decreases performance as memory is allocated from pools instead of keeping it on the stack)
| #define LWIP_TCPIP_CORE_LOCKING 1 |
LWIP_TCPIP_CORE_LOCKING Creates a global mutex that is held during TCPIP thread operations. Can be locked by client code to perform lwIP operations without changing into TCPIP thread using callbacks. See LOCK_TCPIP_CORE() and UNLOCK_TCPIP_CORE(). Your system should provide mutexes supporting priority inversion to use this.
| #define LWIP_TCPIP_CORE_LOCKING_INPUT 0 |
LWIP_TCPIP_CORE_LOCKING_INPUT: when LWIP_TCPIP_CORE_LOCKING is enabled, this lets tcpip_input() grab the mutex for input packets as well, instead of allocating a message and passing it to tcpip_thread.
ATTENTION: this does not work when tcpip_input() is called from interrupt context!
| #define SYS_LIGHTWEIGHT_PROT 1 |
SYS_LIGHTWEIGHT_PROT==1: enable inter-task protection (and task-vs-interrupt protection) for certain critical regions during buffer allocation, deallocation and memory allocation and deallocation. ATTENTION: This is required when using lwIP from more than one context! If you disable this, you must be sure what you are doing!
| #define LWIP_ASSERT_CORE_LOCKED | ( | ) |
Macro/function to check whether lwIP's threading/locking requirements are satisfied during current function call. This macro usually calls a function that is implemented in the OS-dependent sys layer and performs the following checks:
| #define LWIP_MARK_TCPIP_THREAD | ( | ) |
Called as first thing in the lwIP TCPIP thread. Can be used in conjunction with LWIP_ASSERT_CORE_LOCKED to check core locking.