![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Macros | |
| #define | TCPIP_THREAD_NAME "tcpip_thread" |
| #define | TCPIP_THREAD_STACKSIZE 0 |
| #define | TCPIP_THREAD_PRIO 1 |
| #define | TCPIP_MBOX_SIZE 0 |
| #define | LWIP_TCPIP_THREAD_ALIVE() |
| #define | SLIPIF_THREAD_NAME "slipif_loop" |
| #define | SLIPIF_THREAD_STACKSIZE 0 |
| #define | SLIPIF_THREAD_PRIO 1 |
| #define | DEFAULT_THREAD_NAME "lwIP" |
| #define | DEFAULT_THREAD_STACKSIZE 0 |
| #define | DEFAULT_THREAD_PRIO 1 |
| #define | DEFAULT_RAW_RECVMBOX_SIZE 0 |
| #define | DEFAULT_UDP_RECVMBOX_SIZE 0 |
| #define | DEFAULT_TCP_RECVMBOX_SIZE 0 |
| #define | DEFAULT_ACCEPTMBOX_SIZE 0 |
| #define TCPIP_THREAD_NAME "tcpip_thread" |
TCPIP_THREAD_NAME: The name assigned to the main tcpip thread.
| #define TCPIP_THREAD_STACKSIZE 0 |
TCPIP_THREAD_STACKSIZE: The stack size used by the main tcpip thread. The stack size value itself is platform-dependent, but is passed to sys_thread_new() when the thread is created.
| #define TCPIP_THREAD_PRIO 1 |
TCPIP_THREAD_PRIO: The priority assigned to the main tcpip thread. The priority value itself is platform-dependent, but is passed to sys_thread_new() when the thread is created.
| #define TCPIP_MBOX_SIZE 0 |
TCPIP_MBOX_SIZE: The mailbox size for the tcpip thread messages The queue size value itself is platform-dependent, but is passed to sys_mbox_new() when tcpip_init is called.
| #define LWIP_TCPIP_THREAD_ALIVE | ( | ) |
Define this to something that triggers a watchdog. This is called from tcpip_thread after processing a message.
| #define SLIPIF_THREAD_NAME "slipif_loop" |
SLIPIF_THREAD_NAME: The name assigned to the slipif_loop thread.
| #define SLIPIF_THREAD_STACKSIZE 0 |
SLIP_THREAD_STACKSIZE: The stack size used by the slipif_loop thread. The stack size value itself is platform-dependent, but is passed to sys_thread_new() when the thread is created.
| #define SLIPIF_THREAD_PRIO 1 |
SLIPIF_THREAD_PRIO: The priority assigned to the slipif_loop thread. The priority value itself is platform-dependent, but is passed to sys_thread_new() when the thread is created.
| #define DEFAULT_THREAD_NAME "lwIP" |
DEFAULT_THREAD_NAME: The name assigned to any other lwIP thread.
| #define DEFAULT_THREAD_STACKSIZE 0 |
DEFAULT_THREAD_STACKSIZE: The stack size used by any other lwIP thread. The stack size value itself is platform-dependent, but is passed to sys_thread_new() when the thread is created.
| #define DEFAULT_THREAD_PRIO 1 |
DEFAULT_THREAD_PRIO: The priority assigned to any other lwIP thread. The priority value itself is platform-dependent, but is passed to sys_thread_new() when the thread is created.
| #define DEFAULT_RAW_RECVMBOX_SIZE 0 |
DEFAULT_RAW_RECVMBOX_SIZE: The mailbox size for the incoming packets on a NETCONN_RAW. The queue size value itself is platform-dependent, but is passed to sys_mbox_new() when the recvmbox is created.
| #define DEFAULT_UDP_RECVMBOX_SIZE 0 |
DEFAULT_UDP_RECVMBOX_SIZE: The mailbox size for the incoming packets on a NETCONN_UDP. The queue size value itself is platform-dependent, but is passed to sys_mbox_new() when the recvmbox is created.
| #define DEFAULT_TCP_RECVMBOX_SIZE 0 |
DEFAULT_TCP_RECVMBOX_SIZE: The mailbox size for the incoming packets on a NETCONN_TCP. The queue size value itself is platform-dependent, but is passed to sys_mbox_new() when the recvmbox is created.
| #define DEFAULT_ACCEPTMBOX_SIZE 0 |
DEFAULT_ACCEPTMBOX_SIZE: The mailbox size for the incoming connections. The queue size value itself is platform-dependent, but is passed to sys_mbox_new() when the acceptmbox is created.