MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Phy_driver

Overview

Macros

#define FSL_PHY_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
 PHY driver version. More...
 
#define PHY_BASICCONTROL_REG   0x00U
 Defines the PHY registers. More...
 
#define PHY_BASICSTATUS_REG   0x01U
 The PHY basic status register. More...
 
#define PHY_ID1_REG   0x02U
 The PHY ID one register. More...
 
#define PHY_ID2_REG   0x03U
 The PHY ID two register. More...
 
#define PHY_AUTONEG_ADVERTISE_REG   0x04U
 The PHY auto-negotiate advertise register. More...
 
#define PHY_STATUS_REG   0x10
 The PHY Status register. More...
 
#define PHY_CONTROL_ID1   0x2000U
 The PHY ID1 register value. More...
 
#define PHY_BCTL_DUPLEX_MASK   0x0100U
 Defines the mask flag in basic control register. More...
 
#define PHY_BCTL_RESTART_AUTONEG_MASK   0x0200U
 The PHY restart auto negotiation mask. More...
 
#define PHY_BCTL_AUTONEG_MASK   0x1000U
 The PHY auto negotiation bit mask. More...
 
#define PHY_BCTL_SPEED_MASK   0x2000U
 The PHY speed bit mask. More...
 
#define PHY_BCTL_LOOP_MASK   0x4000U
 The PHY loop bit mask. More...
 
#define PHY_BCTL_RESET_MASK   0x8000U
 The PHY reset bit mask. More...
 
#define PHY_BCTL_SPEED_100M_MASK   0x2000U
 The PHY 100M speed mask. More...
 
#define PHY_LINK_READY_MASK   0x0001U
 The PHY link up. More...
 
#define PHY_STATUS_SPEED_MASK   0x0002U
 The PHY speed mask. More...
 
#define PHY_STATUS_DUPLEX_MASK   0x0004U
 The PHY duplex mask. More...
 
#define PHY_STATUS_FULL_DUPLEX_MASK   0x0004U
 The PHY duplex mask. More...
 
#define PHY_BSTATUS_LINKSTATUS_MASK   0x0004U
 Defines the mask flag in basic status register. More...
 
#define PHY_BSTATUS_AUTONEGABLE_MASK   0x0008U
 The PHY auto-negotiation ability mask. More...
 
#define PHY_BSTATUS_AUTONEGCOMP_MASK   0x0020U
 The PHY auto-negotiation complete mask. More...
 
#define PHY_100BaseT4_ABILITY_MASK   0x200U
 Defines the mask flag in PHY auto-negotiation advertise register. More...
 
#define PHY_100BASETX_FULLDUPLEX_MASK   0x100U
 The PHY has the 100M full duplex ability. More...
 
#define PHY_100BASETX_HALFDUPLEX_MASK   0x080U
 The PHY has the 100M full duplex ability. More...
 
#define PHY_10BASETX_FULLDUPLEX_MASK   0x040U
 The PHY has the 10M full duplex ability. More...
 
#define PHY_10BASETX_HALFDUPLEX_MASK   0x020U
 The PHY has the 10M full duplex ability. More...
 
#define FSL_PHY_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
 PHY driver version. More...
 

Enumerations

enum  _phy_status {
  kStatus_PHY_SMIVisitTimeout = MAKE_STATUS(kStatusGroup_PHY, 1),
  kStatus_PHY_AutoNegotiateFail = MAKE_STATUS(kStatusGroup_PHY, 2),
  kStatus_PHY_SMIVisitTimeout = MAKE_STATUS(kStatusGroup_PHY, 1),
  kStatus_PHY_AutoNegotiateFail = MAKE_STATUS(kStatusGroup_PHY, 2)
}
 Defines the PHY status. More...
 
enum  phy_speed_t {
  kPHY_Speed10M = 0U,
  kPHY_Speed100M,
  kPHY_Speed10M = 0U,
  kPHY_Speed100M
}
 Defines the PHY link speed. More...
 
enum  phy_duplex_t {
  kPHY_HalfDuplex = 0U,
  kPHY_FullDuplex,
  kPHY_HalfDuplex = 0U,
  kPHY_FullDuplex
}
 Defines the PHY link duplex. More...
 
enum  phy_loop_t {
  kPHY_LocalLoop = 0U,
  kPHY_RemoteLoop,
  kPHY_LocalLoop = 0U,
  kPHY_RemoteLoop
}
 Defines the PHY loopback mode. More...
 
enum  _phy_status {
  kStatus_PHY_SMIVisitTimeout = MAKE_STATUS(kStatusGroup_PHY, 1),
  kStatus_PHY_AutoNegotiateFail = MAKE_STATUS(kStatusGroup_PHY, 2),
  kStatus_PHY_SMIVisitTimeout = MAKE_STATUS(kStatusGroup_PHY, 1),
  kStatus_PHY_AutoNegotiateFail = MAKE_STATUS(kStatusGroup_PHY, 2)
}
 Defines the PHY status. More...
 
enum  phy_speed_t {
  kPHY_Speed10M = 0U,
  kPHY_Speed100M,
  kPHY_Speed10M = 0U,
  kPHY_Speed100M
}
 Defines the PHY link speed. More...
 
enum  phy_duplex_t {
  kPHY_HalfDuplex = 0U,
  kPHY_FullDuplex,
  kPHY_HalfDuplex = 0U,
  kPHY_FullDuplex
}
 Defines the PHY link duplex. More...
 
enum  phy_loop_t {
  kPHY_LocalLoop = 0U,
  kPHY_RemoteLoop,
  kPHY_LocalLoop = 0U,
  kPHY_RemoteLoop
}
 Defines the PHY loopback mode. More...
 

PHY Driver

status_t PHY_Init (ENET_Type *base, uint32_t phyAddr, uint32_t srcClock_Hz)
 Initializes PHY. More...
 
status_t PHY_Write (ENET_Type *base, uint32_t phyAddr, uint32_t phyReg, uint32_t data)
 PHY Write function. More...
 
status_t PHY_Read (ENET_Type *base, uint32_t phyAddr, uint32_t phyReg, uint32_t *dataPtr)
 PHY Read function. More...
 
status_t PHY_EnableLoopback (ENET_Type *base, uint32_t phyAddr, phy_loop_t mode, phy_speed_t speed, bool enable)
 Enables/disables PHY loopback. More...
 
status_t PHY_GetLinkStatus (ENET_Type *base, uint32_t phyAddr, bool *status)
 Gets the PHY link status. More...
 
status_t PHY_GetLinkSpeedDuplex (ENET_Type *base, uint32_t phyAddr, phy_speed_t *speed, phy_duplex_t *duplex)
 Gets the PHY link speed and duplex. More...
 

Macro Definition Documentation

#define FSL_PHY_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))

Version 2.0.0.

#define PHY_BASICCONTROL_REG   0x00U

The PHY basic control register.

#define PHY_BASICSTATUS_REG   0x01U
#define PHY_ID1_REG   0x02U
#define PHY_ID2_REG   0x03U
#define PHY_AUTONEG_ADVERTISE_REG   0x04U
#define PHY_STATUS_REG   0x10
#define PHY_CONTROL_ID1   0x2000U
#define PHY_BCTL_DUPLEX_MASK   0x0100U

The PHY duplex bit mask.

#define PHY_BCTL_RESTART_AUTONEG_MASK   0x0200U
#define PHY_BCTL_AUTONEG_MASK   0x1000U
#define PHY_BCTL_SPEED_MASK   0x2000U
#define PHY_BCTL_LOOP_MASK   0x4000U
#define PHY_BCTL_RESET_MASK   0x8000U
#define PHY_BCTL_SPEED_100M_MASK   0x2000U
#define PHY_LINK_READY_MASK   0x0001U
#define PHY_STATUS_SPEED_MASK   0x0002U
#define PHY_STATUS_DUPLEX_MASK   0x0004U
#define PHY_STATUS_FULL_DUPLEX_MASK   0x0004U
#define PHY_BSTATUS_LINKSTATUS_MASK   0x0004U

The PHY link status mask.

#define PHY_BSTATUS_AUTONEGABLE_MASK   0x0008U
#define PHY_BSTATUS_AUTONEGCOMP_MASK   0x0020U
#define PHY_100BaseT4_ABILITY_MASK   0x200U

The PHY have the T4 ability.

#define PHY_100BASETX_FULLDUPLEX_MASK   0x100U
#define PHY_100BASETX_HALFDUPLEX_MASK   0x080U
#define PHY_10BASETX_FULLDUPLEX_MASK   0x040U
#define PHY_10BASETX_HALFDUPLEX_MASK   0x020U
#define FSL_PHY_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))

Version 2.0.0.

Enumeration Type Documentation

Enumerator
kStatus_PHY_SMIVisitTimeout 

ENET PHY SMI visit timeout.

kStatus_PHY_AutoNegotiateFail 

ENET PHY AutoNegotiate Fail.

kStatus_PHY_SMIVisitTimeout 

ENET PHY SMI visit timeout.

kStatus_PHY_AutoNegotiateFail 

ENET PHY AutoNegotiate Fail.

This is align with the speed for ENET MAC.

Enumerator
kPHY_Speed10M 

ENET PHY 10M speed.

kPHY_Speed100M 

ENET PHY 100M speed.

kPHY_Speed10M 

ENET PHY 10M speed.

kPHY_Speed100M 

ENET PHY 100M speed.

Enumerator
kPHY_HalfDuplex 

ENET PHY half duplex.

kPHY_FullDuplex 

ENET PHY full duplex.

kPHY_HalfDuplex 

ENET PHY half duplex.

kPHY_FullDuplex 

ENET PHY full duplex.

enum phy_loop_t
Enumerator
kPHY_LocalLoop 

ENET PHY local loopback.

kPHY_RemoteLoop 

ENET PHY remote loopback.

kPHY_LocalLoop 

ENET PHY local loopback.

kPHY_RemoteLoop 

ENET PHY remote loopback.

Enumerator
kStatus_PHY_SMIVisitTimeout 

ENET PHY SMI visit timeout.

kStatus_PHY_AutoNegotiateFail 

ENET PHY AutoNegotiate Fail.

kStatus_PHY_SMIVisitTimeout 

ENET PHY SMI visit timeout.

kStatus_PHY_AutoNegotiateFail 

ENET PHY AutoNegotiate Fail.

This is align with the speed for ENET MAC.

Enumerator
kPHY_Speed10M 

ENET PHY 10M speed.

kPHY_Speed100M 

ENET PHY 100M speed.

kPHY_Speed10M 

ENET PHY 10M speed.

kPHY_Speed100M 

ENET PHY 100M speed.

Enumerator
kPHY_HalfDuplex 

ENET PHY half duplex.

kPHY_FullDuplex 

ENET PHY full duplex.

kPHY_HalfDuplex 

ENET PHY half duplex.

kPHY_FullDuplex 

ENET PHY full duplex.

enum phy_loop_t
Enumerator
kPHY_LocalLoop 

ENET PHY local loopback.

kPHY_RemoteLoop 

ENET PHY remote loopback.

kPHY_LocalLoop 

ENET PHY local loopback.

kPHY_RemoteLoop 

ENET PHY remote loopback.

Function Documentation

status_t PHY_Init ( ENET_Type *  base,
uint32_t  phyAddr,
uint32_t  srcClock_Hz 
)

This function initialize the SMI interface and initialize PHY. The SMI is the MII management interface between PHY and MAC, which should be firstly initialized before any other operation for PHY. The PHY initialize with auto-negotiation.

Parameters
baseENET peripheral base address.
phyAddrThe PHY address.
srcClock_HzThe module clock frequency - system clock for MII management interface - SMI.
Return values
kStatus_SuccessPHY initialize success
kStatus_PHY_SMIVisitTimeoutPHY SMI visit time out
kStatus_PHY_AutoNegotiateFailPHY auto negotiate fail
status_t PHY_Write ( ENET_Type *  base,
uint32_t  phyAddr,
uint32_t  phyReg,
uint32_t  data 
)

This function write data over the SMI to the specified PHY register. This function is called by all PHY interfaces.

Parameters
baseENET peripheral base address.
phyAddrThe PHY address.
phyRegThe PHY register.
dataThe data written to the PHY register.
Return values
kStatus_SuccessPHY write success
kStatus_PHY_SMIVisitTimeoutPHY SMI visit time out
status_t PHY_Read ( ENET_Type *  base,
uint32_t  phyAddr,
uint32_t  phyReg,
uint32_t *  dataPtr 
)

This interface read data over the SMI from the specified PHY register. This function is called by all PHY interfaces.

Parameters
baseENET peripheral base address.
phyAddrThe PHY address.
phyRegThe PHY register.
dataPtrThe address to store the data read from the PHY register.
Return values
kStatus_SuccessPHY read success
kStatus_PHY_SMIVisitTimeoutPHY SMI visit time out
status_t PHY_EnableLoopback ( ENET_Type *  base,
uint32_t  phyAddr,
phy_loop_t  mode,
phy_speed_t  speed,
bool  enable 
)
Parameters
baseENET peripheral base address.
phyAddrThe PHY address.
modeThe loopback mode to be enabled, please see "phy_loop_t". the two loopback mode should not be both set. when one loopback mode is set the other one should be disabled.
speedPHY speed for loopback mode.
enableTrue to enable, false to disable.
Return values
kStatus_SuccessPHY loopback success
kStatus_PHY_SMIVisitTimeoutPHY SMI visit time out
status_t PHY_GetLinkStatus ( ENET_Type *  base,
uint32_t  phyAddr,
bool *  status 
)
Parameters
baseENET peripheral base address.
phyAddrThe PHY address.
statusThe link up or down status of the PHY.
  • true the link is up.
  • false the link is down.
Return values
kStatus_SuccessPHY get link status success
kStatus_PHY_SMIVisitTimeoutPHY SMI visit time out
status_t PHY_GetLinkSpeedDuplex ( ENET_Type *  base,
uint32_t  phyAddr,
phy_speed_t *  speed,
phy_duplex_t *  duplex 
)
Parameters
baseENET peripheral base address.
phyAddrThe PHY address.
speedThe address of PHY link speed.
duplexThe link duplex of PHY.
Return values
kStatus_SuccessPHY get link speed and duplex success
kStatus_PHY_SMIVisitTimeoutPHY SMI visit time out