![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the Computer Operating Properly module (COP) of MCUXpresso SDK devices.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/cop
Data Structures | |
struct | cop_config_t |
Describes COP configuration structure. More... | |
Enumerations | |
enum | cop_clock_source_t { kCOP_LpoClock = 0U, kCOP_McgIrClock = 1U, kCOP_OscErClock = 2U, kCOP_BusClock = 3U } |
COP clock source selection. More... | |
enum | cop_timeout_cycles_t { kCOP_2Power5CyclesOr2Power13Cycles = 1U, kCOP_2Power8CyclesOr2Power16Cycles = 2U, kCOP_2Power10CyclesOr2Power18Cycles = 3U } |
Define the COP timeout cycles. More... | |
enum | cop_timeout_mode_t { kCOP_ShortTimeoutMode = 0U, kCOP_LongTimeoutMode = 1U } |
Define the COP timeout mode. More... | |
Driver version | |
#define | FSL_COP_DRIVER_VERSION (MAKE_VERSION(2, 0, 1)) |
COP driver version 2.0.1. More... | |
COP refresh sequence. | |
#define | COP_FIRST_BYTE_OF_REFRESH (0x55U) |
First byte of refresh sequence. | |
#define | COP_SECOND_BYTE_OF_REFRESH (0xAAU) |
Second byte of refresh sequence. | |
COP Functional Operation | |
void | COP_GetDefaultConfig (cop_config_t *config) |
Initializes the COP configuration structure. More... | |
void | COP_Init (SIM_Type *base, const cop_config_t *config) |
Initializes the COP module. More... | |
static void | COP_Disable (SIM_Type *base) |
De-initializes the COP module. More... | |
void | COP_Refresh (SIM_Type *base) |
Refreshes the COP timer. More... | |
struct cop_config_t |
Data Fields | |
bool | enableWindowMode |
COP run mode: window mode or normal mode. | |
cop_timeout_mode_t | timeoutMode |
COP timeout mode: long timeout or short timeout. | |
bool | enableStop |
Enable or disable COP in STOP mode. | |
bool | enableDebug |
Enable or disable COP in DEBUG mode. | |
cop_clock_source_t | clockSource |
Set COP clock source. | |
cop_timeout_cycles_t | timeoutCycles |
Set COP timeout value. | |
#define FSL_COP_DRIVER_VERSION (MAKE_VERSION(2, 0, 1)) |
enum cop_clock_source_t |
enum cop_timeout_cycles_t |
enum cop_timeout_mode_t |
void COP_GetDefaultConfig | ( | cop_config_t * | config | ) |
This function initializes the COP configuration structure to default values. The default values are:
config | Pointer to the COP configuration structure. |
void COP_Init | ( | SIM_Type * | base, |
const cop_config_t * | config | ||
) |
This function configures the COP. After it is called, the COP starts running according to the configuration. Because all COP control registers are write-once only, the COP_Init function and the COP_Disable function can be called only once. A second call has no effect.
Example:
base | SIM peripheral base address. |
config | The configuration of COP. |
|
inlinestatic |
This dedicated function is not provided. Instead, the COP_Disable function can be used to disable the COP.
Disables the COP module.
This function disables the COP Watchdog. Note: The COP configuration register is a write-once after reset. To disable the COP Watchdog, call this function first.
base | SIM peripheral base address. |
void COP_Refresh | ( | SIM_Type * | base | ) |
This function feeds the COP.
base | SIM peripheral base address. |