![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
This section describes the programming interface of the LTC eDMA Non Blocking functions
Modules | |
| LTC eDMA AES driver | |
| LTC eDMA DES driver | |
Data Structures | |
| struct | ltc_edma_handle_t |
| LTC eDMA handle. More... | |
Typedefs | |
| typedef void(* | ltc_edma_callback_t )(LTC_Type *base, ltc_edma_handle_t *handle, status_t status, void *userData) |
| LTC eDMA callback function. More... | |
| typedef status_t(* | ltc_edma_state_machine_t )(LTC_Type *base, ltc_edma_handle_t *handle) |
| LTC eDMA state machine function. More... | |
Functions | |
| void | LTC_CreateHandleEDMA (LTC_Type *base, ltc_edma_handle_t *handle, ltc_edma_callback_t callback, void *userData, edma_handle_t *inputFifoEdmaHandle, edma_handle_t *outputFifoEdmaHandle) |
| Init the LTC eDMA handle which is used in transactional functions. More... | |
Driver version | |
| #define | FSL_LTC_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 7)) |
| LTC EDMA driver version. More... | |
| struct _ltc_edma_handle |
It is defined only for private usage inside LTC eDMA driver.
Data Fields | |
| ltc_edma_callback_t | callback |
| Callback function. More... | |
| void * | userData |
| LTC callback function parameter. More... | |
| edma_handle_t * | inputFifoEdmaHandle |
| The eDMA TX channel used. More... | |
| edma_handle_t * | outputFifoEdmaHandle |
| The eDMA RX channel used. More... | |
| ltc_edma_state_machine_t | state_machine |
| State machine. More... | |
| uint32_t | state |
| Internal state. More... | |
| const uint8_t * | inData |
| Input data. More... | |
| uint8_t * | outData |
| Output data. More... | |
| uint32_t | size |
| Size of input and output data in bytes. More... | |
| uint32_t | modeReg |
| LTC mode register. More... | |
| uint8_t * | counter |
| Input counter (updates on return) | |
| const uint8_t * | key |
| Input key to use for forward AES cipher. | |
| uint32_t | keySize |
| Size of the input key, in bytes. More... | |
| uint8_t * | counterlast |
| Output cipher of last counter, for chained CTR calls. More... | |
| uint32_t * | szLeft |
| Output number of bytes in left unused in counterlast block. More... | |
| uint32_t | lastSize |
| Last size. More... | |
| ltc_edma_callback_t ltc_edma_handle_t::callback |
| void* ltc_edma_handle_t::userData |
| edma_handle_t* ltc_edma_handle_t::inputFifoEdmaHandle |
| edma_handle_t* ltc_edma_handle_t::outputFifoEdmaHandle |
| ltc_edma_state_machine_t ltc_edma_handle_t::state_machine |
| uint32_t ltc_edma_handle_t::state |
| const uint8_t* ltc_edma_handle_t::inData |
| uint8_t* ltc_edma_handle_t::outData |
| uint32_t ltc_edma_handle_t::size |
| uint32_t ltc_edma_handle_t::modeReg |
| uint32_t ltc_edma_handle_t::keySize |
Must be 16, 24, or 32.
| uint8_t* ltc_edma_handle_t::counterlast |
NULL can be passed if chained calls are not used.
| uint32_t* ltc_edma_handle_t::szLeft |
NULL can be passed if chained calls are not used.
| uint32_t ltc_edma_handle_t::lastSize |
| #define FSL_LTC_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 7)) |
Version 2.0.7.
| typedef void(* ltc_edma_callback_t)(LTC_Type *base, ltc_edma_handle_t *handle, status_t status, void *userData) |
| typedef status_t(* ltc_edma_state_machine_t)(LTC_Type *base, ltc_edma_handle_t *handle) |
It is defined only for private usage inside LTC eDMA driver.
| void LTC_CreateHandleEDMA | ( | LTC_Type * | base, |
| ltc_edma_handle_t * | handle, | ||
| ltc_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | inputFifoEdmaHandle, | ||
| edma_handle_t * | outputFifoEdmaHandle | ||
| ) |
| base | LTC module base address |
| handle | Pointer to ltc_edma_handle_t structure |
| callback | Callback function, NULL means no callback. |
| userData | Callback function parameter. |
| inputFifoEdmaHandle | User requested eDMA handle for Input FIFO eDMA. |
| outputFifoEdmaHandle | User requested eDMA handle for Output FIFO eDMA. |