The MCUXpresso SDK provides a peripheral driver for the Power Management Controller (PMC) module of MCUXpresso SDK devices. The PMC module contains internal voltage regulator, power on reset, low-voltage detect system, and high-voltage detect system.
| struct pmc_low_volt_detect_config_t |
| struct pmc_low_volt_warning_config_t |
| struct pmc_bandgap_buffer_config_t |
| bool pmc_bandgap_buffer_config_t::enable |
| bool pmc_bandgap_buffer_config_t::enableInLowPowerMode |
| Enumerator |
|---|
| kPMC_LowVoltDetectLowTrip |
Low-trip point selected (VLVD = VLVDL )
|
| kPMC_LowVoltDetectHighTrip |
High-trip point selected (VLVD = VLVDH )
|
| Enumerator |
|---|
| kPMC_LowVoltWarningLowTrip |
Low-trip point selected (VLVW = VLVW1)
|
| kPMC_LowVoltWarningMid1Trip |
Mid 1 trip point selected (VLVW = VLVW2)
|
| kPMC_LowVoltWarningMid2Trip |
Mid 2 trip point selected (VLVW = VLVW3)
|
| kPMC_LowVoltWarningHighTrip |
High-trip point selected (VLVW = VLVW4)
|
| Enumerator |
|---|
| kPMC_FreqRestrict |
Frequency is restricted in VLPx mode.
|
| kPMC_FreqUnrestrict |
Frequency is unrestricted in VLPx mode.
|
This function configures the low-voltage detect setting, including the trip point voltage setting, enables or disables the interrupt, enables or disables the system reset.
- Parameters
-
| base | PMC peripheral base address. |
| config | Low-voltage detect configuration structure. |
| static bool PMC_GetLowVoltDetectFlag |
( |
PMC_Type * |
base | ) |
|
|
inlinestatic |
This function reads the current LVDF status. If it returns 1, a low-voltage event is detected.
- Parameters
-
| base | PMC peripheral base address. |
- Returns
- Current low-voltage detect flag
- true: Low-voltage detected
- false: Low-voltage not detected
| static void PMC_ClearLowVoltDetectFlag |
( |
PMC_Type * |
base | ) |
|
|
inlinestatic |
This function acknowledges the low-voltage detection errors (write 1 to clear LVDF).
- Parameters
-
| base | PMC peripheral base address. |
This function configures the low-voltage warning setting, including the trip point voltage setting and enabling or disabling the interrupt.
- Parameters
-
| base | PMC peripheral base address. |
| config | Low-voltage warning configuration structure. |
| static bool PMC_GetLowVoltWarningFlag |
( |
PMC_Type * |
base | ) |
|
|
inlinestatic |
This function polls the current LVWF status. When 1 is returned, it indicates a low-voltage warning event. LVWF is set when V Supply transitions below the trip point or after reset and V Supply is already below the V LVW.
- Parameters
-
| base | PMC peripheral base address. |
- Returns
- Current LVWF status
- true: Low-voltage Warning Flag is set.
- false: the Low-voltage Warning does not happen.
| static void PMC_ClearLowVoltWarningFlag |
( |
PMC_Type * |
base | ) |
|
|
inlinestatic |
This function acknowledges the low voltage warning errors (write 1 to clear LVWF).
- Parameters
-
| base | PMC peripheral base address. |
This function configures the PMC bandgap, including the drive select and behavior in low-power mode.
- Parameters
-
| base | PMC peripheral base address. |
| config | Pointer to the configuration structure |
| static bool PMC_GetPeriphIOIsolationFlag |
( |
PMC_Type * |
base | ) |
|
|
inlinestatic |
This function reads the Acknowledge Isolation setting that indicates whether certain peripherals and the I/O pads are in a latched state as a result of having been in the VLLS mode.
- Parameters
-
| base | PMC peripheral base address. |
| base | Base address for current PMC instance. |
- Returns
- ACK isolation 0 - Peripherals and I/O pads are in a normal run state. 1 - Certain peripherals and I/O pads are in an isolated and latched state.
| static void PMC_ClearPeriphIOIsolationFlag |
( |
PMC_Type * |
base | ) |
|
|
inlinestatic |
This function clears the ACK Isolation flag. Writing one to this setting when it is set releases the I/O pads and certain peripherals to their normal run mode state.
- Parameters
-
| base | PMC peripheral base address. |
| static bool PMC_IsRegulatorInRunRegulation |
( |
PMC_Type * |
base | ) |
|
|
inlinestatic |
This function returns the regulator to run a regulation status. It provides the current status of the internal voltage regulator.
- Parameters
-
| base | PMC peripheral base address. |
| base | Base address for current PMC instance. |
- Returns
- Regulation status 0 - Regulator is in a stop regulation or in transition to/from the regulation. 1 - Regulator is in a run regulation.