![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | sai_dma_handle_t |
| SAI DMA transfer handle, users should not touch the content of the handle. More... | |
Typedefs | |
| typedef void(* | sai_dma_callback_t )(I2S_Type *base, sai_dma_handle_t *handle, status_t status, void *userData) |
| Define SAI DMA callback. | |
Driver version | |
| #define | FSL_SAI_DMA_DRIVER_VERSION (MAKE_VERSION(2, 3, 1)) |
| Version 2.3.1. | |
DMA Transactional | |
| void | SAI_TransferTxCreateHandleDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_dma_callback_t callback, void *userData, dma_handle_t *dmaHandle) |
| Initializes the SAI master DMA handle. More... | |
| void | SAI_TransferRxCreateHandleDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_dma_callback_t callback, void *userData, dma_handle_t *dmaHandle) |
| Initializes the SAI slave DMA handle. More... | |
| void | SAI_TransferTxSetFormatDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz) |
| Configures the SAI Tx audio format. More... | |
| void | SAI_TransferRxSetFormatDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz) |
| Configures the SAI Rx audio format. More... | |
| status_t | SAI_TransferSendDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_transfer_t *xfer) |
| Performs a non-blocking SAI transfer using DMA. More... | |
| status_t | SAI_TransferReceiveDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_transfer_t *xfer) |
| Performs a non-blocking SAI transfer using DMA. More... | |
| void | SAI_TransferAbortSendDMA (I2S_Type *base, sai_dma_handle_t *handle) |
| Aborts a SAI transfer using DMA. More... | |
| void | SAI_TransferAbortReceiveDMA (I2S_Type *base, sai_dma_handle_t *handle) |
| Aborts a SAI transfer using DMA. More... | |
| status_t | SAI_TransferGetSendCountDMA (I2S_Type *base, sai_dma_handle_t *handle, size_t *count) |
| Gets byte count sent by SAI. More... | |
| status_t | SAI_TransferGetReceiveCountDMA (I2S_Type *base, sai_dma_handle_t *handle, size_t *count) |
| Gets byte count received by SAI. More... | |
| void | SAI_TransferTxSetConfigDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_transceiver_t *saiConfig) |
| Configures the SAI Tx. More... | |
| void | SAI_TransferRxSetConfigDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_transceiver_t *saiConfig) |
| Configures the SAI Rx. More... | |
| struct _sai_dma_handle |
Data Fields | |
| dma_handle_t * | dmaHandle |
| DMA handler for SAI send. | |
| uint8_t | bytesPerFrame |
| Bytes in a frame. | |
| uint8_t | channel |
| Which Data channel SAI use. | |
| uint32_t | state |
| SAI DMA transfer internal state. | |
| sai_dma_callback_t | callback |
| Callback for users while transfer finish or error occurred. | |
| void * | userData |
| User callback parameter. | |
| sai_transfer_t | saiQueue [SAI_XFER_QUEUE_SIZE] |
| Transfer queue storing queued transfer. More... | |
| size_t | transferSize [SAI_XFER_QUEUE_SIZE] |
| Data bytes need to transfer. | |
| volatile uint8_t | queueUser |
| Index for user to queue transfer. More... | |
| volatile uint8_t | queueDriver |
| Index for driver to get the transfer data and size. | |
| sai_transfer_t sai_dma_handle_t::saiQueue[SAI_XFER_QUEUE_SIZE] |
| volatile uint8_t sai_dma_handle_t::queueUser |
| void SAI_TransferTxCreateHandleDMA | ( | I2S_Type * | base, |
| sai_dma_handle_t * | handle, | ||
| sai_dma_callback_t | callback, | ||
| void * | userData, | ||
| dma_handle_t * | dmaHandle | ||
| ) |
This function initializes the SAI master DMA handle, which can be used for other SAI master transactional APIs. Usually, for a specified SAI instance, call this API once to get the initialized handle.
| base | SAI base pointer. |
| handle | SAI DMA handle pointer. |
| base | SAI peripheral base address. |
| callback | Pointer to user callback function. |
| userData | User parameter passed to the callback function. |
| dmaHandle | DMA handle pointer, this handle shall be static allocated by users. |
| void SAI_TransferRxCreateHandleDMA | ( | I2S_Type * | base, |
| sai_dma_handle_t * | handle, | ||
| sai_dma_callback_t | callback, | ||
| void * | userData, | ||
| dma_handle_t * | dmaHandle | ||
| ) |
This function initializes the SAI slave DMA handle, which can be used for other SAI master transactional APIs. Usually, for a specified SAI instance, call this API once to get the initialized handle.
| base | SAI base pointer. |
| handle | SAI DMA handle pointer. |
| base | SAI peripheral base address. |
| callback | Pointer to user callback function. |
| userData | User parameter passed to the callback function. |
| dmaHandle | DMA handle pointer, this handle shall be static allocated by users. |
| void SAI_TransferTxSetFormatDMA | ( | I2S_Type * | base, |
| sai_dma_handle_t * | handle, | ||
| sai_transfer_format_t * | format, | ||
| uint32_t | mclkSourceClockHz, | ||
| uint32_t | bclkSourceClockHz | ||
| ) |
The audio format can be changed at run-time. This function configures the sample rate and audio data format to be transferred. This function also sets the eDMA parameter according to the format.
| base | SAI base pointer. |
| handle | SAI DMA handle pointer. |
| format | Pointer to SAI audio data format structure. |
| mclkSourceClockHz | SAI master clock source frequency in Hz. |
| bclkSourceClockHz | SAI bit clock source frequency in Hz. If bit clock source is master. clock, this value should equals to masterClockHz in format. |
| kStatus_Success | Audio format set successfully. |
| kStatus_InvalidArgument | The input arguments is invalid. |
| void SAI_TransferRxSetFormatDMA | ( | I2S_Type * | base, |
| sai_dma_handle_t * | handle, | ||
| sai_transfer_format_t * | format, | ||
| uint32_t | mclkSourceClockHz, | ||
| uint32_t | bclkSourceClockHz | ||
| ) |
The audio format can be changed at run-time. This function configures the sample rate and audio data format to be transferred. This function also sets eDMA parameter according to format.
| base | SAI base pointer. |
| handle | SAI DMA handle pointer. |
| format | Pointer to SAI audio data format structure. |
| mclkSourceClockHz | SAI master clock source frequency in Hz. |
| bclkSourceClockHz | SAI bit clock source frequency in Hz. If bit clock source is master. clock, this value should equals to masterClockHz in format. |
| kStatus_Success | Audio format set successfully. |
| kStatus_InvalidArgument | The input arguments is invalid. |
| status_t SAI_TransferSendDMA | ( | I2S_Type * | base, |
| sai_dma_handle_t * | handle, | ||
| sai_transfer_t * | xfer | ||
| ) |
| base | SAI base pointer. |
| handle | SAI DMA handle pointer. |
| xfer | Pointer to DMA transfer structure. |
| kStatus_Success | Successfully start the data receive. |
| kStatus_SAI_TxBusy | Previous receive still not finished. |
| kStatus_InvalidArgument | The input parameter is invalid. |
| status_t SAI_TransferReceiveDMA | ( | I2S_Type * | base, |
| sai_dma_handle_t * | handle, | ||
| sai_transfer_t * | xfer | ||
| ) |
| base | SAI base pointer |
| handle | SAI DMA handle pointer. |
| xfer | Pointer to DMA transfer structure. |
| kStatus_Success | Successfully start the data receive. |
| kStatus_SAI_RxBusy | Previous receive still not finished. |
| kStatus_InvalidArgument | The input parameter is invalid. |
| void SAI_TransferAbortSendDMA | ( | I2S_Type * | base, |
| sai_dma_handle_t * | handle | ||
| ) |
| base | SAI base pointer. |
| handle | SAI DMA handle pointer. |
| void SAI_TransferAbortReceiveDMA | ( | I2S_Type * | base, |
| sai_dma_handle_t * | handle | ||
| ) |
| base | SAI base pointer. |
| handle | SAI DMA handle pointer. |
| status_t SAI_TransferGetSendCountDMA | ( | I2S_Type * | base, |
| sai_dma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | SAI base pointer. |
| handle | SAI DMA handle pointer. |
| count | Bytes count sent by SAI. |
| kStatus_Success | Succeed get the transfer count. |
| kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. |
| status_t SAI_TransferGetReceiveCountDMA | ( | I2S_Type * | base, |
| sai_dma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | SAI base pointer. |
| handle | SAI DMA handle pointer. |
| count | Bytes count received by SAI. |
| kStatus_Success | Succeed get the transfer count. |
| kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. |
| void SAI_TransferTxSetConfigDMA | ( | I2S_Type * | base, |
| sai_dma_handle_t * | handle, | ||
| sai_transceiver_t * | saiConfig | ||
| ) |
| base | SAI base pointer. |
| handle | SAI DMA handle pointer. |
| saiConfig | sai configurations. |
| void SAI_TransferRxSetConfigDMA | ( | I2S_Type * | base, |
| sai_dma_handle_t * | handle, | ||
| sai_transceiver_t * | saiConfig | ||
| ) |
| base | SAI base pointer. |
| handle | SAI DMA handle pointer. |
| saiConfig | sai configurations. |