MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Deprecated List
Global CS42888_SetFuncMode (cs42888_handle_t *handle, cs42888_func_mode mode)
api, Do not use it anymore. It has been superceded by CS42888_SelectFunctionalMode.
Global ENET_StartExtC45SMIRead (ENET_Type *base, uint32_t phyAddr, uint32_t phyReg)
Do not use this function. It has been superceded by ENET_StartExtC45SMIWriteReg and ENET_StartExtC45SMIReadData.
Global ENET_StartExtC45SMIWrite (ENET_Type *base, uint32_t phyAddr, uint32_t phyReg, uint32_t data)
Do not use this function. It has been superceded by ENET_StartExtC45SMIWriteReg and ENET_StartExtC45SMIWriteData.
Global flexcan_clock_source_t

Do not use the kFLEXCAN_ClkSrcOs. It has been superceded kFLEXCAN_ClkSrc0

Do not use the kFLEXCAN_ClkSrcPeri. It has been superceded kFLEXCAN_ClkSrc1

Global GPIO_ClearPinsOutput (GPIO_Type *base, uint32_t mask)
Do not use this function. It has been superceded by GPIO_PortClear.
Global GPIO_DisableInterrupts (GPIO_Type *base, uint32_t mask)
Do not use this function. It has been superceded by GPIO_PortDisableInterrupts.
Global GPIO_ReadPadStatus (GPIO_Type *base, uint32_t pin)
Do not use this function. It has been superceded by GPIO_PinReadPadStatus.
Global GPIO_ReadPinInput (GPIO_Type *base, uint32_t pin)
Do not use this function. It has been superceded by GPIO_PinRead.
Global GPIO_SetPinInterruptConfig (GPIO_Type *base, uint32_t pin, gpio_interrupt_mode_t pinInterruptMode)
Do not use this function. It has been superceded by GPIO_PinSetInterruptConfig.
Global GPIO_SetPinsOutput (GPIO_Type *base, uint32_t mask)
Do not use this function. It has been superceded by GPIO_PortSet.
Global GPIO_WritePinOutput (GPIO_Type *base, uint32_t pin, uint8_t output)
Do not use this function. It has been superceded by GPIO_PinWrite.
Global RGPIO_ClearPinsOutput (RGPIO_Type *base, uint32_t mask)
Do not use this function. It has been superceded by RGPIO_PortClear.
Global RGPIO_ReadPinInput (RGPIO_Type *base, uint32_t pin)
Do not use this function. It has been superceded by RGPIO_PinRead.
Global RGPIO_SetPinsOutput (RGPIO_Type *base, uint32_t mask)
Do not use this function. It has been superceded by RGPIO_PortSet.
Global RGPIO_TogglePinsOutput (RGPIO_Type *base, uint32_t mask)
Do not use this function. It has been superceded by RGPIO_PortToggle.
Global RGPIO_WritePinOutput (RGPIO_Type *base, uint32_t pin, uint8_t output)
Do not use this function. It has been superceded by RGPIO_PinWrite.
Global SAI_RxGetDefaultConfig (sai_config_t *config)
Do not use this function. It has been superceded by SAI_GetClassicI2SConfig, SAI_GetLeftJustifiedConfig , SAI_GetRightJustifiedConfig, SAI_GetDSPConfig, SAI_GetTDMConfig
Global SAI_RxInit (I2S_Type *base, const sai_config_t *config)
Do not use this function. It has been superceded by SAI_Init
Global SAI_RxSetFormat (I2S_Type *base, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz)
Do not use this function. It has been superceded by SAI_RxSetConfig
Global SAI_TransferRxSetFormat (I2S_Type *base, sai_handle_t *handle, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz)
Do not use this function. It has been superceded by SAI_TransferRxSetConfig
Global SAI_TransferTxSetFormat (I2S_Type *base, sai_handle_t *handle, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz)
Do not use this function. It has been superceded by SAI_TransferTxSetConfig
Global SAI_TxGetDefaultConfig (sai_config_t *config)
Do not use this function. It has been superceded by SAI_GetClassicI2SConfig, SAI_GetLeftJustifiedConfig , SAI_GetRightJustifiedConfig, SAI_GetDSPConfig, SAI_GetTDMConfig
Global SAI_TxInit (I2S_Type *base, const sai_config_t *config)
Do not use this function. It has been superceded by SAI_Init
Global SAI_TxSetFormat (I2S_Type *base, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz)
Do not use this function. It has been superceded by SAI_TxSetConfig
Global WM8904_SetMasterSlave (wm8904_handle_t *handle, bool master)
DO NOT USE THIS API ANYMORE. IT HAS BEEN SUPERCEDED BY WM8904_SeMasterClock