MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
CMT: Carrier Modulator Transmitter Driver

Overview

The carrier modulator transmitter (CMT) module provides the means to generate the protocol timing and carrier signals for a side variety of encoding schemes. The CMT incorporates hardware to off-load the critical and/or lengthy timing requirements associated with signal generation from the CPU. The MCUXpresso SDK provides a driver for the CMT module of the MCUXpresso SDK devices.

Clock formulas

The CMT module has internal clock dividers. It was originally designed to be based on an 8 MHz bus clock that can be divided by 1, 2, 4, or 8 according to the specification. To be compatible with a higher bus frequency, the primary prescaler (PPS) was developed to receive a higher frequency and generate a clock enable signal called an intermediate frequency (IF). The IF must be approximately equal to 8 MHz and works as a clock enable to the secondary prescaler. For the PPS, the prescaler is selected according to the bus clock to generate an intermediate clock approximate to 8 MHz and is selected as (bus_clock_hz/8000000). The secondary prescaler is the "cmtDivider". The clocks for the CMT module are listed below.

  1. CMT clock frequency = bus_clock_Hz / (bus_clock_Hz / 8000000) / cmtDivider
  2. CMT carrier and generator frequency = CMT clock frequency / (highCount1 + lowCount1)
    (In FSK mode, the second frequency = CMT clock frequency / (highCount2 + lowCount2))
  3. CMT infrared output signal frequency
    a. In Time and Baseband mode
    CMT IRO signal mark time = (markCount + 1) / (CMT clock frequency / 8)
    CMT IRO signal space time = spaceCount / (CMT clock frequency / 8)
    b. In FSK mode
    CMT IRO signal mark time = (markCount + 1) / CMT carrier and generator frequency
    CMT IRO signal space time = spaceCount / CMT carrier and generator frequency

Typical use case

This is an example code to initialize data.

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/cmt This is an example IRQ handler to change the mark and space count to complete data modulation.

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/cmt

Data Structures

struct  cmt_modulate_config_t
 CMT carrier generator and modulator configuration structure. More...
 
struct  cmt_config_t
 CMT basic configuration structure. More...
 

Enumerations

enum  cmt_mode_t {
  kCMT_DirectIROCtl = 0x00U,
  kCMT_TimeMode = 0x01U,
  kCMT_FSKMode = 0x05U,
  kCMT_BasebandMode = 0x09U
}
 The modes of CMT. More...
 
enum  cmt_primary_clkdiv_t {
  kCMT_PrimaryClkDiv1 = 0U,
  kCMT_PrimaryClkDiv2 = 1U,
  kCMT_PrimaryClkDiv3 = 2U,
  kCMT_PrimaryClkDiv4 = 3U,
  kCMT_PrimaryClkDiv5 = 4U,
  kCMT_PrimaryClkDiv6 = 5U,
  kCMT_PrimaryClkDiv7 = 6U,
  kCMT_PrimaryClkDiv8 = 7U,
  kCMT_PrimaryClkDiv9 = 8U,
  kCMT_PrimaryClkDiv10 = 9U,
  kCMT_PrimaryClkDiv11 = 10U,
  kCMT_PrimaryClkDiv12 = 11U,
  kCMT_PrimaryClkDiv13 = 12U,
  kCMT_PrimaryClkDiv14 = 13U,
  kCMT_PrimaryClkDiv15 = 14U,
  kCMT_PrimaryClkDiv16 = 15U
}
 The CMT clock divide primary prescaler. More...
 
enum  cmt_second_clkdiv_t {
  kCMT_SecondClkDiv1 = 0U,
  kCMT_SecondClkDiv2 = 1U,
  kCMT_SecondClkDiv4 = 2U,
  kCMT_SecondClkDiv8 = 3U
}
 The CMT clock divide secondary prescaler. More...
 
enum  cmt_infrared_output_polarity_t {
  kCMT_IROActiveLow = 0U,
  kCMT_IROActiveHigh = 1U
}
 The CMT infrared output polarity. More...
 
enum  cmt_infrared_output_state_t {
  kCMT_IROCtlLow = 0U,
  kCMT_IROCtlHigh = 1U
}
 The CMT infrared output signal state control. More...
 
enum  _cmt_interrupt_enable { kCMT_EndOfCycleInterruptEnable = CMT_MSC_EOCIE_MASK }
 CMT interrupt configuration structure, default settings all disabled. More...
 

Driver version

#define FSL_CMT_DRIVER_VERSION   (MAKE_VERSION(2, 0, 3))
 CMT driver version 2.0.3. More...
 

Initialization and deinitialization

void CMT_GetDefaultConfig (cmt_config_t *config)
 Gets the CMT default configuration structure. More...
 
void CMT_Init (CMT_Type *base, const cmt_config_t *config, uint32_t busClock_Hz)
 Initializes the CMT module. More...
 
void CMT_Deinit (CMT_Type *base)
 Disables the CMT module and gate control. More...
 

Basic Control Operations

void CMT_SetMode (CMT_Type *base, cmt_mode_t mode, cmt_modulate_config_t *modulateConfig)
 Selects the mode for CMT. More...
 
cmt_mode_t CMT_GetMode (CMT_Type *base)
 Gets the mode of the CMT module. More...
 
uint32_t CMT_GetCMTFrequency (CMT_Type *base, uint32_t busClock_Hz)
 Gets the actual CMT clock frequency. More...
 
static void CMT_SetCarrirGenerateCountOne (CMT_Type *base, uint32_t highCount, uint32_t lowCount)
 Sets the primary data set for the CMT carrier generator counter. More...
 
static void CMT_SetCarrirGenerateCountTwo (CMT_Type *base, uint32_t highCount, uint32_t lowCount)
 Sets the secondary data set for the CMT carrier generator counter. More...
 
void CMT_SetModulateMarkSpace (CMT_Type *base, uint32_t markCount, uint32_t spaceCount)
 Sets the modulation mark and space time period for the CMT modulator. More...
 
static void CMT_EnableExtendedSpace (CMT_Type *base, bool enable)
 Enables or disables the extended space operation. More...
 
void CMT_SetIroState (CMT_Type *base, cmt_infrared_output_state_t state)
 Sets the IRO (infrared output) signal state. More...
 
static void CMT_EnableInterrupts (CMT_Type *base, uint32_t mask)
 Enables the CMT interrupt. More...
 
static void CMT_DisableInterrupts (CMT_Type *base, uint32_t mask)
 Disables the CMT interrupt. More...
 
static uint32_t CMT_GetStatusFlags (CMT_Type *base)
 Gets the end of the cycle status flag. More...
 

Data Structure Documentation

struct cmt_modulate_config_t

Data Fields

uint8_t highCount1
 The high-time for carrier generator first register. More...
 
uint8_t lowCount1
 The low-time for carrier generator first register. More...
 
uint8_t highCount2
 The high-time for carrier generator second register for FSK mode. More...
 
uint8_t lowCount2
 The low-time for carrier generator second register for FSK mode. More...
 
uint16_t markCount
 The mark time for the modulator gate. More...
 
uint16_t spaceCount
 The space time for the modulator gate. More...
 

Field Documentation

uint8_t cmt_modulate_config_t::highCount1
uint8_t cmt_modulate_config_t::lowCount1
uint8_t cmt_modulate_config_t::highCount2
uint8_t cmt_modulate_config_t::lowCount2
uint16_t cmt_modulate_config_t::markCount
uint16_t cmt_modulate_config_t::spaceCount
struct cmt_config_t

Data Fields

bool isInterruptEnabled
 Timer interrupt 0-disable, 1-enable. More...
 
bool isIroEnabled
 The IRO output 0-disabled, 1-enabled. More...
 
cmt_infrared_output_polarity_t iroPolarity
 The IRO polarity. More...
 
cmt_second_clkdiv_t divider
 The CMT clock divide prescaler. More...
 

Field Documentation

bool cmt_config_t::isInterruptEnabled
bool cmt_config_t::isIroEnabled
cmt_infrared_output_polarity_t cmt_config_t::iroPolarity
cmt_second_clkdiv_t cmt_config_t::divider

Macro Definition Documentation

#define FSL_CMT_DRIVER_VERSION   (MAKE_VERSION(2, 0, 3))

Enumeration Type Documentation

enum cmt_mode_t
Enumerator
kCMT_DirectIROCtl 

Carrier modulator is disabled and the IRO signal is directly in software control.

kCMT_TimeMode 

Carrier modulator is enabled in time mode.

kCMT_FSKMode 

Carrier modulator is enabled in FSK mode.

kCMT_BasebandMode 

Carrier modulator is enabled in baseband mode.

The primary clock divider is used to divider the bus clock to get the intermediate frequency to approximately equal to 8 MHZ. When the bus clock is 8 MHZ, set primary prescaler to "kCMT_PrimaryClkDiv1".

Enumerator
kCMT_PrimaryClkDiv1 

The intermediate frequency is the bus clock divided by 1.

kCMT_PrimaryClkDiv2 

The intermediate frequency is the bus clock divided by 2.

kCMT_PrimaryClkDiv3 

The intermediate frequency is the bus clock divided by 3.

kCMT_PrimaryClkDiv4 

The intermediate frequency is the bus clock divided by 4.

kCMT_PrimaryClkDiv5 

The intermediate frequency is the bus clock divided by 5.

kCMT_PrimaryClkDiv6 

The intermediate frequency is the bus clock divided by 6.

kCMT_PrimaryClkDiv7 

The intermediate frequency is the bus clock divided by 7.

kCMT_PrimaryClkDiv8 

The intermediate frequency is the bus clock divided by 8.

kCMT_PrimaryClkDiv9 

The intermediate frequency is the bus clock divided by 9.

kCMT_PrimaryClkDiv10 

The intermediate frequency is the bus clock divided by 10.

kCMT_PrimaryClkDiv11 

The intermediate frequency is the bus clock divided by 11.

kCMT_PrimaryClkDiv12 

The intermediate frequency is the bus clock divided by 12.

kCMT_PrimaryClkDiv13 

The intermediate frequency is the bus clock divided by 13.

kCMT_PrimaryClkDiv14 

The intermediate frequency is the bus clock divided by 14.

kCMT_PrimaryClkDiv15 

The intermediate frequency is the bus clock divided by 15.

kCMT_PrimaryClkDiv16 

The intermediate frequency is the bus clock divided by 16.

The second prescaler can be used to divide the 8 MHZ CMT clock by 1, 2, 4, or 8 according to the specification.

Enumerator
kCMT_SecondClkDiv1 

The CMT clock is the intermediate frequency frequency divided by 1.

kCMT_SecondClkDiv2 

The CMT clock is the intermediate frequency frequency divided by 2.

kCMT_SecondClkDiv4 

The CMT clock is the intermediate frequency frequency divided by 4.

kCMT_SecondClkDiv8 

The CMT clock is the intermediate frequency frequency divided by 8.

Enumerator
kCMT_IROActiveLow 

The CMT infrared output signal polarity is active-low.

kCMT_IROActiveHigh 

The CMT infrared output signal polarity is active-high.

Enumerator
kCMT_IROCtlLow 

The CMT Infrared output signal state is controlled to low.

kCMT_IROCtlHigh 

The CMT Infrared output signal state is controlled to high.

This structure contains the settings for all of the CMT interrupt configurations.

Enumerator
kCMT_EndOfCycleInterruptEnable 

CMT end of cycle interrupt.

Function Documentation

void CMT_GetDefaultConfig ( cmt_config_t *  config)

This API gets the default configuration structure for the CMT_Init(). Use the initialized structure unchanged in CMT_Init() or modify fields of the structure before calling the CMT_Init().

Parameters
configThe CMT configuration structure pointer.
void CMT_Init ( CMT_Type *  base,
const cmt_config_t *  config,
uint32_t  busClock_Hz 
)

This function ungates the module clock and sets the CMT internal clock, interrupt, and infrared output signal for the CMT module.

Parameters
baseCMT peripheral base address.
configThe CMT basic configuration structure.
busClock_HzThe CMT module input clock - bus clock frequency.
void CMT_Deinit ( CMT_Type *  base)

This function disables CMT modulator, interrupts, and gates the CMT clock control. CMT_Init must be called to use the CMT again.

Parameters
baseCMT peripheral base address.
void CMT_SetMode ( CMT_Type *  base,
cmt_mode_t  mode,
cmt_modulate_config_t *  modulateConfig 
)
Parameters
baseCMT peripheral base address.
modeThe CMT feature mode enumeration. See "cmt_mode_t".
modulateConfigThe carrier generation and modulator configuration.
cmt_mode_t CMT_GetMode ( CMT_Type *  base)
Parameters
baseCMT peripheral base address.
Returns
The CMT mode. kCMT_DirectIROCtl Carrier modulator is disabled; the IRO signal is directly in software control. kCMT_TimeMode Carrier modulator is enabled in time mode. kCMT_FSKMode Carrier modulator is enabled in FSK mode. kCMT_BasebandMode Carrier modulator is enabled in baseband mode.
uint32_t CMT_GetCMTFrequency ( CMT_Type *  base,
uint32_t  busClock_Hz 
)
Parameters
baseCMT peripheral base address.
busClock_HzCMT module input clock - bus clock frequency.
Returns
The CMT clock frequency.
static void CMT_SetCarrirGenerateCountOne ( CMT_Type *  base,
uint32_t  highCount,
uint32_t  lowCount 
)
inlinestatic

This function sets the high-time and low-time of the primary data set for the CMT carrier generator counter to control the period and the duty cycle of the output carrier signal. If the CMT clock period is Tcmt, the period of the carrier generator signal equals (highCount + lowCount) * Tcmt. The duty cycle equals to highCount / (highCount + lowCount).

Parameters
baseCMT peripheral base address.
highCountThe number of CMT clocks for carrier generator signal high time, integer in the range of 1 ~ 0xFF.
lowCountThe number of CMT clocks for carrier generator signal low time, integer in the range of 1 ~ 0xFF.
static void CMT_SetCarrirGenerateCountTwo ( CMT_Type *  base,
uint32_t  highCount,
uint32_t  lowCount 
)
inlinestatic

This function is used for FSK mode setting the high-time and low-time of the secondary data set CMT carrier generator counter to control the period and the duty cycle of the output carrier signal. If the CMT clock period is Tcmt, the period of the carrier generator signal equals (highCount + lowCount) * Tcmt. The duty cycle equals highCount / (highCount + lowCount).

Parameters
baseCMT peripheral base address.
highCountThe number of CMT clocks for carrier generator signal high time, integer in the range of 1 ~ 0xFF.
lowCountThe number of CMT clocks for carrier generator signal low time, integer in the range of 1 ~ 0xFF.
void CMT_SetModulateMarkSpace ( CMT_Type *  base,
uint32_t  markCount,
uint32_t  spaceCount 
)

This function sets the mark time period of the CMT modulator counter to control the mark time of the output modulated signal from the carrier generator output signal. If the CMT clock frequency is Fcmt and the carrier out signal frequency is fcg:

  • In Time and Baseband mode: The mark period of the generated signal equals (markCount + 1) / (Fcmt/8). The space period of the generated signal equals spaceCount / (Fcmt/8).
  • In FSK mode: The mark period of the generated signal equals (markCount + 1)/fcg. The space period of the generated signal equals spaceCount / fcg.
Parameters
baseBase address for current CMT instance.
markCountThe number of clock period for CMT modulator signal mark period, in the range of 0 ~ 0xFFFF.
spaceCountThe number of clock period for CMT modulator signal space period, in the range of the 0 ~ 0xFFFF.
static void CMT_EnableExtendedSpace ( CMT_Type *  base,
bool  enable 
)
inlinestatic

This function is used to make the space period longer for time, baseband, and FSK modes.

Parameters
baseCMT peripheral base address.
enableTrue enable the extended space, false disable the extended space.
void CMT_SetIroState ( CMT_Type *  base,
cmt_infrared_output_state_t  state 
)

Changes the states of the IRO signal when the kCMT_DirectIROMode mode is set and the IRO signal is enabled.

Parameters
baseCMT peripheral base address.
stateThe control of the IRO signal. See "cmt_infrared_output_state_t"
static void CMT_EnableInterrupts ( CMT_Type *  base,
uint32_t  mask 
)
inlinestatic

This function enables the CMT interrupts according to the provided mask if enabled. The CMT only has the end of the cycle interrupt - an interrupt occurs at the end of the modulator cycle. This interrupt provides a means for the user to reload the new mark/space values into the CMT modulator data registers and verify the modulator mark and space. For example, to enable the end of cycle, do the following.

Parameters
baseCMT peripheral base address.
maskThe interrupts to enable. Logical OR of _cmt_interrupt_enable.
static void CMT_DisableInterrupts ( CMT_Type *  base,
uint32_t  mask 
)
inlinestatic

This function disables the CMT interrupts according to the provided maskIf enabled. The CMT only has the end of the cycle interrupt. For example, to disable the end of cycle, do the following.

Parameters
baseCMT peripheral base address.
maskThe interrupts to enable. Logical OR of _cmt_interrupt_enable.
static uint32_t CMT_GetStatusFlags ( CMT_Type *  base)
inlinestatic

The flag is set:

  • When the modulator is not currently active and carrier and modulator are set to start the initial CMT transmission.
  • At the end of each modulation cycle when the counter is reloaded and the carrier and modulator are enabled.
    Parameters
    baseCMT peripheral base address.
    Returns
    Current status of the end of cycle status flag
    • non-zero: End-of-cycle has occurred.
    • zero: End-of-cycle has not yet occurred since the flag last cleared.