MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

Data Structures

struct  lpuart_rtos_config_t
 LPUART RTOS configuration structure. More...
 

Driver version

#define FSL_LPUART_FREERTOS_DRIVER_VERSION   (MAKE_VERSION(2, 3, 0))
 LPUART FreeRTOS driver version 2.3.0. More...
 

LPUART RTOS Operation

int LPUART_RTOS_Init (lpuart_rtos_handle_t *handle, lpuart_handle_t *t_handle, const lpuart_rtos_config_t *cfg)
 Initializes an LPUART instance for operation in RTOS. More...
 
int LPUART_RTOS_Deinit (lpuart_rtos_handle_t *handle)
 Deinitializes an LPUART instance for operation. More...
 

LPUART transactional Operation

int LPUART_RTOS_Send (lpuart_rtos_handle_t *handle, const uint8_t *buffer, uint32_t length)
 Sends data in the background. More...
 
int LPUART_RTOS_Receive (lpuart_rtos_handle_t *handle, uint8_t *buffer, uint32_t length, size_t *received)
 Receives data. More...
 

Data Structure Documentation

struct lpuart_rtos_config_t

Data Fields

LPUART_Type * base
 UART base address.
 
uint32_t srcclk
 UART source clock in Hz.
 
uint32_t baudrate
 Desired communication speed.
 
lpuart_parity_mode_t parity
 Parity setting.
 
lpuart_stop_bit_count_t stopbits
 Number of stop bits to use.
 
uint8_t * buffer
 Buffer for background reception.
 
uint32_t buffer_size
 Size of buffer for background reception.
 
bool enableRxRTS
 RX RTS enable.
 
bool enableTxCTS
 TX CTS enable.
 
lpuart_transmit_cts_source_t txCtsSource
 TX CTS source.
 
lpuart_transmit_cts_config_t txCtsConfig
 TX CTS configure.
 

Macro Definition Documentation

#define FSL_LPUART_FREERTOS_DRIVER_VERSION   (MAKE_VERSION(2, 3, 0))

Function Documentation

int LPUART_RTOS_Init ( lpuart_rtos_handle_t *  handle,
lpuart_handle_t *  t_handle,
const lpuart_rtos_config_t *  cfg 
)
Parameters
handleThe RTOS LPUART handle, the pointer to an allocated space for RTOS context.
t_handleThe pointer to an allocated space to store the transactional layer internal state.
cfgThe pointer to the parameters required to configure the LPUART after initialization.
Returns
0 succeed, others failed
int LPUART_RTOS_Deinit ( lpuart_rtos_handle_t *  handle)

This function deinitializes the LPUART module, sets all register value to the reset value, and releases the resources.

Parameters
handleThe RTOS LPUART handle.
int LPUART_RTOS_Send ( lpuart_rtos_handle_t *  handle,
const uint8_t *  buffer,
uint32_t  length 
)

This function sends data. It is an synchronous API. If the hardware buffer is full, the task is in the blocked state.

Parameters
handleThe RTOS LPUART handle.
bufferThe pointer to buffer to send.
lengthThe number of bytes to send.
int LPUART_RTOS_Receive ( lpuart_rtos_handle_t *  handle,
uint8_t *  buffer,
uint32_t  length,
size_t *  received 
)

This function receives data from LPUART. It is an synchronous API. If any data is immediately available it is returned immediately and the number of bytes received.

Parameters
handleThe RTOS LPUART handle.
bufferThe pointer to buffer where to write received data.
lengthThe number of bytes to receive.
receivedThe pointer to a variable of size_t where the number of received data is filled.