MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
SWM: Switch Matrix Module

Overview

The MCUXpresso SDK provides a peripheral driver for the Switch Matrix Module (SWM) module of MCUXpresso SDK devices.

SWM: Switch Matrix Module

SWM Operations

The function SWM_SetMovablePinSelect() will selects a movable pin designated by its GPIO port and bit numbers to a function.

The function SWM_SetFixedMovablePinSelect() will selects a fixed movable pin designated by its GPIO port and bit numbers to a function.

The function SWM_SetFixedPinSelect() will enables a fixed-pin function in PINENABLE0 or PINENABLE1.

Files

file  fsl_swm.h
 

Functions

void SWM_SetMovablePinSelect (SWM_Type *base, swm_select_movable_t func, swm_port_pin_type_t swm_port_pin)
 Assignment of digital peripheral functions to pins. More...
 
void SWM_SetFixedPinSelect (SWM_Type *base, swm_select_fixed_pin_t func, bool enable)
 Enable the fixed-pin function. More...
 

swm connections

enum  swm_port_pin_type_t {
  kSWM_PortPin_P0_0 = 0U,
  kSWM_PortPin_P0_1 = 1U,
  kSWM_PortPin_P0_2 = 2U,
  kSWM_PortPin_P0_3 = 3U,
  kSWM_PortPin_P0_4 = 4U,
  kSWM_PortPin_P0_5 = 5U,
  kSWM_PortPin_P0_6 = 6U,
  kSWM_PortPin_P0_7 = 7U,
  kSWM_PortPin_P0_8 = 8U,
  kSWM_PortPin_P0_9 = 9U,
  kSWM_PortPin_P0_10 = 10U,
  kSWM_PortPin_P0_11 = 11U,
  kSWM_PortPin_P0_12 = 12U,
  kSWM_PortPin_P0_13 = 13U,
  kSWM_PortPin_P0_14 = 14U,
  kSWM_PortPin_P0_15 = 15U,
  kSWM_PortPin_P0_16 = 16U,
  kSWM_PortPin_P0_17 = 17U,
  kSWM_PortPin_P0_18 = 18U,
  kSWM_PortPin_P0_19 = 19U,
  kSWM_PortPin_P0_20 = 20U,
  kSWM_PortPin_P0_21 = 21U,
  kSWM_PortPin_P0_22 = 22U,
  kSWM_PortPin_P0_23 = 23U,
  kSWM_PortPin_P0_24 = 24U,
  kSWM_PortPin_P0_25 = 25U,
  kSWM_PortPin_P0_26 = 26U,
  kSWM_PortPin_P0_27 = 27U,
  kSWM_PortPin_P0_28 = 28U,
  kSWM_PortPin_P0_29 = 29U,
  kSWM_PortPin_P0_30 = 30U,
  kSWM_PortPin_P0_31 = 31U,
  kSWM_PortPin_P1_0 = 32U,
  kSWM_PortPin_P1_1 = 33U,
  kSWM_PortPin_P1_2 = 34U,
  kSWM_PortPin_P1_3 = 35U,
  kSWM_PortPin_P1_4 = 36U,
  kSWM_PortPin_P1_5 = 37U,
  kSWM_PortPin_P1_6 = 38U,
  kSWM_PortPin_P1_7 = 39U,
  kSWM_PortPin_P1_8 = 40U,
  kSWM_PortPin_P1_9 = 41U,
  kSWM_PortPin_P1_10 = 42U,
  kSWM_PortPin_P1_11 = 43U,
  kSWM_PortPin_P1_12 = 44U,
  kSWM_PortPin_P1_13 = 45U,
  kSWM_PortPin_P1_14 = 46U,
  kSWM_PortPin_P1_15 = 47U,
  kSWM_PortPin_P1_16 = 48U,
  kSWM_PortPin_P1_17 = 49U,
  kSWM_PortPin_P1_18 = 50U,
  kSWM_PortPin_P1_19 = 51U,
  kSWM_PortPin_P1_20 = 52U,
  kSWM_PortPin_P1_21 = 53U,
  kSWM_PortPin_Reset = 0xffU
}
 SWM port_pin number. More...
 
enum  swm_select_movable_t {
  kSWM_USART0_TXD = 0U,
  kSWM_USART0_RXD = 1U,
  kSWM_USART0_RTS = 2U,
  kSWM_USART0_CTS = 3U,
  kSWM_USART0_SCLK = 4U,
  kSWM_USART1_TXD = 5U,
  kSWM_USART1_RXD = 6U,
  kSWM_USART1_RTS = 7U,
  kSWM_USART1_CTS = 8U,
  kSWM_USART1_SCLK = 9U,
  kSWM_USART2_TXD = 10U,
  kSWM_USART2_RXD = 11U,
  kSWM_USART2_RTS = 12U,
  kSWM_USART2_CTS = 13U,
  kSWM_USART2_SCLK = 14U,
  kSWM_SPI0_SCK = 15U,
  kSWM_SPI0_MOSI = 16U,
  kSWM_SPI0_MISO = 17U,
  kSWM_SPI0_SSEL0 = 18U,
  kSWM_SPI0_SSEL1 = 19U,
  kSWM_SPI0_SSEL2 = 20U,
  kSWM_SPI0_SSEL3 = 21U,
  kSWM_SPI1_SCK = 22U,
  kSWM_SPI1_MOSI = 23U,
  kSWM_SPI1_MISO = 24U,
  kSWM_SPI1_SSEL0 = 25U,
  kSWM_SPI1_SSEL1 = 26U,
  kSWM_SCT_PIN0 = 27U,
  kSWM_SCT_PIN1 = 28U,
  kSWM_SCT_PIN2 = 29U,
  kSWM_SCT_PIN3 = 30U,
  kSWM_SCT_OUT0 = 31U,
  kSWM_SCT_OUT1 = 32U,
  kSWM_SCT_OUT2 = 33U,
  kSWM_SCT_OUT3 = 34U,
  kSWM_SCT_OUT4 = 35U,
  kSWM_SCT_OUT5 = 36U,
  kSWM_SCT_OUT6 = 37U,
  kSWM_I2C1_SDA = 38U,
  kSWM_I2C1_SCL = 39U,
  kSWM_I2C2_SDA = 40U,
  kSWM_I2C2_SCL = 41U,
  kSWM_I2C3_SDA = 42U,
  kSWM_I2C3_SCL = 43U,
  kSWM_ACMP_OUT = 44U,
  kSWM_CLKOUT = 45U,
  kSWM_GPIO_INT_BMAT = 46U,
  kSWM_USART3_TXD = 47U,
  kSWM_USART3_RXD = 48U,
  kSWM_USART3_SCLK = 49U,
  kSWM_USART4_TXD = 50U,
  kSWM_USART4_RXD = 51U,
  kSWM_USART4_SCLK = 52U,
  kSWM_T0_MAT_CHN0 = 53U,
  kSWM_T0_MAT_CHN1 = 54U,
  kSWM_T0_MAT_CHN2 = 55U,
  kSWM_T0_MAT_CHN3 = 56U,
  kSWM_T0_CAP_CHN0 = 57U,
  kSWM_T0_CAP_CHN1 = 58U,
  kSWM_T0_CAP_CHN2 = 59U,
  kSWM_MOVABLE_NUM_FUNCS = 60U
}
 SWM movable selection. More...
 
enum  swm_select_fixed_pin_t {
  kSWM_ACMP_INPUT1 = SWM_PINENABLE0_ACMP_I1_MASK,
  kSWM_ACMP_INPUT2 = SWM_PINENABLE0_ACMP_I2_MASK,
  kSWM_ACMP_INPUT3 = SWM_PINENABLE0_ACMP_I3_MASK,
  kSWM_ACMP_INPUT4 = SWM_PINENABLE0_ACMP_I4_MASK,
  kSWM_ACMP_INPUT5 = SWM_PINENABLE0_ACMP_I5_MASK,
  kSWM_SWCLK = SWM_PINENABLE0_SWCLK_MASK,
  kSWM_SWDIO = SWM_PINENABLE0_SWDIO_MASK,
  kSWM_XTALIN = SWM_PINENABLE0_XTALIN_MASK,
  kSWM_XTALOUT = SWM_PINENABLE0_XTALOUT_MASK,
  kSWM_RESETN = SWM_PINENABLE0_RESETN_MASK,
  kSWM_CLKIN = SWM_PINENABLE0_CLKIN_MASK,
  kSWM_VDDCMP = SWM_PINENABLE0_VDDCMP_MASK,
  kSWM_I2C0_SDA = SWM_PINENABLE0_I2C0_SDA_MASK,
  kSWM_I2C0_SCL = SWM_PINENABLE0_I2C0_SCL_MASK,
  kSWM_ADC_CHN0 = SWM_PINENABLE0_ADC_0_MASK,
  kSWM_ADC_CHN1 = SWM_PINENABLE0_ADC_1_MASK,
  kSWM_ADC_CHN2 = SWM_PINENABLE0_ADC_2_MASK,
  kSWM_ADC_CHN3 = SWM_PINENABLE0_ADC_3_MASK,
  kSWM_ADC_CHN4 = SWM_PINENABLE0_ADC_4_MASK,
  kSWM_ADC_CHN5 = SWM_PINENABLE0_ADC_5_MASK,
  kSWM_ADC_CHN6 = SWM_PINENABLE0_ADC_6_MASK,
  kSWM_ADC_CHN7 = SWM_PINENABLE0_ADC_7_MASK,
  kSWM_ADC_CHN8 = SWM_PINENABLE0_ADC_8_MASK,
  kSWM_ADC_CHN9 = SWM_PINENABLE0_ADC_9_MASK,
  kSWM_ADC_CHN10 = SWM_PINENABLE0_ADC_10_MASK,
  kSWM_ADC_CHN11 = SWM_PINENABLE0_ADC_11_MASK,
  kSWM_DAC_OUT0 = SWM_PINENABLE0_DACOUT0_MASK,
  kSWM_DAC_OUT1 = SWM_PINENABLE0_DACOUT1_MASK,
  kSWM_CAPT_X0,
  kSWM_CAPT_X1 = SWM_PINENABLE0_CAPT_X1_MASK,
  kSWM_CAPT_X2 = SWM_PINENABLE0_CAPT_X2_MASK,
  kSWM_CAPT_X3 = (int)SWM_PINENABLE0_CAPT_X3_MASK,
  kSWM_CAPT_X4 = (int)(SWM_PINENABLE1_CAPT_X4_MASK | 0x80000000U),
  kSWM_CAPT_X5 = (int)(SWM_PINENABLE1_CAPT_X5_MASK | 0x80000000U),
  kSWM_CAPT_X6 = (int)(SWM_PINENABLE1_CAPT_X6_MASK | 0x80000000U),
  kSWM_CAPT_X7 = (int)(SWM_PINENABLE1_CAPT_X7_MASK | 0x80000000U),
  kSWM_CAPT_X8 = (int)(SWM_PINENABLE1_CAPT_X8_MASK | 0x80000000U),
  kSWM_CAPT_YL,
  kSWM_CAPT_YH = (int)(SWM_PINENABLE1_CAPT_YH_MASK | 0x80000000U),
  kSWM_FIXEDPIN_NUM_FUNCS = (int)0x80000041U
}
 SWM fixed pin selection. More...
 

Driver version

#define FSL_SWM_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))
 Version 2.0.1.
 

Enumeration Type Documentation

Enumerator
kSWM_PortPin_P0_0 

port_pin number P0_0.

kSWM_PortPin_P0_1 

port_pin number P0_1.

kSWM_PortPin_P0_2 

port_pin number P0_2.

kSWM_PortPin_P0_3 

port_pin number P0_3.

kSWM_PortPin_P0_4 

port_pin number P0_4.

kSWM_PortPin_P0_5 

port_pin number P0_5.

kSWM_PortPin_P0_6 

port_pin number P0_6.

kSWM_PortPin_P0_7 

port_pin number P0_7.

kSWM_PortPin_P0_8 

port_pin number P0_8.

kSWM_PortPin_P0_9 

port_pin number P0_9.

kSWM_PortPin_P0_10 

port_pin number P0_10.

kSWM_PortPin_P0_11 

port_pin number P0_11.

kSWM_PortPin_P0_12 

port_pin number P0_12.

kSWM_PortPin_P0_13 

port_pin number P0_13.

kSWM_PortPin_P0_14 

port_pin number P0_14.

kSWM_PortPin_P0_15 

port_pin number P0_15.

kSWM_PortPin_P0_16 

port_pin number P0_16.

kSWM_PortPin_P0_17 

port_pin number P0_17.

kSWM_PortPin_P0_18 

port_pin number P0_18.

kSWM_PortPin_P0_19 

port_pin number P0_19.

kSWM_PortPin_P0_20 

port_pin number P0_20.

kSWM_PortPin_P0_21 

port_pin number P0_21.

kSWM_PortPin_P0_22 

port_pin number P0_22.

kSWM_PortPin_P0_23 

port_pin number P0_23.

kSWM_PortPin_P0_24 

port_pin number P0_24.

kSWM_PortPin_P0_25 

port_pin number P0_25.

kSWM_PortPin_P0_26 

port_pin number P0_26.

kSWM_PortPin_P0_27 

port_pin number P0_27.

kSWM_PortPin_P0_28 

port_pin number P0_28.

kSWM_PortPin_P0_29 

port_pin number P0_29.

kSWM_PortPin_P0_30 

port_pin number P0_30.

kSWM_PortPin_P0_31 

port_pin number P0_31.

kSWM_PortPin_P1_0 

port_pin number P1_0.

kSWM_PortPin_P1_1 

port_pin number P1_1.

kSWM_PortPin_P1_2 

port_pin number P1_2.

kSWM_PortPin_P1_3 

port_pin number P1_3.

kSWM_PortPin_P1_4 

port_pin number P1_4.

kSWM_PortPin_P1_5 

port_pin number P1_5.

kSWM_PortPin_P1_6 

port_pin number P1_6.

kSWM_PortPin_P1_7 

port_pin number P1_7.

kSWM_PortPin_P1_8 

port_pin number P1_8.

kSWM_PortPin_P1_9 

port_pin number P1_9.

kSWM_PortPin_P1_10 

port_pin number P1_10.

kSWM_PortPin_P1_11 

port_pin number P1_11.

kSWM_PortPin_P1_12 

port_pin number P1_12.

kSWM_PortPin_P1_13 

port_pin number P1_13.

kSWM_PortPin_P1_14 

port_pin number P1_14.

kSWM_PortPin_P1_15 

port_pin number P1_15.

kSWM_PortPin_P1_16 

port_pin number P1_16.

kSWM_PortPin_P1_17 

port_pin number P1_17.

kSWM_PortPin_P1_18 

port_pin number P1_18.

kSWM_PortPin_P1_19 

port_pin number P1_19.

kSWM_PortPin_P1_20 

port_pin number P1_20.

kSWM_PortPin_P1_21 

port_pin number P1_21.

kSWM_PortPin_Reset 

port_pin reset number.

Enumerator
kSWM_USART0_TXD 

Movable function as USART0_TXD.

kSWM_USART0_RXD 

Movable function as USART0_RXD.

kSWM_USART0_RTS 

Movable function as USART0_RTS.

kSWM_USART0_CTS 

Movable function as USART0_CTS.

kSWM_USART0_SCLK 

Movable function as USART0_SCLK.

kSWM_USART1_TXD 

Movable function as USART1_TXD.

kSWM_USART1_RXD 

Movable function as USART1_RXD.

kSWM_USART1_RTS 

Movable function as USART1_RTS.

kSWM_USART1_CTS 

Movable function as USART1_CTS.

kSWM_USART1_SCLK 

Movable function as USART1_SCLK.

kSWM_USART2_TXD 

Movable function as USART2_TXD.

kSWM_USART2_RXD 

Movable function as USART2_RXD.

kSWM_USART2_RTS 

Movable function as USART2_RTS.

kSWM_USART2_CTS 

Movable function as USART2_CTS.

kSWM_USART2_SCLK 

Movable function as USART2_SCLK.

kSWM_SPI0_SCK 

Movable function as SPI0_SCK.

kSWM_SPI0_MOSI 

Movable function as SPI0_MOSI.

kSWM_SPI0_MISO 

Movable function as SPI0_MISO.

kSWM_SPI0_SSEL0 

Movable function as SPI0_SSEL0.

kSWM_SPI0_SSEL1 

Movable function as SPI0_SSEL1.

kSWM_SPI0_SSEL2 

Movable function as SPI0_SSEL2.

kSWM_SPI0_SSEL3 

Movable function as SPI0_SSEL3.

kSWM_SPI1_SCK 

Movable function as SPI1_SCK.

kSWM_SPI1_MOSI 

Movable function as SPI1_MOSI.

kSWM_SPI1_MISO 

Movable function as SPI1_MISO.

kSWM_SPI1_SSEL0 

Movable function as SPI1_SSEL0.

kSWM_SPI1_SSEL1 

Movable function as SPI1_SSEL1.

kSWM_SCT_PIN0 

Movable function as SCT_PIN0.

kSWM_SCT_PIN1 

Movable function as SCT_PIN1.

kSWM_SCT_PIN2 

Movable function as SCT_PIN2.

kSWM_SCT_PIN3 

Movable function as SCT_PIN3.

kSWM_SCT_OUT0 

Movable function as SCT_OUT0.

kSWM_SCT_OUT1 

Movable function as SCT_OUT1.

kSWM_SCT_OUT2 

Movable function as SCT_OUT2.

kSWM_SCT_OUT3 

Movable function as SCT_OUT3.

kSWM_SCT_OUT4 

Movable function as SCT_OUT4.

kSWM_SCT_OUT5 

Movable function as SCT_OUT5.

kSWM_SCT_OUT6 

Movable function as SCT_OUT6.

kSWM_I2C1_SDA 

Movable function as I2C1_SDA.

kSWM_I2C1_SCL 

Movable function as I2C1_SCL.

kSWM_I2C2_SDA 

Movable function as I2C2_SDA.

kSWM_I2C2_SCL 

Movable function as I2C2_SCL.

kSWM_I2C3_SDA 

Movable function as I2C3_SDA.

kSWM_I2C3_SCL 

Movable function as I2C3_SCL.

kSWM_ACMP_OUT 

Movable function as ACMP_OUT.

kSWM_CLKOUT 

Movable function as CLKOUT.

kSWM_GPIO_INT_BMAT 

Movable function as GPIO_INT_BMAT.

kSWM_USART3_TXD 

Movable function as USART3_TXD.

kSWM_USART3_RXD 

Movable function as USART3_RXD.

kSWM_USART3_SCLK 

Movable function as USART3_SCLK.

kSWM_USART4_TXD 

Movable function as USART4_TXD.

kSWM_USART4_RXD 

Movable function as USART4_RXD.

kSWM_USART4_SCLK 

Movable function as USART4_SCLK.

kSWM_T0_MAT_CHN0 

Movable function as Timer Match Channel 0.

kSWM_T0_MAT_CHN1 

Movable function as Timer Match Channel 1.

kSWM_T0_MAT_CHN2 

Movable function as Timer Match Channel 2.

kSWM_T0_MAT_CHN3 

Movable function as Timer Match Channel 3.

kSWM_T0_CAP_CHN0 

Movable function as Timer Capture Channel 0.

kSWM_T0_CAP_CHN1 

Movable function as Timer Capture Channel 1.

kSWM_T0_CAP_CHN2 

Movable function as Timer Capture Channel 2.

kSWM_MOVABLE_NUM_FUNCS 

Movable function number.

Enumerator
kSWM_ACMP_INPUT1 

Fixed-pin function as ACMP_INPUT1.

kSWM_ACMP_INPUT2 

Fixed-pin function as ACMP_INPUT2.

kSWM_ACMP_INPUT3 

Fixed-pin function as ACMP_INPUT3.

kSWM_ACMP_INPUT4 

Fixed-pin function as ACMP_INPUT4.

kSWM_ACMP_INPUT5 

Fixed-pin function as ACMP_INPUT5.

kSWM_SWCLK 

Fixed-pin function as SWCLK.

kSWM_SWDIO 

Fixed-pin function as SWDIO.

kSWM_XTALIN 

Fixed-pin function as XTALIN.

kSWM_XTALOUT 

Fixed-pin function as XTALOUT.

kSWM_RESETN 

Fixed-pin function as RESETN.

kSWM_CLKIN 

Fixed-pin function as CLKIN.

kSWM_VDDCMP 

Fixed-pin function as VDDCMP.

kSWM_I2C0_SDA 

Fixed-pin function as I2C0_SDA.

kSWM_I2C0_SCL 

Fixed-pin function as I2C0_SCL.

kSWM_ADC_CHN0 

Fixed-pin function as ADC_CHN0.

kSWM_ADC_CHN1 

Fixed-pin function as ADC_CHN1.

kSWM_ADC_CHN2 

Fixed-pin function as ADC_CHN2.

kSWM_ADC_CHN3 

Fixed-pin function as ADC_CHN3.

kSWM_ADC_CHN4 

Fixed-pin function as ADC_CHN4.

kSWM_ADC_CHN5 

Fixed-pin function as ADC_CHN5.

kSWM_ADC_CHN6 

Fixed-pin function as ADC_CHN6.

kSWM_ADC_CHN7 

Fixed-pin function as ADC_CHN7.

kSWM_ADC_CHN8 

Fixed-pin function as ADC_CHN8.

kSWM_ADC_CHN9 

Fixed-pin function as ADC_CHN9.

kSWM_ADC_CHN10 

Fixed-pin function as ADC_CHN10.

kSWM_ADC_CHN11 

Fixed-pin function as ADC_CHN11.

kSWM_DAC_OUT0 

Fixed-pin function as DACOUT0.

kSWM_DAC_OUT1 

Fixed-pin function as DACOUT1.

kSWM_CAPT_X0 

Fixed-pin function as CAPT_X0, an X capacitor(a mutual capacitance touch sensor) .

kSWM_CAPT_X1 

Fixed-pin function as CAPT_X1.

kSWM_CAPT_X2 

Fixed-pin function as CAPT_X2.

kSWM_CAPT_X3 

Fixed-pin function as CAPT_X3.

kSWM_CAPT_X4 

Fixed-pin function as CAPT_X4.

kSWM_CAPT_X5 

Fixed-pin function as CAPT_X5.

kSWM_CAPT_X6 

Fixed-pin function as CAPT_X6.

kSWM_CAPT_X7 

Fixed-pin function as CAPT_X7.

kSWM_CAPT_X8 

Fixed-pin function as CAPT_X8.

kSWM_CAPT_YL 

Fixed-pin function as CAPT_YL, an Y capacitor(the measurement capacitor) .

kSWM_CAPT_YH 

Fixed-pin function as CAPT_YH.

kSWM_FIXEDPIN_NUM_FUNCS 

Fixed-pin function number.

Function Documentation

void SWM_SetMovablePinSelect ( SWM_Type *  base,
swm_select_movable_t  func,
swm_port_pin_type_t  swm_port_pin 
)

This function will selects a pin (designated by its GPIO port and bit numbers) to a function.

Parameters
baseSWM peripheral base address.
funcany function name that is movable.
swm_port_pinany pin which has a GPIO port number and bit number.
void SWM_SetFixedPinSelect ( SWM_Type *  base,
swm_select_fixed_pin_t  func,
bool  enable 
)

This function will enables a fixed-pin function in PINENABLE0 or PINENABLE1.

Parameters
baseSWM peripheral base address.
funcany function name that is fixed pin.
enableenable or disable.