The MCUXpresso SDK provides a peripheral driver for the Auxiliary System Mode Controller (ASMC) module of MCUXpresso SDK devices. The ASMC module is responsible for sequencing Core 1 into and out of all low-power Stop and Run modes. The ASMC (Auxiliary System Mode Control) provides status and control registers for Core 1.
API functions are provided for configuring the system working in a dedicated power mode. For different power modes, the function ASMC_SetPowerModexxx accepts different parameters. System power mode state transitions are not available for between power modes. For details about available transitions, see the Power mode transitions section in the SoC reference manual.
Typical use case
Enter wait or stop modes
The ASMC driver provides APIs to set the MCU to different wait modes and stop modes. At the same time, there are pre function and post function for the modes setting. The pre function and post function are used to:
- Disable/Enable the interrupt through PRIMASK. In practise, there is such a scenario: the application sets the wakeup interrupt and calls SMC function ASMC_SetPowerModeStop to set MCU to STOP mode, but the wakeup interrupt happens so quickly that the ISR completes before the function ASMC_SetPowerModeStop. As a result, the MCU enters STOP mode and is never waken up by the interrupt. In this case, the application could first disable the interrupt through PRIMASK, then set the wakeup interrupt and enter STOP mode. After wakeup, the first thing you need to do is enable the interrupt through PRIMASK. The MCU can still wakeup when you disable interrupt through PRIMASK. The pre and post functions handle the PRIMASK inside.
|
| enum | _asmc_system_reset_status_flags {
kASMC_LowLeakageWakeupResetFlag = ASMC_SRS_WAKEUP_MASK,
kASMC_WatchdogResetFlag = ASMC_SRS_WDOG1_MASK,
kASMC_ChipResetNotPORFlag = ASMC_SRS_RES_MASK,
kASMC_PowerOnResetFlag = ASMC_SRS_POR_MASK,
kASMC_Core1LockupResetFlag = ASMC_SRS_LOCKUP_MASK,
kASMC_SoftwareResetFlag = ASMC_SRS_SW_MASK,
kASMC_StopModeAcknowledgeErrorResetFlag
} |
| | System Reset Status. More...
|
| |
| enum | asmc_power_mode_protection_t {
kASMC_AllowPowerModeVlls = ASMC_PMPROT_AVLLS_MASK,
kASMC_AllowPowerModeLls = ASMC_PMPROT_ALLS_MASK,
kASMC_AllowPowerModeVlp = ASMC_PMPROT_AVLP_MASK,
kASMC_AllowPowerModeAll
} |
| | Power Modes Protection. More...
|
| |
| enum | asmc_power_state_t {
kASMC_PowerStateRun = 0x01U << 0U,
kASMC_PowerStateStop = 0x01U << 1U,
kASMC_PowerStateVlpr = 0x01U << 2U,
kASMC_PowerStateVlpw = 0x01U << 3U,
kASMC_PowerStateVlps = 0x01U << 4U,
kASMC_PowerStateLls = 0x01U << 5U,
kASMC_PowerStateVlls = 0x01U << 6U
} |
| | Power Modes in PMSTAT. More...
|
| |
| enum | asmc_run_mode_t {
kASMC_RunNormal = 0U,
kASMC_RunVlpr = 2U
} |
| | Run mode definition. More...
|
| |
| enum | asmc_stop_mode_t {
kASMC_StopNormal = 0U,
kASMC_StopVlps = 2U,
kASMC_StopLls = 3U,
kASMC_StopVlls = 4U
} |
| | Stop mode definition. More...
|
| |
| enum | asmc_partial_stop_option_t {
kASMC_PartialStop = 0U,
kASMC_PartialStop1 = 1U,
kASMC_PartialStop2 = 2U
} |
| | Partial STOP option. More...
|
| |
| Enumerator |
|---|
| kASMC_LowLeakageWakeupResetFlag |
Reset caused by LLWU module wakeup source.
|
| kASMC_WatchdogResetFlag |
Reset caused by watchdog timeout.
|
| kASMC_ChipResetNotPORFlag |
Chip Reset caused by a source other than POR occurred.
|
| kASMC_PowerOnResetFlag |
Reset caused by POR.
|
| kASMC_Core1LockupResetFlag |
Reset caused by core LOCKUP event.
|
| kASMC_SoftwareResetFlag |
Reset caused by software setting of SYSRESETREQ bit.
|
| kASMC_StopModeAcknowledgeErrorResetFlag |
Reset caused by peripheral failure to acknowledge attempt to enter stop mode.
|
| Enumerator |
|---|
| kASMC_AllowPowerModeVlls |
Allow Very-Low-Leakage Stop Mode.
|
| kASMC_AllowPowerModeLls |
Allow Low-Leakage Stop Mode.
|
| kASMC_AllowPowerModeVlp |
Allow Very-Low-Power Mode.
|
| kASMC_AllowPowerModeAll |
Allow all power mode.
|
| Enumerator |
|---|
| kASMC_PowerStateRun |
0000_0001 - Current power mode is RUN
|
| kASMC_PowerStateStop |
0000_0010 - Current power mode is STOP
|
| kASMC_PowerStateVlpr |
0000_0100 - Current power mode is VLPR
|
| kASMC_PowerStateVlpw |
0000_1000 - Current power mode is VLPW
|
| kASMC_PowerStateVlps |
0001_0000 - Current power mode is VLPS
|
| kASMC_PowerStateLls |
0010_0000 - Current power mode is LLS
|
| kASMC_PowerStateVlls |
0100_0000 - Current power mode is VLLS
|
| Enumerator |
|---|
| kASMC_RunNormal |
normal RUN mode.
|
| kASMC_RunVlpr |
Very-Low-Power RUN mode.
|
| Enumerator |
|---|
| kASMC_StopNormal |
Normal STOP mode.
|
| kASMC_StopVlps |
Very-Low-Power STOP mode.
|
| kASMC_StopLls |
Low-Leakage Stop mode.
|
| kASMC_StopVlls |
Very-Low-Leakage Stop mode.
|
| Enumerator |
|---|
| kASMC_PartialStop |
STOP - Normal Stop mode.
|
| kASMC_PartialStop1 |
Partial Stop with both system and bus clocks disabled.
|
| kASMC_PartialStop2 |
Partial Stop with system clock disabled and bus clock enabled.
|
| static uint32_t ASMC_GetSystemResetStatusFlags |
( |
ASMC_Type * |
base | ) |
|
|
inlinestatic |
This function gets all ASMC system reset status flags. The flag indicates the source of the most recent MCU reset. The reset state of these bits depends on what caused the MCU to reset. The flags are returned as the logical OR value of the enumerators _asmc_system_reset_status_flags. To check for a specific status, compare the return value with enumerators in the _asmc_system_reset_status_flags. For example, to check whether the reset is caused by POR:
- Parameters
-
| base | ASMC peripheral base address. |
- Returns
- ASMC system reset status flags. See "_asmc_system_reset_status_flags".
| static void ASMC_SetPowerModeProtection |
( |
ASMC_Type * |
base, |
|
|
uint8_t |
allowedModes |
|
) |
| |
|
inlinestatic |
This function configures the power mode protection settings for supported power modes in the specified chip family. The available power modes are defined in the smc_power_mode_protection_t. This should be done at an early system level initialization stage. See the reference manual for details. This register can only write once after the power reset.
The allowed modes are passed as bit map, for example, to allow LLS and VLLS, use ASMC_SetPowerModeProtection(kASMC_AllowPowerModeVlls | kASMC_AllowPowerModeVlps). To allow all modes, use ASMC_SetPowerModeProtection(kASMC_AllowPowerModeAll).
- Parameters
-
| base | ASMC peripheral base address. |
| allowedModes | Bitmap of the allowed power modes. See "asmc_power_mode_protection_t". |
This function returns the current power mode stat. Once application switches the power mode, it should always check the stat to check whether it runs into the specified mode or not. An application should check this mode before switching to a different mode. The system requires that only certain modes can switch to other specific modes. See the reference manual for details and the asmc_power_state_t for information about the power stat.
- Parameters
-
| base | ASMC peripheral base address. |
- Returns
- Current power mode status.
| static void ASMC_PreEnterStopModes |
( |
void |
| ) |
|
|
inlinestatic |
This function should be called before entering STOP/VLPS/LLS/VLLS modes.
| static void ASMC_PostExitStopModes |
( |
void |
| ) |
|
|
inlinestatic |
This function should be called after wake up from STOP/VLPS/LLS/VLLS modes. It is used together with ASMC_PreEnterStopModes.
| static void ASMC_PreEnterWaitModes |
( |
void |
| ) |
|
|
inlinestatic |
This function should be called before entering WAIT/VLPW modes..
| static void ASMC_PostExitWaitModes |
( |
void |
| ) |
|
|
inlinestatic |
This function should be called after wake up from WAIT/VLPW modes. It is used together with ASMC_PreEnterWaitModes.
| status_t ASMC_SetPowerModeRun |
( |
ASMC_Type * |
base | ) |
|
- Parameters
-
| base | ASMC peripheral base address. |
- Returns
- ASMC configuration error code.
| status_t ASMC_SetPowerModeWait |
( |
ASMC_Type * |
base | ) |
|
- Parameters
-
| base | ASMC peripheral base address. |
- Returns
- ASMC configuration error code.
- Parameters
-
| base | ASMC peripheral base address. |
| option | Partial Stop mode option. |
- Returns
- ASMC configuration error code.
| status_t ASMC_SetPowerModeVlpr |
( |
ASMC_Type * |
base | ) |
|
- Parameters
-
| base | ASMC peripheral base address. |
- Returns
- ASMC configuration error code.
| status_t ASMC_SetPowerModeVlpw |
( |
ASMC_Type * |
base | ) |
|
- Parameters
-
| base | ASMC peripheral base address. |
- Returns
- ASMC configuration error code.
| status_t ASMC_SetPowerModeVlps |
( |
ASMC_Type * |
base | ) |
|
- Parameters
-
| base | ASMC peripheral base address. |
- Returns
- ASMC configuration error code.
| status_t ASMC_SetPowerModeLls |
( |
ASMC_Type * |
base | ) |
|
- Parameters
-
| base | ASMC peripheral base address. |
- Returns
- ASMC configuration error code.
| status_t ASMC_SetPowerModeVlls |
( |
ASMC_Type * |
base | ) |
|
- Parameters
-
| base | ASMC peripheral base address. |
- Returns
- ASMC configuration error code.