MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
SLCD: Segment LCD Driver

Overview

The MCUXpresso SDK provides a peripheral driver for the Segment LCD (SLCD) module of MCUXpresso SDK devices. The SLCD module is a CMOS charge pump voltage inverter that is designed for low voltage and low-power operation. SLCD is designed to generate the appropriate waveforms to drive multiplexed numeric, alphanumeric, or custom segment LCD panels. SLCD also has several timing and control settings that can be software-configured depending on the application's requirements. Timing and control consists of registers and control logic for the following:

  1. LCD frame frequency
  2. Duty cycle selection
  3. Front plane/back plane selection and enabling
  4. Blink modes and frequency
  5. Operation in low-power modes

Plane Setting and Display Control

After the SLCD general initialization, the SLCD_SetBackPlanePhase(), SLCD_SetFrontPlaneSegments(), and SLCD_SetFrontPlaneOnePhase() are used to set the special back/front Plane to make SLCD display correctly. Then, the independent display control APIs, SLCD_StartDisplay() and SLCD_StopDisplay(), start and stop the SLCD display.

The SLCD_StartBlinkMode() and SLCD_StopBlinkMode() are provided for the runtime special blink mode control. To get the SLCD fault detection result, call the SLCD_GetFaultDetectCounter().

Typical use case

SLCD Initialization operation

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/slcd

Data Structures

struct  slcd_fault_detect_config_t
 SLCD fault frame detection configuration structure. More...
 
struct  slcd_clock_config_t
 SLCD clock configuration structure. More...
 
struct  slcd_config_t
 SLCD configuration structure. More...
 

Enumerations

enum  slcd_power_supply_option_t {
  kSLCD_InternalVll3UseChargePump,
  kSLCD_ExternalVll3UseResistorBiasNetwork,
  kSLCD_ExteranlVll3UseChargePump,
  kSLCD_InternalVll1UseChargePump
}
 SLCD power supply option. More...
 
enum  slcd_regulated_voltage_trim_t {
  kSLCD_RegulatedVolatgeTrim00 = 0U,
  kSLCD_RegulatedVolatgeTrim01,
  kSLCD_RegulatedVolatgeTrim02,
  kSLCD_RegulatedVolatgeTrim03,
  kSLCD_RegulatedVolatgeTrim04,
  kSLCD_RegulatedVolatgeTrim05,
  kSLCD_RegulatedVolatgeTrim06,
  kSLCD_RegulatedVolatgeTrim07,
  kSLCD_RegulatedVolatgeTrim08,
  kSLCD_RegulatedVolatgeTrim09,
  kSLCD_RegulatedVolatgeTrim10,
  kSLCD_RegulatedVolatgeTrim11,
  kSLCD_RegulatedVolatgeTrim12,
  kSLCD_RegulatedVolatgeTrim13,
  kSLCD_RegulatedVolatgeTrim14,
  kSLCD_RegulatedVolatgeTrim15
}
 SLCD regulated voltage trim parameter, be used to meet the desired contrast. More...
 
enum  slcd_load_adjust_t {
  kSLCD_LowLoadOrFastestClkSrc = 0U,
  kSLCD_LowLoadOrIntermediateClkSrc,
  kSLCD_HighLoadOrIntermediateClkSrc,
  kSLCD_HighLoadOrSlowestClkSrc
}
 SLCD load adjust to handle different LCD glass capacitance or configure the LCD charge pump clock source. More...
 
enum  slcd_clock_src_t {
  kSLCD_DefaultClk = 0U,
  kSLCD_AlternateClk1 = 1U,
  kSLCD_AlternateClk2 = 3U
}
 SLCD clock source. More...
 
enum  slcd_alt_clock_div_t {
  kSLCD_AltClkDivFactor1 = 0U,
  kSLCD_AltClkDivFactor64,
  kSLCD_AltClkDivFactor256,
  kSLCD_AltClkDivFactor512
}
 SLCD alternate clock divider. More...
 
enum  slcd_clock_prescaler_t {
  kSLCD_ClkPrescaler00 = 0U,
  kSLCD_ClkPrescaler01,
  kSLCD_ClkPrescaler02,
  kSLCD_ClkPrescaler03,
  kSLCD_ClkPrescaler04,
  kSLCD_ClkPrescaler05,
  kSLCD_ClkPrescaler06,
  kSLCD_ClkPrescaler07
}
 SLCD clock prescaler to generate frame frequency. More...
 
enum  slcd_duty_cycle_t {
  kSLCD_1Div1DutyCycle = 0U,
  kSLCD_1Div2DutyCycle,
  kSLCD_1Div3DutyCycle,
  kSLCD_1Div4DutyCycle,
  kSLCD_1Div5DutyCycle,
  kSLCD_1Div6DutyCycle,
  kSLCD_1Div7DutyCycle,
  kSLCD_1Div8DutyCycle
}
 SLCD duty cycle. More...
 
enum  slcd_phase_type_t {
  kSLCD_NoPhaseActivate = 0x00U,
  kSLCD_PhaseAActivate = 0x01U,
  kSLCD_PhaseBActivate = 0x02U,
  kSLCD_PhaseCActivate = 0x04U,
  kSLCD_PhaseDActivate = 0x08U,
  kSLCD_PhaseEActivate = 0x10U,
  kSLCD_PhaseFActivate = 0x20U,
  kSLCD_PhaseGActivate = 0x40U,
  kSLCD_PhaseHActivate = 0x80U
}
 SLCD segment phase type. More...
 
enum  slcd_phase_index_t {
  kSLCD_PhaseAIndex = 0x0U,
  kSLCD_PhaseBIndex = 0x1U,
  kSLCD_PhaseCIndex = 0x2U,
  kSLCD_PhaseDIndex = 0x3U,
  kSLCD_PhaseEIndex = 0x4U,
  kSLCD_PhaseFIndex = 0x5U,
  kSLCD_PhaseGIndex = 0x6U,
  kSLCD_PhaseHIndex = 0x7U
}
 SLCD segment phase bit index. More...
 
enum  slcd_display_mode_t {
  kSLCD_NormalMode = 0U,
  kSLCD_AlternateMode,
  kSLCD_BlankMode
}
 SLCD display mode. More...
 
enum  slcd_blink_mode_t {
  kSLCD_BlankDisplayBlink = 0U,
  kSLCD_AltDisplayBlink
}
 SLCD blink mode. More...
 
enum  slcd_blink_rate_t {
  kSLCD_BlinkRate00 = 0U,
  kSLCD_BlinkRate01,
  kSLCD_BlinkRate02,
  kSLCD_BlinkRate03,
  kSLCD_BlinkRate04,
  kSLCD_BlinkRate05,
  kSLCD_BlinkRate06,
  kSLCD_BlinkRate07
}
 SLCD blink rate. More...
 
enum  slcd_fault_detect_clock_prescaler_t {
  kSLCD_FaultSampleFreqDivider1 = 0U,
  kSLCD_FaultSampleFreqDivider2,
  kSLCD_FaultSampleFreqDivider4,
  kSLCD_FaultSampleFreqDivider8,
  kSLCD_FaultSampleFreqDivider16,
  kSLCD_FaultSampleFreqDivider32,
  kSLCD_FaultSampleFreqDivider64,
  kSLCD_FaultSampleFreqDivider128
}
 SLCD fault detect clock prescaler. More...
 
enum  slcd_fault_detect_sample_window_width_t {
  kSLCD_FaultDetectWindowWidth4SampleClk = 0U,
  kSLCD_FaultDetectWindowWidth8SampleClk,
  kSLCD_FaultDetectWindowWidth16SampleClk,
  kSLCD_FaultDetectWindowWidth32SampleClk,
  kSLCD_FaultDetectWindowWidth64SampleClk,
  kSLCD_FaultDetectWindowWidth128SampleClk,
  kSLCD_FaultDetectWindowWidth256SampleClk,
  kSLCD_FaultDetectWindowWidth512SampleClk
}
 SLCD fault detect sample window width. More...
 
enum  slcd_interrupt_enable_t { kSLCD_FaultDetectCompleteInterrupt = 1U }
 SLCD interrupt source. More...
 
enum  slcd_lowpower_behavior {
  kSLCD_EnabledInWaitStop = 0,
  kSLCD_EnabledInWaitOnly,
  kSLCD_EnabledInStopOnly,
  kSLCD_DisabledInWaitStop
}
 SLCD behavior in low power mode. More...
 

Driver version

#define FSL_SLCD_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))
 SLCD driver version. More...
 

Initialization and deinitialization

void SLCD_Init (LCD_Type *base, slcd_config_t *configure)
 Initializes the SLCD, ungates the module clock, initializes the power setting, enables all used plane pins, and sets with interrupt and work mode with the configuration. More...
 
void SLCD_Deinit (LCD_Type *base)
 Deinitializes the SLCD module, gates the module clock, disables an interrupt, and displays the SLCD. More...
 
void SLCD_GetDefaultConfig (slcd_config_t *configure)
 Gets the SLCD default configuration structure. More...
 

Plane Setting and Display Control

static void SLCD_StartDisplay (LCD_Type *base)
 Enables the SLCD controller, starts generation, and displays the front plane and back plane waveform. More...
 
static void SLCD_StopDisplay (LCD_Type *base)
 Stops the SLCD controller. More...
 
void SLCD_StartBlinkMode (LCD_Type *base, slcd_blink_mode_t mode, slcd_blink_rate_t rate)
 Starts the SLCD blink mode. More...
 
static void SLCD_StopBlinkMode (LCD_Type *base)
 Stops the SLCD blink mode. More...
 
static void SLCD_SetBackPlanePhase (LCD_Type *base, uint32_t pinIndx, slcd_phase_type_t phase)
 Sets the SLCD back plane pin phase. More...
 
static void SLCD_SetFrontPlaneSegments (LCD_Type *base, uint32_t pinIndx, uint8_t operation)
 Sets the SLCD front plane segment operation for a front plane pin. More...
 
static void SLCD_SetFrontPlaneOnePhase (LCD_Type *base, uint32_t pinIndx, slcd_phase_index_t phaseIndx, bool enable)
 Sets one SLCD front plane pin for one phase. More...
 
static void SLCD_EnablePadSafeState (LCD_Type *base, bool enable)
 Enables/disables the SLCD pad safe state. More...
 
static uint32_t SLCD_GetFaultDetectCounter (LCD_Type *base)
 Gets the SLCD fault detect counter. More...
 

Interrupts.

void SLCD_EnableInterrupts (LCD_Type *base, uint32_t mask)
 Enables the SLCD interrupt. More...
 
void SLCD_DisableInterrupts (LCD_Type *base, uint32_t mask)
 Disables the SLCD interrupt. More...
 
uint32_t SLCD_GetInterruptStatus (LCD_Type *base)
 Gets the SLCD interrupt status flag. More...
 
void SLCD_ClearInterruptStatus (LCD_Type *base, uint32_t mask)
 Clears the SLCD interrupt events status flag. More...
 

Data Structure Documentation

struct slcd_fault_detect_config_t

Data Fields

bool faultDetectIntEnable
 Fault frame detection interrupt enable flag. More...
 
bool faultDetectBackPlaneEnable
 True means the pin id fault detected is back plane otherwise front plane. More...
 
uint8_t faultDetectPinIndex
 Fault detected pin id from 0 to 63. More...
 
slcd_fault_detect_clock_prescaler_t faultPrescaler
 Fault detect clock prescaler. More...
 
slcd_fault_detect_sample_window_width_t width
 Fault detect sample window width. More...
 

Field Documentation

bool slcd_fault_detect_config_t::faultDetectIntEnable
bool slcd_fault_detect_config_t::faultDetectBackPlaneEnable
uint8_t slcd_fault_detect_config_t::faultDetectPinIndex
slcd_fault_detect_clock_prescaler_t slcd_fault_detect_config_t::faultPrescaler
slcd_fault_detect_sample_window_width_t slcd_fault_detect_config_t::width
struct slcd_clock_config_t

Data Fields

slcd_clock_src_t clkSource
 Clock source. More...
 
slcd_alt_clock_div_t altClkDivider
 The divider to divide the alternate clock used for alternate clock source. More...
 
slcd_clock_prescaler_t clkPrescaler
 Clock prescaler. More...
 
bool fastFrameRateEnable
 Fast frame rate enable flag. More...
 

Field Documentation

slcd_clock_src_t slcd_clock_config_t::clkSource

"slcd_clock_src_t" is recommended to be used. The SLCD is optimized to operate using a 32.768kHz clock input.

slcd_alt_clock_div_t slcd_clock_config_t::altClkDivider
slcd_clock_prescaler_t slcd_clock_config_t::clkPrescaler
bool slcd_clock_config_t::fastFrameRateEnable
struct slcd_config_t

Data Fields

slcd_power_supply_option_t powerSupply
 Power supply option. More...
 
slcd_regulated_voltage_trim_t voltageTrim
 Regulated voltage trim used for the internal regulator VIREG to adjust to facilitate contrast control. More...
 
slcd_clock_config_t * clkConfig
 Clock configure. More...
 
slcd_display_mode_t displayMode
 SLCD display mode. More...
 
slcd_load_adjust_t loadAdjust
 Load adjust to handle glass capacitance. More...
 
slcd_duty_cycle_t dutyCycle
 Duty cycle. More...
 
slcd_lowpower_behavior lowPowerBehavior
 SLCD behavior in low power mode. More...
 
uint32_t slcdLowPinEnabled
 Setting enabled SLCD pin 0 ~ pin 31. More...
 
uint32_t slcdHighPinEnabled
 Setting enabled SLCD pin 32 ~ pin 63. More...
 
uint32_t backPlaneLowPin
 Setting back plane pin 0 ~ pin 31. More...
 
uint32_t backPlaneHighPin
 Setting back plane pin 32 ~ pin 63. More...
 
slcd_fault_detect_config_t * faultConfig
 Fault frame detection configure. More...
 

Field Documentation

slcd_power_supply_option_t slcd_config_t::powerSupply
slcd_regulated_voltage_trim_t slcd_config_t::voltageTrim
slcd_clock_config_t* slcd_config_t::clkConfig
slcd_display_mode_t slcd_config_t::displayMode
slcd_load_adjust_t slcd_config_t::loadAdjust
slcd_duty_cycle_t slcd_config_t::dutyCycle
slcd_lowpower_behavior slcd_config_t::lowPowerBehavior
uint32_t slcd_config_t::slcdLowPinEnabled

Setting bit n to 1 means enable pin n.

uint32_t slcd_config_t::slcdHighPinEnabled

Setting bit n to 1 means enable pin (n + 32).

uint32_t slcd_config_t::backPlaneLowPin

Setting bit n to 1 means setting pin n as back plane. It should never have the same bit setting as the frontPlane Pin.

uint32_t slcd_config_t::backPlaneHighPin

Setting bit n to 1 means setting pin (n + 32) as back plane. It should never have the same bit setting as the frontPlane Pin.

slcd_fault_detect_config_t* slcd_config_t::faultConfig

If not requirement, set to NULL.

Macro Definition Documentation

#define FSL_SLCD_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))

Enumeration Type Documentation

Enumerator
kSLCD_InternalVll3UseChargePump 

VLL3 connected to VDD internally, charge pump is used to generate VLL1 and VLL2.

kSLCD_ExternalVll3UseResistorBiasNetwork 

VLL3 is driven externally and resistor bias network is used to generate VLL1 and VLL2.

kSLCD_ExteranlVll3UseChargePump 

VLL3 is driven externally and charge pump is used to generate VLL1 and VLL2.

kSLCD_InternalVll1UseChargePump 

VIREG is connected to VLL1 internally and charge pump is used to generate VLL2 and VLL3.

Enumerator
kSLCD_RegulatedVolatgeTrim00 

Increase the voltage to 0.91 V.

kSLCD_RegulatedVolatgeTrim01 

Increase the voltage to 1.01 V.

kSLCD_RegulatedVolatgeTrim02 

Increase the voltage to 0.96 V.

kSLCD_RegulatedVolatgeTrim03 

Increase the voltage to 1.06 V.

kSLCD_RegulatedVolatgeTrim04 

Increase the voltage to 0.93 V.

kSLCD_RegulatedVolatgeTrim05 

Increase the voltage to 1.02 V.

kSLCD_RegulatedVolatgeTrim06 

Increase the voltage to 0.98 V.

kSLCD_RegulatedVolatgeTrim07 

Increase the voltage to 1.08 V.

kSLCD_RegulatedVolatgeTrim08 

Increase the voltage to 0.92 V.

kSLCD_RegulatedVolatgeTrim09 

Increase the voltage to 1.02 V.

kSLCD_RegulatedVolatgeTrim10 

Increase the voltage to 0.97 V.

kSLCD_RegulatedVolatgeTrim11 

Increase the voltage to 1.07 V.

kSLCD_RegulatedVolatgeTrim12 

Increase the voltage to 0.94 V.

kSLCD_RegulatedVolatgeTrim13 

Increase the voltage to 1.05 V.

kSLCD_RegulatedVolatgeTrim14 

Increase the voltage to 0.99 V.

kSLCD_RegulatedVolatgeTrim15 

Increase the voltage to 1.09 V.

Adjust the LCD glass capacitance if resistor bias network is enabled: kSLCD_LowLoadOrFastestClkSrc - Low load (LCD glass capacitance 2000pF or lower. LCD or GPIO function can be used on VLL1,VLL2,Vcap1 and Vcap2 pins) kSLCD_LowLoadOrIntermediateClkSrc - low load (LCD glass capacitance 2000pF or lower. LCD or GPIO function can be used on VLL1,VLL2,Vcap1 and Vcap2 pins) kSLCD_HighLoadOrIntermediateClkSrc - high load (LCD glass capacitance 8000pF or lower. LCD or GPIO function can be used on Vcap1 and Vcap2 pins) kSLCD_HighLoadOrSlowestClkSrc - high load (LCD glass capacitance 8000pF or lower LCD or GPIO function can be used on Vcap1 and Vcap2 pins) Adjust clock for charge pump if charge pump is enabled: kSLCD_LowLoadOrFastestClkSrc - Fasten clock source (LCD glass capacitance 8000pF or 4000pF or lower if Fast Frame Rate is set) kSLCD_LowLoadOrIntermediateClkSrc - Intermediate clock source (LCD glass capacitance 4000pF or 2000pF or lower if Fast Frame Rate is set) kSLCD_HighLoadOrIntermediateClkSrc - Intermediate clock source (LCD glass capacitance 2000pF or 1000pF or lower if Fast Frame Rate is set) kSLCD_HighLoadOrSlowestClkSrc - slowest clock source (LCD glass capacitance 1000pF or 500pF or lower if Fast Frame Rate is set)

Enumerator
kSLCD_LowLoadOrFastestClkSrc 

Adjust in low load or selects fastest clock.

kSLCD_LowLoadOrIntermediateClkSrc 

Adjust in low load or selects intermediate clock.

kSLCD_HighLoadOrIntermediateClkSrc 

Adjust in high load or selects intermediate clock.

kSLCD_HighLoadOrSlowestClkSrc 

Adjust in high load or selects slowest clock.

Enumerator
kSLCD_DefaultClk 

Select default clock ERCLK32K.

kSLCD_AlternateClk1 

Select alternate clock source 1 : MCGIRCLK.

kSLCD_AlternateClk2 

Select alternate clock source 2 : OSCERCLK.

Enumerator
kSLCD_AltClkDivFactor1 

No divide for alternate clock.

kSLCD_AltClkDivFactor64 

Divide alternate clock with factor 64.

kSLCD_AltClkDivFactor256 

Divide alternate clock with factor 256.

kSLCD_AltClkDivFactor512 

Divide alternate clock with factor 512.

Enumerator
kSLCD_ClkPrescaler00 

Prescaler 0.

kSLCD_ClkPrescaler01 

Prescaler 1.

kSLCD_ClkPrescaler02 

Prescaler 2.

kSLCD_ClkPrescaler03 

Prescaler 3.

kSLCD_ClkPrescaler04 

Prescaler 4.

kSLCD_ClkPrescaler05 

Prescaler 5.

kSLCD_ClkPrescaler06 

Prescaler 6.

kSLCD_ClkPrescaler07 

Prescaler 7.

Enumerator
kSLCD_1Div1DutyCycle 

LCD use 1 BP 1/1 duty cycle.

kSLCD_1Div2DutyCycle 

LCD use 2 BP 1/2 duty cycle.

kSLCD_1Div3DutyCycle 

LCD use 3 BP 1/3 duty cycle.

kSLCD_1Div4DutyCycle 

LCD use 4 BP 1/4 duty cycle.

kSLCD_1Div5DutyCycle 

LCD use 5 BP 1/5 duty cycle.

kSLCD_1Div6DutyCycle 

LCD use 6 BP 1/6 duty cycle.

kSLCD_1Div7DutyCycle 

LCD use 7 BP 1/7 duty cycle.

kSLCD_1Div8DutyCycle 

LCD use 8 BP 1/8 duty cycle.

Enumerator
kSLCD_NoPhaseActivate 

LCD wareform no phase activates.

kSLCD_PhaseAActivate 

LCD waveform phase A activates.

kSLCD_PhaseBActivate 

LCD waveform phase B activates.

kSLCD_PhaseCActivate 

LCD waveform phase C activates.

kSLCD_PhaseDActivate 

LCD waveform phase D activates.

kSLCD_PhaseEActivate 

LCD waveform phase E activates.

kSLCD_PhaseFActivate 

LCD waveform phase F activates.

kSLCD_PhaseGActivate 

LCD waveform phase G activates.

kSLCD_PhaseHActivate 

LCD waveform phase H activates.

Enumerator
kSLCD_PhaseAIndex 

LCD phase A bit index.

kSLCD_PhaseBIndex 

LCD phase B bit index.

kSLCD_PhaseCIndex 

LCD phase C bit index.

kSLCD_PhaseDIndex 

LCD phase D bit index.

kSLCD_PhaseEIndex 

LCD phase E bit index.

kSLCD_PhaseFIndex 

LCD phase F bit index.

kSLCD_PhaseGIndex 

LCD phase G bit index.

kSLCD_PhaseHIndex 

LCD phase H bit index.

Enumerator
kSLCD_NormalMode 

LCD Normal display mode.

kSLCD_AlternateMode 

LCD Alternate display mode.

For four back planes or less.

kSLCD_BlankMode 

LCD Blank display mode.

Enumerator
kSLCD_BlankDisplayBlink 

Display blank during the blink period.

kSLCD_AltDisplayBlink 

Display alternate display during the blink period if duty cycle is lower than 5.

Enumerator
kSLCD_BlinkRate00 

SLCD blink rate is LCD clock/((2^12)).

kSLCD_BlinkRate01 

SLCD blink rate is LCD clock/((2^13)).

kSLCD_BlinkRate02 

SLCD blink rate is LCD clock/((2^14)).

kSLCD_BlinkRate03 

SLCD blink rate is LCD clock/((2^15)).

kSLCD_BlinkRate04 

SLCD blink rate is LCD clock/((2^16)).

kSLCD_BlinkRate05 

SLCD blink rate is LCD clock/((2^17)).

kSLCD_BlinkRate06 

SLCD blink rate is LCD clock/((2^18)).

kSLCD_BlinkRate07 

SLCD blink rate is LCD clock/((2^19)).

Enumerator
kSLCD_FaultSampleFreqDivider1 

Fault detect sample clock frequency is 1/1 bus clock.

kSLCD_FaultSampleFreqDivider2 

Fault detect sample clock frequency is 1/2 bus clock.

kSLCD_FaultSampleFreqDivider4 

Fault detect sample clock frequency is 1/4 bus clock.

kSLCD_FaultSampleFreqDivider8 

Fault detect sample clock frequency is 1/8 bus clock.

kSLCD_FaultSampleFreqDivider16 

Fault detect sample clock frequency is 1/16 bus clock.

kSLCD_FaultSampleFreqDivider32 

Fault detect sample clock frequency is 1/32 bus clock.

kSLCD_FaultSampleFreqDivider64 

Fault detect sample clock frequency is 1/64 bus clock.

kSLCD_FaultSampleFreqDivider128 

Fault detect sample clock frequency is 1/128 bus clock.

Enumerator
kSLCD_FaultDetectWindowWidth4SampleClk 

Sample window width is 4 sample clock cycles.

kSLCD_FaultDetectWindowWidth8SampleClk 

Sample window width is 8 sample clock cycles.

kSLCD_FaultDetectWindowWidth16SampleClk 

Sample window width is 16 sample clock cycles.

kSLCD_FaultDetectWindowWidth32SampleClk 

Sample window width is 32 sample clock cycles.

kSLCD_FaultDetectWindowWidth64SampleClk 

Sample window width is 64 sample clock cycles.

kSLCD_FaultDetectWindowWidth128SampleClk 

Sample window width is 128 sample clock cycles.

kSLCD_FaultDetectWindowWidth256SampleClk 

Sample window width is 256 sample clock cycles.

kSLCD_FaultDetectWindowWidth512SampleClk 

Sample window width is 512 sample clock cycles.

Enumerator
kSLCD_FaultDetectCompleteInterrupt 

SLCD fault detection complete interrupt source.

Enumerator
kSLCD_EnabledInWaitStop 

SLCD works in wait and stop mode.

kSLCD_EnabledInWaitOnly 

SLCD works in wait mode and is disabled in stop mode.

kSLCD_EnabledInStopOnly 

SLCD works in stop mode and is disabled in wait mode.

kSLCD_DisabledInWaitStop 

SLCD is disabled in stop mode and wait mode.

Function Documentation

void SLCD_Init ( LCD_Type *  base,
slcd_config_t *  configure 
)
Parameters
baseSLCD peripheral base address.
configureSLCD configuration pointer. For the configuration structure, many parameters have the default setting and the SLCD_Getdefaultconfig() is provided to get them. Use it verified for their applications. The others have no default settings, such as "clkConfig", and must be provided by the application before calling the SLCD_Init() API.
void SLCD_Deinit ( LCD_Type *  base)
Parameters
baseSLCD peripheral base address.
void SLCD_GetDefaultConfig ( slcd_config_t *  configure)

The purpose of this API is to get default parameters of the configuration structure for the SLCD_Init(). Use these initialized parameters unchanged in SLCD_Init() or modify fields of the structure before the calling SLCD_Init(). All default parameters of the configure structuration are listed.

config.displayMode = kSLCD_NormalMode;
config.powerSupply = kSLCD_InternalVll3UseChargePump;
config.voltageTrim = kSLCD_RegulatedVolatgeTrim00;
config.lowPowerBehavior = kSLCD_EnabledInWaitStop;
config.interruptSrc = 0;
config.faultConfig = NULL;
config.frameFreqIntEnable = false;
Parameters
configureThe SLCD configuration structure pointer.
static void SLCD_StartDisplay ( LCD_Type *  base)
inlinestatic
Parameters
baseSLCD peripheral base address.
static void SLCD_StopDisplay ( LCD_Type *  base)
inlinestatic

There is no waveform generator and all enabled pins only output a low value.

Parameters
baseSLCD peripheral base address.
void SLCD_StartBlinkMode ( LCD_Type *  base,
slcd_blink_mode_t  mode,
slcd_blink_rate_t  rate 
)
Parameters
baseSLCD peripheral base address.
modeSLCD blink mode.
rateSLCD blink rate.
static void SLCD_StopBlinkMode ( LCD_Type *  base)
inlinestatic
Parameters
baseSLCD peripheral base address.
static void SLCD_SetBackPlanePhase ( LCD_Type *  base,
uint32_t  pinIndx,
slcd_phase_type_t  phase 
)
inlinestatic

This function sets the SLCD back plane pin phase. "kSLCD_PhaseXActivate" setting means the phase X is active for the back plane pin. "kSLCD_NoPhaseActivate" setting means there is no phase active for the back plane pin. For example, set the back plane pin 20 for phase A.

Parameters
baseSLCD peripheral base address.
pinIndxSLCD back plane pin index. Range from 0 to 63.
phaseThe phase activates for the back plane pin.
static void SLCD_SetFrontPlaneSegments ( LCD_Type *  base,
uint32_t  pinIndx,
uint8_t  operation 
)
inlinestatic

This function sets the SLCD front plane segment on or off operation. Each bit turns on or off the segments associated with the front plane pin in the following pattern: HGFEDCBA (most significant bit controls segment H and least significant bit controls segment A). For example, turn on the front plane pin 20 for phase B and phase C.

Parameters
baseSLCD peripheral base address.
pinIndxSLCD back plane pin index. Range from 0 to 63.
operationThe operation for the segment on the front plane pin. This is a logical OR of the enumeration :: slcd_phase_type_t.
static void SLCD_SetFrontPlaneOnePhase ( LCD_Type *  base,
uint32_t  pinIndx,
slcd_phase_index_t  phaseIndx,
bool  enable 
)
inlinestatic

This function can be used to set one phase on or off for the front plane pin. It can be call many times to set the plane pin for different phase indexes. For example, turn on the front plane pin 20 for phase B and phase C.

Parameters
baseSLCD peripheral base address.
pinIndxSLCD back plane pin index. Range from 0 to 63.
phaseIndxThe phase bit index slcd_phase_index_t.
enableTrue to turn on the segment for phaseIndx phase false to turn off the segment for phaseIndx phase.
static void SLCD_EnablePadSafeState ( LCD_Type *  base,
bool  enable 
)
inlinestatic

Forces the safe state on the LCD pad controls. All LCD front plane and backplane functions are disabled.

Parameters
baseSLCD peripheral base address.
enableTrue enable, false disable.
static uint32_t SLCD_GetFaultDetectCounter ( LCD_Type *  base)
inlinestatic

This function gets the number of samples inside the fault detection sample window.

Parameters
baseSLCD peripheral base address.
Returns
The fault detect counter. The maximum return value is 255. If the maximum 255 returns, the overflow may happen. Reconfigure the fault detect sample window and fault detect clock prescaler for proper sampling.
void SLCD_EnableInterrupts ( LCD_Type *  base,
uint32_t  mask 
)

For example, to enable fault detect complete interrupt and frame frequency interrupt, for FSL_FEATURE_SLCD_HAS_FRAME_FREQUENCY_INTERRUPT enabled case, do the following.

*
Parameters
baseSLCD peripheral base address.
maskSLCD interrupts to enable. This is a logical OR of the enumeration :: slcd_interrupt_enable_t.
void SLCD_DisableInterrupts ( LCD_Type *  base,
uint32_t  mask 
)

For example, to disable fault detect complete interrupt and frame frequency interrupt, for FSL_FEATURE_SLCD_HAS_FRAME_FREQUENCY_INTERRUPT enabled case, do the following.

*
Parameters
baseSLCD peripheral base address.
maskSLCD interrupts to disable. This is a logical OR of the enumeration :: slcd_interrupt_enable_t.
uint32_t SLCD_GetInterruptStatus ( LCD_Type *  base)
Parameters
baseSLCD peripheral base address.
Returns
The event status of the interrupt source. This is the logical OR of members of the enumeration :: slcd_interrupt_enable_t.
void SLCD_ClearInterruptStatus ( LCD_Type *  base,
uint32_t  mask 
)
Parameters
baseSLCD peripheral base address.
maskSLCD interrupt source to be cleared. This is the logical OR of members of the enumeration :: slcd_interrupt_enable_t.