The MCUXpresso SDK provides a peripheral driver for the Pulse Width Modulation (PWM) module of MCUXpresso SDK devices.
PWM Driver
Initialization and deinitialization
The function PWM_Init() initializes the PWM with a specified configurations. The function PWM_GetDefaultConfig() gets the default configurations.The initialization function configures the PWM for the requested register update mode for registers with buffers.
The function PWM_Deinit() disables the PWM counter and turns off the module clock.
Typical use case
PWM output
Output PWM signal on PWM3 module with different dutycycles. Periodically update the PWM signal duty cycle. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/pwm
|
| enum | pwm_clock_source_t {
kPWM_PeripheralClock = 1U,
kPWM_HighFrequencyClock,
kPWM_LowFrequencyClock
} |
| | PWM clock source select. More...
|
| |
| enum | pwm_fifo_water_mark_t {
kPWM_FIFOWaterMark_1 = 0U,
kPWM_FIFOWaterMark_2,
kPWM_FIFOWaterMark_3,
kPWM_FIFOWaterMark_4
} |
| | PWM FIFO water mark select. More...
|
| |
| enum | pwm_byte_data_swap_t {
kPWM_ByteNoSwap = 0U,
kPWM_ByteSwap
} |
| | PWM byte data swap select. More...
|
| |
| enum | pwm_half_word_data_swap_t {
kPWM_HalfWordNoSwap = 0U,
kPWM_HalfWordSwap
} |
| | PWM half-word data swap select. More...
|
| |
| enum | pwm_output_configuration_t {
kPWM_SetAtRolloverAndClearAtcomparison = 0U,
kPWM_ClearAtRolloverAndSetAtcomparison,
kPWM_NoConfigure
} |
| | PWM Output Configuration. More...
|
| |
| enum | pwm_sample_repeat_t {
kPWM_EachSampleOnce = 0u,
kPWM_EachSampletwice,
kPWM_EachSampleFourTimes,
kPWM_EachSampleEightTimes
} |
| | PWM FIFO sample repeat It determines the number of times each sample from the FIFO is to be used. More...
|
| |
| enum | pwm_interrupt_enable_t {
kPWM_FIFOEmptyInterruptEnable = (1U << 0),
kPWM_RolloverInterruptEnable = (1U << 1),
kPWM_CompareInterruptEnable = (1U << 2)
} |
| | List of PWM interrupt options. More...
|
| |
| enum | pwm_status_flags_t {
kPWM_FIFOEmptyFlag = (1U << 3),
kPWM_RolloverFlag = (1U << 4),
kPWM_CompareFlag = (1U << 5),
kPWM_FIFOWriteErrorFlag
} |
| | List of PWM status flags. More...
|
| |
| enum | pwm_fifo_available_t {
kPWM_NoDataInFIFOFlag = 0U,
kPWM_OneWordInFIFOFlag,
kPWM_TwoWordsInFIFOFlag,
kPWM_ThreeWordsInFIFOFlag,
kPWM_FourWordsInFIFOFlag
} |
| | List of PWM FIFO available. More...
|
| |
| Enumerator |
|---|
| kPWM_PeripheralClock |
The Peripheral clock is used as the clock.
|
| kPWM_HighFrequencyClock |
High-frequency reference clock is used as the clock.
|
| kPWM_LowFrequencyClock |
Low-frequency reference clock(32KHz) is used as the clock.
|
Sets the data level at which the FIFO empty flag will be set
| Enumerator |
|---|
| kPWM_FIFOWaterMark_1 |
FIFO empty flag is set when there are more than or equal to 1 empty slots.
|
| kPWM_FIFOWaterMark_2 |
FIFO empty flag is set when there are more than or equal to 2 empty slots.
|
| kPWM_FIFOWaterMark_3 |
FIFO empty flag is set when there are more than or equal to 3 empty slots.
|
| kPWM_FIFOWaterMark_4 |
FIFO empty flag is set when there are more than or equal to 4 empty slots.
|
It determines the byte ordering of the 16-bit data when it goes into the FIFO from the sample register.
| Enumerator |
|---|
| kPWM_ByteNoSwap |
byte ordering remains the same
|
| kPWM_ByteSwap |
byte ordering is reversed
|
| Enumerator |
|---|
| kPWM_HalfWordNoSwap |
Half word swapping does not take place.
|
| kPWM_HalfWordSwap |
Half word from write data bus are swapped.
|
| Enumerator |
|---|
| kPWM_SetAtRolloverAndClearAtcomparison |
Output pin is set at rollover and cleared at comparison.
|
| kPWM_ClearAtRolloverAndSetAtcomparison |
Output pin is cleared at rollover and set at comparison.
|
| kPWM_NoConfigure |
PWM output is disconnected.
|
| Enumerator |
|---|
| kPWM_EachSampleOnce |
Use each sample once.
|
| kPWM_EachSampletwice |
Use each sample twice.
|
| kPWM_EachSampleFourTimes |
Use each sample four times.
|
| kPWM_EachSampleEightTimes |
Use each sample eight times.
|
| Enumerator |
|---|
| kPWM_FIFOEmptyInterruptEnable |
This bit controls the generation of the FIFO Empty interrupt.
|
| kPWM_RolloverInterruptEnable |
This bit controls the generation of the Rollover interrupt.
|
| kPWM_CompareInterruptEnable |
This bit controls the generation of the Compare interrupt.
|
| Enumerator |
|---|
| kPWM_FIFOEmptyFlag |
This bit indicates the FIFO data level in comparison to the water level set by FWM field in the control register.
|
| kPWM_RolloverFlag |
This bit shows that a roll-over event has occurred.
|
| kPWM_CompareFlag |
This bit shows that a compare event has occurred.
|
| kPWM_FIFOWriteErrorFlag |
This bit shows that an attempt has been made to write FIFO when it is full.
|
| Enumerator |
|---|
| kPWM_NoDataInFIFOFlag |
No data available.
|
| kPWM_OneWordInFIFOFlag |
1 word of data in FIFO
|
| kPWM_TwoWordsInFIFOFlag |
2 word of data in FIFO
|
| kPWM_ThreeWordsInFIFOFlag |
3 word of data in FIFO
|
| kPWM_FourWordsInFIFOFlag |
4 word of data in FIFO
|
| status_t PWM_Init |
( |
PWM_Type * |
base, |
|
|
const pwm_config_t * |
config |
|
) |
| |
- Note
- This API should be called at the beginning of the application using the PWM driver.
- Parameters
-
| base | PWM peripheral base address |
| config | Pointer to user's PWM config structure. |
- Returns
- kStatus_Success means success; else failed.
| void PWM_Deinit |
( |
PWM_Type * |
base | ) |
|
- Parameters
-
| base | PWM peripheral base address |
| void PWM_GetDefaultConfig |
( |
pwm_config_t * |
config | ) |
|
The default values are:
* config->enableStopMode = false;
* config->enableDozeMode = false;
* config->enableWaitMode = false;
* config->enableDozeMode = false;
* config->prescale = 0U;
*
- Parameters
-
| config | Pointer to user's PWM config structure. |
| static void PWM_StartTimer |
( |
PWM_Type * |
base | ) |
|
|
inlinestatic |
When the PWM is enabled, it begins a new period, the output pin is set to start a new period while the prescaler and counter are released and counting begins.
- Parameters
-
| base | PWM peripheral base address |
| static void PWM_StopTimer |
( |
PWM_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | PWM peripheral base address |
| static void PWM_SoftwareReset |
( |
PWM_Type * |
base | ) |
|
|
inlinestatic |
PWM is reset when this bit is set to 1. It is a self clearing bit. Setting this bit resets all the registers to their reset values except for the STOPEN, DOZEN, WAITEN, and DBGEN bits in this control register.
- Parameters
-
| base | PWM peripheral base address |
| static void PWM_EnableInterrupts |
( |
PWM_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | PWM peripheral base address |
| mask | The interrupts to enable. This is a logical OR of members of the enumeration pwm_interrupt_enable_t |
| static void PWM_DisableInterrupts |
( |
PWM_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | PWM peripheral base address |
| mask | The interrupts to disable. This is a logical OR of members of the enumeration pwm_interrupt_enable_t |
| static uint32_t PWM_GetEnabledInterrupts |
( |
PWM_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | PWM peripheral base address |
- Returns
- The enabled interrupts. This is the logical OR of members of the enumeration pwm_interrupt_enable_t
| static uint32_t PWM_GetStatusFlags |
( |
PWM_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | PWM peripheral base address |
- Returns
- The status flags. This is the logical OR of members of the enumeration pwm_status_flags_t
| static void PWM_clearStatusFlags |
( |
PWM_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | PWM peripheral base address |
| mask | The status flags to clear. This is a logical OR of members of the enumeration pwm_status_flags_t |
| static uint32_t PWM_GetFIFOAvailable |
( |
PWM_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | PWM peripheral base address |
- Returns
- The status flags. This is the logical OR of members of the enumeration pwm_fifo_available_t
| static void PWM_SetSampleValue |
( |
PWM_Type * |
base, |
|
|
uint32_t |
value |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | PWM peripheral base address |
| value | The sample value. This is the input to the 4x16 FIFO. The value in this register denotes the value of the sample being currently used. |
| static uint32_t PWM_GetSampleValue |
( |
PWM_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | PWM peripheral base address |
- Returns
- The sample value. It can be read only when the PWM is enable.
| static void PWM_SetPeriodValue |
( |
PWM_Type * |
base, |
|
|
uint32_t |
value |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | PWM peripheral base address |
| value | The period value. The PWM period register (PWM_PWMPR) determines the period of the PWM output signal. Writing 0xFFFF to this register will achieve the same result as writing 0xFFFE. PWMO (Hz) = PCLK(Hz) / (period +2) |
| static uint32_t PWM_GetPeriodValue |
( |
PWM_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | PWM peripheral base address |
- Returns
- The period value. The PWM period register (PWM_PWMPR) determines the period of the PWM output signal.
| static uint32_t PWM_GetCounterValue |
( |
PWM_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | PWM peripheral base address |
- Returns
- The counter value. The current count value.