![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The SDIF host adapter driver provide adapter for blocking/non_blocking mode.
Data Structures | |
struct | sdmmchost_pwr_card_t |
card power control More... | |
struct | sdmmchost_t |
sdmmc host handler More... | |
Macros | |
#define | FSL_SDMMC_HOST_ADAPTER_VERSION (MAKE_VERSION(2U, 3U, 0U)) /*2.3.0*/ |
Middleware adapter version. More... | |
#define | SDMMCHOST_SUPPORT_HIGH_SPEED (1U) |
host capability | |
#define | SDMMCHOST_DMA_DESCRIPTOR_BUFFER_ALIGN_SIZE (4U) |
SDMMC host dma descriptor buffer address align size. | |
Typedefs | |
typedef sdif_transfer_t | sdmmchost_transfer_t |
sdmmc host transfer function | |
typedef void(* | sdmmchost_pwr_t )(void) |
card power control function pointer | |
Enumerations | |
enum | _sdmmchost_endian_mode { kSDMMCHOST_EndianModeBig = 0U, kSDMMCHOST_EndianModeHalfWordBig = 1U, kSDMMCHOST_EndianModeLittle = 2U } |
host Endian mode corresponding to driver define More... | |
SDIF host controller function | |
void | SDMMCHOST_SetCardBusWidth (sdmmchost_t *host, uint32_t dataBusWidth) |
set data bus width. More... | |
static void | SDMMCHOST_SendCardActive (sdmmchost_t *host) |
Send initilization active 80 clocks to card. More... | |
static uint32_t | SDMMCHOST_SetCardClock (sdmmchost_t *host, uint32_t targetClock) |
Set card bus clock. More... | |
static bool | SDMMCHOST_IsCardBusy (sdmmchost_t *host) |
check card status by DATA0. More... | |
status_t | SDMMCHOST_StartBoot (sdmmchost_t *host, sdmmchost_boot_config_t *hostConfig, sdmmchost_cmd_t *cmd, uint8_t *buffer) |
start read boot data. More... | |
status_t | SDMMCHOST_ReadBootData (sdmmchost_t *host, sdmmchost_boot_config_t *hostConfig, uint8_t *buffer) |
read boot data. More... | |
static void | SDMMCHOST_EnableBoot (sdmmchost_t *host, bool enable) |
enable boot mode. More... | |
static void | SDMMCHOST_EnableCardInt (sdmmchost_t *host, bool enable) |
enable card interrupt. More... | |
status_t | SDMMCHOST_CardIntInit (sdmmchost_t *host, void *sdioInt) |
card interrupt function. More... | |
status_t | SDMMCHOST_CardDetectInit (sdmmchost_t *host, void *cd) |
card detect init function. More... | |
status_t | SDMMCHOST_PollingCardDetectStatus (sdmmchost_t *host, uint32_t waitCardStatus, uint32_t timeout) |
Detect card insert, only need for SD cases. More... | |
uint32_t | SDMMCHOST_CardDetectStatus (sdmmchost_t *host) |
card detect status. More... | |
status_t | SDMMCHOST_Init (sdmmchost_t *host) |
Init host controller. More... | |
void | SDMMCHOST_Deinit (sdmmchost_t *host) |
Deinit host controller. More... | |
void | SDMMCHOST_SetCardPower (sdmmchost_t *host, bool enable) |
host power off card function. More... | |
status_t | SDMMCHOST_TransferFunction (sdmmchost_t *host, sdmmchost_transfer_t *content) |
host transfer function. More... | |
void | SDMMCHOST_Reset (sdmmchost_t *host) |
host reset function. More... | |
status_t | SDMMCHOST_WaitCardDetectStatus (SDMMCHOST_TYPE *hostBase, const sdmmchost_detect_card_t *cd, bool waitCardStatus) |
wait card detect status More... | |
void | SDMMCHOST_PowerOffCard (SDMMCHOST_TYPE *base, const sdmmchost_pwr_card_t *pwr) |
host power off card function. More... | |
void | SDMMCHOST_PowerOnCard (SDMMCHOST_TYPE *base, const sdmmchost_pwr_card_t *pwr) |
host power on card function. More... | |
struct sdmmchost_pwr_card_t |
Data Fields | |
sdmmchost_pwr_t | powerOn |
power on function pointer | |
uint32_t | powerOnDelay_ms |
power on delay | |
sdmmchost_pwr_t | powerOff |
power off function pointer | |
uint32_t | powerOffDelay_ms |
power off delay | |
struct sdmmchost_t |
Data Fields | |
sdif_host_t | hostController |
host configuration | |
uint8_t | hostPort |
host port number, used for one instance support two card | |
void * | dmaDesBuffer |
DMA descriptor buffer address. | |
uint32_t | dmaDesBufferWordsNum |
DMA descriptor buffer size in byte. | |
sdif_handle_t | handle |
host controller handler | |
void * | hostEvent |
host event handler pointer | |
void * | cd |
card detect | |
void * | cardInt |
call back function for card interrupt | |
#define FSL_SDMMC_HOST_ADAPTER_VERSION (MAKE_VERSION(2U, 3U, 0U)) /*2.3.0*/ |
void SDMMCHOST_SetCardBusWidth | ( | sdmmchost_t * | host, |
uint32_t | dataBusWidth | ||
) |
host | host handler |
dataBusWidth | data bus width |
|
inlinestatic |
host | host handler |
|
inlinestatic |
host | host handler |
targetClock | target clock frequency |
actual | clock frequency can be reach. |
|
inlinestatic |
host | host handler |
true | is busy, false is idle. |
status_t SDMMCHOST_StartBoot | ( | sdmmchost_t * | host, |
sdmmchost_boot_config_t * | hostConfig, | ||
sdmmchost_cmd_t * | cmd, | ||
uint8_t * | buffer | ||
) |
host | host handler |
hostConfig | boot configuration |
cmd | boot command |
buffer | buffer address |
status_t SDMMCHOST_ReadBootData | ( | sdmmchost_t * | host, |
sdmmchost_boot_config_t * | hostConfig, | ||
uint8_t * | buffer | ||
) |
host | host handler |
hostConfig | boot configuration |
buffer | buffer address |
|
inlinestatic |
host | host handler |
enable | true is enable, false is disable |
|
inlinestatic |
host | host handler |
enable | true is enable, false is disable. |
status_t SDMMCHOST_CardIntInit | ( | sdmmchost_t * | host, |
void * | sdioInt | ||
) |
host | host handler |
sdioInt | card interrupt configuration |
status_t SDMMCHOST_CardDetectInit | ( | sdmmchost_t * | host, |
void * | cd | ||
) |
host | host handler |
cd | card detect configuration |
status_t SDMMCHOST_PollingCardDetectStatus | ( | sdmmchost_t * | host, |
uint32_t | waitCardStatus, | ||
uint32_t | timeout | ||
) |
host | host handler |
waitCardStatus | status which user want to wait |
timeout | wait time out. |
kStatus_Success | detect card insert |
kStatus_Fail | card insert event fail |
uint32_t SDMMCHOST_CardDetectStatus | ( | sdmmchost_t * | host | ) |
host | host handler |
kSD_Inserted,kSD_Removed |
status_t SDMMCHOST_Init | ( | sdmmchost_t * | host | ) |
host | host handler |
kStatus_Success | host init success |
kStatus_Fail | event fail |
void SDMMCHOST_Deinit | ( | sdmmchost_t * | host | ) |
host | host handler |
void SDMMCHOST_SetCardPower | ( | sdmmchost_t * | host, |
bool | enable | ||
) |
host | host handler |
enable | true is power on, false is power down. |
status_t SDMMCHOST_TransferFunction | ( | sdmmchost_t * | host, |
sdmmchost_transfer_t * | content | ||
) |
host | host handler |
content | transfer content. |
void SDMMCHOST_Reset | ( | sdmmchost_t * | host | ) |
host | host handler |
status_t SDMMCHOST_WaitCardDetectStatus | ( | SDMMCHOST_TYPE * | hostBase, |
const sdmmchost_detect_card_t * | cd, | ||
bool | waitCardStatus | ||
) |
hostBase | host handler |
cd | card detect configuration. |
waitCardStatus | status to wait. |
void SDMMCHOST_PowerOffCard | ( | SDMMCHOST_TYPE * | base, |
const sdmmchost_pwr_card_t * | pwr | ||
) |
base | host base address. |
pwr | depend on user define power configuration. |
void SDMMCHOST_PowerOnCard | ( | SDMMCHOST_TYPE * | base, |
const sdmmchost_pwr_card_t * | pwr | ||
) |
base | host base address. |
pwr | depend on user define power configuration. |