Power driver provides APIs to control peripherals power and control the system power mode.
static void POWER_EnablePD |
( |
pd_bit_t |
en | ) |
|
|
inlinestatic |
Note that enabling the bit powers down the peripheral
- Parameters
-
en | peripheral for which to enable the PDRUNCFG bit |
- Returns
- none
static void POWER_DisablePD |
( |
pd_bit_t |
en | ) |
|
|
inlinestatic |
Note that disabling the bit powers up the peripheral
- Parameters
-
en | peripheral for which to disable the PDRUNCFG bit |
- Returns
- none
static void POWER_EnableDeepSleep |
( |
void |
| ) |
|
|
inlinestatic |
static void POWER_DisableDeepSleep |
( |
void |
| ) |
|
|
inlinestatic |
void POWER_OtpReload |
( |
void |
| ) |
|
This API must be called if VD6 is power down
and power back again since FROHF TRIM value
is store in OTP. If not, when calling FROHF settng
API in clock driver then the FROHF clock out put
will be inaccurate.
- Returns
- none
void POWER_SetPLL |
( |
void |
| ) |
|
void POWER_SetUsbPhy |
( |
void |
| ) |
|
void POWER_EnterPowerMode |
( |
power_mode_cfg_t |
mode, |
|
|
uint64_t |
exclude_from_pd |
|
) |
| |
- Parameters
-
mode | Power mode. |
exclude_from_pd | Bit mask of the PDRUNCFG0(low 32bits) and PDRUNCFG1(high 32bits) that needs to be powered on during power mode selected. |
- Returns
- none
void POWER_EnterSleep |
( |
void |
| ) |
|
void POWER_EnterDeepSleep |
( |
uint64_t |
exclude_from_pd | ) |
|
- Parameters
-
exclude_from_pd | Bit mask of the PDRUNCFG0(low 32bits) and PDRUNCFG1(high 32bits) bits that needs to be powered on during deep sleep |
- Returns
- none
void POWER_EnterDeepPowerDown |
( |
uint64_t |
exclude_from_pd | ) |
|
- Parameters
-
exclude_from_pd | Bit mask of the PDRUNCFG0(low 32bits) and PDRUNCFG1(high 32bits) that needs to be powered on during deep power down mode, but this is has no effect as the voltages are cut off. |
- Returns
- none
void POWER_SetVoltageForFreq |
( |
uint32_t |
freq | ) |
|
- Parameters
-
freq | - The desired frequency at which the part would like to operate, note that the voltage and flash wait states should be set before changing frequency |
- Returns
- none
uint32_t POWER_GetLibVersion |
( |
void |
| ) |
|
- Returns
- version number of the power library