MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Pdm_sdma

Overview

Data Structures

struct  pdm_sdma_handle_t
 PDM DMA transfer handle, users should not touch the content of the handle. More...
 

Typedefs

typedef void(* pdm_sdma_callback_t )(PDM_Type *base, pdm_sdma_handle_t *handle, status_t status, void *userData)
 PDM eDMA transfer callback function for finish and error.
 

Driver version

#define FSL_PDM_SDMA_DRIVER_VERSION   (MAKE_VERSION(2, 1, 2))
 Version 2.1.2.
 

eDMA Transactional

void PDM_TransferCreateHandleSDMA (PDM_Type *base, pdm_sdma_handle_t *handle, pdm_sdma_callback_t callback, void *userData, sdma_handle_t *dmaHandle, uint32_t eventSource)
 Initializes the PDM eDMA handle. More...
 
status_t PDM_TransferReceiveSDMA (PDM_Type *base, pdm_sdma_handle_t *handle, pdm_transfer_t *xfer)
 Performs a non-blocking PDM receive using eDMA. More...
 
void PDM_TransferAbortReceiveSDMA (PDM_Type *base, pdm_sdma_handle_t *handle)
 Aborts a PDM receive using eDMA. More...
 
void PDM_SetChannelConfigSDMA (PDM_Type *base, pdm_sdma_handle_t *handle, uint32_t channel, const pdm_channel_config_t *config)
 PDM channel configurations. More...
 

Data Structure Documentation

struct _pdm_sdma_handle

Data Fields

sdma_handle_t * dmaHandle
 DMA handler for PDM send.
 
uint8_t nbytes
 eDMA minor byte transfer count initially configured. More...
 
uint8_t fifoWidth
 fifo width
 
uint8_t endChannel
 The last enabled channel.
 
uint8_t channelNums
 total channel numbers
 
uint8_t count
 The transfer data count in a DMA request.
 
uint32_t state
 Internal state for PDM eDMA transfer.
 
uint32_t eventSource
 PDM event source number.
 
pdm_sdma_callback_t callback
 Callback for users while transfer finish or error occurs.
 
void * userData
 User callback parameter.
 
sdma_buffer_descriptor_t bdPool [PDM_XFER_QUEUE_SIZE]
 BD pool for SDMA transfer. More...
 
pdm_transfer_t pdmQueue [PDM_XFER_QUEUE_SIZE]
 Transfer queue storing queued transfer. More...
 
size_t transferSize [PDM_XFER_QUEUE_SIZE]
 Data bytes need to transfer.
 
volatile uint8_t queueUser
 Index for user to queue transfer. More...
 
volatile uint8_t queueDriver
 Index for driver to get the transfer data and size.
 

Field Documentation

uint8_t pdm_sdma_handle_t::nbytes
sdma_buffer_descriptor_t pdm_sdma_handle_t::bdPool[PDM_XFER_QUEUE_SIZE]
pdm_transfer_t pdm_sdma_handle_t::pdmQueue[PDM_XFER_QUEUE_SIZE]
volatile uint8_t pdm_sdma_handle_t::queueUser

Function Documentation

void PDM_TransferCreateHandleSDMA ( PDM_Type *  base,
pdm_sdma_handle_t *  handle,
pdm_sdma_callback_t  callback,
void *  userData,
sdma_handle_t *  dmaHandle,
uint32_t  eventSource 
)

This function initializes the PDM DMA handle, which can be used for other PDM master transactional APIs. Usually, for a specified PDM instance, call this API once to get the initialized handle.

Parameters
basePDM base pointer.
handlePDM eDMA handle pointer.
callbackPointer to user callback function.
userDataUser parameter passed to the callback function.
dmaHandleeDMA handle pointer, this handle shall be static allocated by users.
eventSourcePDM event source number.
status_t PDM_TransferReceiveSDMA ( PDM_Type *  base,
pdm_sdma_handle_t *  handle,
pdm_transfer_t *  xfer 
)
Note
This interface returns immediately after the transfer initiates. Call the PDM_GetReceiveRemainingBytes to poll the transfer status and check whether the PDM transfer is finished.
Parameters
basePDM base pointer
handlePDM eDMA handle pointer.
xferPointer to DMA transfer structure.
Return values
kStatus_SuccessStart a PDM eDMA receive successfully.
kStatus_InvalidArgumentThe input argument is invalid.
kStatus_RxBusyPDM is busy receiving data.
void PDM_TransferAbortReceiveSDMA ( PDM_Type *  base,
pdm_sdma_handle_t *  handle 
)
Parameters
basePDM base pointer
handlePDM eDMA handle pointer.
void PDM_SetChannelConfigSDMA ( PDM_Type *  base,
pdm_sdma_handle_t *  handle,
uint32_t  channel,
const pdm_channel_config_t *  config 
)
Parameters
basePDM base pointer.
handlePDM eDMA handle pointer.
channelchannel number.
configchannel configurations.