The SDK provides a peripheral driver for the Mailbox module of JN devices.
The mailbox driver API provide:
Typical use case
Example of code on primary core, which causes an interrupt on the secondary core by writing to mailbox register.
int main(void)
{
uint32_t message = 1;
}
Example of code on secondary core to handle interrupt from primary core.
void MAILBOX_IRQHandler()
{
uint32_t message;
}
int main(void)
{
NVIC_EnableIRQ(MAILBOX_IRQn);
while (1)
{
__WFI();
}
}
Example of code to get/set mutex.
volatile uint32_t g_shared = 0;
int main(void)
{
{}
g_shared++;
}
| static void MAILBOX_Init |
( |
MAILBOX_Type * |
base | ) |
|
|
inlinestatic |
This function enables the MAILBOX clock only.
- Parameters
-
| base | MAILBOX peripheral base address. |
| static void MAILBOX_Deinit |
( |
MAILBOX_Type * |
base | ) |
|
|
inlinestatic |
This function disables the MAILBOX clock only.
- Parameters
-
| base | MAILBOX peripheral base address. |
| static void MAILBOX_SetValue |
( |
MAILBOX_Type * |
base, |
|
|
mailbox_cpu_id_t |
cpu_id, |
|
|
uint32_t |
mboxData |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | MAILBOX peripheral base address. |
| cpu_id | CPU id, kMAILBOX_CM41 is APPCORE or kMAILBOX_CM40 is eSCORE. |
| mboxData | Data to send in the mailbox. |
- Note
- Sets a data value to send via the MAILBOX to the other core.
| static uint32_t MAILBOX_GetValue |
( |
MAILBOX_Type * |
base, |
|
|
mailbox_cpu_id_t |
cpu_id |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | MAILBOX peripheral base address. |
| cpu_id | CPU id, kMAILBOX_CM41 is APPCORE or kMAILBOX_CM40 is eSCORE. |
- Returns
- Current mailbox data.
| static void MAILBOX_SetValueBits |
( |
MAILBOX_Type * |
base, |
|
|
mailbox_cpu_id_t |
cpu_id, |
|
|
uint32_t |
mboxSetBits |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | MAILBOX peripheral base address. |
| cpu_id | CPU id, kMAILBOX_CM41 is APPCORE or kMAILBOX_CM40 is eSCORE. |
| mboxSetBits | Data bits to set in the mailbox. |
- Note
- Sets data bits to send via the MAILBOX to the other core. A value of 0 will do nothing. Only sets bits selected with a 1 in it's bit position.
| static void MAILBOX_ClearValueBits |
( |
MAILBOX_Type * |
base, |
|
|
mailbox_cpu_id_t |
cpu_id, |
|
|
uint32_t |
mboxClrBits |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | MAILBOX peripheral base address. |
| cpu_id | CPU id, kMAILBOX_CM41 is APPCORE or kMAILBOX_CM40 is eSCORE. |
| mboxClrBits | Data bits to clear in the mailbox. |
- Note
- Clear data bits to send via the MAILBOX to the other core. A value of 0 will do nothing. Only clears bits selected with a 1 in it's bit position.
| static uint32_t MAILBOX_GetMutex |
( |
MAILBOX_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | MAILBOX peripheral base address. |
- Returns
- See note
- Note
- Returns '1' if the mutex was taken or '0' if another resources has the mutex locked. Once a mutex is taken, it can be returned with the MAILBOX_SetMutex() function.
| static void MAILBOX_SetMutex |
( |
MAILBOX_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | MAILBOX peripheral base address. |
- Note
- Sets mutex state to '1' and allows other resources to get the mutex.