![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Modules | |
SPIFI DMA Driver | |
SPIFI Driver | |
Data Structures | |
struct | spifi_command_t |
SPIFI command structure. More... | |
struct | spifi_config_t |
SPIFI region configuration structure. More... | |
struct | spifi_transfer_t |
Transfer structure for SPIFI. More... | |
struct | spifi_dma_handle_t |
SPIFI DMA transfer handle, users should not touch the content of the handle. More... | |
Typedefs | |
typedef void(* | spifi_dma_callback_t )(SPIFI_Type *base, spifi_dma_handle_t *handle, status_t status, void *userData) |
SPIFI DMA transfer callback function for finish and error. | |
Functions | |
static void | SPIFI_EnableDMA (SPIFI_Type *base, bool enable) |
Enable or disable DMA request for SPIFI. More... | |
static uint32_t | SPIFI_GetDataRegisterAddress (SPIFI_Type *base) |
Gets the SPIFI data register address. More... | |
static void | SPIFI_WriteData (SPIFI_Type *base, uint32_t data) |
Write a word data in address of SPIFI. More... | |
static uint32_t | SPIFI_ReadData (SPIFI_Type *base) |
Read data from serial flash. More... | |
Driver version | |
#define | FSL_SPIFI_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
SPIFI driver version 2.0.0. More... | |
Initialization and deinitialization | |
void | SPIFI_Init (SPIFI_Type *base, const spifi_config_t *config) |
Initializes the SPIFI with the user configuration structure. More... | |
void | SPIFI_GetDefaultConfig (spifi_config_t *config) |
Get SPIFI default configure settings. More... | |
void | SPIFI_Deinit (SPIFI_Type *base) |
Deinitializes the SPIFI regions. More... | |
Basic Control Operations | |
void | SPIFI_SetCommand (SPIFI_Type *base, spifi_command_t *cmd) |
Set SPIFI flash command. More... | |
static void | SPIFI_SetCommandAddress (SPIFI_Type *base, uint32_t addr) |
Set SPIFI command address. More... | |
static void | SPIFI_SetIntermediateData (SPIFI_Type *base, uint32_t val) |
Set SPIFI intermediate data. More... | |
static void | SPIFI_SetCacheLimit (SPIFI_Type *base, uint32_t val) |
Set SPIFI Cache limit value. More... | |
static void | SPIFI_ResetCommand (SPIFI_Type *base) |
Reset the command field of SPIFI. More... | |
void | SPIFI_SetMemoryCommand (SPIFI_Type *base, spifi_command_t *cmd) |
Set SPIFI flash AHB read command. More... | |
static void | SPIFI_EnableInterrupt (SPIFI_Type *base, uint32_t mask) |
Enable SPIFI interrupt. More... | |
static void | SPIFI_DisableInterrupt (SPIFI_Type *base, uint32_t mask) |
Disable SPIFI interrupt. More... | |
Status | |
static uint32_t | SPIFI_GetStatusFlag (SPIFI_Type *base) |
Get the status of all interrupt flags for SPIFI. More... | |
DMA Transactional | |
void | SPIFI_TransferTxCreateHandleDMA (SPIFI_Type *base, spifi_dma_handle_t *handle, spifi_dma_callback_t callback, void *userData, dma_handle_t *dmaHandle) |
Initializes the SPIFI handle for send which is used in transactional functions and set the callback. More... | |
void | SPIFI_TransferRxCreateHandleDMA (SPIFI_Type *base, spifi_dma_handle_t *handle, spifi_dma_callback_t callback, void *userData, dma_handle_t *dmaHandle) |
Initializes the SPIFI handle for receive which is used in transactional functions and set the callback. More... | |
status_t | SPIFI_TransferSendDMA (SPIFI_Type *base, spifi_dma_handle_t *handle, spifi_transfer_t *xfer) |
Transfers SPIFI data using an DMA non-blocking method. More... | |
status_t | SPIFI_TransferReceiveDMA (SPIFI_Type *base, spifi_dma_handle_t *handle, spifi_transfer_t *xfer) |
Receives data using an DMA non-blocking method. More... | |
void | SPIFI_TransferAbortSendDMA (SPIFI_Type *base, spifi_dma_handle_t *handle) |
Aborts the sent data using DMA. More... | |
void | SPIFI_TransferAbortReceiveDMA (SPIFI_Type *base, spifi_dma_handle_t *handle) |
Aborts the receive data using DMA. More... | |
status_t | SPIFI_TransferGetSendCountDMA (SPIFI_Type *base, spifi_dma_handle_t *handle, size_t *count) |
Gets the transferred counts of send. More... | |
status_t | SPIFI_TransferGetReceiveCountDMA (SPIFI_Type *base, spifi_dma_handle_t *handle, size_t *count) |
Gets the status of the receive transfer. More... | |
struct spifi_command_t |
Data Fields | |
uint16_t | dataLen |
How many data bytes are needed in this command. More... | |
bool | isPollMode |
For command need to read data from serial flash. | |
spifi_data_direction_t | direction |
Data direction of this command. More... | |
uint8_t | intermediateBytes |
How many intermediate bytes needed. | |
spifi_command_format_t | format |
Command format. | |
spifi_command_type_t | type |
Command type. | |
uint8_t | opcode |
Command opcode value. | |
uint16_t spifi_command_t::dataLen |
spifi_data_direction_t spifi_command_t::direction |
struct spifi_config_t |
Data Fields | |
uint16_t | timeout |
SPI transfer timeout, the unit is SCK cycles. | |
uint8_t | csHighTime |
CS high time cycles. | |
bool | disablePrefetch |
True means SPIFI will not attempt a speculative prefetch. More... | |
bool | disableCachePrefech |
Disable prefetch of cache line. | |
bool | isFeedbackClock |
Is data sample uses feedback clock. More... | |
spifi_spi_mode_t | spiMode |
SPIFI spi mode select. | |
bool | isReadFullClockCycle |
If enable read full clock cycle. More... | |
spifi_dual_mode_t | dualMode |
SPIFI dual mode, dual or quad. More... | |
bool spifi_config_t::disablePrefetch |
bool spifi_config_t::isFeedbackClock |
bool spifi_config_t::isReadFullClockCycle |
spifi_dual_mode_t spifi_config_t::dualMode |
struct spifi_transfer_t |
struct _spifi_dma_handle |
Data Fields | |
dma_handle_t * | dmaHandle |
DMA handler for SPIFI send. | |
size_t | transferSize |
Bytes need to transfer. More... | |
uint32_t | state |
Internal state for SPIFI DMA transfer. | |
spifi_dma_callback_t | callback |
Callback for users while transfer finish or error occurred. | |
void * | userData |
User callback parameter. | |
size_t spifi_dma_handle_t::transferSize |
#define FSL_SPIFI_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
enum _status_t |
enum spifi_spi_mode_t |
enum spifi_dual_mode_t |
enum spifi_command_type_t |
enum _spifi_status_flags |
void SPIFI_Init | ( | SPIFI_Type * | base, |
const spifi_config_t * | config | ||
) |
This function configures the SPIFI module with the user-defined configuration.
base | SPIFI peripheral base address. |
config | The pointer to the configuration structure. |
void SPIFI_GetDefaultConfig | ( | spifi_config_t * | config | ) |
config | SPIFI config structure pointer. |
void SPIFI_Deinit | ( | SPIFI_Type * | base | ) |
base | SPIFI peripheral base address. |
void SPIFI_SetCommand | ( | SPIFI_Type * | base, |
spifi_command_t * | cmd | ||
) |
base | SPIFI peripheral base address. |
cmd | SPIFI command structure pointer. |
|
inlinestatic |
base | SPIFI peripheral base address. |
addr | Address value for the command. |
|
inlinestatic |
Before writing a command wihch needs specific intermediate value, users shall call this function to write it. The main use of this function for current serial flash is to select no-opcode mode and cancelling this mode. As dummy cycle do not care about the value, no need to call this function.
base | SPIFI peripheral base address. |
val | Intermediate data. |
|
inlinestatic |
SPIFI includes caching of prevously-accessed data to improve performance. Software can write an address to this function, to prevent such caching at and above the address.
base | SPIFI peripheral base address. |
val | Zero-based upper limit of cacheable memory. |
|
inlinestatic |
This function is used to abort the current command or memory mode.
base | SPIFI peripheral base address. |
void SPIFI_SetMemoryCommand | ( | SPIFI_Type * | base, |
spifi_command_t * | cmd | ||
) |
Call this function means SPIFI enters to memory mode, while users need to use command, a SPIFI_ResetCommand shall be called.
base | SPIFI peripheral base address. |
cmd | SPIFI command structure pointer. |
|
inlinestatic |
The interrupt is triggered only in command mode, and it means the command now is finished.
base | SPIFI peripheral base address. |
mask | SPIFI interrupt enable mask. It is a logic OR of members the enumeration :: spifi_interrupt_enable_t |
|
inlinestatic |
The interrupt is triggered only in command mode, and it means the command now is finished.
base | SPIFI peripheral base address. |
mask | SPIFI interrupt enable mask. It is a logic OR of members the enumeration :: spifi_interrupt_enable_t |
|
inlinestatic |
base | SPIFI peripheral base address. |
|
inlinestatic |
base | SPIFI peripheral base address. |
enable | True means enable DMA and false means disable DMA. |
|
inlinestatic |
This API is used to provide a transfer address for the SPIFI DMA transfer configuration.
base | SPIFI base pointer |
|
inlinestatic |
Users can write a page or at least a word data into SPIFI address.
base | SPIFI peripheral base address. |
data | Data need be write. |
|
inlinestatic |
Users should notice before call this function, the data length field in command register shall larger than 4, otherwise a hardfault will happen.
base | SPIFI peripheral base address. |
void SPIFI_TransferTxCreateHandleDMA | ( | SPIFI_Type * | base, |
spifi_dma_handle_t * | handle, | ||
spifi_dma_callback_t | callback, | ||
void * | userData, | ||
dma_handle_t * | dmaHandle | ||
) |
base | SPIFI peripheral base address |
handle | Pointer to spifi_dma_handle_t structure |
callback | SPIFI callback, NULL means no callback. |
userData | User callback function data. |
rxDmaHandle | User requested DMA handle for DMA transfer |
void SPIFI_TransferRxCreateHandleDMA | ( | SPIFI_Type * | base, |
spifi_dma_handle_t * | handle, | ||
spifi_dma_callback_t | callback, | ||
void * | userData, | ||
dma_handle_t * | dmaHandle | ||
) |
base | SPIFI peripheral base address |
handle | Pointer to spifi_dma_handle_t structure |
callback | SPIFI callback, NULL means no callback. |
userData | User callback function data. |
rxDmaHandle | User requested DMA handle for DMA transfer |
status_t SPIFI_TransferSendDMA | ( | SPIFI_Type * | base, |
spifi_dma_handle_t * | handle, | ||
spifi_transfer_t * | xfer | ||
) |
This function writes data to the SPIFI transmit FIFO. This function is non-blocking.
base | Pointer to QuadSPI Type. |
handle | Pointer to spifi_dma_handle_t structure |
xfer | SPIFI transfer structure. |
status_t SPIFI_TransferReceiveDMA | ( | SPIFI_Type * | base, |
spifi_dma_handle_t * | handle, | ||
spifi_transfer_t * | xfer | ||
) |
This function receive data from the SPIFI receive buffer/FIFO. This function is non-blocking.
base | Pointer to QuadSPI Type. |
handle | Pointer to spifi_dma_handle_t structure |
xfer | SPIFI transfer structure. |
void SPIFI_TransferAbortSendDMA | ( | SPIFI_Type * | base, |
spifi_dma_handle_t * | handle | ||
) |
This function aborts the sent data using DMA.
base | SPIFI peripheral base address. |
handle | Pointer to spifi_dma_handle_t structure |
void SPIFI_TransferAbortReceiveDMA | ( | SPIFI_Type * | base, |
spifi_dma_handle_t * | handle | ||
) |
This function abort receive data which using DMA.
base | SPIFI peripheral base address. |
handle | Pointer to spifi_dma_handle_t structure |
status_t SPIFI_TransferGetSendCountDMA | ( | SPIFI_Type * | base, |
spifi_dma_handle_t * | handle, | ||
size_t * | count | ||
) |
base | Pointer to QuadSPI Type. |
handle | Pointer to spifi_dma_handle_t structure. |
count | Bytes sent. |
kStatus_Success | Succeed get the transfer count. |
kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. |
status_t SPIFI_TransferGetReceiveCountDMA | ( | SPIFI_Type * | base, |
spifi_dma_handle_t * | handle, | ||
size_t * | count | ||
) |
base | Pointer to QuadSPI Type. |
handle | Pointer to spifi_dma_handle_t structure |
count | Bytes received. |
kStatus_Success | Succeed get the transfer count. |
kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. |