![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
struct | panic_data_t |
panic data structure. More... | |
Macros | |
#define | PANIC_ENABLE_LOG (1) |
More... | |
Typedefs | |
typedef uint32_t | panic_id_t |
More... | |
Functions | |
void | panic (panic_id_t id, uint32_t location, uint32_t extra1, uint32_t extra2) |
More... | |
struct panic_data_t |
#define PANIC_ENABLE_LOG (1) |
Public macros
typedef uint32_t panic_id_t |
Include
Public type definitionspanic id.
void panic | ( | panic_id_t | id, |
uint32_t | location, | ||
uint32_t | extra1, | ||
uint32_t | extra2 | ||
) |
Public prototypes
Panic function.
id | Panic ID |
location | location address where the Panic occurred |
extra1 | extra1 parameter to be stored in Panic structure. |
extra2 | extra2 parameter to be stored in Panic structure |
No | return vaule. |