![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Macros | |
| #define | FSL_OSA_BM_TIMER_NONE 0U |
| Bare Metal does not use timer. More... | |
| #define | FSL_OSA_BM_TIMER_SYSTICK 1U |
| Bare Metal uses SYSTICK as timer. More... | |
| #define | FSL_OSA_BM_TIMER_CONFIG FSL_OSA_BM_TIMER_NONE |
| Configure what timer is used in Bare Metal. More... | |
| #define | OSA_WAIT_FOREVER 0xFFFFFFFFU |
| Constant to pass as timeout value in order to wait indefinitely. More... | |
| #define | TASK_MAX_NUM 7 |
| How many tasks can the bare metal support. More... | |
| #define | FSL_OSA_TIME_RANGE 0xFFFFFFFFU |
| OSA's time range in millisecond, OSA time wraps if exceeds this value. More... | |
| #define | OSA_DEFAULT_INT_HANDLER ((osa_int_handler_t)(&DefaultISR)) |
| The default interrupt handler installed in vector table. More... | |
Typedefs | |
| typedef void * | task_param_t |
| Type for task parameter. | |
| typedef uint32_t | event_flags_t |
| Type for an event flags group, bit 32 is reserved. | |
Functions | |
| void | DefaultISR (void) |
| The default interrupt handler installed in vector table. More... | |
Thread management | |
| #define | PRIORITY_OSA_TO_RTOS(osa_prio) (osa_prio) |
| To provide unified priority for upper layer, OSA layer makes conversation. | |
| #define | PRIORITY_RTOS_TO_OSA(rtos_prio) (rtos_prio) |
| #define FSL_OSA_BM_TIMER_NONE 0U |
| #define FSL_OSA_BM_TIMER_SYSTICK 1U |
| #define FSL_OSA_BM_TIMER_CONFIG FSL_OSA_BM_TIMER_NONE |
| #define OSA_WAIT_FOREVER 0xFFFFFFFFU |
| #define TASK_MAX_NUM 7 |
| #define FSL_OSA_TIME_RANGE 0xFFFFFFFFU |
| #define OSA_DEFAULT_INT_HANDLER ((osa_int_handler_t)(&DefaultISR)) |
| void DefaultISR | ( | void | ) |