![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Modules | |
| Nand Flash Component | |
| Nor Flash Component | |
Data Structures | |
| struct | flash_config_t |
| Flash config structure. More... | |
| struct | flash_transfer_t |
| Flash transfer structure. More... | |
| struct | flash_handle_t |
| Flash handle. More... | |
Enumerations | |
| enum | flash_err_t { flash_ok, flash_too_big, flash_not_aligned, flash_busy, flash_error } |
| Flash error code structure. More... | |
| enum | flash_op_code_t { kNorFlash_WriteEnable = 0x0, kNorFlash_Write = 0x1, kNorFlash_Read = 0x2, kNorFlash_ReadStatus = 0x3, kNorFlash_EraseSector = 0x4, kNorFlash_EraseChip = 0x5 } |
| Flash operation code structure. More... | |
| struct flash_config_t |
Data Fields | |
| uint32_t | totalSize |
| Total flash size. More... | |
| uint32_t | pageSize |
| Page size. More... | |
| uint32_t | sectorSize |
| Sector size. More... | |
| bool | needWriteEnable |
| Need do write enable before write/erase operation. More... | |
| uint8_t | statusValueSize |
| Status value size in bytes. More... | |
| uint32_t | statusBusyMask |
| Status busy mask. More... | |
| uint8_t | statusBusyValue |
| Status busy value. More... | |
| uint32_t flash_config_t::totalSize |
| uint32_t flash_config_t::pageSize |
| uint32_t flash_config_t::sectorSize |
| bool flash_config_t::needWriteEnable |
| uint8_t flash_config_t::statusValueSize |
| uint32_t flash_config_t::statusBusyMask |
| uint8_t flash_config_t::statusBusyValue |
| struct flash_transfer_t |
Data Fields | |
| flash_op_code_t | opCode |
| Operation code. More... | |
| uint8_t | address |
| Program/write address. More... | |
| uint8_t * | data |
| Data buffer pointer for program buffer or store buffer. More... | |
| uint32_t | dataSize |
| Data buffer size. More... | |
| flash_op_code_t flash_transfer_t::opCode |
| uint8_t flash_transfer_t::address |
| uint8_t* flash_transfer_t::data |
| uint32_t flash_transfer_t::dataSize |
| struct flash_handle_t |
Data Fields | |
| flash_err_t(* | executeCommand )(void *resource, flash_transfer_t *xfer) |
| Execute command function. More... | |
| void * | resource |
| Pointer for resource, resource mean the SPI adapter resource. More... | |
| uint32_t | totalSize |
| Flash total size. More... | |
| uint32_t | pageSize |
| Flash page size. More... | |
| uint32_t | sectorSize |
| Flash sector size. More... | |
| bool | needWriteEnable |
| Need do write enable before write/erase operation. More... | |
| uint8_t | statusValueSize |
| Status value size in bytes. More... | |
| uint32_t | statusBusyMask |
| Status busy mask. More... | |
| uint8_t | statusBusyValue |
| Status busy value. More... | |
| flash_err_t(* flash_handle_t::executeCommand)(void *resource, flash_transfer_t *xfer) |
| void* flash_handle_t::resource |
| uint32_t flash_handle_t::totalSize |
| uint32_t flash_handle_t::pageSize |
| uint32_t flash_handle_t::sectorSize |
| bool flash_handle_t::needWriteEnable |
| uint8_t flash_handle_t::statusValueSize |
| uint32_t flash_handle_t::statusBusyMask |
| uint8_t flash_handle_t::statusBusyValue |
| enum flash_err_t |
| enum flash_op_code_t |