![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
This section describes the programming interface of the DSPI peripheral driver. The DSPI driver configures the DSPI module and provides functional and transactional interfaces to build the DSPI application.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/dspi.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/dspi.
Data Structures | |
| struct | dspi_command_data_config_t |
| DSPI master command date configuration used for the SPIx_PUSHR. More... | |
| struct | dspi_master_ctar_config_t |
| DSPI master ctar configuration structure. More... | |
| struct | dspi_master_config_t |
| DSPI master configuration structure. More... | |
| struct | dspi_slave_ctar_config_t |
| DSPI slave ctar configuration structure. More... | |
| struct | dspi_slave_config_t |
| DSPI slave configuration structure. More... | |
| struct | dspi_transfer_t |
| DSPI master/slave transfer structure. More... | |
| struct | dspi_half_duplex_transfer_t |
| DSPI half-duplex(master) transfer structure. More... | |
| struct | dspi_master_handle_t |
| DSPI master transfer handle structure used for transactional API. More... | |
| struct | dspi_slave_handle_t |
| DSPI slave transfer handle structure used for the transactional API. More... | |
Macros | |
| #define | DSPI_DUMMY_DATA (0x00U) |
| DSPI dummy data if there is no Tx data. More... | |
| #define | DSPI_MASTER_CTAR_SHIFT (0U) |
| DSPI master CTAR shift macro; used internally. More... | |
| #define | DSPI_MASTER_CTAR_MASK (0x0FU) |
| DSPI master CTAR mask macro; used internally. More... | |
| #define | DSPI_MASTER_PCS_SHIFT (4U) |
| DSPI master PCS shift macro; used internally. More... | |
| #define | DSPI_MASTER_PCS_MASK (0xF0U) |
| DSPI master PCS mask macro; used internally. More... | |
| #define | DSPI_SLAVE_CTAR_SHIFT (0U) |
| DSPI slave CTAR shift macro; used internally. More... | |
| #define | DSPI_SLAVE_CTAR_MASK (0x07U) |
| DSPI slave CTAR mask macro; used internally. More... | |
Typedefs | |
| typedef void(* | dspi_master_transfer_callback_t )(SPI_Type *base, dspi_master_handle_t *handle, status_t status, void *userData) |
| Completion callback function pointer type. More... | |
| typedef void(* | dspi_slave_transfer_callback_t )(SPI_Type *base, dspi_slave_handle_t *handle, status_t status, void *userData) |
| Completion callback function pointer type. More... | |
Enumerations | |
| enum | { kStatus_DSPI_Busy = MAKE_STATUS(kStatusGroup_DSPI, 0), kStatus_DSPI_Error = MAKE_STATUS(kStatusGroup_DSPI, 1), kStatus_DSPI_Idle = MAKE_STATUS(kStatusGroup_DSPI, 2), kStatus_DSPI_OutOfRange = MAKE_STATUS(kStatusGroup_DSPI, 3) } |
| Status for the DSPI driver. More... | |
| enum | _dspi_flags { kDSPI_TxCompleteFlag = (int)SPI_SR_TCF_MASK, kDSPI_EndOfQueueFlag = SPI_SR_EOQF_MASK, kDSPI_TxFifoUnderflowFlag = SPI_SR_TFUF_MASK, kDSPI_TxFifoFillRequestFlag = SPI_SR_TFFF_MASK, kDSPI_RxFifoOverflowFlag = SPI_SR_RFOF_MASK, kDSPI_RxFifoDrainRequestFlag = SPI_SR_RFDF_MASK, kDSPI_TxAndRxStatusFlag = SPI_SR_TXRXS_MASK, kDSPI_AllStatusFlag } |
| DSPI status flags in SPIx_SR register. More... | |
| enum | _dspi_interrupt_enable { kDSPI_TxCompleteInterruptEnable = (int)SPI_RSER_TCF_RE_MASK, kDSPI_EndOfQueueInterruptEnable = SPI_RSER_EOQF_RE_MASK, kDSPI_TxFifoUnderflowInterruptEnable = SPI_RSER_TFUF_RE_MASK, kDSPI_TxFifoFillRequestInterruptEnable = SPI_RSER_TFFF_RE_MASK, kDSPI_RxFifoOverflowInterruptEnable = SPI_RSER_RFOF_RE_MASK, kDSPI_RxFifoDrainRequestInterruptEnable = SPI_RSER_RFDF_RE_MASK, kDSPI_AllInterruptEnable } |
| DSPI interrupt source. More... | |
| enum | _dspi_dma_enable { kDSPI_TxDmaEnable = (SPI_RSER_TFFF_RE_MASK | SPI_RSER_TFFF_DIRS_MASK), kDSPI_RxDmaEnable = (SPI_RSER_RFDF_RE_MASK | SPI_RSER_RFDF_DIRS_MASK) } |
| DSPI DMA source. More... | |
| enum | dspi_master_slave_mode_t { kDSPI_Master = 1U, kDSPI_Slave = 0U } |
| DSPI master or slave mode configuration. More... | |
| enum | dspi_master_sample_point_t { kDSPI_SckToSin0Clock = 0U, kDSPI_SckToSin1Clock = 1U, kDSPI_SckToSin2Clock = 2U } |
| DSPI Sample Point: Controls when the DSPI master samples SIN in the Modified Transfer Format. More... | |
| enum | dspi_which_pcs_t { kDSPI_Pcs0 = 1U << 0, kDSPI_Pcs1 = 1U << 1, kDSPI_Pcs2 = 1U << 2, kDSPI_Pcs3 = 1U << 3, kDSPI_Pcs4 = 1U << 4, kDSPI_Pcs5 = 1U << 5 } |
| DSPI Peripheral Chip Select (Pcs) configuration (which Pcs to configure). More... | |
| enum | dspi_pcs_polarity_config_t { kDSPI_PcsActiveHigh = 0U, kDSPI_PcsActiveLow = 1U } |
| DSPI Peripheral Chip Select (Pcs) Polarity configuration. More... | |
| enum | _dspi_pcs_polarity { kDSPI_Pcs0ActiveLow = 1U << 0, kDSPI_Pcs1ActiveLow = 1U << 1, kDSPI_Pcs2ActiveLow = 1U << 2, kDSPI_Pcs3ActiveLow = 1U << 3, kDSPI_Pcs4ActiveLow = 1U << 4, kDSPI_Pcs5ActiveLow = 1U << 5, kDSPI_PcsAllActiveLow = 0xFFU } |
| DSPI Peripheral Chip Select (Pcs) Polarity. More... | |
| enum | dspi_clock_polarity_t { kDSPI_ClockPolarityActiveHigh = 0U, kDSPI_ClockPolarityActiveLow = 1U } |
| DSPI clock polarity configuration for a given CTAR. More... | |
| enum | dspi_clock_phase_t { kDSPI_ClockPhaseFirstEdge = 0U, kDSPI_ClockPhaseSecondEdge = 1U } |
| DSPI clock phase configuration for a given CTAR. More... | |
| enum | dspi_shift_direction_t { kDSPI_MsbFirst = 0U, kDSPI_LsbFirst = 1U } |
| DSPI data shifter direction options for a given CTAR. More... | |
| enum | dspi_delay_type_t { kDSPI_PcsToSck = 1U, kDSPI_LastSckToPcs, kDSPI_BetweenTransfer } |
| DSPI delay type selection. More... | |
| enum | dspi_ctar_selection_t { kDSPI_Ctar0 = 0U, kDSPI_Ctar1 = 1U, kDSPI_Ctar2 = 2U, kDSPI_Ctar3 = 3U, kDSPI_Ctar4 = 4U, kDSPI_Ctar5 = 5U, kDSPI_Ctar6 = 6U, kDSPI_Ctar7 = 7U } |
| DSPI Clock and Transfer Attributes Register (CTAR) selection. More... | |
| enum | _dspi_transfer_config_flag_for_master { kDSPI_MasterCtar0 = 0U << DSPI_MASTER_CTAR_SHIFT, kDSPI_MasterCtar1 = 1U << DSPI_MASTER_CTAR_SHIFT, kDSPI_MasterCtar2 = 2U << DSPI_MASTER_CTAR_SHIFT, kDSPI_MasterCtar3 = 3U << DSPI_MASTER_CTAR_SHIFT, kDSPI_MasterCtar4 = 4U << DSPI_MASTER_CTAR_SHIFT, kDSPI_MasterCtar5 = 5U << DSPI_MASTER_CTAR_SHIFT, kDSPI_MasterCtar6 = 6U << DSPI_MASTER_CTAR_SHIFT, kDSPI_MasterCtar7 = 7U << DSPI_MASTER_CTAR_SHIFT, kDSPI_MasterPcs0 = 0U << DSPI_MASTER_PCS_SHIFT, kDSPI_MasterPcs1 = 1U << DSPI_MASTER_PCS_SHIFT, kDSPI_MasterPcs2 = 2U << DSPI_MASTER_PCS_SHIFT, kDSPI_MasterPcs3 = 3U << DSPI_MASTER_PCS_SHIFT, kDSPI_MasterPcs4 = 4U << DSPI_MASTER_PCS_SHIFT, kDSPI_MasterPcs5 = 5U << DSPI_MASTER_PCS_SHIFT, kDSPI_MasterPcsContinuous = 1U << 20, kDSPI_MasterActiveAfterTransfer = 1U << 21 } |
| Use this enumeration for the DSPI master transfer configFlags. More... | |
| enum | _dspi_transfer_config_flag_for_slave { kDSPI_SlaveCtar0 = 0U << DSPI_SLAVE_CTAR_SHIFT } |
| Use this enumeration for the DSPI slave transfer configFlags. More... | |
| enum | _dspi_transfer_state { kDSPI_Idle = 0x0U, kDSPI_Busy, kDSPI_Error } |
| DSPI transfer state, which is used for DSPI transactional API state machine. More... | |
Variables | |
| volatile uint8_t | g_dspiDummyData [] |
| Global variable for dummy data value setting. More... | |
Driver version | |
| #define | FSL_DSPI_DRIVER_VERSION (MAKE_VERSION(2, 2, 4)) |
| DSPI driver version 2.2.4. More... | |
Initialization and deinitialization | |
| void | DSPI_MasterInit (SPI_Type *base, const dspi_master_config_t *masterConfig, uint32_t srcClock_Hz) |
| Initializes the DSPI master. More... | |
| void | DSPI_MasterGetDefaultConfig (dspi_master_config_t *masterConfig) |
| Sets the dspi_master_config_t structure to default values. More... | |
| void | DSPI_SlaveInit (SPI_Type *base, const dspi_slave_config_t *slaveConfig) |
| DSPI slave configuration. More... | |
| void | DSPI_SlaveGetDefaultConfig (dspi_slave_config_t *slaveConfig) |
| Sets the dspi_slave_config_t structure to a default value. More... | |
| void | DSPI_Deinit (SPI_Type *base) |
| De-initializes the DSPI peripheral. More... | |
| static void | DSPI_Enable (SPI_Type *base, bool enable) |
| Enables the DSPI peripheral and sets the MCR MDIS to 0. More... | |
Status | |
| static uint32_t | DSPI_GetStatusFlags (SPI_Type *base) |
| Gets the DSPI status flag state. More... | |
| static void | DSPI_ClearStatusFlags (SPI_Type *base, uint32_t statusFlags) |
| Clears the DSPI status flag. More... | |
Interrupts | |
| void | DSPI_EnableInterrupts (SPI_Type *base, uint32_t mask) |
| Enables the DSPI interrupts. More... | |
| static void | DSPI_DisableInterrupts (SPI_Type *base, uint32_t mask) |
| Disables the DSPI interrupts. More... | |
DMA Control | |
| static void | DSPI_EnableDMA (SPI_Type *base, uint32_t mask) |
| Enables the DSPI DMA request. More... | |
| static void | DSPI_DisableDMA (SPI_Type *base, uint32_t mask) |
| Disables the DSPI DMA request. More... | |
| static uint32_t | DSPI_MasterGetTxRegisterAddress (SPI_Type *base) |
| Gets the DSPI master PUSHR data register address for the DMA operation. More... | |
| static uint32_t | DSPI_SlaveGetTxRegisterAddress (SPI_Type *base) |
| Gets the DSPI slave PUSHR data register address for the DMA operation. More... | |
| static uint32_t | DSPI_GetRxRegisterAddress (SPI_Type *base) |
| Gets the DSPI POPR data register address for the DMA operation. More... | |
Bus Operations | |
| uint32_t | DSPI_GetInstance (SPI_Type *base) |
| Get instance number for DSPI module. More... | |
| static void | DSPI_SetMasterSlaveMode (SPI_Type *base, dspi_master_slave_mode_t mode) |
| Configures the DSPI for master or slave. More... | |
| static bool | DSPI_IsMaster (SPI_Type *base) |
| Returns whether the DSPI module is in master mode. More... | |
| static void | DSPI_StartTransfer (SPI_Type *base) |
| Starts the DSPI transfers and clears HALT bit in MCR. More... | |
| static void | DSPI_StopTransfer (SPI_Type *base) |
| Stops DSPI transfers and sets the HALT bit in MCR. More... | |
| static void | DSPI_SetFifoEnable (SPI_Type *base, bool enableTxFifo, bool enableRxFifo) |
| Enables or disables the DSPI FIFOs. More... | |
| static void | DSPI_FlushFifo (SPI_Type *base, bool flushTxFifo, bool flushRxFifo) |
| Flushes the DSPI FIFOs. More... | |
| static void | DSPI_SetAllPcsPolarity (SPI_Type *base, uint32_t mask) |
| Configures the DSPI peripheral chip select polarity simultaneously. More... | |
| uint32_t | DSPI_MasterSetBaudRate (SPI_Type *base, dspi_ctar_selection_t whichCtar, uint32_t baudRate_Bps, uint32_t srcClock_Hz) |
| Sets the DSPI baud rate in bits per second. More... | |
| void | DSPI_MasterSetDelayScaler (SPI_Type *base, dspi_ctar_selection_t whichCtar, uint32_t prescaler, uint32_t scaler, dspi_delay_type_t whichDelay) |
| Manually configures the delay prescaler and scaler for a particular CTAR. More... | |
| uint32_t | DSPI_MasterSetDelayTimes (SPI_Type *base, dspi_ctar_selection_t whichCtar, dspi_delay_type_t whichDelay, uint32_t srcClock_Hz, uint32_t delayTimeInNanoSec) |
| Calculates the delay prescaler and scaler based on the desired delay input in nanoseconds. More... | |
| static void | DSPI_MasterWriteData (SPI_Type *base, dspi_command_data_config_t *command, uint16_t data) |
| Writes data into the data buffer for master mode. More... | |
| void | DSPI_GetDefaultDataCommandConfig (dspi_command_data_config_t *command) |
| Sets the dspi_command_data_config_t structure to default values. More... | |
| void | DSPI_MasterWriteDataBlocking (SPI_Type *base, dspi_command_data_config_t *command, uint16_t data) |
| Writes data into the data buffer master mode and waits till complete to return. More... | |
| static uint32_t | DSPI_MasterGetFormattedCommand (dspi_command_data_config_t *command) |
| Returns the DSPI command word formatted to the PUSHR data register bit field. More... | |
| void | DSPI_MasterWriteCommandDataBlocking (SPI_Type *base, uint32_t data) |
| Writes a 32-bit data word (16-bit command appended with 16-bit data) into the data buffer master mode and waits till complete to return. More... | |
| static void | DSPI_SlaveWriteData (SPI_Type *base, uint32_t data) |
| Writes data into the data buffer in slave mode. More... | |
| void | DSPI_SlaveWriteDataBlocking (SPI_Type *base, uint32_t data) |
| Writes data into the data buffer in slave mode, waits till data was transmitted, and returns. More... | |
| static uint32_t | DSPI_ReadData (SPI_Type *base) |
| Reads data from the data buffer. More... | |
| void | DSPI_SetDummyData (SPI_Type *base, uint8_t dummyData) |
| Set up the dummy data. More... | |
Transactional APIs | |
| void | DSPI_MasterTransferCreateHandle (SPI_Type *base, dspi_master_handle_t *handle, dspi_master_transfer_callback_t callback, void *userData) |
| Initializes the DSPI master handle. More... | |
| status_t | DSPI_MasterTransferBlocking (SPI_Type *base, dspi_transfer_t *transfer) |
| DSPI master transfer data using polling. More... | |
| status_t | DSPI_MasterTransferNonBlocking (SPI_Type *base, dspi_master_handle_t *handle, dspi_transfer_t *transfer) |
| DSPI master transfer data using interrupts. More... | |
| status_t | DSPI_MasterHalfDuplexTransferBlocking (SPI_Type *base, dspi_half_duplex_transfer_t *xfer) |
| Transfers a block of data using a polling method. More... | |
| status_t | DSPI_MasterHalfDuplexTransferNonBlocking (SPI_Type *base, dspi_master_handle_t *handle, dspi_half_duplex_transfer_t *xfer) |
| Performs a non-blocking DSPI interrupt transfer. More... | |
| status_t | DSPI_MasterTransferGetCount (SPI_Type *base, dspi_master_handle_t *handle, size_t *count) |
| Gets the master transfer count. More... | |
| void | DSPI_MasterTransferAbort (SPI_Type *base, dspi_master_handle_t *handle) |
| DSPI master aborts a transfer using an interrupt. More... | |
| void | DSPI_MasterTransferHandleIRQ (SPI_Type *base, dspi_master_handle_t *handle) |
| DSPI Master IRQ handler function. More... | |
| void | DSPI_SlaveTransferCreateHandle (SPI_Type *base, dspi_slave_handle_t *handle, dspi_slave_transfer_callback_t callback, void *userData) |
| Initializes the DSPI slave handle. More... | |
| status_t | DSPI_SlaveTransferNonBlocking (SPI_Type *base, dspi_slave_handle_t *handle, dspi_transfer_t *transfer) |
| DSPI slave transfers data using an interrupt. More... | |
| status_t | DSPI_SlaveTransferGetCount (SPI_Type *base, dspi_slave_handle_t *handle, size_t *count) |
| Gets the slave transfer count. More... | |
| void | DSPI_SlaveTransferAbort (SPI_Type *base, dspi_slave_handle_t *handle) |
| DSPI slave aborts a transfer using an interrupt. More... | |
| void | DSPI_SlaveTransferHandleIRQ (SPI_Type *base, dspi_slave_handle_t *handle) |
| DSPI Master IRQ handler function. More... | |
| uint8_t | DSPI_GetDummyDataInstance (SPI_Type *base) |
| brief Dummy data for each instance. More... | |
| struct dspi_command_data_config_t |
Data Fields | |
| bool | isPcsContinuous |
| Option to enable the continuous assertion of the chip select between transfers. More... | |
| uint8_t | whichCtar |
| The desired Clock and Transfer Attributes Register (CTAR) to use for CTAS. More... | |
| uint8_t | whichPcs |
| The desired PCS signal to use for the data transfer. More... | |
| bool | isEndOfQueue |
| Signals that the current transfer is the last in the queue. More... | |
| bool | clearTransferCount |
| Clears the SPI Transfer Counter (SPI_TCNT) before transmission starts. More... | |
| bool dspi_command_data_config_t::isPcsContinuous |
| uint8_t dspi_command_data_config_t::whichCtar |
| uint8_t dspi_command_data_config_t::whichPcs |
| bool dspi_command_data_config_t::isEndOfQueue |
| bool dspi_command_data_config_t::clearTransferCount |
| struct dspi_master_ctar_config_t |
Data Fields | |
| uint32_t | baudRate |
| Baud Rate for DSPI. More... | |
| uint32_t | bitsPerFrame |
| Bits per frame, minimum 4, maximum 16. More... | |
| dspi_clock_polarity_t | cpol |
| Clock polarity. More... | |
| dspi_clock_phase_t | cpha |
| Clock phase. More... | |
| dspi_shift_direction_t | direction |
| MSB or LSB data shift direction. More... | |
| uint32_t | pcsToSckDelayInNanoSec |
| PCS to SCK delay time in nanoseconds; setting to 0 sets the minimum delay. More... | |
| uint32_t | lastSckToPcsDelayInNanoSec |
| The last SCK to PCS delay time in nanoseconds; setting to 0 sets the minimum delay. More... | |
| uint32_t | betweenTransferDelayInNanoSec |
| After the SCK delay time in nanoseconds; setting to 0 sets the minimum delay. More... | |
| uint32_t dspi_master_ctar_config_t::baudRate |
| uint32_t dspi_master_ctar_config_t::bitsPerFrame |
| dspi_clock_polarity_t dspi_master_ctar_config_t::cpol |
| dspi_clock_phase_t dspi_master_ctar_config_t::cpha |
| dspi_shift_direction_t dspi_master_ctar_config_t::direction |
| uint32_t dspi_master_ctar_config_t::pcsToSckDelayInNanoSec |
It also sets the boundary value if out of range.
| uint32_t dspi_master_ctar_config_t::lastSckToPcsDelayInNanoSec |
It also sets the boundary value if out of range.
| uint32_t dspi_master_ctar_config_t::betweenTransferDelayInNanoSec |
It also sets the boundary value if out of range.
| struct dspi_master_config_t |
Data Fields | |
| dspi_ctar_selection_t | whichCtar |
| The desired CTAR to use. More... | |
| dspi_master_ctar_config_t | ctarConfig |
| Set the ctarConfig to the desired CTAR. More... | |
| dspi_which_pcs_t | whichPcs |
| The desired Peripheral Chip Select (pcs). More... | |
| dspi_pcs_polarity_config_t | pcsActiveHighOrLow |
| The desired PCS active high or low. More... | |
| bool | enableContinuousSCK |
| CONT_SCKE, continuous SCK enable. More... | |
| bool | enableRxFifoOverWrite |
| ROOE, receive FIFO overflow overwrite enable. More... | |
| bool | enableModifiedTimingFormat |
| Enables a modified transfer format to be used if true. More... | |
| dspi_master_sample_point_t | samplePoint |
| Controls when the module master samples SIN in the Modified Transfer Format. More... | |
| dspi_ctar_selection_t dspi_master_config_t::whichCtar |
| dspi_master_ctar_config_t dspi_master_config_t::ctarConfig |
| dspi_which_pcs_t dspi_master_config_t::whichPcs |
| dspi_pcs_polarity_config_t dspi_master_config_t::pcsActiveHighOrLow |
| bool dspi_master_config_t::enableContinuousSCK |
Note that the continuous SCK is only supported for CPHA = 1.
| bool dspi_master_config_t::enableRxFifoOverWrite |
If ROOE = 0, the incoming data is ignored and the data from the transfer that generated the overflow is also ignored. If ROOE = 1, the incoming data is shifted to the shift register.
| bool dspi_master_config_t::enableModifiedTimingFormat |
| dspi_master_sample_point_t dspi_master_config_t::samplePoint |
It's valid only when CPHA=0.
| struct dspi_slave_ctar_config_t |
Data Fields | |
| uint32_t | bitsPerFrame |
| Bits per frame, minimum 4, maximum 16. More... | |
| dspi_clock_polarity_t | cpol |
| Clock polarity. More... | |
| dspi_clock_phase_t | cpha |
| Clock phase. More... | |
| uint32_t dspi_slave_ctar_config_t::bitsPerFrame |
| dspi_clock_polarity_t dspi_slave_ctar_config_t::cpol |
| dspi_clock_phase_t dspi_slave_ctar_config_t::cpha |
Slave only supports MSB and does not support LSB.
| struct dspi_slave_config_t |
Data Fields | |
| dspi_ctar_selection_t | whichCtar |
| The desired CTAR to use. More... | |
| dspi_slave_ctar_config_t | ctarConfig |
| Set the ctarConfig to the desired CTAR. More... | |
| bool | enableContinuousSCK |
| CONT_SCKE, continuous SCK enable. More... | |
| bool | enableRxFifoOverWrite |
| ROOE, receive FIFO overflow overwrite enable. More... | |
| bool | enableModifiedTimingFormat |
| Enables a modified transfer format to be used if true. More... | |
| dspi_master_sample_point_t | samplePoint |
| Controls when the module master samples SIN in the Modified Transfer Format. More... | |
| dspi_ctar_selection_t dspi_slave_config_t::whichCtar |
| dspi_slave_ctar_config_t dspi_slave_config_t::ctarConfig |
| bool dspi_slave_config_t::enableContinuousSCK |
Note that the continuous SCK is only supported for CPHA = 1.
| bool dspi_slave_config_t::enableRxFifoOverWrite |
If ROOE = 0, the incoming data is ignored and the data from the transfer that generated the overflow is also ignored. If ROOE = 1, the incoming data is shifted to the shift register.
| bool dspi_slave_config_t::enableModifiedTimingFormat |
| dspi_master_sample_point_t dspi_slave_config_t::samplePoint |
It's valid only when CPHA=0.
| struct dspi_transfer_t |
Data Fields | |
| uint8_t * | txData |
| Send buffer. More... | |
| uint8_t * | rxData |
| Receive buffer. More... | |
| volatile size_t | dataSize |
| Transfer bytes. More... | |
| uint32_t | configFlags |
| Transfer transfer configuration flags. More... | |
| uint8_t* dspi_transfer_t::txData |
| uint8_t* dspi_transfer_t::rxData |
| volatile size_t dspi_transfer_t::dataSize |
| uint32_t dspi_transfer_t::configFlags |
Set from _dspi_transfer_config_flag_for_master if the transfer is used for master or _dspi_transfer_config_flag_for_slave enumeration if the transfer is used for slave.
| struct dspi_half_duplex_transfer_t |
Data Fields | |
| uint8_t * | txData |
| Send buffer. | |
| uint8_t * | rxData |
| Receive buffer. | |
| size_t | txDataSize |
| Transfer bytes for transmit. | |
| size_t | rxDataSize |
| Transfer bytes. | |
| uint32_t | configFlags |
| Transfer configuration flags; set from _dspi_transfer_config_flag_for_master. More... | |
| bool | isPcsAssertInTransfer |
| If Pcs pin keep assert between transmit and receive. More... | |
| bool | isTransmitFirst |
| True for transmit first and false for receive first. More... | |
| uint32_t dspi_half_duplex_transfer_t::configFlags |
| bool dspi_half_duplex_transfer_t::isPcsAssertInTransfer |
true for assert and false for de-assert.
| bool dspi_half_duplex_transfer_t::isTransmitFirst |
| struct _dspi_master_handle |
Forward declaration of the _dspi_master_handle typedefs.
The master handle.
Data Fields | |
| uint32_t | bitsPerFrame |
| The desired number of bits per frame. More... | |
| volatile uint32_t | command |
| The desired data command. More... | |
| volatile uint32_t | lastCommand |
| The desired last data command. More... | |
| uint8_t | fifoSize |
| FIFO dataSize. More... | |
| volatile bool | isPcsActiveAfterTransfer |
| Indicates whether the PCS signal is active after the last frame transfer. More... | |
| volatile bool | isThereExtraByte |
| Indicates whether there are extra bytes. More... | |
| uint8_t *volatile | txData |
| Send buffer. More... | |
| uint8_t *volatile | rxData |
| Receive buffer. More... | |
| volatile size_t | remainingSendByteCount |
| A number of bytes remaining to send. More... | |
| volatile size_t | remainingReceiveByteCount |
| A number of bytes remaining to receive. More... | |
| size_t | totalByteCount |
| A number of transfer bytes. | |
| volatile uint8_t | state |
| DSPI transfer state, see _dspi_transfer_state. More... | |
| dspi_master_transfer_callback_t | callback |
| Completion callback. More... | |
| void * | userData |
| Callback user data. More... | |
| uint32_t dspi_master_handle_t::bitsPerFrame |
| volatile uint32_t dspi_master_handle_t::command |
| volatile uint32_t dspi_master_handle_t::lastCommand |
| uint8_t dspi_master_handle_t::fifoSize |
| volatile bool dspi_master_handle_t::isPcsActiveAfterTransfer |
| volatile bool dspi_master_handle_t::isThereExtraByte |
| uint8_t* volatile dspi_master_handle_t::txData |
| uint8_t* volatile dspi_master_handle_t::rxData |
| volatile size_t dspi_master_handle_t::remainingSendByteCount |
| volatile size_t dspi_master_handle_t::remainingReceiveByteCount |
| volatile uint8_t dspi_master_handle_t::state |
| dspi_master_transfer_callback_t dspi_master_handle_t::callback |
| void* dspi_master_handle_t::userData |
| struct _dspi_slave_handle |
Forward declaration of the _dspi_slave_handle typedefs.
The slave handle.
Data Fields | |
| uint32_t | bitsPerFrame |
| The desired number of bits per frame. More... | |
| volatile bool | isThereExtraByte |
| Indicates whether there are extra bytes. More... | |
| uint8_t *volatile | txData |
| Send buffer. More... | |
| uint8_t *volatile | rxData |
| Receive buffer. More... | |
| volatile size_t | remainingSendByteCount |
| A number of bytes remaining to send. More... | |
| volatile size_t | remainingReceiveByteCount |
| A number of bytes remaining to receive. More... | |
| size_t | totalByteCount |
| A number of transfer bytes. | |
| volatile uint8_t | state |
| DSPI transfer state. More... | |
| volatile uint32_t | errorCount |
| Error count for slave transfer. More... | |
| dspi_slave_transfer_callback_t | callback |
| Completion callback. More... | |
| void * | userData |
| Callback user data. More... | |
| uint32_t dspi_slave_handle_t::bitsPerFrame |
| volatile bool dspi_slave_handle_t::isThereExtraByte |
| uint8_t* volatile dspi_slave_handle_t::txData |
| uint8_t* volatile dspi_slave_handle_t::rxData |
| volatile size_t dspi_slave_handle_t::remainingSendByteCount |
| volatile size_t dspi_slave_handle_t::remainingReceiveByteCount |
| volatile uint8_t dspi_slave_handle_t::state |
| volatile uint32_t dspi_slave_handle_t::errorCount |
| dspi_slave_transfer_callback_t dspi_slave_handle_t::callback |
| void* dspi_slave_handle_t::userData |
| #define FSL_DSPI_DRIVER_VERSION (MAKE_VERSION(2, 2, 4)) |
| #define DSPI_DUMMY_DATA (0x00U) |
Dummy data used for Tx if there is no txData.
| #define DSPI_MASTER_CTAR_SHIFT (0U) |
| #define DSPI_MASTER_CTAR_MASK (0x0FU) |
| #define DSPI_MASTER_PCS_SHIFT (4U) |
| #define DSPI_MASTER_PCS_MASK (0xF0U) |
| #define DSPI_SLAVE_CTAR_SHIFT (0U) |
| #define DSPI_SLAVE_CTAR_MASK (0x07U) |
| typedef void(* dspi_master_transfer_callback_t)(SPI_Type *base, dspi_master_handle_t *handle, status_t status, void *userData) |
| base | DSPI peripheral address. |
| handle | Pointer to the handle for the DSPI master. |
| status | Success or error code describing whether the transfer completed. |
| userData | Arbitrary pointer-dataSized value passed from the application. |
| typedef void(* dspi_slave_transfer_callback_t)(SPI_Type *base, dspi_slave_handle_t *handle, status_t status, void *userData) |
| base | DSPI peripheral address. |
| handle | Pointer to the handle for the DSPI slave. |
| status | Success or error code describing whether the transfer completed. |
| userData | Arbitrary pointer-dataSized value passed from the application. |
| anonymous enum |
| enum _dspi_flags |
| enum _dspi_dma_enable |
| enum dspi_which_pcs_t |
| enum _dspi_pcs_polarity |
| enum dspi_clock_phase_t |
| enum dspi_delay_type_t |
| enum _dspi_transfer_state |
| void DSPI_MasterInit | ( | SPI_Type * | base, |
| const dspi_master_config_t * | masterConfig, | ||
| uint32_t | srcClock_Hz | ||
| ) |
This function initializes the DSPI master configuration. This is an example use case.
| base | DSPI peripheral address. |
| masterConfig | Pointer to the structure dspi_master_config_t. |
| srcClock_Hz | Module source input clock in Hertz. |
| void DSPI_MasterGetDefaultConfig | ( | dspi_master_config_t * | masterConfig | ) |
The purpose of this API is to get the configuration structure initialized for the DSPI_MasterInit(). Users may use the initialized structure unchanged in the DSPI_MasterInit() or modify the structure before calling the DSPI_MasterInit(). Example:
| masterConfig | pointer to dspi_master_config_t structure |
| void DSPI_SlaveInit | ( | SPI_Type * | base, |
| const dspi_slave_config_t * | slaveConfig | ||
| ) |
This function initializes the DSPI slave configuration. This is an example use case.
| base | DSPI peripheral address. |
| slaveConfig | Pointer to the structure dspi_master_config_t. |
| void DSPI_SlaveGetDefaultConfig | ( | dspi_slave_config_t * | slaveConfig | ) |
The purpose of this API is to get the configuration structure initialized for the DSPI_SlaveInit(). Users may use the initialized structure unchanged in the DSPI_SlaveInit() or modify the structure before calling the DSPI_SlaveInit(). This is an example.
| slaveConfig | Pointer to the dspi_slave_config_t structure. |
| void DSPI_Deinit | ( | SPI_Type * | base | ) |
Call this API to disable the DSPI clock.
| base | DSPI peripheral address. |
|
inlinestatic |
| base | DSPI peripheral address. |
| enable | Pass true to enable module, false to disable module. |
|
inlinestatic |
| base | DSPI peripheral address. |
|
inlinestatic |
This function clears the desired status bit by using a write-1-to-clear. The user passes in the base and the desired status bit to clear. The list of status bits is defined in the dspi_status_and_interrupt_request_t. The function uses these bit positions in its algorithm to clear the desired flag state. This is an example.
| base | DSPI peripheral address. |
| statusFlags | The status flag used from the type dspi_flags. |
< The status flags are cleared by writing 1 (w1c).
| void DSPI_EnableInterrupts | ( | SPI_Type * | base, |
| uint32_t | mask | ||
| ) |
This function configures various interrupt masks of the DSPI. The parameters are a base and an interrupt mask.
| base | DSPI peripheral address. |
| mask | The interrupt mask; use the enum _dspi_interrupt_enable. |
|
inlinestatic |
| base | DSPI peripheral address. |
| mask | The interrupt mask; use the enum _dspi_interrupt_enable. |
|
inlinestatic |
This function configures the Rx and Tx DMA mask of the DSPI. The parameters are a base and a DMA mask.
| base | DSPI peripheral address. |
| mask | The interrupt mask; use the enum _dspi_dma_enable. |
|
inlinestatic |
This function configures the Rx and Tx DMA mask of the DSPI. The parameters are a base and a DMA mask.
| base | DSPI peripheral address. |
| mask | The interrupt mask; use the enum _dspi_dma_enable. |
|
inlinestatic |
This function gets the DSPI master PUSHR data register address because this value is needed for the DMA operation.
| base | DSPI peripheral address. |
|
inlinestatic |
This function gets the DSPI slave PUSHR data register address as this value is needed for the DMA operation.
| base | DSPI peripheral address. |
|
inlinestatic |
This function gets the DSPI POPR data register address as this value is needed for the DMA operation.
| base | DSPI peripheral address. |
| uint32_t DSPI_GetInstance | ( | SPI_Type * | base | ) |
| base | DSPI peripheral base address. |
|
inlinestatic |
| base | DSPI peripheral address. |
| mode | Mode setting (master or slave) of type dspi_master_slave_mode_t. |
|
inlinestatic |
| base | DSPI peripheral address. |
|
inlinestatic |
This function sets the module to start data transfer in either master or slave mode.
| base | DSPI peripheral address. |
|
inlinestatic |
This function stops data transfers in either master or slave modes.
| base | DSPI peripheral address. |
|
inlinestatic |
This function allows the caller to disable/enable the Tx and Rx FIFOs independently.
| base | DSPI peripheral address. |
| enableTxFifo | Disables (false) the TX FIFO; Otherwise, enables (true) the TX FIFO |
| enableRxFifo | Disables (false) the RX FIFO; Otherwise, enables (true) the RX FIFO |
|
inlinestatic |
| base | DSPI peripheral address. |
| flushTxFifo | Flushes (true) the Tx FIFO; Otherwise, does not flush (false) the Tx FIFO |
| flushRxFifo | Flushes (true) the Rx FIFO; Otherwise, does not flush (false) the Rx FIFO |
|
inlinestatic |
For example, PCS0 and PCS1 are set to active low and other PCS is set to active high. Note that the number of PCSs is specific to the device.
| base | DSPI peripheral address. |
| mask | The PCS polarity mask; use the enum _dspi_pcs_polarity. |
| uint32_t DSPI_MasterSetBaudRate | ( | SPI_Type * | base, |
| dspi_ctar_selection_t | whichCtar, | ||
| uint32_t | baudRate_Bps, | ||
| uint32_t | srcClock_Hz | ||
| ) |
This function takes in the desired baudRate_Bps (baud rate) and calculates the nearest possible baud rate without exceeding the desired baud rate, and returns the calculated baud rate in bits-per-second. It requires that the caller also provide the frequency of the module source clock (in Hertz).
| base | DSPI peripheral address. |
| whichCtar | The desired Clock and Transfer Attributes Register (CTAR) of the type dspi_ctar_selection_t |
| baudRate_Bps | The desired baud rate in bits per second |
| srcClock_Hz | Module source input clock in Hertz |
| void DSPI_MasterSetDelayScaler | ( | SPI_Type * | base, |
| dspi_ctar_selection_t | whichCtar, | ||
| uint32_t | prescaler, | ||
| uint32_t | scaler, | ||
| dspi_delay_type_t | whichDelay | ||
| ) |
This function configures the PCS to SCK delay pre-scalar (PcsSCK) and scalar (CSSCK), after SCK delay pre-scalar (PASC) and scalar (ASC), and the delay after transfer pre-scalar (PDT) and scalar (DT).
These delay names are available in the type dspi_delay_type_t.
The user passes the delay to the configuration along with the prescaler and scaler value. This allows the user to directly set the prescaler/scaler values if pre-calculated or to manually increment either value.
| base | DSPI peripheral address. |
| whichCtar | The desired Clock and Transfer Attributes Register (CTAR) of type dspi_ctar_selection_t. |
| prescaler | The prescaler delay value (can be an integer 0, 1, 2, or 3). |
| scaler | The scaler delay value (can be any integer between 0 to 15). |
| whichDelay | The desired delay to configure; must be of type dspi_delay_type_t |
| uint32_t DSPI_MasterSetDelayTimes | ( | SPI_Type * | base, |
| dspi_ctar_selection_t | whichCtar, | ||
| dspi_delay_type_t | whichDelay, | ||
| uint32_t | srcClock_Hz, | ||
| uint32_t | delayTimeInNanoSec | ||
| ) |
This function calculates the values for the following. PCS to SCK delay pre-scalar (PCSSCK) and scalar (CSSCK), or After SCK delay pre-scalar (PASC) and scalar (ASC), or Delay after transfer pre-scalar (PDT) and scalar (DT).
These delay names are available in the type dspi_delay_type_t.
The user passes which delay to configure along with the desired delay value in nanoseconds. The function calculates the values needed for the prescaler and scaler. Note that returning the calculated delay as an exact delay match may not be possible. In this case, the closest match is calculated without going below the desired delay value input. It is possible to input a very large delay value that exceeds the capability of the part, in which case the maximum supported delay is returned. The higher-level peripheral driver alerts the user of an out of range delay input.
| base | DSPI peripheral address. |
| whichCtar | The desired Clock and Transfer Attributes Register (CTAR) of type dspi_ctar_selection_t. |
| whichDelay | The desired delay to configure, must be of type dspi_delay_type_t |
| srcClock_Hz | Module source input clock in Hertz |
| delayTimeInNanoSec | The desired delay value in nanoseconds. |
|
inlinestatic |
In master mode, the 16-bit data is appended to the 16-bit command info. The command portion provides characteristics of the data, such as the optional continuous chip select operation between transfers, the desired Clock and Transfer Attributes register to use for the associated SPI frame, the desired PCS signal to use for the data transfer, whether the current transfer is the last in the queue, and whether to clear the transfer count (normally needed when sending the first frame of a data packet). This is an example.
| base | DSPI peripheral address. |
| command | Pointer to the command structure. |
| data | The data word to be sent. |
| void DSPI_GetDefaultDataCommandConfig | ( | dspi_command_data_config_t * | command | ) |
The purpose of this API is to get the configuration structure initialized for use in the DSPI_MasterWrite_xx(). Users may use the initialized structure unchanged in the DSPI_MasterWrite_xx() or modify the structure before calling the DSPI_MasterWrite_xx(). This is an example.
| command | Pointer to the dspi_command_data_config_t structure. |
| void DSPI_MasterWriteDataBlocking | ( | SPI_Type * | base, |
| dspi_command_data_config_t * | command, | ||
| uint16_t | data | ||
| ) |
In master mode, the 16-bit data is appended to the 16-bit command info. The command portion provides characteristics of the data, such as the optional continuous chip select operation between transfers, the desired Clock and Transfer Attributes register to use for the associated SPI frame, the desired PCS signal to use for the data transfer, whether the current transfer is the last in the queue, and whether to clear the transfer count (normally needed when sending the first frame of a data packet). This is an example.
| base | DSPI peripheral address. |
| command | Pointer to the command structure. |
| data | The data word to be sent. |
|
inlinestatic |
This function allows the caller to pass in the data command structure and returns the command word formatted according to the DSPI PUSHR register bit field placement. The user can then "OR" the returned command word with the desired data to send and use the function DSPI_HAL_WriteCommandDataMastermode or DSPI_HAL_WriteCommandDataMastermodeBlocking to write the entire 32-bit command data word to the PUSHR. This helps improve performance in cases where the command structure is constant. For example, the user calls this function before starting a transfer to generate the command word. When they are ready to transmit the data, they OR this formatted command word with the desired data to transmit. This process increases transmit performance when compared to calling send functions, such as DSPI_HAL_WriteDataMastermode, which format the command word each time a data word is to be sent.
| command | Pointer to the command structure. |
| void DSPI_MasterWriteCommandDataBlocking | ( | SPI_Type * | base, |
| uint32_t | data | ||
| ) |
In this function, the user must append the 16-bit data to the 16-bit command information and then provide the total 32-bit word as the data to send. The command portion provides characteristics of the data, such as the optional continuous chip select operation between transfers, the desired Clock and Transfer Attributes register to use for the associated SPI frame, the desired PCS signal to use for the data transfer, whether the current transfer is the last in the queue, and whether to clear the transfer count (normally needed when sending the first frame of a data packet). The user is responsible for appending this command with the data to send. This is an example:
For a blocking polling transfer, see methods below.
| Option 1 |
|---|
| uint32_t command_to_send = DSPI_MasterGetFormattedCommand(&command); |
| uint32_t data0 = command_to_send | data_need_to_send_0; |
| uint32_t data1 = command_to_send | data_need_to_send_1; |
| uint32_t data2 = command_to_send | data_need_to_send_2; |
| DSPI_MasterWriteCommandDataBlocking(base,data0); |
| DSPI_MasterWriteCommandDataBlocking(base,data1); |
| DSPI_MasterWriteCommandDataBlocking(base,data2); |
| Option 2 |
|---|
| DSPI_MasterWriteDataBlocking(base,&command,data_need_to_send_0); |
| DSPI_MasterWriteDataBlocking(base,&command,data_need_to_send_1); |
| DSPI_MasterWriteDataBlocking(base,&command,data_need_to_send_2); |
| base | DSPI peripheral address. |
| data | The data word (command and data combined) to be sent. |
|
inlinestatic |
In slave mode, up to 16-bit words may be written.
| base | DSPI peripheral address. |
| data | The data to send. |
| void DSPI_SlaveWriteDataBlocking | ( | SPI_Type * | base, |
| uint32_t | data | ||
| ) |
In slave mode, up to 16-bit words may be written. The function first clears the transmit complete flag, writes data into data register, and finally waits until the data is transmitted.
| base | DSPI peripheral address. |
| data | The data to send. |
|
inlinestatic |
| base | DSPI peripheral address. |
| void DSPI_SetDummyData | ( | SPI_Type * | base, |
| uint8_t | dummyData | ||
| ) |
| base | DSPI peripheral address. |
| dummyData | Data to be transferred when tx buffer is NULL. |
| void DSPI_MasterTransferCreateHandle | ( | SPI_Type * | base, |
| dspi_master_handle_t * | handle, | ||
| dspi_master_transfer_callback_t | callback, | ||
| void * | userData | ||
| ) |
This function initializes the DSPI handle, which can be used for other DSPI transactional APIs. Usually, for a specified DSPI instance, call this API once to get the initialized handle.
| base | DSPI peripheral base address. |
| handle | DSPI handle pointer to _dspi_master_handle. |
| callback | DSPI callback. |
| userData | Callback function parameter. |
| status_t DSPI_MasterTransferBlocking | ( | SPI_Type * | base, |
| dspi_transfer_t * | transfer | ||
| ) |
This function transfers data using polling. This is a blocking function, which does not return until all transfers have been completed.
| base | DSPI peripheral base address. |
| transfer | Pointer to the dspi_transfer_t structure. |
| status_t DSPI_MasterTransferNonBlocking | ( | SPI_Type * | base, |
| dspi_master_handle_t * | handle, | ||
| dspi_transfer_t * | transfer | ||
| ) |
This function transfers data using interrupts. This is a non-blocking function, which returns right away. When all data is transferred, the callback function is called.
| base | DSPI peripheral base address. |
| handle | Pointer to the _dspi_master_handle structure which stores the transfer state. |
| transfer | Pointer to the dspi_transfer_t structure. |
| status_t DSPI_MasterHalfDuplexTransferBlocking | ( | SPI_Type * | base, |
| dspi_half_duplex_transfer_t * | xfer | ||
| ) |
This function will do a half-duplex transfer for DSPI master, This is a blocking function, which does not retuen until all transfer have been completed. And data transfer will be half-duplex, users can set transmit first or receive first.
| base | DSPI base pointer |
| xfer | pointer to dspi_half_duplex_transfer_t structure |
| status_t DSPI_MasterHalfDuplexTransferNonBlocking | ( | SPI_Type * | base, |
| dspi_master_handle_t * | handle, | ||
| dspi_half_duplex_transfer_t * | xfer | ||
| ) |
This function transfers data using interrupts, the transfer mechanism is half-duplex. This is a non-blocking function, which returns right away. When all data is transferred, the callback function is called.
| base | DSPI peripheral base address. |
| handle | pointer to _dspi_master_handle structure which stores the transfer state |
| xfer | pointer to dspi_half_duplex_transfer_t structure |
| status_t DSPI_MasterTransferGetCount | ( | SPI_Type * | base, |
| dspi_master_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
This function gets the master transfer count.
| base | DSPI peripheral base address. |
| handle | Pointer to the _dspi_master_handle structure which stores the transfer state. |
| count | The number of bytes transferred by using the non-blocking transaction. |
| void DSPI_MasterTransferAbort | ( | SPI_Type * | base, |
| dspi_master_handle_t * | handle | ||
| ) |
This function aborts a transfer using an interrupt.
| base | DSPI peripheral base address. |
| handle | Pointer to the _dspi_master_handle structure which stores the transfer state. |
| void DSPI_MasterTransferHandleIRQ | ( | SPI_Type * | base, |
| dspi_master_handle_t * | handle | ||
| ) |
This function processes the DSPI transmit and receive IRQ.
| base | DSPI peripheral base address. |
| handle | Pointer to the _dspi_master_handle structure which stores the transfer state. |
| void DSPI_SlaveTransferCreateHandle | ( | SPI_Type * | base, |
| dspi_slave_handle_t * | handle, | ||
| dspi_slave_transfer_callback_t | callback, | ||
| void * | userData | ||
| ) |
This function initializes the DSPI handle, which can be used for other DSPI transactional APIs. Usually, for a specified DSPI instance, call this API once to get the initialized handle.
| handle | DSPI handle pointer to the _dspi_slave_handle. |
| base | DSPI peripheral base address. |
| callback | DSPI callback. |
| userData | Callback function parameter. |
| status_t DSPI_SlaveTransferNonBlocking | ( | SPI_Type * | base, |
| dspi_slave_handle_t * | handle, | ||
| dspi_transfer_t * | transfer | ||
| ) |
This function transfers data using an interrupt. This is a non-blocking function, which returns right away. When all data is transferred, the callback function is called.
| base | DSPI peripheral base address. |
| handle | Pointer to the _dspi_slave_handle structure which stores the transfer state. |
| transfer | Pointer to the dspi_transfer_t structure. |
| status_t DSPI_SlaveTransferGetCount | ( | SPI_Type * | base, |
| dspi_slave_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
This function gets the slave transfer count.
| base | DSPI peripheral base address. |
| handle | Pointer to the _dspi_master_handle structure which stores the transfer state. |
| count | The number of bytes transferred by using the non-blocking transaction. |
| void DSPI_SlaveTransferAbort | ( | SPI_Type * | base, |
| dspi_slave_handle_t * | handle | ||
| ) |
This function aborts a transfer using an interrupt.
| base | DSPI peripheral base address. |
| handle | Pointer to the _dspi_slave_handle structure which stores the transfer state. |
| void DSPI_SlaveTransferHandleIRQ | ( | SPI_Type * | base, |
| dspi_slave_handle_t * | handle | ||
| ) |
This function processes the DSPI transmit and receive IRQ.
| base | DSPI peripheral base address. |
| handle | Pointer to the _dspi_slave_handle structure which stores the transfer state. |
| uint8_t DSPI_GetDummyDataInstance | ( | SPI_Type * | base | ) |
The purpose of this API is to avoid MISRA rule8.5 : Multiple declarations of externally-linked object or function g_dspiDummyData.
param base DSPI peripheral base address.
| volatile uint8_t g_dspiDummyData[] |