MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
RCM: Reset Control Module Driver

Overview

The MCUXpresso SDK provides a peripheral driver for the Reset Control Module (RCM) module of MCUXpresso SDK devices.

Data Structures

struct  rcm_reset_pin_filter_config_t
 Reset pin filter configuration. More...
 

Enumerations

enum  rcm_reset_source_t {
  kRCM_SourceWakeup = RCM_SRS0_WAKEUP_MASK,
  kRCM_SourceLvd = RCM_SRS0_LVD_MASK,
  kRCM_SourceLoc = RCM_SRS0_LOC_MASK,
  kRCM_SourceLol = RCM_SRS0_LOL_MASK,
  kRCM_SourceWdog = RCM_SRS0_WDOG_MASK,
  kRCM_SourcePin = RCM_SRS0_PIN_MASK,
  kRCM_SourcePor = RCM_SRS0_POR_MASK,
  kRCM_SourceJtag = RCM_SRS1_JTAG_MASK << 8U,
  kRCM_SourceLockup = RCM_SRS1_LOCKUP_MASK << 8U,
  kRCM_SourceSw = RCM_SRS1_SW_MASK << 8U,
  kRCM_SourceMdmap = RCM_SRS1_MDM_AP_MASK << 8U,
  kRCM_SourceEzpt = RCM_SRS1_EZPT_MASK << 8U,
  kRCM_SourceSackerr = RCM_SRS1_SACKERR_MASK << 8U
}
 System Reset Source Name definitions. More...
 
enum  rcm_run_wait_filter_mode_t {
  kRCM_FilterDisable = 0U,
  kRCM_FilterBusClock = 1U,
  kRCM_FilterLpoClock = 2U
}
 Reset pin filter select in Run and Wait modes. More...
 

Driver version

#define FSL_RCM_DRIVER_VERSION   (MAKE_VERSION(2, 0, 4))
 RCM driver version 2.0.4. More...
 

Reset Control Module APIs

static uint32_t RCM_GetPreviousResetSources (RCM_Type *base)
 Gets the reset source status which caused a previous reset. More...
 
static uint32_t RCM_GetStickyResetSources (RCM_Type *base)
 Gets the sticky reset source status. More...
 
static void RCM_ClearStickyResetSources (RCM_Type *base, uint32_t sourceMasks)
 Clears the sticky reset source status. More...
 
void RCM_ConfigureResetPinFilter (RCM_Type *base, const rcm_reset_pin_filter_config_t *config)
 Configures the reset pin filter. More...
 
static bool RCM_GetEasyPortModePinStatus (RCM_Type *base)
 Gets the EZP_MS_B pin assert status. More...
 

Data Structure Documentation

struct rcm_reset_pin_filter_config_t

Data Fields

bool enableFilterInStop
 Reset pin filter select in stop mode. More...
 
rcm_run_wait_filter_mode_t filterInRunWait
 Reset pin filter in run/wait mode. More...
 
uint8_t busClockFilterCount
 Reset pin bus clock filter width. More...
 

Field Documentation

bool rcm_reset_pin_filter_config_t::enableFilterInStop
rcm_run_wait_filter_mode_t rcm_reset_pin_filter_config_t::filterInRunWait
uint8_t rcm_reset_pin_filter_config_t::busClockFilterCount

Macro Definition Documentation

#define FSL_RCM_DRIVER_VERSION   (MAKE_VERSION(2, 0, 4))

Enumeration Type Documentation

Enumerator
kRCM_SourceWakeup 

Low-leakage wakeup reset.

kRCM_SourceLvd 

Low-voltage detect reset.

kRCM_SourceLoc 

Loss of clock reset.

kRCM_SourceLol 

Loss of lock reset.

kRCM_SourceWdog 

Watchdog reset.

kRCM_SourcePin 

External pin reset.

kRCM_SourcePor 

Power on reset.

kRCM_SourceJtag 

JTAG generated reset.

kRCM_SourceLockup 

Core lock up reset.

kRCM_SourceSw 

Software reset.

kRCM_SourceMdmap 

MDM-AP system reset.

kRCM_SourceEzpt 

EzPort reset.

kRCM_SourceSackerr 

Parameter could get all reset flags.

Enumerator
kRCM_FilterDisable 

All filtering disabled.

kRCM_FilterBusClock 

Bus clock filter enabled.

kRCM_FilterLpoClock 

LPO clock filter enabled.

Function Documentation

static uint32_t RCM_GetPreviousResetSources ( RCM_Type *  base)
inlinestatic

This function gets the current reset source status. Use source masks defined in the rcm_reset_source_t to get the desired source status.

This is an example.

* uint32_t resetStatus;
*
* To get all reset source statuses.
* resetStatus = RCM_GetPreviousResetSources(RCM) & kRCM_SourceAll;
*
* To test whether the MCU is reset using Watchdog.
*
* To test multiple reset sources.
*
Parameters
baseRCM peripheral base address.
Returns
All reset source status bit map.
static uint32_t RCM_GetStickyResetSources ( RCM_Type *  base)
inlinestatic

This function gets the current reset source status that has not been cleared by software for a specific source.

This is an example.

* uint32_t resetStatus;
*
* To get all reset source statuses.
* resetStatus = RCM_GetStickyResetSources(RCM) & kRCM_SourceAll;
*
* To test whether the MCU is reset using Watchdog.
*
* To test multiple reset sources.
*
Parameters
baseRCM peripheral base address.
Returns
All reset source status bit map.
static void RCM_ClearStickyResetSources ( RCM_Type *  base,
uint32_t  sourceMasks 
)
inlinestatic

This function clears the sticky system reset flags indicated by source masks.

This is an example.

* Clears multiple reset sources.
*
Parameters
baseRCM peripheral base address.
sourceMasksreset source status bit map
void RCM_ConfigureResetPinFilter ( RCM_Type *  base,
const rcm_reset_pin_filter_config_t *  config 
)

This function sets the reset pin filter including the filter source, filter width, and so on.

Parameters
baseRCM peripheral base address.
configPointer to the configuration structure.
static bool RCM_GetEasyPortModePinStatus ( RCM_Type *  base)
inlinestatic

This function gets the easy port mode status (EZP_MS_B) pin assert status.

Parameters
baseRCM peripheral base address.
Returns
status true - asserted, false - reasserted