![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | sdmmc_osa_event_t |
| sdmmc osa event More... | |
Macros | |
| #define | SDMMC_OSA_EVENT_TRANSFER_CMD_SUCCESS (1UL << 0U) |
| transfer event | |
| #define | SDMMC_OSA_EVENT_CARD_INSERTED (1UL << 8U) |
| card detect event, start from index 8 | |
| #define | SDMMC_OSA_POLLING_EVENT_BY_SEMPHORE 1 |
| enable semphore by default | |
sdmmc osa Function | |
| void | SDMMC_OSAInit (void) |
| Initialize OSA. | |
| status_t | SDMMC_OSAEventCreate (void *eventHandle) |
| OSA Create event. More... | |
| status_t | SDMMC_OSAEventWait (void *eventHandle, uint32_t eventType, uint32_t timeoutMilliseconds, uint32_t *event) |
| Wait event. More... | |
| status_t | SDMMC_OSAEventSet (void *eventHandle, uint32_t eventType) |
| set event. More... | |
| status_t | SDMMC_OSAEventGet (void *eventHandle, uint32_t eventType, uint32_t *flag) |
| Get event flag. More... | |
| status_t | SDMMC_OSAEventClear (void *eventHandle, uint32_t eventType) |
| clear event flag. More... | |
| status_t | SDMMC_OSAEventDestroy (void *eventHandle) |
| Delete event. More... | |
| void | SDMMC_OSADelay (uint32_t milliseconds) |
| sdmmc delay. More... | |
| struct sdmmc_osa_event_t |
| status_t SDMMC_OSAEventCreate | ( | void * | eventHandle | ) |
| eventHandle | event handle. |
| kStatus_Fail | or kStatus_Success. |
| status_t SDMMC_OSAEventWait | ( | void * | eventHandle, |
| uint32_t | eventType, | ||
| uint32_t | timeoutMilliseconds, | ||
| uint32_t * | event | ||
| ) |
| eventHandle | The event type |
| eventType | Timeout time in milliseconds. |
| timeoutMilliseconds | timeout value in ms. |
| event | event flags. |
| kStatus_Fail | or kStatus_Success. |
| status_t SDMMC_OSAEventSet | ( | void * | eventHandle, |
| uint32_t | eventType | ||
| ) |
| eventHandle | event handle. |
| eventType | The event type |
| kStatus_Fail | or kStatus_Success. |
| status_t SDMMC_OSAEventGet | ( | void * | eventHandle, |
| uint32_t | eventType, | ||
| uint32_t * | flag | ||
| ) |
| eventHandle | event handle. |
| eventType | event type. |
| flag | pointer to store event value. |
| kStatus_Fail | or kStatus_Success. |
| status_t SDMMC_OSAEventClear | ( | void * | eventHandle, |
| uint32_t | eventType | ||
| ) |
| eventHandle | event handle. |
| eventType | The event type |
| kStatus_Fail | or kStatus_Success. |
| status_t SDMMC_OSAEventDestroy | ( | void * | eventHandle | ) |
| eventHandle | The event handle. |
| void SDMMC_OSADelay | ( | uint32_t | milliseconds | ) |
| milliseconds | time to delay |