![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | tsi_calibration_data_t |
| TSI calibration data storage. More... | |
| struct | tsi_common_config_t |
| TSI common configuration structure. More... | |
| struct | tsi_selfCap_config_t |
| TSI configuration structure for self-cap mode. More... | |
| struct | tsi_mutualCap_config_t |
| TSI configuration structure for mutual-cap mode. More... | |
Macros | |
| #define | FSL_TSI_DRIVER_VERSION (MAKE_VERSION(2, 1, 2)) |
| TSI driver version. | |
| #define | ALL_FLAGS_MASK (TSI_GENCS_EOSF_MASK | TSI_GENCS_OUTRGF_MASK) |
| TSI status flags macro collection. | |
Functions | |
| void | TSI_InitSelfCapMode (TSI_Type *base, const tsi_selfCap_config_t *config) |
| Initialize hardware to Self-cap mode. More... | |
| void | TSI_InitMutualCapMode (TSI_Type *base, const tsi_mutualCap_config_t *config) |
| Initialize hardware to Mutual-cap mode. More... | |
| void | TSI_Deinit (TSI_Type *base) |
| De-initialize hardware. More... | |
| void | TSI_GetSelfCapModeDefaultConfig (tsi_selfCap_config_t *userConfig) |
| Get TSI self-cap mode user configure structure. More... | |
| void | TSI_GetMutualCapModeDefaultConfig (tsi_mutualCap_config_t *userConfig) |
| Get TSI mutual-cap mode default user configure structure. More... | |
| void | TSI_SelfCapCalibrate (TSI_Type *base, tsi_calibration_data_t *calBuff) |
| Hardware base counter value for calibration. More... | |
| void | TSI_EnableInterrupts (TSI_Type *base, uint32_t mask) |
| Enables TSI interrupt requests. More... | |
| void | TSI_DisableInterrupts (TSI_Type *base, uint32_t mask) |
| Disables TSI interrupt requests. More... | |
| static uint32_t | TSI_GetStatusFlags (TSI_Type *base) |
| Get interrupt flag. More... | |
| void | TSI_ClearStatusFlags (TSI_Type *base, uint32_t mask) |
| Clear interrupt flag. More... | |
| static uint32_t | TSI_GetScanTriggerMode (TSI_Type *base) |
| Get TSI scan trigger mode. More... | |
| static bool | TSI_IsScanInProgress (TSI_Type *base) |
| Get scan in progress flag. More... | |
| static void | TSI_EnableModule (TSI_Type *base, bool enable) |
| Enables the TSI Module or not. More... | |
| static void | TSI_EnableLowPower (TSI_Type *base, bool enable) |
| Sets the TSI low power STOP mode enable or not. More... | |
| static void | TSI_EnableHardwareTriggerScan (TSI_Type *base, bool enable) |
| Enable the hardware trigger scan or not. More... | |
| static void | TSI_StartSoftwareTrigger (TSI_Type *base) |
| Start one sotware trigger measurement (trigger a new measurement). More... | |
| static void | TSI_SetSelfCapMeasuredChannel (TSI_Type *base, uint8_t channel) |
| Set the measured channel number for self-cap mode. More... | |
| static uint8_t | TSI_GetSelfCapMeasuredChannel (TSI_Type *base) |
| Get the current measured channel number, in self-cap mode. More... | |
| static void | TSI_EnableDmaTransfer (TSI_Type *base, bool enable) |
| Enable DMA transfer or not. More... | |
| static void | TSI_EnableEndOfScanDmaTransferOnly (TSI_Type *base, bool enable) |
| Decide whether to enable End of Scan DMA transfer request only. More... | |
| static uint16_t | TSI_GetCounter (TSI_Type *base) |
| Gets the conversion counter value. More... | |
| static void | TSI_SetLowThreshold (TSI_Type *base, uint16_t low_threshold) |
| Set the TSI wake-up channel low threshold. More... | |
| static void | TSI_SetHighThreshold (TSI_Type *base, uint16_t high_threshold) |
| Set the TSI wake-up channel high threshold. More... | |
| static void | TSI_SetMainClock (TSI_Type *base, tsi_main_clock_selection_t mainClock) |
| Set the main clock of the TSI module. More... | |
| static void | TSI_SetSensingMode (TSI_Type *base, tsi_sensing_mode_selection_t mode) |
| Set the sensing mode of the TSI module. More... | |
| static tsi_sensing_mode_selection_t | TSI_GetSensingMode (TSI_Type *base) |
| Get the sensing mode of the TSI module. More... | |
| static void | TSI_SetDvolt (TSI_Type *base, tsi_dvolt_option_t dvolt) |
| Set the DVOLT settings. More... | |
| static void | TSI_EnableNoiseCancellation (TSI_Type *base, bool enableCancellation) |
| Enable self-cap mode noise cancellation function or not. More... | |
| static void | TSI_SetMutualCapTxChannel (TSI_Type *base, tsi_mutual_tx_channel_t txChannel) |
| Set the mutual-cap mode TX channel. More... | |
| static tsi_mutual_tx_channel_t | TSI_GetTxMutualCapMeasuredChannel (TSI_Type *base) |
| Get the current measured TX channel number, in mutual-cap mode. More... | |
| static void | TSI_SetMutualCapRxChannel (TSI_Type *base, tsi_mutual_rx_channel_t rxChannel) |
| Set the mutual-cap mode RX channel. More... | |
| static tsi_mutual_rx_channel_t | TSI_GetRxMutualCapMeasuredChannel (TSI_Type *base) |
| Get the current measured RX channel number, in mutual-cap mode. More... | |
| static void | TSI_SetSscMode (TSI_Type *base, tsi_ssc_mode_t mode) |
| Set the SSC clock mode of the TSI module. More... | |
| static void | TSI_SetSscPrescaler (TSI_Type *base, tsi_ssc_prescaler_t prescaler) |
| Set the SSC prescaler of the TSI module. More... | |
| struct tsi_calibration_data_t |
Data Fields | |
| uint16_t | calibratedData [FSL_FEATURE_TSI_CHANNEL_COUNT] |
| TSI calibration data storage buffer. | |
| struct tsi_common_config_t |
This structure contains the common settings for TSI self-cap or mutual-cap mode, configurations including the TSI module main clock, sensing mode, DVOLT options, SINC and SSC configurations.
Data Fields | |
| tsi_main_clock_selection_t | mainClock |
| Set main clock. More... | |
| tsi_sensing_mode_selection_t | mode |
| Choose sensing mode. More... | |
| tsi_dvolt_option_t | dvolt |
| DVOLT option value. More... | |
| tsi_sinc_cutoff_div_t | cutoff |
| Cutoff divider. More... | |
| tsi_sinc_filter_order_t | order |
| SINC filter order. More... | |
| tsi_sinc_decimation_value_t | decimation |
| SINC decimation value. More... | |
| tsi_ssc_charge_num_t | chargeNum |
| SSC High Width (t1), SSC output bit0's period setting. More... | |
| tsi_ssc_prbs_outsel_t | prbsOutsel |
| SSC High Random Width (t2), length of PRBS(Pseudo-RandomBinarySequence),SSC output bit2's period setting. More... | |
| tsi_ssc_nocharge_num_t | noChargeNum |
| SSC Low Width (t3), SSC output bit1's period setting. More... | |
| tsi_ssc_mode_t | ssc_mode |
| Clock mode selection (basic - from main clock by divider,advanced - using SSC(Switching Speed Clock) by three configurable intervals. More... | |
| tsi_ssc_prescaler_t | ssc_prescaler |
| Set clock divider for basic mode. More... | |
| tsi_main_clock_selection_t tsi_common_config_t::mainClock |
| tsi_sensing_mode_selection_t tsi_common_config_t::mode |
| tsi_dvolt_option_t tsi_common_config_t::dvolt |
| tsi_sinc_cutoff_div_t tsi_common_config_t::cutoff |
| tsi_sinc_filter_order_t tsi_common_config_t::order |
| tsi_sinc_decimation_value_t tsi_common_config_t::decimation |
| tsi_ssc_charge_num_t tsi_common_config_t::chargeNum |
| tsi_ssc_prbs_outsel_t tsi_common_config_t::prbsOutsel |
| tsi_ssc_nocharge_num_t tsi_common_config_t::noChargeNum |
| tsi_ssc_mode_t tsi_common_config_t::ssc_mode |
| tsi_ssc_prescaler_t tsi_common_config_t::ssc_prescaler |
| struct tsi_selfCap_config_t |
This structure contains the settings for the most common TSI self-cap configurations including the TSI module charge currents, sensitivity configuration and so on.
Data Fields | |
| tsi_common_config_t | commonConfig |
| Common settings. More... | |
| bool | enableSensitivity |
| Enable sensitivity boost of self-cap or not. More... | |
| bool | enableShield |
| Enable shield of self-cap mode or not. More... | |
| tsi_sensitivity_xdn_option_t | xdn |
| Sensitivity XDN option. More... | |
| tsi_sensitivity_ctrim_option_t | ctrim |
| Sensitivity CTRIM option. More... | |
| tsi_current_multiple_input_t | inputCurrent |
| Input current multiple. More... | |
| tsi_current_multiple_charge_t | chargeCurrent |
| Charge/Discharge current multiple. More... | |
| tsi_common_config_t tsi_selfCap_config_t::commonConfig |
| bool tsi_selfCap_config_t::enableSensitivity |
| bool tsi_selfCap_config_t::enableShield |
| tsi_sensitivity_xdn_option_t tsi_selfCap_config_t::xdn |
| tsi_sensitivity_ctrim_option_t tsi_selfCap_config_t::ctrim |
| tsi_current_multiple_input_t tsi_selfCap_config_t::inputCurrent |
| tsi_current_multiple_charge_t tsi_selfCap_config_t::chargeCurrent |
| struct tsi_mutualCap_config_t |
This structure contains the settings for the most common TSI mutual-cap configurations including the TSI module generator settings, sensitivity related current settings and so on.
Data Fields | |
| tsi_common_config_t | commonConfig |
| Common settings. More... | |
| tsi_mutual_pre_current_t | preCurrent |
| Vref generator current. More... | |
| tsi_mutual_pre_resistor_t | preResistor |
| Vref generator resistor. More... | |
| tsi_mutual_sense_resistor_t | senseResistor |
| I-sense generator resistor. More... | |
| tsi_mutual_sense_boost_current_t | boostCurrent |
| Sensitivity boost current setting. More... | |
| tsi_mutual_tx_drive_mode_t | txDriveMode |
| TX drive mode control setting. More... | |
| tsi_mutual_pmos_current_left_t | pmosLeftCurrent |
| Pmos current mirror on the left side. More... | |
| tsi_mutual_pmos_current_right_t | pmosRightCurrent |
| Pmos current mirror on the right side. More... | |
| bool | enableNmosMirror |
| Enable Nmos current mirror setting or not. More... | |
| tsi_mutual_nmos_current_t | nmosCurrent |
| Nmos current mirror setting. More... | |
| tsi_common_config_t tsi_mutualCap_config_t::commonConfig |
| tsi_mutual_pre_current_t tsi_mutualCap_config_t::preCurrent |
| tsi_mutual_pre_resistor_t tsi_mutualCap_config_t::preResistor |
| tsi_mutual_sense_resistor_t tsi_mutualCap_config_t::senseResistor |
| tsi_mutual_sense_boost_current_t tsi_mutualCap_config_t::boostCurrent |
| tsi_mutual_tx_drive_mode_t tsi_mutualCap_config_t::txDriveMode |
| tsi_mutual_pmos_current_left_t tsi_mutualCap_config_t::pmosLeftCurrent |
| tsi_mutual_pmos_current_right_t tsi_mutualCap_config_t::pmosRightCurrent |
| bool tsi_mutualCap_config_t::enableNmosMirror |
| tsi_mutual_nmos_current_t tsi_mutualCap_config_t::nmosCurrent |
These constants set the tsi main clock.
| enum tsi_dvolt_option_t |
These bits indicate the comparator vp, vm and dvolt voltage.
These constants define the tsi sensitivity ajustment in self-cap mode, when TSI_MODE[S_SEN] = 1.
These constants define the tsi sensitivity ajustment in self-cap mode, when TSI_MODE[S_SEN] = 1.
These constants set the tsi charge/discharge current multiple in self-cap mode.
These constants Choose the current used in vref generator.
These constants Choose the resistor used in pre-charge.
These constants Choose the resistor used in I-sense generator.
These constants Choose the TX channel used in mutual-cap mode.
These constants Choose the RX channel used in mutual-cap mode.
These constants set the sensitivity boost current.
These constants set the Pmos current mirror on the left side used in mutual-cap mode.
These constants set the Pmos current mirror on the right side used in mutual-cap mode.
These constants set the Nmos current mirror used in mutual-cap mode.
These bits set the SINC cutoff divider.
These bits set the SINC decimation value.
| enum tsi_ssc_charge_num_t |
These bits set the SSC output bit0's period setting.
These bits set the SSC output bit1's period setting.
These bits set the SSC PRBS length.
| enum tsi_status_flags_t |
| enum tsi_ssc_mode_t |
| enum tsi_ssc_prescaler_t |
These constants set select the divider ratio for the clock used for generating the SSC output bit.
| void TSI_InitSelfCapMode | ( | TSI_Type * | base, |
| const tsi_selfCap_config_t * | config | ||
| ) |
Initialize the peripheral to the targeted state specified by parameter config, such as sets sensitivity adjustment, current settings.
| base | TSI peripheral base address. |
| config | Pointer to TSI self-cap configuration structure. |
| void TSI_InitMutualCapMode | ( | TSI_Type * | base, |
| const tsi_mutualCap_config_t * | config | ||
| ) |
Initialize the peripheral to the targeted state specified by parameter config, such as sets Vref generator setting, sensitivity boost settings, Pmos/Nmos settings.
| base | TSI peripheral base address. |
| config | Pointer to TSI mutual-cap configuration structure. |
| void TSI_Deinit | ( | TSI_Type * | base | ) |
De-initialize the peripheral to default state.
| base | TSI peripheral base address. |
| void TSI_GetSelfCapModeDefaultConfig | ( | tsi_selfCap_config_t * | userConfig | ) |
This interface sets userConfig structure to a default value. The configuration structure only includes the settings for the whole TSI. The user configure is set to a value:
| userConfig | Pointer to TSI user configure structure. |
| void TSI_GetMutualCapModeDefaultConfig | ( | tsi_mutualCap_config_t * | userConfig | ) |
This interface sets userConfig structure to a default value. The configuration structure only includes the settings for the whole TSI. The user configure is set to a value:
| userConfig | Pointer to TSI user configure structure. |
| void TSI_SelfCapCalibrate | ( | TSI_Type * | base, |
| tsi_calibration_data_t * | calBuff | ||
| ) |
Calibrate the peripheral to fetch the initial counter value of the enabled channels. This API is mostly used at initial application setup, it shall be called after the TSI_Init API, then user can use the calibrated counter values to setup applications(such as to determine under which counter value we can confirm a touch event occurrs).
| base | TSI peripheral base address. |
| calBuff | Data buffer that store the calibrated counter value. |
| void TSI_EnableInterrupts | ( | TSI_Type * | base, |
| uint32_t | mask | ||
| ) |
| base | TSI peripheral base address. |
| mask | interrupt source The parameter can be combination of the following source if defined:
|
| void TSI_DisableInterrupts | ( | TSI_Type * | base, |
| uint32_t | mask | ||
| ) |
| base | TSI peripheral base address. |
| mask | interrupt source The parameter can be combination of the following source if defined:
|
|
inlinestatic |
This function get tsi interrupt flags.
| base | TSI peripheral base address. |
| void TSI_ClearStatusFlags | ( | TSI_Type * | base, |
| uint32_t | mask | ||
| ) |
This function clear tsi interrupt flag, automatically cleared flags can not be cleared by this function.
| base | TSI peripheral base address. |
| mask | The status flags to clear. |
|
inlinestatic |
| base | TSI peripheral base address. |
|
inlinestatic |
| base | TSI peripheral base address. |
|
inlinestatic |
| base | TSI peripheral base address. |
| enable | Choose whether to enable or disable module;
|
|
inlinestatic |
This enables TSI module function in low power modes.
| base | TSI peripheral base address. |
| enable | Choose to enable or disable STOP mode.
|
|
inlinestatic |
| base | TSI peripheral base address. |
| enable | Choose to enable hardware trigger or software trigger scan.
|
|
inlinestatic |
| base | TSI peripheral base address. |
|
inlinestatic |
| base | TSI peripheral base address. |
| channel | Channel number 0 ... 24. |
|
inlinestatic |
| base | TSI peripheral base address. |
|
inlinestatic |
| base | TSI peripheral base address. |
| enable | Choose to enable DMA transfer or not.
|
|
inlinestatic |
| base | TSI peripheral base address. |
| enable | Choose whether to enable End of Scan DMA transfer request only.
|
|
inlinestatic |
| base | TSI peripheral base address. |
|
inlinestatic |
| base | TSI peripheral base address. |
| low_threshold | Low counter threshold. |
|
inlinestatic |
| base | TSI peripheral base address. |
| high_threshold | High counter threshold. |
|
inlinestatic |
| base | TSI peripheral base address. |
| mainClock | clock option value. |
|
inlinestatic |
| base | TSI peripheral base address. |
| mode | Mode value. |
|
inlinestatic |
| base | TSI peripheral base address. |
|
inlinestatic |
| base | TSI peripheral base address. |
| dvolt | The voltage rails. |
|
inlinestatic |
| base | TSI peripheral base address. |
| enableCancellation | Choose whether to enable noise cancellation in self-cap mode
|
|
inlinestatic |
| base | TSI peripheral base address. |
| txChannel | Mutual-cap mode TX channel number |
|
inlinestatic |
| base | TSI peripheral base address; |
|
inlinestatic |
| base | TSI peripheral base address. |
| rxChannel | Mutual-cap mode RX channel number |
|
inlinestatic |
| base | TSI peripheral base address; |
|
inlinestatic |
| base | TSI peripheral base address. |
| mode | SSC mode option value. |
|
inlinestatic |
| base | TSI peripheral base address. |
| prescaler | SSC prescaler option value. |