![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the CI_PI module of MCUXpresso SDK devices.
The CI_PI module receives the camera input frame, so it should work together with ISI.
Functions | |
| void | CI_PI_Init (CI_PI_CSR_Type *base, const ci_pi_config_t *config) |
| Enables and configures the CI_PI peripheral module. More... | |
| void | CI_PI_Deinit (CI_PI_CSR_Type *base) |
| Disables the CI_PI peripheral module. More... | |
| void | CI_PI_GetDefaultConfig (ci_pi_config_t *config) |
| Get the default configuration to initialize CI_PI. More... | |
| static void | CI_PI_Reset (CI_PI_CSR_Type *base) |
| Resets the CI_PI peripheral module. More... | |
| void | CI_PI_Start (CI_PI_CSR_Type *base) |
| Starts the CI_PI peripheral module to output captured frame. More... | |
| void | CI_PI_Stop (CI_PI_CSR_Type *base) |
| Stops the CI_PI peripheral module. More... | |
| static uint32_t | CI_PI_GetStatus (CI_PI_CSR_Type *base) |
| Gets the CI_PI peripheral module status. More... | |
Driver version | |
| #define | FSL_CI_PI_DRIVER_VERSION (MAKE_VERSION(2, 0, 2)) |
| CI_PI driver version. More... | |
| #define FSL_CI_PI_DRIVER_VERSION (MAKE_VERSION(2, 0, 2)) |
| enum _ci_pi_flags |
| enum ci_pi_input_format_t |
| enum ci_pi_work_mode_t |
The CCIR656 interlace mode is not supported currently.
| void CI_PI_Init | ( | CI_PI_CSR_Type * | base, |
| const ci_pi_config_t * | config | ||
| ) |
| base | CI_PI peripheral address. |
| config | CI_PI module configuration structure. |
| void CI_PI_Deinit | ( | CI_PI_CSR_Type * | base | ) |
| base | CI_PI peripheral address. |
| void CI_PI_GetDefaultConfig | ( | ci_pi_config_t * | config | ) |
The default configuration value is:
| config | Pointer to the configuration. |
|
inlinestatic |
| base | CI_PI peripheral address. |
| void CI_PI_Start | ( | CI_PI_CSR_Type * | base | ) |
| base | CI_PI peripheral address. |
| void CI_PI_Stop | ( | CI_PI_CSR_Type * | base | ) |
| base | CI_PI peripheral address. |
|
inlinestatic |
| base | CI_PI peripheral address. |