MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Cs42888_adapter

Overview

Macros

#define HAL_CODEC_HANDLER_SIZE   (CS42888_I2C_HANDLER_SIZE + 4)
 codec handler size
 

Enumerations

enum  _codec_type { kCODEC_CS42888 }
 codec type More...
 

Functions

status_t HAL_CODEC_Init (void *handle, void *config)
 Codec initilization. More...
 
status_t HAL_CODEC_Deinit (void *handle)
 Codec de-initilization. More...
 
status_t HAL_CODEC_SetFormat (void *handle, uint32_t mclk, uint32_t sampleRate, uint32_t bitWidth)
 set audio data format. More...
 
status_t HAL_CODEC_SetVolume (void *handle, uint32_t playChannel, uint32_t volume)
 set audio codec module volume. More...
 
status_t HAL_CODEC_SetMute (void *handle, uint32_t playChannel, bool isMute)
 set audio codec module mute. More...
 
status_t HAL_CODEC_SetPower (void *handle, uint32_t module, bool powerOn)
 set audio codec module power. More...
 
status_t HAL_CODEC_SetRecord (void *handle, uint32_t recordSource)
 codec set record source. More...
 
status_t HAL_CODEC_SetRecordChannel (void *handle, uint32_t leftRecordChannel, uint32_t rightRecordChannel)
 codec set record channel. More...
 
status_t HAL_CODEC_SetPlay (void *handle, uint32_t playSource)
 codec set play source. More...
 
status_t HAL_CODEC_ModuleControl (void *handle, uint32_t cmd, uint32_t data)
 codec module control. More...
 

Enumeration Type Documentation

Enumerator
kCODEC_CS42888 

CS42888.

Function Documentation

status_t HAL_CODEC_Init ( void *  handle,
void *  config 
)
Parameters
handlecodec handle.
configcodec configuration.
Returns
kStatus_Success is success, else initial failed.
status_t HAL_CODEC_Deinit ( void *  handle)
Parameters
handlecodec handle.
Returns
kStatus_Success is success, else de-initial failed.
status_t HAL_CODEC_SetFormat ( void *  handle,
uint32_t  mclk,
uint32_t  sampleRate,
uint32_t  bitWidth 
)
Parameters
handlecodec handle.
mclkmaster clock frequency in HZ.
sampleRatesample rate in HZ.
bitWidthbit width.
Returns
kStatus_Success is success, else configure failed.
status_t HAL_CODEC_SetVolume ( void *  handle,
uint32_t  playChannel,
uint32_t  volume 
)
Parameters
handlecodec handle.
playChannelaudio codec play channel, can be a value or combine value of _codec_play_channel.
volumevolume value, support 0 ~ 100, 0 is mute, 100 is the maximum volume value.
Returns
kStatus_Success is success, else configure failed.
status_t HAL_CODEC_SetMute ( void *  handle,
uint32_t  playChannel,
bool  isMute 
)
Parameters
handlecodec handle.
playChannelaudio codec play channel, can be a value or combine value of _codec_play_channel.
isMutetrue is mute, false is unmute.
Returns
kStatus_Success is success, else configure failed.
status_t HAL_CODEC_SetPower ( void *  handle,
uint32_t  module,
bool  powerOn 
)
Parameters
handlecodec handle.
moduleaudio codec module.
powerOntrue is power on, false is power down.
Returns
kStatus_Success is success, else configure failed.
status_t HAL_CODEC_SetRecord ( void *  handle,
uint32_t  recordSource 
)
Parameters
handlecodec handle.
recordSourceaudio codec record source, can be a value or combine value of _codec_record_source.
Returns
kStatus_Success is success, else configure failed.
status_t HAL_CODEC_SetRecordChannel ( void *  handle,
uint32_t  leftRecordChannel,
uint32_t  rightRecordChannel 
)
Parameters
handlecodec handle.
leftRecordChannelaudio codec record channel, reference _codec_record_channel, can be a value or combine value of member in _codec_record_channel.
rightRecordChannelaudio codec record channel, reference _codec_record_channel, can be a value combine of member in _codec_record_channel.
Returns
kStatus_Success is success, else configure failed.
status_t HAL_CODEC_SetPlay ( void *  handle,
uint32_t  playSource 
)
Parameters
handlecodec handle.
playSourceaudio codec play source, can be a value or combine value of _codec_play_source.
Returns
kStatus_Success is success, else configure failed.
status_t HAL_CODEC_ModuleControl ( void *  handle,
uint32_t  cmd,
uint32_t  data 
)

This function is used for codec module control, support switch digital interface cmd, can be expand to support codec module specific feature

Parameters
handlecodec handle.
cmdmodule control cmd, reference _codec_module_ctrl_cmd.
datavalue to write, when cmd is kCODEC_ModuleRecordSourceChannel, the data should be a value combine of channel and source, please reference macro CODEC_MODULE_RECORD_SOURCE_CHANNEL(source, LP, LN, RP, RN), reference codec specific driver for detail configurations.
Returns
kStatus_Success is success, else configure failed.