MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Clock Driver

Overview

The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.

The clock driver supports:

Files

file  fsl_clock.h
 

Data Structures

struct  pll_config_t
 PLL configuration structure. More...
 
struct  pll_setup_t
 PLL0 setup structure This structure can be used to pre-build a PLL setup configuration at run-time and quickly set the PLL to the configuration. More...
 

Macros

#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0
 Configure whether driver controls clock. More...
 
#define CLOCK_USR_CFG_PLL_CONFIG_CACHE_COUNT   2U
 User-defined the size of cache for CLOCK_PllGetConfig() function. More...
 
#define ROM_CLOCKS
 Clock ip name array for ROM. More...
 
#define SRAM_CLOCKS
 Clock ip name array for SRAM. More...
 
#define FLASH_CLOCKS
 Clock ip name array for FLASH. More...
 
#define FMC_CLOCKS
 Clock ip name array for FMC. More...
 
#define INPUTMUX_CLOCKS
 Clock ip name array for INPUTMUX. More...
 
#define IOCON_CLOCKS
 Clock ip name array for IOCON. More...
 
#define GPIO_CLOCKS
 Clock ip name array for GPIO. More...
 
#define PINT_CLOCKS
 Clock ip name array for PINT. More...
 
#define GINT_CLOCKS
 Clock ip name array for GINT. More...
 
#define DMA_CLOCKS
 Clock ip name array for DMA. More...
 
#define CRC_CLOCKS
 Clock ip name array for CRC. More...
 
#define WWDT_CLOCKS
 Clock ip name array for WWDT. More...
 
#define RTC_CLOCKS
 Clock ip name array for RTC. More...
 
#define MAILBOX_CLOCKS
 Clock ip name array for Mailbox. More...
 
#define LPADC_CLOCKS
 Clock ip name array for LPADC. More...
 
#define MRT_CLOCKS
 Clock ip name array for MRT. More...
 
#define OSTIMER_CLOCKS
 Clock ip name array for OSTIMER. More...
 
#define SCT_CLOCKS
 Clock ip name array for SCT0. More...
 
#define UTICK_CLOCKS
 Clock ip name array for UTICK. More...
 
#define FLEXCOMM_CLOCKS
 Clock ip name array for FLEXCOMM. More...
 
#define LPUART_CLOCKS
 Clock ip name array for LPUART. More...
 
#define BI2C_CLOCKS
 Clock ip name array for BI2C. More...
 
#define LPSPI_CLOCKS
 Clock ip name array for LSPI. More...
 
#define FLEXI2S_CLOCKS
 Clock ip name array for FLEXI2S. More...
 
#define CTIMER_CLOCKS
 Clock ip name array for CTIMER. More...
 
#define COMP_CLOCKS
 Clock ip name array for COMP.
 
#define SDIO_CLOCKS
 Clock ip name array for SDIO. More...
 
#define USB1CLK_CLOCKS
 Clock ip name array for USB1CLK. More...
 
#define FREQME_CLOCKS
 Clock ip name array for FREQME. More...
 
#define USBRAM_CLOCKS
 Clock ip name array for USBRAM. More...
 
#define RNG_CLOCKS
 Clock ip name array for RNG. More...
 
#define USBHMR0_CLOCKS
 Clock ip name array for USBHMR0. More...
 
#define USBHSL0_CLOCKS
 Clock ip name array for USBHSL0. More...
 
#define HASHCRYPT_CLOCKS
 Clock ip name array for HashCrypt. More...
 
#define POWERQUAD_CLOCKS
 Clock ip name array for PowerQuad. More...
 
#define PLULUT_CLOCKS
 Clock ip name array for PLULUT. More...
 
#define PUF_CLOCKS
 Clock ip name array for PUF. More...
 
#define CASPER_CLOCKS
 Clock ip name array for CASPER. More...
 
#define ANALOGCTRL_CLOCKS
 Clock ip name array for ANALOGCTRL. More...
 
#define HS_LSPI_CLOCKS
 Clock ip name array for HS_LSPI. More...
 
#define GPIO_SEC_CLOCKS
 Clock ip name array for GPIO_SEC. More...
 
#define GPIO_SEC_INT_CLOCKS
 Clock ip name array for GPIO_SEC_INT. More...
 
#define USBD_CLOCKS
 Clock ip name array for USBD. More...
 
#define USBH_CLOCKS
 Clock ip name array for USBH. More...
 
#define CLK_GATE_REG_OFFSET_SHIFT   8U
 Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More...
 
#define BUS_CLK   kCLOCK_BusClk
 Peripherals clock source definition. More...
 
#define CLK_ATTACH_ID(mux, sel, pos)   ((((uint32_t)(mux) << 0U) | (((uint32_t)(sel) + 1U) & 0xFU) << 8U) << ((uint32_t)(pos)*12U))
 Clock Mux Switches The encoding is as follows each connection identified is 32bits wide while 24bits are valuable starting from LSB upwards. More...
 
#define PLL_CONFIGFLAG_USEINRATE   (1U << 0U)
 PLL configuration structure flags for 'flags' field These flags control how the PLL configuration function sets up the PLL setup structure. More...
 
#define PLL_CONFIGFLAG_FORCENOFRACT   (1U << 2U)
 Force non-fractional output mode, PLL output will not use the fractional, automatic bandwidth, or SS hardware.
 
#define PLL_SETUPFLAG_POWERUP   (1U << 0U)
 PLL setup structure flags for 'flags' field These flags control how the PLL setup function sets up the PLL. More...
 
#define PLL_SETUPFLAG_WAITLOCK   (1U << 1U)
 Setup will wait for PLL lock, implies the PLL will be pwoered on.
 
#define PLL_SETUPFLAG_ADGVOLT   (1U << 2U)
 Optimize system voltage for the new PLL rate.
 
#define PLL_SETUPFLAG_USEFEEDBACKDIV2   (1U << 3U)
 Use feedback divider by 2 in divider path.
 

Enumerations

enum  clock_ip_name_t
 Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More...
 
enum  clock_name_t {
  kCLOCK_CoreSysClk,
  kCLOCK_BusClk,
  kCLOCK_ClockOut,
  kCLOCK_FroHf,
  kCLOCK_Pll1Out,
  kCLOCK_Mclk,
  kCLOCK_Fro12M,
  kCLOCK_ExtClk,
  kCLOCK_Pll0Out,
  kCLOCK_FlexI2S
}
 Clock name used to get clock frequency. More...
 
enum  ss_progmodfm_t {
  kSS_MF_512 = (0 << 20),
  kSS_MF_384 = (1 << 20),
  kSS_MF_256 = (2 << 20),
  kSS_MF_128 = (3 << 20),
  kSS_MF_64 = (4 << 20),
  kSS_MF_32 = (5 << 20),
  kSS_MF_24 = (6 << 20),
  kSS_MF_16 = (7 << 20)
}
 PLL Spread Spectrum (SS) Programmable modulation frequency See (MF) field in the PLL0SSCG1 register in the UM. More...
 
enum  ss_progmoddp_t {
  kSS_MR_K0 = (0 << 23),
  kSS_MR_K1 = (1 << 23),
  kSS_MR_K1_5 = (2 << 23),
  kSS_MR_K2 = (3 << 23),
  kSS_MR_K3 = (4 << 23),
  kSS_MR_K4 = (5 << 23),
  kSS_MR_K6 = (6 << 23),
  kSS_MR_K8 = (7 << 23)
}
 PLL Spread Spectrum (SS) Programmable frequency modulation depth See (MR) field in the PLL0SSCG1 register in the UM. More...
 
enum  ss_modwvctrl_t {
  kSS_MC_NOC = (0 << 26),
  kSS_MC_RECC = (2 << 26),
  kSS_MC_MAXC = (3 << 26)
}
 PLL Spread Spectrum (SS) Modulation waveform control See (MC) field in the PLL0SSCG1 register in the UM. More...
 
enum  pll_error_t {
  kStatus_PLL_Success = MAKE_STATUS(kStatusGroup_Generic, 0),
  kStatus_PLL_OutputTooLow = MAKE_STATUS(kStatusGroup_Generic, 1),
  kStatus_PLL_OutputTooHigh = MAKE_STATUS(kStatusGroup_Generic, 2),
  kStatus_PLL_InputTooLow = MAKE_STATUS(kStatusGroup_Generic, 3),
  kStatus_PLL_InputTooHigh = MAKE_STATUS(kStatusGroup_Generic, 4),
  kStatus_PLL_OutsideIntLimit = MAKE_STATUS(kStatusGroup_Generic, 5),
  kStatus_PLL_CCOTooLow = MAKE_STATUS(kStatusGroup_Generic, 6),
  kStatus_PLL_CCOTooHigh = MAKE_STATUS(kStatusGroup_Generic, 7)
}
 PLL status definitions. More...
 
enum  clock_usbfs_src_t {
  kCLOCK_UsbfsSrcFro = (uint32_t)kCLOCK_FroHf,
  kCLOCK_UsbfsSrcPll0 = (uint32_t)kCLOCK_Pll0Out,
  kCLOCK_UsbfsSrcMainClock = (uint32_t)kCLOCK_CoreSysClk,
  kCLOCK_UsbfsSrcPll1 = (uint32_t)kCLOCK_Pll1Out,
  kCLOCK_UsbfsSrcNone
}
 USB FS clock source definition. More...
 
enum  clock_usbhs_src_t { kCLOCK_UsbSrcUnused = 0xFFFFFFFFU }
 USBhs clock source definition. More...
 
enum  clock_usb_phy_src_t { kCLOCK_UsbPhySrcExt = 0U }
 Source of the USB HS PHY. More...
 

Functions

static void CLOCK_EnableClock (clock_ip_name_t clk)
 Enable the clock for specific IP. More...
 
static void CLOCK_DisableClock (clock_ip_name_t clk)
 Disable the clock for specific IP. More...
 
status_t CLOCK_SetupFROClocking (uint32_t iFreq)
 Initialize the Core clock to given frequency (12, 48 or 96 MHz). Turns on FRO and uses default CCO, if freq is 12000000, then high speed output is off, else high speed output is enabled. More...
 
void CLOCK_SetFLASHAccessCyclesForFreq (uint32_t iFreq)
 Set the flash wait states for the input freuqency. More...
 
status_t CLOCK_SetupExtClocking (uint32_t iFreq)
 Initialize the external osc clock to given frequency. More...
 
status_t CLOCK_SetupI2SMClkClocking (uint32_t iFreq)
 Initialize the I2S MCLK clock to given frequency. More...
 
status_t CLOCK_SetupPLUClkInClocking (uint32_t iFreq)
 Initialize the PLU CLKIN clock to given frequency. More...
 
void CLOCK_AttachClk (clock_attach_id_t connection)
 Configure the clock selection muxes. More...
 
clock_attach_id_t CLOCK_GetClockAttachId (clock_attach_id_t attachId)
 Get the actual clock attach id. This fuction uses the offset in input attach id, then it reads the actual source value in the register and combine the offset to obtain an actual attach id. More...
 
void CLOCK_SetClkDiv (clock_div_name_t div_name, uint32_t divided_by_value, bool reset)
 Setup peripheral clock dividers. More...
 
void CLOCK_SetRtc1khzClkDiv (uint32_t divided_by_value)
 Setup rtc 1khz clock divider. More...
 
void CLOCK_SetRtc1hzClkDiv (uint32_t divided_by_value)
 Setup rtc 1hz clock divider. More...
 
uint32_t CLOCK_SetFlexCommClock (uint32_t id, uint32_t freq)
 Set the flexcomm output frequency. More...
 
uint32_t CLOCK_GetFlexCommInputClock (uint32_t id)
 Return Frequency of flexcomm input clock. More...
 
uint32_t CLOCK_GetFreq (clock_name_t clockName)
 Return Frequency of selected clock. More...
 
uint32_t CLOCK_GetFro12MFreq (void)
 Return Frequency of FRO 12MHz. More...
 
uint32_t CLOCK_GetFro1MFreq (void)
 Return Frequency of FRO 1MHz. More...
 
uint32_t CLOCK_GetClockOutClkFreq (void)
 Return Frequency of ClockOut. More...
 
uint32_t CLOCK_GetAdcClkFreq (void)
 Return Frequency of Adc Clock. More...
 
uint32_t CLOCK_GetUsb0ClkFreq (void)
 Return Frequency of Usb0 Clock. More...
 
uint32_t CLOCK_GetUsb1ClkFreq (void)
 Return Frequency of Usb1 Clock. More...
 
uint32_t CLOCK_GetMclkClkFreq (void)
 Return Frequency of MClk Clock. More...
 
uint32_t CLOCK_GetSctClkFreq (void)
 Return Frequency of SCTimer Clock. More...
 
uint32_t CLOCK_GetSdioClkFreq (void)
 Return Frequency of SDIO Clock. More...
 
uint32_t CLOCK_GetExtClkFreq (void)
 Return Frequency of External Clock. More...
 
uint32_t CLOCK_GetWdtClkFreq (void)
 Return Frequency of Watchdog. More...
 
uint32_t CLOCK_GetFroHfFreq (void)
 Return Frequency of High-Freq output of FRO. More...
 
uint32_t CLOCK_GetPll0OutFreq (void)
 Return Frequency of PLL. More...
 
uint32_t CLOCK_GetPll1OutFreq (void)
 Return Frequency of USB PLL. More...
 
uint32_t CLOCK_GetOsc32KFreq (void)
 Return Frequency of 32kHz osc. More...
 
uint32_t CLOCK_GetCoreSysClkFreq (void)
 Return Frequency of Core System. More...
 
uint32_t CLOCK_GetI2SMClkFreq (void)
 Return Frequency of I2S MCLK Clock. More...
 
uint32_t CLOCK_GetPLUClkInFreq (void)
 Return Frequency of PLU CLKIN Clock. More...
 
uint32_t CLOCK_GetFlexCommClkFreq (uint32_t id)
 Return Frequency of FlexComm Clock. More...
 
uint32_t CLOCK_GetHsLspiClkFreq (void)
 Return Frequency of High speed SPI Clock. More...
 
uint32_t CLOCK_GetCTimerClkFreq (uint32_t id)
 Return Frequency of CTimer functional Clock. More...
 
uint32_t CLOCK_GetSystickClkFreq (uint32_t id)
 Return Frequency of SystickClock. More...
 
uint32_t CLOCK_GetPLL0InClockRate (void)
 Return PLL0 input clock rate. More...
 
uint32_t CLOCK_GetPLL1InClockRate (void)
 Return PLL1 input clock rate. More...
 
uint32_t CLOCK_GetPLL0OutClockRate (bool recompute)
 Return PLL0 output clock rate. More...
 
__STATIC_INLINE void CLOCK_SetBypassPLL0 (bool bypass)
 Enables and disables PLL0 bypass mode. More...
 
__STATIC_INLINE void CLOCK_SetBypassPLL1 (bool bypass)
 Enables and disables PLL1 bypass mode. More...
 
__STATIC_INLINE bool CLOCK_IsPLL0Locked (void)
 Check if PLL is locked or not. More...
 
__STATIC_INLINE bool CLOCK_IsPLL1Locked (void)
 Check if PLL1 is locked or not. More...
 
void CLOCK_SetStoredPLL0ClockRate (uint32_t rate)
 Store the current PLL0 rate. More...
 
uint32_t CLOCK_GetPLL0OutFromSetup (pll_setup_t *pSetup)
 Return PLL0 output clock rate from setup structure. More...
 
pll_error_t CLOCK_SetupPLL0Data (pll_config_t *pControl, pll_setup_t *pSetup)
 Set PLL0 output based on the passed PLL setup data. More...
 
pll_error_t CLOCK_SetupPLL0Prec (pll_setup_t *pSetup, uint32_t flagcfg)
 Set PLL output from PLL setup structure (precise frequency) More...
 
pll_error_t CLOCK_SetPLL0Freq (const pll_setup_t *pSetup)
 Set PLL output from PLL setup structure (precise frequency) More...
 
pll_error_t CLOCK_SetPLL1Freq (const pll_setup_t *pSetup)
 Set PLL output from PLL setup structure (precise frequency) More...
 
void CLOCK_SetupPLL0Mult (uint32_t multiply_by, uint32_t input_freq)
 Set PLL0 output based on the multiplier and input frequency. More...
 
static void CLOCK_DisableUsbDevicefs0Clock (clock_ip_name_t clk)
 Disable USB clock. More...
 
bool CLOCK_EnableUsbfs0DeviceClock (clock_usbfs_src_t src, uint32_t freq)
 Enable USB Device FS clock. More...
 
bool CLOCK_EnableUsbfs0HostClock (clock_usbfs_src_t src, uint32_t freq)
 Enable USB HOST FS clock. More...
 
bool CLOCK_EnableUsbhs0PhyPllClock (clock_usb_phy_src_t src, uint32_t freq)
 Enable USB phy clock. More...
 
bool CLOCK_EnableUsbhs0DeviceClock (clock_usbhs_src_t src, uint32_t freq)
 Enable USB Device HS clock. More...
 
bool CLOCK_EnableUsbhs0HostClock (clock_usbhs_src_t src, uint32_t freq)
 Enable USB HOST HS clock. More...
 

Driver version

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 3, 4))
 CLOCK driver version 2.3.4. More...
 

Data Structure Documentation

struct pll_config_t

This structure can be used to configure the settings for a PLL setup structure. Fill in the desired configuration for the PLL and call the PLL setup function to fill in a PLL setup structure.

Data Fields

uint32_t desiredRate
 Desired PLL rate in Hz.
 
uint32_t inputRate
 PLL input clock in Hz, only used if PLL_CONFIGFLAG_USEINRATE flag is set.
 
uint32_t flags
 PLL configuration flags, Or'ed value of PLL_CONFIGFLAG_* definitions.
 
ss_progmodfm_t ss_mf
 SS Programmable modulation frequency, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag.
 
ss_progmoddp_t ss_mr
 SS Programmable frequency modulation depth, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag.
 
ss_modwvctrl_t ss_mc
 SS Modulation waveform control, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag.
 
bool mfDither
 false for fixed modulation frequency or true for dithering, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag
 
struct pll_setup_t

It can be populated with the PLL setup function. If powering up or waiting for PLL lock, the PLL input clock source should be configured prior to PLL setup.

Data Fields

uint32_t pllctrl
 PLL control register PLL0CTRL.
 
uint32_t pllndec
 PLL NDEC register PLL0NDEC.
 
uint32_t pllpdec
 PLL PDEC register PLL0PDEC.
 
uint32_t pllmdec
 PLL MDEC registers PLL0PDEC.
 
uint32_t pllsscg [2]
 PLL SSCTL registers PLL0SSCG.
 
uint32_t pllRate
 Acutal PLL rate.
 
uint32_t flags
 PLL setup flags, Or'ed value of PLL_SETUPFLAG_* definitions.
 

Macro Definition Documentation

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 3, 4))
#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0

When set to 0, peripheral drivers will enable clock in initialize function and disable clock in de-initialize function. When set to 1, peripheral driver will not control the clock, application could control the clock out of the driver.

Note
All drivers share this feature switcher. If it is set to 1, application should handle clock enable and disable for all drivers.
#define CLOCK_USR_CFG_PLL_CONFIG_CACHE_COUNT   2U

Once define this MACRO to be non-zero value, CLOCK_PllGetConfig() function would cache the recent calulation and accelerate the execution to get the right settings.

#define ROM_CLOCKS
Value:
{ \
kCLOCK_Rom \
}
#define SRAM_CLOCKS
Value:
{ \
kCLOCK_Sram1, kCLOCK_Sram2, kCLOCK_Sram3, kCLOCK_Sram4 \
}
#define FLASH_CLOCKS
Value:
{ \
kCLOCK_Flash \
}
#define FMC_CLOCKS
Value:
{ \
kCLOCK_Fmc \
}
#define INPUTMUX_CLOCKS
Value:
{ \
kCLOCK_InputMux0 \
}
#define IOCON_CLOCKS
Value:
{ \
kCLOCK_Iocon \
}
#define GPIO_CLOCKS
Value:
{ \
kCLOCK_Gpio0, kCLOCK_Gpio1, kCLOCK_Gpio2, kCLOCK_Gpio3 \
}
#define PINT_CLOCKS
Value:
{ \
kCLOCK_Pint \
}
#define GINT_CLOCKS
Value:
{ \
kCLOCK_Gint, kCLOCK_Gint \
}
#define DMA_CLOCKS
Value:
{ \
kCLOCK_Dma0, kCLOCK_Dma1 \
}
#define CRC_CLOCKS
Value:
{ \
kCLOCK_Crc \
}
#define WWDT_CLOCKS
Value:
{ \
kCLOCK_Wwdt \
}
#define RTC_CLOCKS
Value:
{ \
kCLOCK_Rtc \
}
#define MAILBOX_CLOCKS
Value:
{ \
kCLOCK_Mailbox \
}
#define LPADC_CLOCKS
Value:
{ \
kCLOCK_Adc0 \
}
#define MRT_CLOCKS
Value:
{ \
kCLOCK_Mrt \
}
#define OSTIMER_CLOCKS
Value:
{ \
kCLOCK_OsTimer0 \
}
#define SCT_CLOCKS
Value:
{ \
kCLOCK_Sct0 \
}
#define UTICK_CLOCKS
Value:
{ \
kCLOCK_Utick0 \
}
#define FLEXCOMM_CLOCKS
Value:
{ \
kCLOCK_FlexComm0, kCLOCK_FlexComm1, kCLOCK_FlexComm2, kCLOCK_FlexComm3, kCLOCK_FlexComm4, kCLOCK_FlexComm5, \
kCLOCK_FlexComm6, kCLOCK_FlexComm7, kCLOCK_Hs_Lspi \
}
#define LPUART_CLOCKS
Value:
{ \
kCLOCK_MinUart0, kCLOCK_MinUart1, kCLOCK_MinUart2, kCLOCK_MinUart3, kCLOCK_MinUart4, kCLOCK_MinUart5, \
kCLOCK_MinUart6, kCLOCK_MinUart7 \
}
#define BI2C_CLOCKS
Value:
{ \
kCLOCK_BI2c0, kCLOCK_BI2c1, kCLOCK_BI2c2, kCLOCK_BI2c3, kCLOCK_BI2c4, kCLOCK_BI2c5, kCLOCK_BI2c6, kCLOCK_BI2c7 \
}
#define LPSPI_CLOCKS
Value:
{ \
kCLOCK_LSpi0, kCLOCK_LSpi1, kCLOCK_LSpi2, kCLOCK_LSpi3, kCLOCK_LSpi4, kCLOCK_LSpi5, kCLOCK_LSpi6, kCLOCK_LSpi7 \
}
#define FLEXI2S_CLOCKS
Value:
{ \
kCLOCK_FlexI2s0, kCLOCK_FlexI2s1, kCLOCK_FlexI2s2, kCLOCK_FlexI2s3, kCLOCK_FlexI2s4, kCLOCK_FlexI2s5, \
kCLOCK_FlexI2s6, kCLOCK_FlexI2s7 \
}
#define CTIMER_CLOCKS
Value:
{ \
kCLOCK_Timer0, kCLOCK_Timer1, kCLOCK_Timer2, kCLOCK_Timer3, kCLOCK_Timer4 \
}
#define SDIO_CLOCKS
Value:
{ \
kCLOCK_Sdio \
}
#define USB1CLK_CLOCKS
Value:
{ \
kCLOCK_Usb1Clk \
}
#define FREQME_CLOCKS
Value:
{ \
kCLOCK_Freqme \
}
#define USBRAM_CLOCKS
Value:
{ \
kCLOCK_UsbRam1 \
}
#define RNG_CLOCKS
Value:
{ \
kCLOCK_Rng \
}
#define USBHMR0_CLOCKS
Value:
{ \
kCLOCK_Usbhmr0 \
}
#define USBHSL0_CLOCKS
Value:
{ \
kCLOCK_Usbhsl0 \
}
#define HASHCRYPT_CLOCKS
Value:
{ \
kCLOCK_HashCrypt \
}
#define POWERQUAD_CLOCKS
Value:
{ \
kCLOCK_PowerQuad \
}
#define PLULUT_CLOCKS
Value:
{ \
kCLOCK_PluLut \
}
#define PUF_CLOCKS
Value:
{ \
kCLOCK_Puf \
}
#define CASPER_CLOCKS
Value:
{ \
kCLOCK_Casper \
}
#define ANALOGCTRL_CLOCKS
Value:
{ \
kCLOCK_AnalogCtrl \
}
#define HS_LSPI_CLOCKS
Value:
{ \
kCLOCK_Hs_Lspi \
}
#define GPIO_SEC_CLOCKS
Value:
{ \
kCLOCK_Gpio_Sec \
}
#define GPIO_SEC_INT_CLOCKS
Value:
{ \
kCLOCK_Gpio_Sec_Int \
}
#define USBD_CLOCKS
Value:
{ \
kCLOCK_Usbd0, kCLOCK_Usbh1, kCLOCK_Usbd1 \
}
#define USBH_CLOCKS
Value:
{ \
kCLOCK_Usbh1 \
}
#define CLK_GATE_REG_OFFSET_SHIFT   8U
#define BUS_CLK   kCLOCK_BusClk
#define CLK_ATTACH_ID (   mux,
  sel,
  pos 
)    ((((uint32_t)(mux) << 0U) | (((uint32_t)(sel) + 1U) & 0xFU) << 8U) << ((uint32_t)(pos)*12U))

[4 bits for choice, 0 means invalid choice] [8 bits mux ID]*

#define PLL_CONFIGFLAG_USEINRATE   (1U << 0U)


When the PLL_CONFIGFLAG_USEINRATE flag is selected, the 'InputRate' field in the configuration structure must be assigned with the expected PLL frequency. If the PLL_CONFIGFLAG_USEINRATE is not used, 'InputRate' is ignored in the configuration function and the driver will determine the PLL rate from the currently selected PLL source. This flag might be used to configure the PLL input clock more accurately when using the WDT oscillator or a more dyanmic CLKIN source.

When the PLL_CONFIGFLAG_FORCENOFRACT flag is selected, the PLL hardware for the automatic bandwidth selection, Spread Spectrum (SS) support, and fractional M-divider are not used.
Flag to use InputRate in PLL configuration structure for setup

#define PLL_SETUPFLAG_POWERUP   (1U << 0U)

Setup will power on the PLL after setup

Enumeration Type Documentation

Enumerator
kCLOCK_CoreSysClk 

Core/system clock (aka MAIN_CLK)

kCLOCK_BusClk 

Bus clock (AHB clock)

kCLOCK_ClockOut 

CLOCKOUT.

kCLOCK_FroHf 

FRO48/96.

kCLOCK_Pll1Out 

PLL1 Output.

kCLOCK_Mclk 

MCLK.

kCLOCK_Fro12M 

FRO12M.

kCLOCK_ExtClk 

External Clock.

kCLOCK_Pll0Out 

PLL0 Output.

kCLOCK_FlexI2S 

FlexI2S clock.

Enumerator
kSS_MF_512 

Nss = 512 (fm ? 3.9 - 7.8 kHz)

kSS_MF_384 

Nss ?= 384 (fm ? 5.2 - 10.4 kHz)

kSS_MF_256 

Nss = 256 (fm ? 7.8 - 15.6 kHz)

kSS_MF_128 

Nss = 128 (fm ? 15.6 - 31.3 kHz)

kSS_MF_64 

Nss = 64 (fm ? 32.3 - 64.5 kHz)

kSS_MF_32 

Nss = 32 (fm ? 62.5- 125 kHz)

kSS_MF_24 

Nss ?= 24 (fm ? 83.3- 166.6 kHz)

kSS_MF_16 

Nss = 16 (fm ? 125- 250 kHz)

Enumerator
kSS_MR_K0 

k = 0 (no spread spectrum)

kSS_MR_K1 

k = 1

kSS_MR_K1_5 

k = 1.5

kSS_MR_K2 

k = 2

kSS_MR_K3 

k = 3

kSS_MR_K4 

k = 4

kSS_MR_K6 

k = 6

kSS_MR_K8 

k = 8


Compensation for low pass filtering of the PLL to get a triangular modulation at the output of the PLL, giving a flat frequency spectrum.

Enumerator
kSS_MC_NOC 

no compensation

kSS_MC_RECC 

recommended setting

kSS_MC_MAXC 

max.

compensation

Enumerator
kStatus_PLL_Success 

PLL operation was successful.

kStatus_PLL_OutputTooLow 

PLL output rate request was too low.

kStatus_PLL_OutputTooHigh 

PLL output rate request was too high.

kStatus_PLL_InputTooLow 

PLL input rate is too low.

kStatus_PLL_InputTooHigh 

PLL input rate is too high.

kStatus_PLL_OutsideIntLimit 

Requested output rate isn't possible.

kStatus_PLL_CCOTooLow 

Requested CCO rate isn't possible.

kStatus_PLL_CCOTooHigh 

Requested CCO rate isn't possible.

Enumerator
kCLOCK_UsbfsSrcFro 

Use FRO 96 MHz.

kCLOCK_UsbfsSrcPll0 

Use PLL0 output.

kCLOCK_UsbfsSrcMainClock 

Use Main clock.

kCLOCK_UsbfsSrcPll1 

Use PLL1 clock.

kCLOCK_UsbfsSrcNone 

this may be selected in order to reduce power when no output is needed.

Enumerator
kCLOCK_UsbSrcUnused 

Used when the function does not care the clock source.

Enumerator
kCLOCK_UsbPhySrcExt 

Use external crystal.

Function Documentation

static void CLOCK_EnableClock ( clock_ip_name_t  clk)
inlinestatic
Parameters
clk: Clock to be enabled.
Returns
Nothing
static void CLOCK_DisableClock ( clock_ip_name_t  clk)
inlinestatic
Parameters
clk: Clock to be Disabled.
Returns
Nothing
status_t CLOCK_SetupFROClocking ( uint32_t  iFreq)
Parameters
iFreq: Desired frequency (must be one of CLK_FRO_12MHZ or CLK_FRO_48MHZ or CLK_FRO_96MHZ)
Returns
returns success or fail status.
void CLOCK_SetFLASHAccessCyclesForFreq ( uint32_t  iFreq)
Parameters
iFreq: Input frequency
Returns
Nothing
status_t CLOCK_SetupExtClocking ( uint32_t  iFreq)
Parameters
iFreq: Desired frequency (must be equal to exact rate in Hz)
Returns
returns success or fail status.
status_t CLOCK_SetupI2SMClkClocking ( uint32_t  iFreq)
Parameters
iFreq: Desired frequency (must be equal to exact rate in Hz)
Returns
returns success or fail status.
status_t CLOCK_SetupPLUClkInClocking ( uint32_t  iFreq)
Parameters
iFreq: Desired frequency (must be equal to exact rate in Hz)
Returns
returns success or fail status.
void CLOCK_AttachClk ( clock_attach_id_t  connection)
Parameters
connection: Clock to be configured.
Returns
Nothing
clock_attach_id_t CLOCK_GetClockAttachId ( clock_attach_id_t  attachId)
Parameters
attachId: Clock attach id to get.
Returns
Clock source value.
void CLOCK_SetClkDiv ( clock_div_name_t  div_name,
uint32_t  divided_by_value,
bool  reset 
)
Parameters
div_name: Clock divider name
divided_by_value,:Value to be divided
reset: Whether to reset the divider counter.
Returns
Nothing
void CLOCK_SetRtc1khzClkDiv ( uint32_t  divided_by_value)
Parameters
divided_by_value,:Value to be divided
Returns
Nothing
void CLOCK_SetRtc1hzClkDiv ( uint32_t  divided_by_value)
Parameters
divided_by_value,:Value to be divided
Returns
Nothing
uint32_t CLOCK_SetFlexCommClock ( uint32_t  id,
uint32_t  freq 
)
Parameters
id: flexcomm instance id
freq: output frequency
Returns
0 : the frequency range is out of range. 1 : switch successfully.
uint32_t CLOCK_GetFlexCommInputClock ( uint32_t  id)
Parameters
id: flexcomm instance id
Returns
Frequency value
uint32_t CLOCK_GetFreq ( clock_name_t  clockName)
Returns
Frequency of selected clock
uint32_t CLOCK_GetFro12MFreq ( void  )
Returns
Frequency of FRO 12MHz
uint32_t CLOCK_GetFro1MFreq ( void  )
Returns
Frequency of FRO 1MHz
uint32_t CLOCK_GetClockOutClkFreq ( void  )
Returns
Frequency of ClockOut
uint32_t CLOCK_GetAdcClkFreq ( void  )
Returns
Frequency of Adc.
uint32_t CLOCK_GetUsb0ClkFreq ( void  )
Returns
Frequency of Usb0 Clock.
uint32_t CLOCK_GetUsb1ClkFreq ( void  )
Returns
Frequency of Usb1 Clock.
uint32_t CLOCK_GetMclkClkFreq ( void  )
Returns
Frequency of MClk Clock.
uint32_t CLOCK_GetSctClkFreq ( void  )
Returns
Frequency of SCTimer Clock.
uint32_t CLOCK_GetSdioClkFreq ( void  )
Returns
Frequency of SDIO Clock.
uint32_t CLOCK_GetExtClkFreq ( void  )
Returns
Frequency of External Clock. If no external clock is used returns 0.
uint32_t CLOCK_GetWdtClkFreq ( void  )
Returns
Frequency of Watchdog
uint32_t CLOCK_GetFroHfFreq ( void  )
Returns
Frequency of High-Freq output of FRO
uint32_t CLOCK_GetPll0OutFreq ( void  )
Returns
Frequency of PLL
uint32_t CLOCK_GetPll1OutFreq ( void  )
Returns
Frequency of PLL
uint32_t CLOCK_GetOsc32KFreq ( void  )
Returns
Frequency of 32kHz osc
uint32_t CLOCK_GetCoreSysClkFreq ( void  )
Returns
Frequency of Core System
uint32_t CLOCK_GetI2SMClkFreq ( void  )
Returns
Frequency of I2S MCLK Clock
uint32_t CLOCK_GetPLUClkInFreq ( void  )
Returns
Frequency of PLU CLKIN Clock
uint32_t CLOCK_GetFlexCommClkFreq ( uint32_t  id)
Returns
Frequency of FlexComm Clock
uint32_t CLOCK_GetHsLspiClkFreq ( void  )
Returns
Frequency of High speed SPI Clock
uint32_t CLOCK_GetCTimerClkFreq ( uint32_t  id)
Returns
Frequency of CTimer functional Clock
uint32_t CLOCK_GetSystickClkFreq ( uint32_t  id)
Returns
Frequency of Systick Clock
uint32_t CLOCK_GetPLL0InClockRate ( void  )
Returns
PLL0 input clock rate
uint32_t CLOCK_GetPLL1InClockRate ( void  )
Returns
PLL1 input clock rate
uint32_t CLOCK_GetPLL0OutClockRate ( bool  recompute)
Parameters
recompute: Forces a PLL rate recomputation if true
Returns
PLL0 output clock rate
Note
The PLL rate is cached in the driver in a variable as the rate computation function can take some time to perform. It is recommended to use 'false' with the 'recompute' parameter.
__STATIC_INLINE void CLOCK_SetBypassPLL0 ( bool  bypass)

bypass : true to bypass PLL0 (PLL0 output = PLL0 input, false to disable bypass

Returns
PLL0 output clock rate
__STATIC_INLINE void CLOCK_SetBypassPLL1 ( bool  bypass)

bypass : true to bypass PLL1 (PLL1 output = PLL1 input, false to disable bypass

Returns
PLL1 output clock rate
__STATIC_INLINE bool CLOCK_IsPLL0Locked ( void  )
Returns
true if the PLL is locked, false if not locked
__STATIC_INLINE bool CLOCK_IsPLL1Locked ( void  )
Returns
true if the PLL1 is locked, false if not locked
void CLOCK_SetStoredPLL0ClockRate ( uint32_t  rate)
Parameters
rate,:Current rate of the PLL0
Returns
Nothing
uint32_t CLOCK_GetPLL0OutFromSetup ( pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to a PLL setup structure
Returns
System PLL output clock rate the setup structure will generate
pll_error_t CLOCK_SetupPLL0Data ( pll_config_t *  pControl,
pll_setup_t *  pSetup 
)
Parameters
pControl: Pointer to populated PLL control structure to generate setup with
pSetup: Pointer to PLL setup structure to be filled
Returns
PLL_ERROR_SUCCESS on success, or PLL setup error code
Note
Actual frequency for setup may vary from the desired frequency based on the accuracy of input clocks, rounding, non-fractional PLL mode, etc.
pll_error_t CLOCK_SetupPLL0Prec ( pll_setup_t *  pSetup,
uint32_t  flagcfg 
)
Parameters
pSetup: Pointer to populated PLL setup structure
flagcfg: Flag configuration for PLL config structure
Returns
PLL_ERROR_SUCCESS on success, or PLL setup error code
Note
This function will power off the PLL, setup the PLL with the new setup data, and then optionally powerup the PLL, wait for PLL lock, and adjust system voltages to the new PLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
pll_error_t CLOCK_SetPLL0Freq ( const pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to populated PLL setup structure
Returns
kStatus_PLL_Success on success, or PLL setup error code
Note
This function will power off the PLL, setup the PLL with the new setup data, and then optionally powerup the PLL, wait for PLL lock, and adjust system voltages to the new PLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
pll_error_t CLOCK_SetPLL1Freq ( const pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to populated PLL setup structure
Returns
kStatus_PLL_Success on success, or PLL setup error code
Note
This function will power off the PLL, setup the PLL with the new setup data, and then optionally powerup the PLL, wait for PLL lock, and adjust system voltages to the new PLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
void CLOCK_SetupPLL0Mult ( uint32_t  multiply_by,
uint32_t  input_freq 
)
Parameters
multiply_by: multiplier
input_freq: Clock input frequency of the PLL
Returns
Nothing
Note
Unlike the Chip_Clock_SetupSystemPLLPrec() function, this function does not disable or enable PLL power, wait for PLL lock, or adjust system voltages. These must be done in the application. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
static void CLOCK_DisableUsbDevicefs0Clock ( clock_ip_name_t  clk)
inlinestatic

Disable USB clock.

bool CLOCK_EnableUsbfs0DeviceClock ( clock_usbfs_src_t  src,
uint32_t  freq 
)
Parameters
src: clock source
freq,:clock frequency Enable USB Device Full Speed clock.
bool CLOCK_EnableUsbfs0HostClock ( clock_usbfs_src_t  src,
uint32_t  freq 
)
Parameters
src: clock source
freq,:clock frequency Enable USB HOST Full Speed clock.
bool CLOCK_EnableUsbhs0PhyPllClock ( clock_usb_phy_src_t  src,
uint32_t  freq 
)

Enable USB phy clock.

bool CLOCK_EnableUsbhs0DeviceClock ( clock_usbhs_src_t  src,
uint32_t  freq 
)

Enable USB Device High Speed clock.

bool CLOCK_EnableUsbhs0HostClock ( clock_usbhs_src_t  src,
uint32_t  freq 
)

Enable USB HOST High Speed clock.