MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Clock Driver

Overview

The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.

The clock driver supports:

Files

file  fsl_clock.h
 

Data Structures

struct  pll_config_t
 PLL configuration structure. More...
 
struct  pll_setup_t
 PLL setup structure This structure can be used to pre-build a PLL setup configuration at run-time and quickly set the PLL to the configuration. More...
 

Macros

#define CLOCK_USR_CFG_PLL_CONFIG_CACHE_COUNT   2U
 User-defined the size of cache for CLOCK_PllGetConfig() function. More...
 
#define FLEXCOMM_CLOCKS
 Clock ip name array for FLEXCOMM. More...
 
#define LPUART_CLOCKS
 Clock ip name array for LPUART. More...
 
#define BI2C_CLOCKS
 Clock ip name array for BI2C. More...
 
#define LPSI_CLOCKS
 Clock ip name array for LSPI. More...
 
#define FLEXI2S_CLOCKS
 Clock ip name array for FLEXI2S. More...
 
#define UTICK_CLOCKS
 Clock ip name array for UTICK. More...
 
#define DMA_CLOCKS
 Clock ip name array for DMA. More...
 
#define CTIMER_CLOCKS
 Clock ip name array for CT32B. More...
 
#define GPIO_CLOCKS
 Clock ip name array for GPIO. More...
 
#define ADC_CLOCKS
 Clock ip name array for ADC. More...
 
#define MRT_CLOCKS
 Clock ip name array for MRT. More...
 
#define SCT_CLOCKS
 Clock ip name array for MRT. More...
 
#define RTC_CLOCKS
 Clock ip name array for RTC. More...
 
#define WWDT_CLOCKS
 Clock ip name array for WWDT. More...
 
#define CRC_CLOCKS
 Clock ip name array for CRC. More...
 
#define USBD_CLOCKS
 Clock ip name array for USBD. More...
 
#define GINT_CLOCKS
 Clock ip name array for GINT. More...
 
#define CLK_GATE_REG_OFFSET_SHIFT   8U
 Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More...
 
#define CLK_ATTACH_ID(mux, sel, pos)   ((((uint32_t)(mux) << 0U) | (((uint32_t)(sel) + 1U) & 0xFU) << 8U) << ((pos)*12U))
 Clock Mux Switches The encoding is as follows each connection identified is 32bits wide while 24bits are valuable starting from LSB upwards. More...
 
#define PLL_CONFIGFLAG_USEINRATE   (1U << 0U)
 PLL configuration structure flags for 'flags' field These flags control how the PLL configuration function sets up the PLL setup structure. More...
 
#define PLL_CONFIGFLAG_FORCENOFRACT   (1U << 2U)
 Force non-fractional output mode, PLL output will not use the fractional, automatic bandwidth, or \ SS hardware.
 
#define PLL_SETUPFLAG_POWERUP   (1U << 0U)
 PLL setup structure flags for 'flags' field These flags control how the PLL setup function sets up the PLL. More...
 
#define PLL_SETUPFLAG_WAITLOCK   (1U << 1U)
 Setup will wait for PLL lock, implies the PLL will be pwoered on.
 
#define PLL_SETUPFLAG_ADGVOLT   (1U << 2U)
 Optimize system voltage for the new PLL rate.
 
#define PLL_SETUPFLAG_USEFEEDBACKDIV2   (1U << 3U)
 Use feedback divider by 2 in divider path.
 

Enumerations

enum  clock_ip_name_t
 Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More...
 
enum  clock_name_t {
  kCLOCK_CoreSysClk,
  kCLOCK_BusClk,
  kCLOCK_ClockOut,
  kCLOCK_FroHf,
  kCLOCK_Fro12M,
  kCLOCK_ExtClk,
  kCLOCK_PllOut,
  kCLOCK_WdtOsc,
  kCLOCK_Frg,
  kCLOCK_AsyncApbClk,
  kCLOCK_FlexI2S
}
 Clock name used to get clock frequency. More...
 
enum  async_clock_src_t {
  kCLOCK_AsyncMainClk = 0,
  kCLOCK_AsyncFro12Mhz
}
 
enum  clock_flashtim_t {
  kCLOCK_Flash1Cycle = 0,
  kCLOCK_Flash2Cycle,
  kCLOCK_Flash3Cycle,
  kCLOCK_Flash4Cycle,
  kCLOCK_Flash5Cycle,
  kCLOCK_Flash6Cycle,
  kCLOCK_Flash7Cycle
}
 FLASH Access time definitions. More...
 
enum  ss_progmodfm_t {
  kSS_MF_512 = (0 << 20),
  kSS_MF_384 = (1 << 20),
  kSS_MF_256 = (2 << 20),
  kSS_MF_128 = (3 << 20),
  kSS_MF_64 = (4 << 20),
  kSS_MF_32 = (5 << 20),
  kSS_MF_24 = (6 << 20),
  kSS_MF_16 = (7 << 20)
}
 PLL Spread Spectrum (SS) Programmable modulation frequency See (MF) field in the SYSPLLSSCTRL1 register in the UM. More...
 
enum  ss_progmoddp_t {
  kSS_MR_K0 = (0 << 23),
  kSS_MR_K1 = (1 << 23),
  kSS_MR_K1_5 = (2 << 23),
  kSS_MR_K2 = (3 << 23),
  kSS_MR_K3 = (4 << 23),
  kSS_MR_K4 = (5 << 23),
  kSS_MR_K6 = (6 << 23),
  kSS_MR_K8 = (7 << 23)
}
 PLL Spread Spectrum (SS) Programmable frequency modulation depth See (MR) field in the SYSPLLSSCTRL1 register in the UM. More...
 
enum  ss_modwvctrl_t {
  kSS_MC_NOC = (0 << 26),
  kSS_MC_RECC = (2 << 26),
  kSS_MC_MAXC = (3 << 26)
}
 PLL Spread Spectrum (SS) Modulation waveform control See (MC) field in the SYSPLLSSCTRL1 register in the UM. More...
 
enum  pll_error_t {
  kStatus_PLL_Success = MAKE_STATUS(kStatusGroup_Generic, 0),
  kStatus_PLL_OutputTooLow = MAKE_STATUS(kStatusGroup_Generic, 1),
  kStatus_PLL_OutputTooHigh = MAKE_STATUS(kStatusGroup_Generic, 2),
  kStatus_PLL_InputTooLow = MAKE_STATUS(kStatusGroup_Generic, 3),
  kStatus_PLL_InputTooHigh = MAKE_STATUS(kStatusGroup_Generic, 4),
  kStatus_PLL_OutsideIntLimit = MAKE_STATUS(kStatusGroup_Generic, 5)
}
 PLL status definitions. More...
 
enum  clock_usb_src_t {
  kCLOCK_UsbSrcFro = (uint32_t)kCLOCK_FroHf,
  kCLOCK_UsbSrcSystemPll = (uint32_t)kCLOCK_PllOut,
  kCLOCK_UsbSrcMainClock = (uint32_t)kCLOCK_CoreSysClk,
  kCLOCK_UsbSrcNone
}
 USB clock source definition. More...
 

Functions

static void CLOCK_SetFLASHAccessCycles (clock_flashtim_t clks)
 Set FLASH memory access time in clocks. More...
 
status_t CLOCK_SetupFROClocking (uint32_t iFreq)
 Initialize the Core clock to given frequency (12, 48 or 96 MHz). Turns on FRO and uses default CCO, if freq is 12000000, then high speed output is off, else high speed output is enabled. More...
 
void CLOCK_AttachClk (clock_attach_id_t connection)
 Configure the clock selection muxes. More...
 
clock_attach_id_t CLOCK_GetClockAttachId (clock_attach_id_t attachId)
 Get the actual clock attach id. This fuction uses the offset in input attach id, then it reads the actual source value in the register and combine the offset to obtain an actual attach id. More...
 
void CLOCK_SetClkDiv (clock_div_name_t div_name, uint32_t divided_by_value, bool reset)
 Setup peripheral clock dividers. More...
 
void CLOCK_SetFLASHAccessCyclesForFreq (uint32_t iFreq)
 Set the flash wait states for the input freuqency. More...
 
uint32_t CLOCK_GetFreq (clock_name_t clockName)
 Return Frequency of selected clock. More...
 
uint32_t CLOCK_GetFRGInputClock (void)
 Return Input frequency for the Fractional baud rate generator. More...
 
uint32_t CLOCK_SetFRGClock (uint32_t freq)
 Set output of the Fractional baud rate generator. More...
 
uint32_t CLOCK_GetFro12MFreq (void)
 Return Frequency of FRO 12MHz. More...
 
uint32_t CLOCK_GetExtClkFreq (void)
 Return Frequency of External Clock. More...
 
uint32_t CLOCK_GetWdtOscFreq (void)
 Return Frequency of Watchdog Oscillator. More...
 
uint32_t CLOCK_GetFroHfFreq (void)
 Return Frequency of High-Freq output of FRO. More...
 
uint32_t CLOCK_GetPllOutFreq (void)
 Return Frequency of PLL. More...
 
uint32_t CLOCK_GetOsc32KFreq (void)
 Return Frequency of 32kHz osc. More...
 
uint32_t CLOCK_GetCoreSysClkFreq (void)
 Return Frequency of Core System. More...
 
uint32_t CLOCK_GetI2SMClkFreq (void)
 Return Frequency of I2S MCLK Clock. More...
 
uint32_t CLOCK_GetFlexCommClkFreq (uint32_t id)
 Return Frequency of Flexcomm functional Clock. More...
 
uint32_t CLOCK_GetUsbClkFreq (void)
 brief Return Frequency of Usb Clock return Frequency of Usb Clock.
 
uint32_t CLOCK_GetAdcClkFreq (void)
 Return Frequency of Adc Clock. More...
 
uint32_t CLOCK_GetClockOutClkFreq (void)
 Return Frequency of ClockOut. More...
 
__STATIC_INLINE async_clock_src_t CLOCK_GetAsyncApbClkSrc (void)
 Return Asynchronous APB Clock source. More...
 
uint32_t CLOCK_GetAsyncApbClkFreq (void)
 Return Frequency of Asynchronous APB Clock. More...
 
uint32_t CLOCK_GetSystemPLLInClockRate (void)
 Return System PLL input clock rate. More...
 
uint32_t CLOCK_GetSystemPLLOutClockRate (bool recompute)
 Return System PLL output clock rate. More...
 
__STATIC_INLINE void CLOCK_SetBypassPLL (bool bypass)
 Enables and disables PLL bypass mode. More...
 
__STATIC_INLINE bool CLOCK_IsSystemPLLLocked (void)
 Check if PLL is locked or not. More...
 
void CLOCK_SetStoredPLLClockRate (uint32_t rate)
 Store the current PLL rate. More...
 
uint32_t CLOCK_GetSystemPLLOutFromSetup (pll_setup_t *pSetup)
 Return System PLL output clock rate from setup structure. More...
 
pll_error_t CLOCK_SetupPLLData (pll_config_t *pControl, pll_setup_t *pSetup)
 Set PLL output based on the passed PLL setup data. More...
 
pll_error_t CLOCK_SetupSystemPLLPrec (pll_setup_t *pSetup, uint32_t flagcfg)
 Set PLL output from PLL setup structure (precise frequency) More...
 
pll_error_t CLOCK_SetPLLFreq (const pll_setup_t *pSetup)
 Set PLL output from PLL setup structure (precise frequency) More...
 
void CLOCK_SetupSystemPLLMult (uint32_t multiply_by, uint32_t input_freq)
 Set PLL output based on the multiplier and input frequency. More...
 
static void CLOCK_DisableUsbfs0Clock (void)
 Disable USB FS clock. More...
 

Driver version

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 4, 1))
 CLOCK driver version 2.4.1. More...
 

Data Structure Documentation

struct pll_config_t

This structure can be used to configure the settings for a PLL setup structure. Fill in the desired configuration for the PLL and call the PLL setup function to fill in a PLL setup structure.

Data Fields

uint32_t desiredRate
 Desired PLL rate in Hz.
 
uint32_t inputRate
 PLL input clock in Hz, only used if PLL_CONFIGFLAG_USEINRATE flag is set.
 
uint32_t flags
 PLL configuration flags, Or'ed value of PLL_CONFIGFLAG_* definitions.
 
ss_progmodfm_t ss_mf
 SS Programmable modulation frequency, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag.
 
ss_progmoddp_t ss_mr
 SS Programmable frequency modulation depth, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag.
 
ss_modwvctrl_t ss_mc
 SS Modulation waveform control, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag.
 
bool mfDither
 false for fixed modulation frequency or true for dithering, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag
 
struct pll_setup_t

It can be populated with the PLL setup function. If powering up or waiting for PLL lock, the PLL input clock source should be configured prior to PLL setup.

Data Fields

uint32_t syspllctrl
 PLL control register SYSPLLCTRL.
 
uint32_t syspllndec
 PLL NDEC register SYSPLLNDEC.
 
uint32_t syspllpdec
 PLL PDEC register SYSPLLPDEC.
 
uint32_t syspllssctrl [2]
 PLL SSCTL registers SYSPLLSSCTRL.
 
uint32_t pllRate
 Acutal PLL rate.
 
uint32_t flags
 PLL setup flags, Or'ed value of PLL_SETUPFLAG_* definitions.
 

Macro Definition Documentation

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 4, 1))
#define CLOCK_USR_CFG_PLL_CONFIG_CACHE_COUNT   2U

Once define this MACRO to be non-zero value, CLOCK_PllGetConfig() function would cache the recent calulation and accelerate the execution to get the right settings.

#define FLEXCOMM_CLOCKS
Value:
{ \
kCLOCK_FlexComm0, kCLOCK_FlexComm1, kCLOCK_FlexComm2, kCLOCK_FlexComm3, kCLOCK_FlexComm4, kCLOCK_FlexComm5, \
kCLOCK_FlexComm6, kCLOCK_FlexComm7 \
}
#define LPUART_CLOCKS
Value:
{ \
kCLOCK_MinUart0, kCLOCK_MinUart1, kCLOCK_MinUart2, kCLOCK_MinUart3, kCLOCK_MinUart4, kCLOCK_MinUart5, \
kCLOCK_MinUart6, kCLOCK_MinUart7 \
}
#define BI2C_CLOCKS
Value:
{ \
kCLOCK_BI2c0, kCLOCK_BI2c1, kCLOCK_BI2c2, kCLOCK_BI2c3, kCLOCK_BI2c4, kCLOCK_BI2c5, kCLOCK_BI2c6, kCLOCK_BI2c7 \
}
#define LPSI_CLOCKS
Value:
{ \
kCLOCK_LSpi0, kCLOCK_LSpi1, kCLOCK_LSpi2, kCLOCK_LSpi3, kCLOCK_LSpi4, kCLOCK_LSpi5, kCLOCK_LSpi6, kCLOCK_LSpi7 \
}
#define FLEXI2S_CLOCKS
Value:
{ \
kCLOCK_FlexI2s0, kCLOCK_FlexI2s1, kCLOCK_FlexI2s2, kCLOCK_FlexI2s3, kCLOCK_FlexI2s4, kCLOCK_FlexI2s5, \
kCLOCK_FlexI2s6, kCLOCK_FlexI2s7 \
}
#define UTICK_CLOCKS
Value:
{ \
kCLOCK_Utick \
}
#define DMA_CLOCKS
Value:
{ \
kCLOCK_Dma \
}
#define CTIMER_CLOCKS
Value:
{ \
kCLOCK_Ctimer0, kCLOCK_Ctimer1, kCLOCK_Ctimer3 \
}
#define GPIO_CLOCKS
Value:
{ \
kCLOCK_Gpio0, kCLOCK_Gpio1 \
}
#define ADC_CLOCKS
Value:
{ \
kCLOCK_Adc0 \
}
#define MRT_CLOCKS
Value:
{ \
kCLOCK_Mrt \
}
#define SCT_CLOCKS
Value:
{ \
kCLOCK_Sct0 \
}
#define RTC_CLOCKS
Value:
{ \
kCLOCK_Rtc \
}
#define WWDT_CLOCKS
Value:
{ \
kCLOCK_Wwdt \
}
#define CRC_CLOCKS
Value:
{ \
kCLOCK_Crc \
}
#define USBD_CLOCKS
Value:
{ \
kCLOCK_Usbd0 \
}
#define GINT_CLOCKS
Value:
{ \
kCLOCK_Gint, kCLOCK_Gint \
}

GINT0 & GINT1 share same slot

#define CLK_GATE_REG_OFFSET_SHIFT   8U
#define CLK_ATTACH_ID (   mux,
  sel,
  pos 
)    ((((uint32_t)(mux) << 0U) | (((uint32_t)(sel) + 1U) & 0xFU) << 8U) << ((pos)*12U))

[4 bits for choice, 0 means invalid choice] [8 bits mux ID]*

#define PLL_CONFIGFLAG_USEINRATE   (1U << 0U)


When the PLL_CONFIGFLAG_USEINRATE flag is selected, the 'InputRate' field in the configuration structure must be assigned with the expected PLL frequency. If the PLL_CONFIGFLAG_USEINRATE is not used, 'InputRate' is ignored in the configuration function and the driver will determine the PLL rate from the currently selected PLL source. This flag might be used to configure the PLL input clock more accurately when using the WDT oscillator or a more dyanmic CLKIN source.

When the PLL_CONFIGFLAG_FORCENOFRACT flag is selected, the PLL hardware for the automatic bandwidth selection, Spread Spectrum (SS) support, and fractional M-divider are not used.
Flag to use InputRate in PLL configuration structure for setup

#define PLL_SETUPFLAG_POWERUP   (1U << 0U)

Setup will power on the PLL after setup

Enumeration Type Documentation

Enumerator
kCLOCK_CoreSysClk 

Core/system clock (aka MAIN_CLK)

kCLOCK_BusClk 

Bus clock (AHB clock)

kCLOCK_ClockOut 

CLOCKOUT.

kCLOCK_FroHf 

FRO48/96.

kCLOCK_Fro12M 

FRO12M.

kCLOCK_ExtClk 

External Clock.

kCLOCK_PllOut 

PLL Output.

kCLOCK_WdtOsc 

Watchdog Oscillator.

kCLOCK_Frg 

Frg Clock.

kCLOCK_AsyncApbClk 

Async APB clock.

kCLOCK_FlexI2S 

FlexI2S clock.

Clock source selections for the asynchronous APB clock

Enumerator
kCLOCK_AsyncMainClk 

Main System clock.

kCLOCK_AsyncFro12Mhz 

12MHz FRO

Enumerator
kCLOCK_Flash1Cycle 

Flash accesses use 1 CPU clock.

kCLOCK_Flash2Cycle 

Flash accesses use 2 CPU clocks.

kCLOCK_Flash3Cycle 

Flash accesses use 3 CPU clocks.

kCLOCK_Flash4Cycle 

Flash accesses use 4 CPU clocks.

kCLOCK_Flash5Cycle 

Flash accesses use 5 CPU clocks.

kCLOCK_Flash6Cycle 

Flash accesses use 6 CPU clocks.

kCLOCK_Flash7Cycle 

Flash accesses use 7 CPU clocks.

Enumerator
kSS_MF_512 

Nss = 512 (fm ? 3.9 - 7.8 kHz)

kSS_MF_384 

Nss ?= 384 (fm ? 5.2 - 10.4 kHz)

kSS_MF_256 

Nss = 256 (fm ? 7.8 - 15.6 kHz)

kSS_MF_128 

Nss = 128 (fm ? 15.6 - 31.3 kHz)

kSS_MF_64 

Nss = 64 (fm ? 32.3 - 64.5 kHz)

kSS_MF_32 

Nss = 32 (fm ? 62.5- 125 kHz)

kSS_MF_24 

Nss ?= 24 (fm ? 83.3- 166.6 kHz)

kSS_MF_16 

Nss = 16 (fm ? 125- 250 kHz)

Enumerator
kSS_MR_K0 

k = 0 (no spread spectrum)

kSS_MR_K1 

k = 1

kSS_MR_K1_5 

k = 1.5

kSS_MR_K2 

k = 2

kSS_MR_K3 

k = 3

kSS_MR_K4 

k = 4

kSS_MR_K6 

k = 6

kSS_MR_K8 

k = 8


Compensation for low pass filtering of the PLL to get a triangular modulation at the output of the PLL, giving a flat frequency spectrum.

Enumerator
kSS_MC_NOC 

no compensation

kSS_MC_RECC 

recommended setting

kSS_MC_MAXC 

max.

compensation

Enumerator
kStatus_PLL_Success 

PLL operation was successful.

kStatus_PLL_OutputTooLow 

PLL output rate request was too low.

kStatus_PLL_OutputTooHigh 

PLL output rate request was too high.

kStatus_PLL_InputTooLow 

PLL input rate is too low.

kStatus_PLL_InputTooHigh 

PLL input rate is too high.

kStatus_PLL_OutsideIntLimit 

Requested output rate isn't possible.

Enumerator
kCLOCK_UsbSrcFro 

Use FRO 96 or 48 MHz.

kCLOCK_UsbSrcSystemPll 

Use System PLL output.

kCLOCK_UsbSrcMainClock 

Use Main clock.

kCLOCK_UsbSrcNone 

Use None, this may be selected in order to reduce power when no output is needed.

Function Documentation

static void CLOCK_SetFLASHAccessCycles ( clock_flashtim_t  clks)
inlinestatic
Parameters
clks: Clock cycles for FLASH access
Returns
Nothing
status_t CLOCK_SetupFROClocking ( uint32_t  iFreq)
Parameters
iFreq: Desired frequency (must be one of CLK_FRO_12MHZ or CLK_FRO_48MHZ or CLK_FRO_96MHZ)
Returns
returns success or fail status.
void CLOCK_AttachClk ( clock_attach_id_t  connection)
Parameters
connection: Clock to be configured.
Returns
Nothing
clock_attach_id_t CLOCK_GetClockAttachId ( clock_attach_id_t  attachId)
Parameters
attachId: Clock attach id to get.
Returns
Clock source value.
void CLOCK_SetClkDiv ( clock_div_name_t  div_name,
uint32_t  divided_by_value,
bool  reset 
)
Parameters
div_name: Clock divider name
divided_by_value,:Value to be divided
reset: Whether to reset the divider counter.
Returns
Nothing
void CLOCK_SetFLASHAccessCyclesForFreq ( uint32_t  iFreq)
Parameters
iFreq: Input frequency
Returns
Nothing
uint32_t CLOCK_GetFreq ( clock_name_t  clockName)
Returns
Frequency of selected clock
uint32_t CLOCK_GetFRGInputClock ( void  )
Returns
Input Frequency for FRG
uint32_t CLOCK_SetFRGClock ( uint32_t  freq)
Parameters
freq: Desired output frequency
Returns
Error Code 0 - fail 1 - success
uint32_t CLOCK_GetFro12MFreq ( void  )
Returns
Frequency of FRO 12MHz
uint32_t CLOCK_GetExtClkFreq ( void  )
Returns
Frequency of External Clock. If no external clock is used returns 0.
uint32_t CLOCK_GetWdtOscFreq ( void  )
Returns
Frequency of Watchdog Oscillator
uint32_t CLOCK_GetFroHfFreq ( void  )
Returns
Frequency of High-Freq output of FRO
uint32_t CLOCK_GetPllOutFreq ( void  )
Returns
Frequency of PLL
uint32_t CLOCK_GetOsc32KFreq ( void  )
Returns
Frequency of 32kHz osc
uint32_t CLOCK_GetCoreSysClkFreq ( void  )
Returns
Frequency of Core System
uint32_t CLOCK_GetI2SMClkFreq ( void  )
Returns
Frequency of I2S MCLK Clock
uint32_t CLOCK_GetFlexCommClkFreq ( uint32_t  id)
Returns
Frequency of Flexcomm functional Clock
uint32_t CLOCK_GetAdcClkFreq ( void  )
Returns
Frequency of Adc Clock.
uint32_t CLOCK_GetClockOutClkFreq ( void  )
Returns
Frequency of ClockOut
__STATIC_INLINE async_clock_src_t CLOCK_GetAsyncApbClkSrc ( void  )
Returns
Asynchronous APB CLock source
uint32_t CLOCK_GetAsyncApbClkFreq ( void  )
Returns
Frequency of Asynchronous APB Clock Clock
uint32_t CLOCK_GetSystemPLLInClockRate ( void  )
Returns
System PLL input clock rate
uint32_t CLOCK_GetSystemPLLOutClockRate ( bool  recompute)
Parameters
recompute: Forces a PLL rate recomputation if true
Returns
System PLL output clock rate
Note
The PLL rate is cached in the driver in a variable as the rate computation function can take some time to perform. It is recommended to use 'false' with the 'recompute' parameter.
__STATIC_INLINE void CLOCK_SetBypassPLL ( bool  bypass)

bypass : true to bypass PLL (PLL output = PLL input, false to disable bypass

Returns
System PLL output clock rate
__STATIC_INLINE bool CLOCK_IsSystemPLLLocked ( void  )
Returns
true if the PLL is locked, false if not locked
void CLOCK_SetStoredPLLClockRate ( uint32_t  rate)
Parameters
rate,:Current rate of the PLL
Returns
Nothing
uint32_t CLOCK_GetSystemPLLOutFromSetup ( pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to a PLL setup structure
Returns
System PLL output clock rate calculated from the setup structure
pll_error_t CLOCK_SetupPLLData ( pll_config_t *  pControl,
pll_setup_t *  pSetup 
)
Parameters
pControl: Pointer to populated PLL control structure to generate setup with
pSetup: Pointer to PLL setup structure to be filled
Returns
PLL_ERROR_SUCCESS on success, or PLL setup error code
Note
Actual frequency for setup may vary from the desired frequency based on the accuracy of input clocks, rounding, non-fractional PLL mode, etc.
pll_error_t CLOCK_SetupSystemPLLPrec ( pll_setup_t *  pSetup,
uint32_t  flagcfg 
)
Parameters
pSetup: Pointer to populated PLL setup structure
flagcfg: Flag configuration for PLL config structure
Returns
PLL_ERROR_SUCCESS on success, or PLL setup error code
Note
This function will power off the PLL, setup the PLL with the new setup data, and then optionally powerup the PLL, wait for PLL lock, and adjust system voltages to the new PLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
pll_error_t CLOCK_SetPLLFreq ( const pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to populated PLL setup structure
Returns
kStatus_PLL_Success on success, or PLL setup error code
Note
This function will power off the PLL, setup the PLL with the new setup data, and then optionally powerup the PLL, wait for PLL lock, and adjust system voltages to the new PLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
void CLOCK_SetupSystemPLLMult ( uint32_t  multiply_by,
uint32_t  input_freq 
)
Parameters
multiply_by: multiplier
input_freq: Clock input frequency of the PLL
Returns
Nothing
Note
Unlike the Chip_Clock_SetupSystemPLLPrec() function, this function does not disable or enable PLL power, wait for PLL lock, or adjust system voltages. These must be done in the application. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
static void CLOCK_DisableUsbfs0Clock ( void  )
inlinestatic

Disable USB FS clock.