MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
INPUTMUX: Input Multiplexing Driver

Overview

The MCUXpresso SDK provides a driver for the Input multiplexing (INPUTMUX).
It configures the inputs to the pin interrupt block, DMA trigger, and frequency measure function. Once configured, the clock is not needed for the inputmux.

Input Multiplexing Driver operation

INPUTMUX_AttachSignal function configures the specified input

Typical use case

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/inputmux

Files

file  fsl_inputmux.h
 
file  fsl_inputmux_connections.h
 

Functions

void INPUTMUX_Init (INPUTMUX_Type *base)
 Initialize INPUTMUX peripheral. More...
 
void INPUTMUX_AttachSignal (INPUTMUX_Type *base, uint32_t index, inputmux_connection_t connection)
 Attaches a signal. More...
 
void INPUTMUX_Deinit (INPUTMUX_Type *base)
 Deinitialize INPUTMUX peripheral. More...
 

Input multiplexing connections

enum  inputmux_connection_t {
  kINPUTMUX_AdcASeqaIrqToDma = 0U + (DMA_ITRIG_INMUX_ID << PMUX_SHIFT) ,
  kINPUTMUX_DmaTriggerMux1ToDma = 8U + (DMA_ITRIG_INMUX_ID << PMUX_SHIFT) ,
  kINPUTMUX_DmaChannel17TrigoutToTriginChannels = 17U + (DMA_OTRIG_PMUX_ID << PMUX_SHIFT)
}
 INPUTMUX connections type. More...
 
#define DMA_ITRIG_INMUX_ID   0x00U
 Periphinmux IDs.
 
#define DMA_OTRIG_PMUX_ID   0x4000U
 
#define SCT0_INMUX_ID   0x4020U
 
#define PMUX_SHIFT   16U
 

Driver version

#define FSL_INPUTMUX_DRIVER_VERSION   (MAKE_VERSION(2, 0, 3))
 Group interrupt driver version for SDK.
 

Enumeration Type Documentation

Enumerator
kINPUTMUX_AdcASeqaIrqToDma 

DMA ITRIG INMUX.

kINPUTMUX_DmaTriggerMux1ToDma 

DMA INMUX.

kINPUTMUX_DmaChannel17TrigoutToTriginChannels 

SCT INMUX.

Function Documentation

void INPUTMUX_Init ( INPUTMUX_Type *  base)

This function enables the INPUTMUX clock.

Parameters
baseBase address of the INPUTMUX peripheral.
Return values
None.
void INPUTMUX_AttachSignal ( INPUTMUX_Type *  base,
uint32_t  index,
inputmux_connection_t  connection 
)

This function gates the INPUTPMUX clock.

Parameters
baseBase address of the INPUTMUX peripheral.
indexDestination peripheral to attach the signal to.
connectionSelects connection.
Return values
None.
void INPUTMUX_Deinit ( INPUTMUX_Type *  base)

This function disables the INPUTMUX clock.

Parameters
baseBase address of the INPUTMUX peripheral.
Return values
None.