The MCUXpresso SDK provides a peripheral driver for the Segment LCD (SLCD) module of MCUXpresso SDK devices. The SLCD module is a CMOS charge pump voltage inverter that is designed for low voltage and low-power operation. SLCD is designed to generate the appropriate waveforms to drive multiplexed numeric, alphanumeric, or custom segment LCD panels. SLCD also has several timing and control settings that can be software-configured depending on the application's requirements. Timing and control consists of registers and control logic for the following:
- LCD frame frequency
- Duty cycle selection
- Front plane/back plane selection and enabling
- Blink modes and frequency
- Operation in low-power modes
Plane Setting and Display Control
After the SLCD general initialization, the SLCD_SetBackPlanePhase(), SLCD_SetFrontPlaneSegments(), and SLCD_SetFrontPlaneOnePhase() are used to set the special back/front Plane to make SLCD display correctly. Then, the independent display control APIs, SLCD_StartDisplay() and SLCD_StopDisplay(), start and stop the SLCD display.
The SLCD_StartBlinkMode() and SLCD_StopBlinkMode() are provided for the runtime special blink mode control. To get the SLCD fault detection result, call the SLCD_GetFaultDetectCounter().
Typical use case
SLCD Initialization operation
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/slcd
|
enum | slcd_power_supply_option_t {
kSLCD_InternalVll3UseChargePump,
kSLCD_ExternalVll3UseResistorBiasNetwork,
kSLCD_ExteranlVll3UseChargePump,
kSLCD_InternalVll1UseChargePump
} |
| SLCD power supply option. More...
|
|
enum | slcd_regulated_voltage_trim_t {
kSLCD_RegulatedVolatgeTrim00 = 0U,
kSLCD_RegulatedVolatgeTrim01,
kSLCD_RegulatedVolatgeTrim02,
kSLCD_RegulatedVolatgeTrim03,
kSLCD_RegulatedVolatgeTrim04,
kSLCD_RegulatedVolatgeTrim05,
kSLCD_RegulatedVolatgeTrim06,
kSLCD_RegulatedVolatgeTrim07,
kSLCD_RegulatedVolatgeTrim08,
kSLCD_RegulatedVolatgeTrim09,
kSLCD_RegulatedVolatgeTrim10,
kSLCD_RegulatedVolatgeTrim11,
kSLCD_RegulatedVolatgeTrim12,
kSLCD_RegulatedVolatgeTrim13,
kSLCD_RegulatedVolatgeTrim14,
kSLCD_RegulatedVolatgeTrim15
} |
| SLCD regulated voltage trim parameter, be used to meet the desired contrast. More...
|
|
enum | slcd_load_adjust_t {
kSLCD_LowLoadOrFastestClkSrc = 0U,
kSLCD_LowLoadOrIntermediateClkSrc,
kSLCD_HighLoadOrIntermediateClkSrc,
kSLCD_HighLoadOrSlowestClkSrc
} |
| SLCD load adjust to handle different LCD glass capacitance or configure the LCD charge pump clock source. More...
|
|
enum | slcd_clock_src_t {
kSLCD_DefaultClk = 0U,
kSLCD_AlternateClk1 = 1U
} |
| SLCD clock source. More...
|
|
enum | slcd_alt_clock_div_t {
kSLCD_AltClkDivFactor1 = 0U,
kSLCD_AltClkDivFactor64,
kSLCD_AltClkDivFactor256,
kSLCD_AltClkDivFactor512
} |
| SLCD alternate clock divider. More...
|
|
enum | slcd_clock_prescaler_t {
kSLCD_ClkPrescaler00 = 0U,
kSLCD_ClkPrescaler01,
kSLCD_ClkPrescaler02,
kSLCD_ClkPrescaler03,
kSLCD_ClkPrescaler04,
kSLCD_ClkPrescaler05,
kSLCD_ClkPrescaler06,
kSLCD_ClkPrescaler07
} |
| SLCD clock prescaler to generate frame frequency. More...
|
|
enum | slcd_duty_cycle_t {
kSLCD_1Div1DutyCycle = 0U,
kSLCD_1Div2DutyCycle,
kSLCD_1Div3DutyCycle,
kSLCD_1Div4DutyCycle,
kSLCD_1Div5DutyCycle,
kSLCD_1Div6DutyCycle,
kSLCD_1Div7DutyCycle,
kSLCD_1Div8DutyCycle
} |
| SLCD duty cycle. More...
|
|
enum | slcd_phase_type_t {
kSLCD_NoPhaseActivate = 0x00U,
kSLCD_PhaseAActivate = 0x01U,
kSLCD_PhaseBActivate = 0x02U,
kSLCD_PhaseCActivate = 0x04U,
kSLCD_PhaseDActivate = 0x08U,
kSLCD_PhaseEActivate = 0x10U,
kSLCD_PhaseFActivate = 0x20U,
kSLCD_PhaseGActivate = 0x40U,
kSLCD_PhaseHActivate = 0x80U
} |
| SLCD segment phase type. More...
|
|
enum | slcd_phase_index_t {
kSLCD_PhaseAIndex = 0x0U,
kSLCD_PhaseBIndex = 0x1U,
kSLCD_PhaseCIndex = 0x2U,
kSLCD_PhaseDIndex = 0x3U,
kSLCD_PhaseEIndex = 0x4U,
kSLCD_PhaseFIndex = 0x5U,
kSLCD_PhaseGIndex = 0x6U,
kSLCD_PhaseHIndex = 0x7U
} |
| SLCD segment phase bit index. More...
|
|
enum | slcd_display_mode_t {
kSLCD_NormalMode = 0U,
kSLCD_AlternateMode,
kSLCD_BlankMode
} |
| SLCD display mode. More...
|
|
enum | slcd_blink_mode_t {
kSLCD_BlankDisplayBlink = 0U,
kSLCD_AltDisplayBlink
} |
| SLCD blink mode. More...
|
|
enum | slcd_blink_rate_t {
kSLCD_BlinkRate00 = 0U,
kSLCD_BlinkRate01,
kSLCD_BlinkRate02,
kSLCD_BlinkRate03,
kSLCD_BlinkRate04,
kSLCD_BlinkRate05,
kSLCD_BlinkRate06,
kSLCD_BlinkRate07
} |
| SLCD blink rate. More...
|
|
enum | slcd_fault_detect_clock_prescaler_t {
kSLCD_FaultSampleFreqDivider1 = 0U,
kSLCD_FaultSampleFreqDivider2,
kSLCD_FaultSampleFreqDivider4,
kSLCD_FaultSampleFreqDivider8,
kSLCD_FaultSampleFreqDivider16,
kSLCD_FaultSampleFreqDivider32,
kSLCD_FaultSampleFreqDivider64,
kSLCD_FaultSampleFreqDivider128
} |
| SLCD fault detect clock prescaler. More...
|
|
enum | slcd_fault_detect_sample_window_width_t {
kSLCD_FaultDetectWindowWidth4SampleClk = 0U,
kSLCD_FaultDetectWindowWidth8SampleClk,
kSLCD_FaultDetectWindowWidth16SampleClk,
kSLCD_FaultDetectWindowWidth32SampleClk,
kSLCD_FaultDetectWindowWidth64SampleClk,
kSLCD_FaultDetectWindowWidth128SampleClk,
kSLCD_FaultDetectWindowWidth256SampleClk,
kSLCD_FaultDetectWindowWidth512SampleClk
} |
| SLCD fault detect sample window width. More...
|
|
enum | slcd_interrupt_enable_t { kSLCD_FaultDetectCompleteInterrupt = 1U
} |
| SLCD interrupt source. More...
|
|
enum | slcd_lowpower_behavior {
kSLCD_EnabledInWaitStop = 0,
kSLCD_EnabledInWaitOnly,
kSLCD_EnabledInStopOnly,
kSLCD_DisabledInWaitStop
} |
| SLCD behavior in low power mode. More...
|
|
|
void | SLCD_Init (LCD_Type *base, slcd_config_t *configure) |
| Initializes the SLCD, ungates the module clock, initializes the power setting, enables all used plane pins, and sets with interrupt and work mode with the configuration. More...
|
|
void | SLCD_Deinit (LCD_Type *base) |
| Deinitializes the SLCD module, gates the module clock, disables an interrupt, and displays the SLCD. More...
|
|
void | SLCD_GetDefaultConfig (slcd_config_t *configure) |
| Gets the SLCD default configuration structure. More...
|
|
|
static void | SLCD_StartDisplay (LCD_Type *base) |
| Enables the SLCD controller, starts generation, and displays the front plane and back plane waveform. More...
|
|
static void | SLCD_StopDisplay (LCD_Type *base) |
| Stops the SLCD controller. More...
|
|
void | SLCD_StartBlinkMode (LCD_Type *base, slcd_blink_mode_t mode, slcd_blink_rate_t rate) |
| Starts the SLCD blink mode. More...
|
|
static void | SLCD_StopBlinkMode (LCD_Type *base) |
| Stops the SLCD blink mode. More...
|
|
static void | SLCD_SetBackPlanePhase (LCD_Type *base, uint32_t pinIndx, slcd_phase_type_t phase) |
| Sets the SLCD back plane pin phase. More...
|
|
static void | SLCD_SetFrontPlaneSegments (LCD_Type *base, uint32_t pinIndx, uint8_t operation) |
| Sets the SLCD front plane segment operation for a front plane pin. More...
|
|
static void | SLCD_SetFrontPlaneOnePhase (LCD_Type *base, uint32_t pinIndx, slcd_phase_index_t phaseIndx, bool enable) |
| Sets one SLCD front plane pin for one phase. More...
|
|
static uint32_t | SLCD_GetFaultDetectCounter (LCD_Type *base) |
| Gets the SLCD fault detect counter. More...
|
|
struct slcd_fault_detect_config_t |
bool slcd_fault_detect_config_t::faultDetectIntEnable |
bool slcd_fault_detect_config_t::faultDetectBackPlaneEnable |
uint8_t slcd_fault_detect_config_t::faultDetectPinIndex |
struct slcd_clock_config_t |
"slcd_clock_src_t" is recommended to be used. The SLCD is optimized to operate using a 32.768kHz clock input.
uint32_t slcd_config_t::slcdLowPinEnabled |
Setting bit n to 1 means enable pin n.
uint32_t slcd_config_t::slcdHighPinEnabled |
Setting bit n to 1 means enable pin (n + 32).
uint32_t slcd_config_t::backPlaneLowPin |
Setting bit n to 1 means setting pin n as back plane. It should never have the same bit setting as the frontPlane Pin.
uint32_t slcd_config_t::backPlaneHighPin |
Setting bit n to 1 means setting pin (n + 32) as back plane. It should never have the same bit setting as the frontPlane Pin.
If not requirement, set to NULL.
Enumerator |
---|
kSLCD_InternalVll3UseChargePump |
VLL3 connected to VDD internally, charge pump is used to generate VLL1 and VLL2.
|
kSLCD_ExternalVll3UseResistorBiasNetwork |
VLL3 is driven externally and resistor bias network is used to generate VLL1 and VLL2.
|
kSLCD_ExteranlVll3UseChargePump |
VLL3 is driven externally and charge pump is used to generate VLL1 and VLL2.
|
kSLCD_InternalVll1UseChargePump |
VIREG is connected to VLL1 internally and charge pump is used to generate VLL2 and VLL3.
|
Enumerator |
---|
kSLCD_RegulatedVolatgeTrim00 |
Increase the voltage to 0.91 V.
|
kSLCD_RegulatedVolatgeTrim01 |
Increase the voltage to 1.01 V.
|
kSLCD_RegulatedVolatgeTrim02 |
Increase the voltage to 0.96 V.
|
kSLCD_RegulatedVolatgeTrim03 |
Increase the voltage to 1.06 V.
|
kSLCD_RegulatedVolatgeTrim04 |
Increase the voltage to 0.93 V.
|
kSLCD_RegulatedVolatgeTrim05 |
Increase the voltage to 1.02 V.
|
kSLCD_RegulatedVolatgeTrim06 |
Increase the voltage to 0.98 V.
|
kSLCD_RegulatedVolatgeTrim07 |
Increase the voltage to 1.08 V.
|
kSLCD_RegulatedVolatgeTrim08 |
Increase the voltage to 0.92 V.
|
kSLCD_RegulatedVolatgeTrim09 |
Increase the voltage to 1.02 V.
|
kSLCD_RegulatedVolatgeTrim10 |
Increase the voltage to 0.97 V.
|
kSLCD_RegulatedVolatgeTrim11 |
Increase the voltage to 1.07 V.
|
kSLCD_RegulatedVolatgeTrim12 |
Increase the voltage to 0.94 V.
|
kSLCD_RegulatedVolatgeTrim13 |
Increase the voltage to 1.05 V.
|
kSLCD_RegulatedVolatgeTrim14 |
Increase the voltage to 0.99 V.
|
kSLCD_RegulatedVolatgeTrim15 |
Increase the voltage to 1.09 V.
|
Adjust the LCD glass capacitance if resistor bias network is enabled: kSLCD_LowLoadOrFastestClkSrc - Low load (LCD glass capacitance 2000pF or lower. LCD or GPIO function can be used on VLL1,VLL2,Vcap1 and Vcap2 pins) kSLCD_LowLoadOrIntermediateClkSrc - low load (LCD glass capacitance 2000pF or lower. LCD or GPIO function can be used on VLL1,VLL2,Vcap1 and Vcap2 pins) kSLCD_HighLoadOrIntermediateClkSrc - high load (LCD glass capacitance 8000pF or lower. LCD or GPIO function can be used on Vcap1 and Vcap2 pins) kSLCD_HighLoadOrSlowestClkSrc - high load (LCD glass capacitance 8000pF or lower LCD or GPIO function can be used on Vcap1 and Vcap2 pins) Adjust clock for charge pump if charge pump is enabled: kSLCD_LowLoadOrFastestClkSrc - Fasten clock source (LCD glass capacitance 8000pF or 4000pF or lower if Fast Frame Rate is set) kSLCD_LowLoadOrIntermediateClkSrc - Intermediate clock source (LCD glass capacitance 4000pF or 2000pF or lower if Fast Frame Rate is set) kSLCD_HighLoadOrIntermediateClkSrc - Intermediate clock source (LCD glass capacitance 2000pF or 1000pF or lower if Fast Frame Rate is set) kSLCD_HighLoadOrSlowestClkSrc - slowest clock source (LCD glass capacitance 1000pF or 500pF or lower if Fast Frame Rate is set)
Enumerator |
---|
kSLCD_LowLoadOrFastestClkSrc |
Adjust in low load or selects fastest clock.
|
kSLCD_LowLoadOrIntermediateClkSrc |
Adjust in low load or selects intermediate clock.
|
kSLCD_HighLoadOrIntermediateClkSrc |
Adjust in high load or selects intermediate clock.
|
kSLCD_HighLoadOrSlowestClkSrc |
Adjust in high load or selects slowest clock.
|
Enumerator |
---|
kSLCD_DefaultClk |
Select default clock ERCLK32K.
|
kSLCD_AlternateClk1 |
Select alternate clock source 1 : MCGIRCLK.
|
Enumerator |
---|
kSLCD_AltClkDivFactor1 |
No divide for alternate clock.
|
kSLCD_AltClkDivFactor64 |
Divide alternate clock with factor 64.
|
kSLCD_AltClkDivFactor256 |
Divide alternate clock with factor 256.
|
kSLCD_AltClkDivFactor512 |
Divide alternate clock with factor 512.
|
Enumerator |
---|
kSLCD_ClkPrescaler00 |
Prescaler 0.
|
kSLCD_ClkPrescaler01 |
Prescaler 1.
|
kSLCD_ClkPrescaler02 |
Prescaler 2.
|
kSLCD_ClkPrescaler03 |
Prescaler 3.
|
kSLCD_ClkPrescaler04 |
Prescaler 4.
|
kSLCD_ClkPrescaler05 |
Prescaler 5.
|
kSLCD_ClkPrescaler06 |
Prescaler 6.
|
kSLCD_ClkPrescaler07 |
Prescaler 7.
|
Enumerator |
---|
kSLCD_1Div1DutyCycle |
LCD use 1 BP 1/1 duty cycle.
|
kSLCD_1Div2DutyCycle |
LCD use 2 BP 1/2 duty cycle.
|
kSLCD_1Div3DutyCycle |
LCD use 3 BP 1/3 duty cycle.
|
kSLCD_1Div4DutyCycle |
LCD use 4 BP 1/4 duty cycle.
|
kSLCD_1Div5DutyCycle |
LCD use 5 BP 1/5 duty cycle.
|
kSLCD_1Div6DutyCycle |
LCD use 6 BP 1/6 duty cycle.
|
kSLCD_1Div7DutyCycle |
LCD use 7 BP 1/7 duty cycle.
|
kSLCD_1Div8DutyCycle |
LCD use 8 BP 1/8 duty cycle.
|
Enumerator |
---|
kSLCD_NoPhaseActivate |
LCD wareform no phase activates.
|
kSLCD_PhaseAActivate |
LCD waveform phase A activates.
|
kSLCD_PhaseBActivate |
LCD waveform phase B activates.
|
kSLCD_PhaseCActivate |
LCD waveform phase C activates.
|
kSLCD_PhaseDActivate |
LCD waveform phase D activates.
|
kSLCD_PhaseEActivate |
LCD waveform phase E activates.
|
kSLCD_PhaseFActivate |
LCD waveform phase F activates.
|
kSLCD_PhaseGActivate |
LCD waveform phase G activates.
|
kSLCD_PhaseHActivate |
LCD waveform phase H activates.
|
Enumerator |
---|
kSLCD_PhaseAIndex |
LCD phase A bit index.
|
kSLCD_PhaseBIndex |
LCD phase B bit index.
|
kSLCD_PhaseCIndex |
LCD phase C bit index.
|
kSLCD_PhaseDIndex |
LCD phase D bit index.
|
kSLCD_PhaseEIndex |
LCD phase E bit index.
|
kSLCD_PhaseFIndex |
LCD phase F bit index.
|
kSLCD_PhaseGIndex |
LCD phase G bit index.
|
kSLCD_PhaseHIndex |
LCD phase H bit index.
|
Enumerator |
---|
kSLCD_NormalMode |
LCD Normal display mode.
|
kSLCD_AlternateMode |
LCD Alternate display mode.
For four back planes or less.
|
kSLCD_BlankMode |
LCD Blank display mode.
|
Enumerator |
---|
kSLCD_BlankDisplayBlink |
Display blank during the blink period.
|
kSLCD_AltDisplayBlink |
Display alternate display during the blink period if duty cycle is lower than 5.
|
Enumerator |
---|
kSLCD_BlinkRate00 |
SLCD blink rate is LCD clock/((2^12)).
|
kSLCD_BlinkRate01 |
SLCD blink rate is LCD clock/((2^13)).
|
kSLCD_BlinkRate02 |
SLCD blink rate is LCD clock/((2^14)).
|
kSLCD_BlinkRate03 |
SLCD blink rate is LCD clock/((2^15)).
|
kSLCD_BlinkRate04 |
SLCD blink rate is LCD clock/((2^16)).
|
kSLCD_BlinkRate05 |
SLCD blink rate is LCD clock/((2^17)).
|
kSLCD_BlinkRate06 |
SLCD blink rate is LCD clock/((2^18)).
|
kSLCD_BlinkRate07 |
SLCD blink rate is LCD clock/((2^19)).
|
Enumerator |
---|
kSLCD_FaultSampleFreqDivider1 |
Fault detect sample clock frequency is 1/1 bus clock.
|
kSLCD_FaultSampleFreqDivider2 |
Fault detect sample clock frequency is 1/2 bus clock.
|
kSLCD_FaultSampleFreqDivider4 |
Fault detect sample clock frequency is 1/4 bus clock.
|
kSLCD_FaultSampleFreqDivider8 |
Fault detect sample clock frequency is 1/8 bus clock.
|
kSLCD_FaultSampleFreqDivider16 |
Fault detect sample clock frequency is 1/16 bus clock.
|
kSLCD_FaultSampleFreqDivider32 |
Fault detect sample clock frequency is 1/32 bus clock.
|
kSLCD_FaultSampleFreqDivider64 |
Fault detect sample clock frequency is 1/64 bus clock.
|
kSLCD_FaultSampleFreqDivider128 |
Fault detect sample clock frequency is 1/128 bus clock.
|
Enumerator |
---|
kSLCD_FaultDetectWindowWidth4SampleClk |
Sample window width is 4 sample clock cycles.
|
kSLCD_FaultDetectWindowWidth8SampleClk |
Sample window width is 8 sample clock cycles.
|
kSLCD_FaultDetectWindowWidth16SampleClk |
Sample window width is 16 sample clock cycles.
|
kSLCD_FaultDetectWindowWidth32SampleClk |
Sample window width is 32 sample clock cycles.
|
kSLCD_FaultDetectWindowWidth64SampleClk |
Sample window width is 64 sample clock cycles.
|
kSLCD_FaultDetectWindowWidth128SampleClk |
Sample window width is 128 sample clock cycles.
|
kSLCD_FaultDetectWindowWidth256SampleClk |
Sample window width is 256 sample clock cycles.
|
kSLCD_FaultDetectWindowWidth512SampleClk |
Sample window width is 512 sample clock cycles.
|
Enumerator |
---|
kSLCD_FaultDetectCompleteInterrupt |
SLCD fault detection complete interrupt source.
|
Enumerator |
---|
kSLCD_EnabledInWaitStop |
SLCD works in wait and stop mode.
|
kSLCD_EnabledInWaitOnly |
SLCD works in wait mode and is disabled in stop mode.
|
kSLCD_EnabledInStopOnly |
SLCD works in stop mode and is disabled in wait mode.
|
kSLCD_DisabledInWaitStop |
SLCD is disabled in stop mode and wait mode.
|
- Parameters
-
base | SLCD peripheral base address. |
configure | SLCD configuration pointer. For the configuration structure, many parameters have the default setting and the SLCD_Getdefaultconfig() is provided to get them. Use it verified for their applications. The others have no default settings, such as "clkConfig", and must be provided by the application before calling the SLCD_Init() API. |
void SLCD_Deinit |
( |
LCD_Type * |
base | ) |
|
- Parameters
-
base | SLCD peripheral base address. |
The purpose of this API is to get default parameters of the configuration structure for the SLCD_Init(). Use these initialized parameters unchanged in SLCD_Init() or modify fields of the structure before the calling SLCD_Init(). All default parameters of the configure structuration are listed.
config.interruptSrc = 0;
config.faultConfig = NULL;
config.frameFreqIntEnable = false;
- Parameters
-
configure | The SLCD configuration structure pointer. |
static void SLCD_StartDisplay |
( |
LCD_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
base | SLCD peripheral base address. |
static void SLCD_StopDisplay |
( |
LCD_Type * |
base | ) |
|
|
inlinestatic |
There is no waveform generator and all enabled pins only output a low value.
- Parameters
-
base | SLCD peripheral base address. |
- Parameters
-
base | SLCD peripheral base address. |
mode | SLCD blink mode. |
rate | SLCD blink rate. |
static void SLCD_StopBlinkMode |
( |
LCD_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
base | SLCD peripheral base address. |
static void SLCD_SetBackPlanePhase |
( |
LCD_Type * |
base, |
|
|
uint32_t |
pinIndx, |
|
|
slcd_phase_type_t |
phase |
|
) |
| |
|
inlinestatic |
This function sets the SLCD back plane pin phase. "kSLCD_PhaseXActivate" setting means the phase X is active for the back plane pin. "kSLCD_NoPhaseActivate" setting means there is no phase active for the back plane pin. For example, set the back plane pin 20 for phase A.
- Parameters
-
base | SLCD peripheral base address. |
pinIndx | SLCD back plane pin index. Range from 0 to 63. |
phase | The phase activates for the back plane pin. |
static void SLCD_SetFrontPlaneSegments |
( |
LCD_Type * |
base, |
|
|
uint32_t |
pinIndx, |
|
|
uint8_t |
operation |
|
) |
| |
|
inlinestatic |
This function sets the SLCD front plane segment on or off operation. Each bit turns on or off the segments associated with the front plane pin in the following pattern: HGFEDCBA (most significant bit controls segment H and least significant bit controls segment A). For example, turn on the front plane pin 20 for phase B and phase C.
- Parameters
-
base | SLCD peripheral base address. |
pinIndx | SLCD back plane pin index. Range from 0 to 63. |
operation | The operation for the segment on the front plane pin. This is a logical OR of the enumeration :: slcd_phase_type_t. |
static void SLCD_SetFrontPlaneOnePhase |
( |
LCD_Type * |
base, |
|
|
uint32_t |
pinIndx, |
|
|
slcd_phase_index_t |
phaseIndx, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
This function can be used to set one phase on or off for the front plane pin. It can be call many times to set the plane pin for different phase indexes. For example, turn on the front plane pin 20 for phase B and phase C.
- Parameters
-
base | SLCD peripheral base address. |
pinIndx | SLCD back plane pin index. Range from 0 to 63. |
phaseIndx | The phase bit index slcd_phase_index_t. |
enable | True to turn on the segment for phaseIndx phase false to turn off the segment for phaseIndx phase. |
static uint32_t SLCD_GetFaultDetectCounter |
( |
LCD_Type * |
base | ) |
|
|
inlinestatic |
This function gets the number of samples inside the fault detection sample window.
- Parameters
-
base | SLCD peripheral base address. |
- Returns
- The fault detect counter. The maximum return value is 255. If the maximum 255 returns, the overflow may happen. Reconfigure the fault detect sample window and fault detect clock prescaler for proper sampling.
void SLCD_EnableInterrupts |
( |
LCD_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
For example, to enable fault detect complete interrupt and frame frequency interrupt, for FSL_FEATURE_SLCD_HAS_FRAME_FREQUENCY_INTERRUPT enabled case, do the following.
- Parameters
-
base | SLCD peripheral base address. |
mask | SLCD interrupts to enable. This is a logical OR of the enumeration :: slcd_interrupt_enable_t. |
void SLCD_DisableInterrupts |
( |
LCD_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
For example, to disable fault detect complete interrupt and frame frequency interrupt, for FSL_FEATURE_SLCD_HAS_FRAME_FREQUENCY_INTERRUPT enabled case, do the following.
- Parameters
-
base | SLCD peripheral base address. |
mask | SLCD interrupts to disable. This is a logical OR of the enumeration :: slcd_interrupt_enable_t. |
uint32_t SLCD_GetInterruptStatus |
( |
LCD_Type * |
base | ) |
|
- Parameters
-
base | SLCD peripheral base address. |
- Returns
- The event status of the interrupt source. This is the logical OR of members of the enumeration :: slcd_interrupt_enable_t.
void SLCD_ClearInterruptStatus |
( |
LCD_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
- Parameters
-
base | SLCD peripheral base address. |
mask | SLCD interrupt source to be cleared. This is the logical OR of members of the enumeration :: slcd_interrupt_enable_t. |