MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
DMA: Direct Memory Access Controller Driver

Overview

The MCUXpresso SDK provides a peripheral driver for the Direct Memory Access (DMA) of MCUXpresso SDK devices.

Typical use case

DMA Operation

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/dma

Files

file  fsl_dma.h
 

Data Structures

struct  dma_descriptor_t
 DMA descriptor structure. More...
 
struct  dma_xfercfg_t
 DMA transfer configuration. More...
 
struct  dma_channel_trigger_t
 DMA channel trigger. More...
 
struct  dma_channel_config_t
 DMA channel trigger. More...
 
struct  dma_transfer_config_t
 DMA transfer configuration. More...
 
struct  dma_handle_t
 DMA transfer handle structure. More...
 

Macros

#define DMA_MAX_TRANSFER_COUNT   0x400U
 DMA max transfer size.
 
#define FSL_FEATURE_DMA_NUMBER_OF_CHANNELSn(x)   FSL_FEATURE_DMA_NUMBER_OF_CHANNELS
 DMA channel numbers.
 
#define FSL_FEATURE_DMA_LINK_DESCRIPTOR_ALIGN_SIZE   (16U)
 DMA head link descriptor table align size.
 
#define DMA_ALLOCATE_HEAD_DESCRIPTORS(name, number)   SDK_ALIGN(dma_descriptor_t name[number], FSL_FEATURE_DMA_DESCRIPTOR_ALIGN_SIZE)
 DMA head descriptor table allocate macro To simplify user interface, this macro will help allocate descriptor memory, user just need to provide the name and the number for the allocate descriptor. More...
 
#define DMA_ALLOCATE_HEAD_DESCRIPTORS_AT_NONCACHEABLE(name, number)   AT_NONCACHEABLE_SECTION_ALIGN(dma_descriptor_t name[number], FSL_FEATURE_DMA_DESCRIPTOR_ALIGN_SIZE)
 DMA head descriptor table allocate macro at noncacheable section To simplify user interface, this macro will help allocate descriptor memory at noncacheable section, user just need to provide the name and the number for the allocate descriptor. More...
 
#define DMA_ALLOCATE_LINK_DESCRIPTORS(name, number)   SDK_ALIGN(dma_descriptor_t name[number], FSL_FEATURE_DMA_LINK_DESCRIPTOR_ALIGN_SIZE)
 DMA link descriptor table allocate macro To simplify user interface, this macro will help allocate descriptor memory, user just need to provide the name and the number for the allocate descriptor. More...
 
#define DMA_ALLOCATE_LINK_DESCRIPTORS_AT_NONCACHEABLE(name, number)   AT_NONCACHEABLE_SECTION_ALIGN(dma_descriptor_t name[number], FSL_FEATURE_DMA_LINK_DESCRIPTOR_ALIGN_SIZE)
 DMA link descriptor table allocate macro at noncacheable section To simplify user interface, this macro will help allocate descriptor memory at noncacheable section, user just need to provide the name and the number for the allocate descriptor. More...
 
#define DMA_ALLOCATE_DATA_TRANSFER_BUFFER(name, width)   SDK_ALIGN(name, width)
 DMA transfer buffer address need to align with the transfer width.
 
#define DMA_COMMON_REG_GET(base, channel, reg)   (((volatile uint32_t *)(&((base)->COMMON[0].reg)))[DMA_CHANNEL_GROUP(channel)])
 DMA linked descriptor address algin size.
 
#define DMA_DESCRIPTOR_END_ADDRESS(start, inc, bytes, width)   ((uint32_t *)((uint32_t)(start) + (inc) * (bytes) - (inc) * (width)))
 DMA descriptor end address calculate. More...
 
#define DMA_CHANNEL_XFER(reload, clrTrig, intA, intB, width, srcInc, dstInc, bytes)
 DMA channel transfer configurations macro. More...
 

Typedefs

typedef void(* dma_callback )(struct _dma_handle *handle, void *userData, bool transferDone, uint32_t intmode)
 Define Callback function for DMA. More...
 

Enumerations

enum  { kStatus_DMA_Busy = MAKE_STATUS(kStatusGroup_DMA, 0) }
 _dma_transfer_status DMA transfer status More...
 
enum  {
  kDMA_AddressInterleave0xWidth = 0U,
  kDMA_AddressInterleave1xWidth = 1U,
  kDMA_AddressInterleave2xWidth = 2U,
  kDMA_AddressInterleave4xWidth = 4U
}
 _dma_addr_interleave_size dma address interleave size More...
 
enum  {
  kDMA_Transfer8BitWidth = 1U,
  kDMA_Transfer16BitWidth = 2U,
  kDMA_Transfer32BitWidth = 4U
}
 _dma_transfer_width dma transfer width More...
 
enum  dma_priority_t {
  kDMA_ChannelPriority0 = 0,
  kDMA_ChannelPriority1,
  kDMA_ChannelPriority2,
  kDMA_ChannelPriority3,
  kDMA_ChannelPriority4,
  kDMA_ChannelPriority5,
  kDMA_ChannelPriority6,
  kDMA_ChannelPriority7
}
 DMA channel priority. More...
 
enum  dma_irq_t {
  kDMA_IntA,
  kDMA_IntB,
  kDMA_IntError
}
 DMA interrupt flags. More...
 
enum  dma_trigger_type_t {
  kDMA_NoTrigger = 0,
  kDMA_LowLevelTrigger = DMA_CHANNEL_CFG_HWTRIGEN(1) | DMA_CHANNEL_CFG_TRIGTYPE(1),
  kDMA_HighLevelTrigger,
  kDMA_FallingEdgeTrigger = DMA_CHANNEL_CFG_HWTRIGEN(1),
  kDMA_RisingEdgeTrigger
}
 DMA trigger type. More...
 
enum  {
  kDMA_BurstSize1 = 0U,
  kDMA_BurstSize2 = 1U,
  kDMA_BurstSize4 = 2U,
  kDMA_BurstSize8 = 3U,
  kDMA_BurstSize16 = 4U,
  kDMA_BurstSize32 = 5U,
  kDMA_BurstSize64 = 6U,
  kDMA_BurstSize128 = 7U,
  kDMA_BurstSize256 = 8U,
  kDMA_BurstSize512 = 9U,
  kDMA_BurstSize1024 = 10U
}
 _dma_burst_size DMA burst size More...
 
enum  dma_trigger_burst_t {
  kDMA_SingleTransfer = 0,
  kDMA_LevelBurstTransfer = DMA_CHANNEL_CFG_TRIGBURST(1),
  kDMA_EdgeBurstTransfer1 = DMA_CHANNEL_CFG_TRIGBURST(1),
  kDMA_EdgeBurstTransfer2,
  kDMA_EdgeBurstTransfer4,
  kDMA_EdgeBurstTransfer8,
  kDMA_EdgeBurstTransfer16,
  kDMA_EdgeBurstTransfer32,
  kDMA_EdgeBurstTransfer64,
  kDMA_EdgeBurstTransfer128,
  kDMA_EdgeBurstTransfer256,
  kDMA_EdgeBurstTransfer512,
  kDMA_EdgeBurstTransfer1024
}
 DMA trigger burst. More...
 
enum  dma_burst_wrap_t {
  kDMA_NoWrap = 0,
  kDMA_SrcWrap = DMA_CHANNEL_CFG_SRCBURSTWRAP(1),
  kDMA_DstWrap = DMA_CHANNEL_CFG_DSTBURSTWRAP(1),
  kDMA_SrcAndDstWrap
}
 DMA burst wrapping. More...
 
enum  dma_transfer_type_t {
  kDMA_MemoryToMemory = 0x0U,
  kDMA_PeripheralToMemory,
  kDMA_MemoryToPeripheral,
  kDMA_StaticToStatic
}
 DMA transfer type. More...
 

Driver version

#define FSL_DMA_DRIVER_VERSION   (MAKE_VERSION(2, 4, 2))
 DMA driver version. More...
 

DMA initialization and De-initialization

void DMA_Init (DMA_Type *base)
 Initializes DMA peripheral. More...
 
void DMA_Deinit (DMA_Type *base)
 Deinitializes DMA peripheral. More...
 
void DMA_InstallDescriptorMemory (DMA_Type *base, void *addr)
 Install DMA descriptor memory. More...
 

DMA Channel Operation

static bool DMA_ChannelIsActive (DMA_Type *base, uint32_t channel)
 Return whether DMA channel is processing transfer. More...
 
static bool DMA_ChannelIsBusy (DMA_Type *base, uint32_t channel)
 Return whether DMA channel is busy. More...
 
static void DMA_EnableChannelInterrupts (DMA_Type *base, uint32_t channel)
 Enables the interrupt source for the DMA transfer. More...
 
static void DMA_DisableChannelInterrupts (DMA_Type *base, uint32_t channel)
 Disables the interrupt source for the DMA transfer. More...
 
static void DMA_EnableChannel (DMA_Type *base, uint32_t channel)
 Enable DMA channel. More...
 
static void DMA_DisableChannel (DMA_Type *base, uint32_t channel)
 Disable DMA channel. More...
 
static void DMA_EnableChannelPeriphRq (DMA_Type *base, uint32_t channel)
 Set PERIPHREQEN of channel configuration register. More...
 
static void DMA_DisableChannelPeriphRq (DMA_Type *base, uint32_t channel)
 Get PERIPHREQEN value of channel configuration register. More...
 
void DMA_ConfigureChannelTrigger (DMA_Type *base, uint32_t channel, dma_channel_trigger_t *trigger)
 Set trigger settings of DMA channel. More...
 
void DMA_SetChannelConfig (DMA_Type *base, uint32_t channel, dma_channel_trigger_t *trigger, bool isPeriph)
 set channel config. More...
 
uint32_t DMA_GetRemainingBytes (DMA_Type *base, uint32_t channel)
 Gets the remaining bytes of the current DMA descriptor transfer. More...
 
static void DMA_SetChannelPriority (DMA_Type *base, uint32_t channel, dma_priority_t priority)
 Set priority of channel configuration register. More...
 
static dma_priority_t DMA_GetChannelPriority (DMA_Type *base, uint32_t channel)
 Get priority of channel configuration register. More...
 
static void DMA_SetChannelConfigValid (DMA_Type *base, uint32_t channel)
 Set channel configuration valid. More...
 
static void DMA_DoChannelSoftwareTrigger (DMA_Type *base, uint32_t channel)
 Do software trigger for the channel. More...
 
static void DMA_LoadChannelTransferConfig (DMA_Type *base, uint32_t channel, uint32_t xfer)
 Load channel transfer configurations. More...
 
void DMA_CreateDescriptor (dma_descriptor_t *desc, dma_xfercfg_t *xfercfg, void *srcAddr, void *dstAddr, void *nextDesc)
 Create application specific DMA descriptor to be used in a chain in transfer. More...
 
void DMA_SetupDescriptor (dma_descriptor_t *desc, uint32_t xfercfg, void *srcStartAddr, void *dstStartAddr, void *nextDesc)
 setup dma descriptor More...
 
void DMA_SetupChannelDescriptor (dma_descriptor_t *desc, uint32_t xfercfg, void *srcStartAddr, void *dstStartAddr, void *nextDesc, dma_burst_wrap_t wrapType, uint32_t burstSize)
 setup dma channel descriptor More...
 
void DMA_LoadChannelDescriptor (DMA_Type *base, uint32_t channel, dma_descriptor_t *descriptor)
 load channel transfer decriptor. More...
 

DMA Transactional Operation

void DMA_AbortTransfer (dma_handle_t *handle)
 Abort running transfer by handle. More...
 
void DMA_CreateHandle (dma_handle_t *handle, DMA_Type *base, uint32_t channel)
 Creates the DMA handle. More...
 
void DMA_SetCallback (dma_handle_t *handle, dma_callback callback, void *userData)
 Installs a callback function for the DMA transfer. More...
 
void DMA_PrepareTransfer (dma_transfer_config_t *config, void *srcAddr, void *dstAddr, uint32_t byteWidth, uint32_t transferBytes, dma_transfer_type_t type, void *nextDesc)
 Prepares the DMA transfer structure. More...
 
void DMA_PrepareChannelTransfer (dma_channel_config_t *config, void *srcStartAddr, void *dstStartAddr, uint32_t xferCfg, dma_transfer_type_t type, dma_channel_trigger_t *trigger, void *nextDesc)
 Prepare channel transfer configurations. More...
 
status_t DMA_SubmitTransfer (dma_handle_t *handle, dma_transfer_config_t *config)
 Submits the DMA transfer request. More...
 
void DMA_SubmitChannelTransferParameter (dma_handle_t *handle, uint32_t xferCfg, void *srcStartAddr, void *dstStartAddr, void *nextDesc)
 Submit channel transfer paramter directly. More...
 
void DMA_SubmitChannelDescriptor (dma_handle_t *handle, dma_descriptor_t *descriptor)
 Submit channel descriptor. More...
 
status_t DMA_SubmitChannelTransfer (dma_handle_t *handle, dma_channel_config_t *config)
 Submits the DMA channel transfer request. More...
 
void DMA_StartTransfer (dma_handle_t *handle)
 DMA start transfer. More...
 
void DMA_IRQHandle (DMA_Type *base)
 DMA IRQ handler for descriptor transfer complete. More...
 

Data Structure Documentation

struct dma_descriptor_t

Data Fields

volatile uint32_t xfercfg
 Transfer configuration.
 
void * srcEndAddr
 Last source address of DMA transfer.
 
void * dstEndAddr
 Last destination address of DMA transfer.
 
void * linkToNextDesc
 Address of next DMA descriptor in chain.
 
struct dma_xfercfg_t

Data Fields

bool valid
 Descriptor is ready to transfer.
 
bool reload
 Reload channel configuration register after current descriptor is exhausted.
 
bool swtrig
 Perform software trigger. More...
 
bool clrtrig
 Clear trigger.
 
bool intA
 Raises IRQ when transfer is done and set IRQA status register flag.
 
bool intB
 Raises IRQ when transfer is done and set IRQB status register flag.
 
uint8_t byteWidth
 Byte width of data to transfer.
 
uint8_t srcInc
 Increment source address by 'srcInc' x 'byteWidth'.
 
uint8_t dstInc
 Increment destination address by 'dstInc' x 'byteWidth'.
 
uint16_t transferCount
 Number of transfers.
 

Field Documentation

bool dma_xfercfg_t::swtrig

Transfer if fired when 'valid' is set

struct dma_channel_trigger_t

Data Fields

dma_trigger_type_t type
 Select hardware trigger as edge triggered or level triggered. More...
 
dma_trigger_burst_t burst
 Select whether hardware triggers cause a single or burst transfer. More...
 
dma_burst_wrap_t wrap
 Select wrap type, source wrap or dest wrap, or both. More...
 

Field Documentation

dma_trigger_type_t dma_channel_trigger_t::type
dma_trigger_burst_t dma_channel_trigger_t::burst
dma_burst_wrap_t dma_channel_trigger_t::wrap
struct dma_channel_config_t

Data Fields

void * srcStartAddr
 Source data address.
 
void * dstStartAddr
 Destination data address.
 
void * nextDesc
 Chain custom descriptor.
 
uint32_t xferCfg
 channel transfer configurations
 
dma_channel_trigger_t * trigger
 DMA trigger type.
 
bool isPeriph
 select the request type
 
struct dma_transfer_config_t

Data Fields

uint8_t * srcAddr
 Source data address.
 
uint8_t * dstAddr
 Destination data address.
 
uint8_t * nextDesc
 Chain custom descriptor.
 
dma_xfercfg_t xfercfg
 Transfer options.
 
bool isPeriph
 DMA transfer is driven by peripheral.
 
struct dma_handle_t

Data Fields

dma_callback callback
 Callback function. More...
 
void * userData
 Callback function parameter.
 
DMA_Type * base
 DMA peripheral base address.
 
uint8_t channel
 DMA channel number.
 

Field Documentation

dma_callback dma_handle_t::callback

Invoked when transfer of descriptor with interrupt flag finishes

Macro Definition Documentation

#define FSL_DMA_DRIVER_VERSION   (MAKE_VERSION(2, 4, 2))

Version 2.4.2.

#define DMA_ALLOCATE_HEAD_DESCRIPTORS (   name,
  number 
)    SDK_ALIGN(dma_descriptor_t name[number], FSL_FEATURE_DMA_DESCRIPTOR_ALIGN_SIZE)
Parameters
nameAllocate decriptor name.
numberNumber of descriptor to be allocated.
#define DMA_ALLOCATE_HEAD_DESCRIPTORS_AT_NONCACHEABLE (   name,
  number 
)    AT_NONCACHEABLE_SECTION_ALIGN(dma_descriptor_t name[number], FSL_FEATURE_DMA_DESCRIPTOR_ALIGN_SIZE)
Parameters
nameAllocate decriptor name.
numberNumber of descriptor to be allocated.
#define DMA_ALLOCATE_LINK_DESCRIPTORS (   name,
  number 
)    SDK_ALIGN(dma_descriptor_t name[number], FSL_FEATURE_DMA_LINK_DESCRIPTOR_ALIGN_SIZE)
Parameters
nameAllocate decriptor name.
numberNumber of descriptor to be allocated.
#define DMA_ALLOCATE_LINK_DESCRIPTORS_AT_NONCACHEABLE (   name,
  number 
)    AT_NONCACHEABLE_SECTION_ALIGN(dma_descriptor_t name[number], FSL_FEATURE_DMA_LINK_DESCRIPTOR_ALIGN_SIZE)
Parameters
nameAllocate decriptor name.
numberNumber of descriptor to be allocated.
#define DMA_DESCRIPTOR_END_ADDRESS (   start,
  inc,
  bytes,
  width 
)    ((uint32_t *)((uint32_t)(start) + (inc) * (bytes) - (inc) * (width)))
Parameters
startstart address
incaddress interleave size
bytestransfer bytes
widthtransfer width
#define DMA_CHANNEL_XFER (   reload,
  clrTrig,
  intA,
  intB,
  width,
  srcInc,
  dstInc,
  bytes 
)
Value:
DMA_CHANNEL_XFERCFG_CFGVALID_MASK | DMA_CHANNEL_XFERCFG_RELOAD(reload) | DMA_CHANNEL_XFERCFG_CLRTRIG(clrTrig) | \
DMA_CHANNEL_XFERCFG_SETINTA(intA) | DMA_CHANNEL_XFERCFG_SETINTB(intB) | \
DMA_CHANNEL_XFERCFG_WIDTH(width == 4UL ? 2UL : (width - 1UL)) | \
DMA_CHANNEL_XFERCFG_SRCINC(srcInc == (uint32_t)kDMA_AddressInterleave4xWidth ? (srcInc - 1UL) : srcInc) | \
DMA_CHANNEL_XFERCFG_DSTINC(dstInc == (uint32_t)kDMA_AddressInterleave4xWidth ? (dstInc - 1UL) : dstInc) | \
DMA_CHANNEL_XFERCFG_XFERCOUNT(bytes / width - 1UL)
dma source/destination address interleave 3xwidth
Definition: fsl_dma.h:130
Parameters
reloadtrue is reload link descriptor after current exhaust, false is not
clrTrigtrue is clear trigger status, wait software trigger, false is not
intAenable interruptA
intBenable interruptB
widthtransfer width
srcIncsource address interleave size
dstIncdestination address interleave size
bytestransfer bytes

Typedef Documentation

typedef void(* dma_callback)(struct _dma_handle *handle, void *userData, bool transferDone, uint32_t intmode)

Enumeration Type Documentation

anonymous enum
Enumerator
kStatus_DMA_Busy 

Channel is busy and can't handle the transfer request.

anonymous enum
Enumerator
kDMA_AddressInterleave0xWidth 

dma source/destination address no interleave

kDMA_AddressInterleave1xWidth 

dma source/destination address interleave 1xwidth

kDMA_AddressInterleave2xWidth 

dma source/destination address interleave 2xwidth

kDMA_AddressInterleave4xWidth 

dma source/destination address interleave 3xwidth

anonymous enum
Enumerator
kDMA_Transfer8BitWidth 

dma channel transfer bit width is 8 bit

kDMA_Transfer16BitWidth 

dma channel transfer bit width is 16 bit

kDMA_Transfer32BitWidth 

dma channel transfer bit width is 32 bit

Enumerator
kDMA_ChannelPriority0 

Highest channel priority - priority 0.

kDMA_ChannelPriority1 

Channel priority 1.

kDMA_ChannelPriority2 

Channel priority 2.

kDMA_ChannelPriority3 

Channel priority 3.

kDMA_ChannelPriority4 

Channel priority 4.

kDMA_ChannelPriority5 

Channel priority 5.

kDMA_ChannelPriority6 

Channel priority 6.

kDMA_ChannelPriority7 

Lowest channel priority - priority 7.

enum dma_irq_t
Enumerator
kDMA_IntA 

DMA interrupt flag A.

kDMA_IntB 

DMA interrupt flag B.

kDMA_IntError 

DMA interrupt flag error.

Enumerator
kDMA_NoTrigger 

Trigger is disabled.

kDMA_LowLevelTrigger 

Low level active trigger.

kDMA_HighLevelTrigger 

High level active trigger.

kDMA_FallingEdgeTrigger 

Falling edge active trigger.

kDMA_RisingEdgeTrigger 

Rising edge active trigger.

anonymous enum
Enumerator
kDMA_BurstSize1 

burst size 1 transfer

kDMA_BurstSize2 

burst size 2 transfer

kDMA_BurstSize4 

burst size 4 transfer

kDMA_BurstSize8 

burst size 8 transfer

kDMA_BurstSize16 

burst size 16 transfer

kDMA_BurstSize32 

burst size 32 transfer

kDMA_BurstSize64 

burst size 64 transfer

kDMA_BurstSize128 

burst size 128 transfer

kDMA_BurstSize256 

burst size 256 transfer

kDMA_BurstSize512 

burst size 512 transfer

kDMA_BurstSize1024 

burst size 1024 transfer

Enumerator
kDMA_SingleTransfer 

Single transfer.

kDMA_LevelBurstTransfer 

Burst transfer driven by level trigger.

kDMA_EdgeBurstTransfer1 

Perform 1 transfer by edge trigger.

kDMA_EdgeBurstTransfer2 

Perform 2 transfers by edge trigger.

kDMA_EdgeBurstTransfer4 

Perform 4 transfers by edge trigger.

kDMA_EdgeBurstTransfer8 

Perform 8 transfers by edge trigger.

kDMA_EdgeBurstTransfer16 

Perform 16 transfers by edge trigger.

kDMA_EdgeBurstTransfer32 

Perform 32 transfers by edge trigger.

kDMA_EdgeBurstTransfer64 

Perform 64 transfers by edge trigger.

kDMA_EdgeBurstTransfer128 

Perform 128 transfers by edge trigger.

kDMA_EdgeBurstTransfer256 

Perform 256 transfers by edge trigger.

kDMA_EdgeBurstTransfer512 

Perform 512 transfers by edge trigger.

kDMA_EdgeBurstTransfer1024 

Perform 1024 transfers by edge trigger.

Enumerator
kDMA_NoWrap 

Wrapping is disabled.

kDMA_SrcWrap 

Wrapping is enabled for source.

kDMA_DstWrap 

Wrapping is enabled for destination.

kDMA_SrcAndDstWrap 

Wrapping is enabled for source and destination.

Enumerator
kDMA_MemoryToMemory 

Transfer from memory to memory (increment source and destination)

kDMA_PeripheralToMemory 

Transfer from peripheral to memory (increment only destination)

kDMA_MemoryToPeripheral 

Transfer from memory to peripheral (increment only source)

kDMA_StaticToStatic 

Peripheral to static memory (do not increment source or destination)

Function Documentation

void DMA_Init ( DMA_Type *  base)

This function enable the DMA clock, set descriptor table and enable DMA peripheral.

Parameters
baseDMA peripheral base address.
void DMA_Deinit ( DMA_Type *  base)

This function gates the DMA clock.

Parameters
baseDMA peripheral base address.
void DMA_InstallDescriptorMemory ( DMA_Type *  base,
void *  addr 
)

This function used to register DMA descriptor memory for linked transfer, a typical case is ping pong transfer which will request more than one DMA descriptor memory space, althrough current DMA driver has a default DMA descriptor buffer, but it support one DMA descriptor for one channel only.

Parameters
baseDMA base address.
addrDMA descriptor address
static bool DMA_ChannelIsActive ( DMA_Type *  base,
uint32_t  channel 
)
inlinestatic
Parameters
baseDMA peripheral base address.
channelDMA channel number.
Returns
True for active state, false otherwise.
static bool DMA_ChannelIsBusy ( DMA_Type *  base,
uint32_t  channel 
)
inlinestatic
Parameters
baseDMA peripheral base address.
channelDMA channel number.
Returns
True for busy state, false otherwise.
static void DMA_EnableChannelInterrupts ( DMA_Type *  base,
uint32_t  channel 
)
inlinestatic
Parameters
baseDMA peripheral base address.
channelDMA channel number.
static void DMA_DisableChannelInterrupts ( DMA_Type *  base,
uint32_t  channel 
)
inlinestatic
Parameters
baseDMA peripheral base address.
channelDMA channel number.
static void DMA_EnableChannel ( DMA_Type *  base,
uint32_t  channel 
)
inlinestatic
Parameters
baseDMA peripheral base address.
channelDMA channel number.
static void DMA_DisableChannel ( DMA_Type *  base,
uint32_t  channel 
)
inlinestatic
Parameters
baseDMA peripheral base address.
channelDMA channel number.
static void DMA_EnableChannelPeriphRq ( DMA_Type *  base,
uint32_t  channel 
)
inlinestatic
Parameters
baseDMA peripheral base address.
channelDMA channel number.
static void DMA_DisableChannelPeriphRq ( DMA_Type *  base,
uint32_t  channel 
)
inlinestatic
Parameters
baseDMA peripheral base address.
channelDMA channel number.
Returns
True for enabled PeriphRq, false for disabled.
void DMA_ConfigureChannelTrigger ( DMA_Type *  base,
uint32_t  channel,
dma_channel_trigger_t *  trigger 
)
Deprecated:
Do not use this function. It has been superceded by DMA_SetChannelConfig.
Parameters
baseDMA peripheral base address.
channelDMA channel number.
triggertrigger configuration.
void DMA_SetChannelConfig ( DMA_Type *  base,
uint32_t  channel,
dma_channel_trigger_t *  trigger,
bool  isPeriph 
)

This function provide a interface to configure channel configuration reisters.

Parameters
baseDMA base address.
channelDMA channel number.
triggerchannel configurations structure.
isPeriphtrue is periph request, false is not.
uint32_t DMA_GetRemainingBytes ( DMA_Type *  base,
uint32_t  channel 
)
Parameters
baseDMA peripheral base address.
channelDMA channel number.
Returns
The number of bytes which have not been transferred yet.
static void DMA_SetChannelPriority ( DMA_Type *  base,
uint32_t  channel,
dma_priority_t  priority 
)
inlinestatic
Parameters
baseDMA peripheral base address.
channelDMA channel number.
priorityChannel priority value.
static dma_priority_t DMA_GetChannelPriority ( DMA_Type *  base,
uint32_t  channel 
)
inlinestatic
Parameters
baseDMA peripheral base address.
channelDMA channel number.
Returns
Channel priority value.
static void DMA_SetChannelConfigValid ( DMA_Type *  base,
uint32_t  channel 
)
inlinestatic
Parameters
baseDMA peripheral base address.
channelDMA channel number.
static void DMA_DoChannelSoftwareTrigger ( DMA_Type *  base,
uint32_t  channel 
)
inlinestatic
Parameters
baseDMA peripheral base address.
channelDMA channel number.
static void DMA_LoadChannelTransferConfig ( DMA_Type *  base,
uint32_t  channel,
uint32_t  xfer 
)
inlinestatic
Parameters
baseDMA peripheral base address.
channelDMA channel number.
xfertransfer configurations.
void DMA_CreateDescriptor ( dma_descriptor_t *  desc,
dma_xfercfg_t *  xfercfg,
void *  srcAddr,
void *  dstAddr,
void *  nextDesc 
)
Deprecated:
Do not use this function. It has been superceded by DMA_SetupDescriptor.
Parameters
descDMA descriptor address.
xfercfgTransfer configuration for DMA descriptor.
srcAddrAddress of last item to transmit
dstAddrAddress of last item to receive.
nextDescAddress of next descriptor in chain.
void DMA_SetupDescriptor ( dma_descriptor_t *  desc,
uint32_t  xfercfg,
void *  srcStartAddr,
void *  dstStartAddr,
void *  nextDesc 
)

Note: This function do not support configure wrap descriptor.

Parameters
descDMA descriptor address.
xfercfgTransfer configuration for DMA descriptor.
srcStartAddrStart address of source address.
dstStartAddrStart address of destination address.
nextDescAddress of next descriptor in chain.
void DMA_SetupChannelDescriptor ( dma_descriptor_t *  desc,
uint32_t  xfercfg,
void *  srcStartAddr,
void *  dstStartAddr,
void *  nextDesc,
dma_burst_wrap_t  wrapType,
uint32_t  burstSize 
)

Note: This function support configure wrap descriptor.

Parameters
descDMA descriptor address.
xfercfgTransfer configuration for DMA descriptor.
srcStartAddrStart address of source address.
dstStartAddrStart address of destination address.
nextDescAddress of next descriptor in chain.
wrapTypeburst wrap type.
burstSizeburst size, reference _dma_burst_size.
void DMA_LoadChannelDescriptor ( DMA_Type *  base,
uint32_t  channel,
dma_descriptor_t *  descriptor 
)

This function can be used to load desscriptor to driver internal channel descriptor that is used to start DMA transfer, the head descriptor table is defined in DMA driver, it is useful for the case:

  1. for the polling transfer, application can allocate a local descriptor memory table to prepare a descriptor firstly and then call this api to load the configured descriptor to driver descriptor table.
    * DMA_Init(DMA0);
    * DMA_EnableChannel(DMA0, DEMO_DMA_CHANNEL);
    * DMA_SetupDescriptor(desc, xferCfg, s_srcBuffer, &s_destBuffer[0], NULL);
    * DMA_LoadChannelDescriptor(DMA0, DEMO_DMA_CHANNEL, (dma_descriptor_t *)desc);
    * DMA_DoChannelSoftwareTrigger(DMA0, DEMO_DMA_CHANNEL);
    * while(DMA_ChannelIsBusy(DMA0, DEMO_DMA_CHANNEL))
    * {}
    *
Parameters
baseDMA base address.
channelDMA channel.
descriptorconfigured DMA descriptor.
void DMA_AbortTransfer ( dma_handle_t *  handle)

This function aborts DMA transfer specified by handle.

Parameters
handleDMA handle pointer.
void DMA_CreateHandle ( dma_handle_t *  handle,
DMA_Type *  base,
uint32_t  channel 
)

This function is called if using transaction API for DMA. This function initializes the internal state of DMA handle.

Parameters
handleDMA handle pointer. The DMA handle stores callback function and parameters.
baseDMA peripheral base address.
channelDMA channel number.
void DMA_SetCallback ( dma_handle_t *  handle,
dma_callback  callback,
void *  userData 
)

This callback is called in DMA IRQ handler. Use the callback to do something after the current major loop transfer completes.

Parameters
handleDMA handle pointer.
callbackDMA callback function pointer.
userDataParameter for callback function.
void DMA_PrepareTransfer ( dma_transfer_config_t *  config,
void *  srcAddr,
void *  dstAddr,
uint32_t  byteWidth,
uint32_t  transferBytes,
dma_transfer_type_t  type,
void *  nextDesc 
)
Deprecated:
Do not use this function. It has been superceded by DMA_PrepareChannelTransfer. This function prepares the transfer configuration structure according to the user input.
Parameters
configThe user configuration structure of type dma_transfer_t.
srcAddrDMA transfer source address.
dstAddrDMA transfer destination address.
byteWidthDMA transfer destination address width(bytes).
transferBytesDMA transfer bytes to be transferred.
typeDMA transfer type.
nextDescChain custom descriptor to transfer.
Note
The data address and the data width must be consistent. For example, if the SRC is 4 bytes, so the source address must be 4 bytes aligned, or it shall result in source address error(SAE).
void DMA_PrepareChannelTransfer ( dma_channel_config_t *  config,
void *  srcStartAddr,
void *  dstStartAddr,
uint32_t  xferCfg,
dma_transfer_type_t  type,
dma_channel_trigger_t *  trigger,
void *  nextDesc 
)

This function used to prepare channel transfer configurations.

Parameters
configPointer to DMA channel transfer configuration structure.
srcStartAddrsource start address.
dstStartAddrdestination start address.
xferCfgxfer configuration, user can reference DMA_CHANNEL_XFER about to how to get xferCfg value.
typetransfer type.
triggerDMA channel trigger configurations.
nextDescaddress of next descriptor.
status_t DMA_SubmitTransfer ( dma_handle_t *  handle,
dma_transfer_config_t *  config 
)
Deprecated:
Do not use this function. It has been superceded by DMA_SubmitChannelTransfer.

This function submits the DMA transfer request according to the transfer configuration structure. If the user submits the transfer request repeatedly, this function packs an unprocessed request as a TCD and enables scatter/gather feature to process it in the next time.

Parameters
handleDMA handle pointer.
configPointer to DMA transfer configuration structure.
Return values
kStatus_DMA_SuccessIt means submit transfer request succeed.
kStatus_DMA_QueueFullIt means TCD queue is full. Submit transfer request is not allowed.
kStatus_DMA_BusyIt means the given channel is busy, need to submit request later.
void DMA_SubmitChannelTransferParameter ( dma_handle_t *  handle,
uint32_t  xferCfg,
void *  srcStartAddr,
void *  dstStartAddr,
void *  nextDesc 
)

This function used to configue channel head descriptor that is used to start DMA transfer, the head descriptor table is defined in DMA driver, it is useful for the case:

  1. for the single transfer, application doesn't need to allocate descriptor table, the head descriptor can be used for it.
    DMA_SetChannelConfig(base, channel, trigger, isPeriph);
    DMA_CreateHandle(handle, base, channel)
    DMA_SubmitChannelTransferParameter(handle, DMA_CHANNEL_XFER(reload, clrTrig, intA, intB, width, srcInc, dstInc,
    bytes), srcStartAddr, dstStartAddr, NULL);
    *
  2. for the linked transfer, application should responsible for link descriptor, for example, if 4 transfer is required, then application should prepare three descriptor table with macro , the head descriptor in driver can be used for the first transfer descriptor.
    define link descriptor table in application with macro
    DMA_ALLOCATE_LINK_DESCRIPTOR(nextDesc[3]);
    DMA_SetupDescriptor(nextDesc0, DMA_CHANNEL_XFER(reload, clrTrig, intA, intB, width, srcInc, dstInc, bytes),
    srcStartAddr, dstStartAddr, nextDesc1);
    DMA_SetupDescriptor(nextDesc1, DMA_CHANNEL_XFER(reload, clrTrig, intA, intB, width, srcInc, dstInc, bytes),
    srcStartAddr, dstStartAddr, nextDesc2);
    DMA_SetupDescriptor(nextDesc2, DMA_CHANNEL_XFER(reload, clrTrig, intA, intB, width, srcInc, dstInc, bytes),
    srcStartAddr, dstStartAddr, NULL);
    DMA_SetChannelConfig(base, channel, trigger, isPeriph);
    DMA_CreateHandle(handle, base, channel)
    DMA_SubmitChannelTransferParameter(handle, DMA_CHANNEL_XFER(reload, clrTrig, intA, intB, width, srcInc, dstInc,
    bytes), srcStartAddr, dstStartAddr, nextDesc0);
    *
Parameters
handlePointer to DMA handle.
xferCfgxfer configuration, user can reference DMA_CHANNEL_XFER about to how to get xferCfg value.
srcStartAddrsource start address.
dstStartAddrdestination start address.
nextDescaddress of next descriptor.
void DMA_SubmitChannelDescriptor ( dma_handle_t *  handle,
dma_descriptor_t *  descriptor 
)

This function used to configue channel head descriptor that is used to start DMA transfer, the head descriptor table is defined in DMA driver, this functiono is typical for the ping pong case:

  1. for the ping pong case, application should responsible for the descriptor, for example, application should prepare two descriptor table with macro.
    define link descriptor table in application with macro
    DMA_ALLOCATE_LINK_DESCRIPTOR(nextDesc[2]);
    DMA_SetupDescriptor(nextDesc0, DMA_CHANNEL_XFER(reload, clrTrig, intA, intB, width, srcInc, dstInc, bytes),
    srcStartAddr, dstStartAddr, nextDesc1);
    DMA_SetupDescriptor(nextDesc1, DMA_CHANNEL_XFER(reload, clrTrig, intA, intB, width, srcInc, dstInc, bytes),
    srcStartAddr, dstStartAddr, nextDesc0);
    DMA_SetChannelConfig(base, channel, trigger, isPeriph);
    DMA_CreateHandle(handle, base, channel)
    DMA_SubmitChannelDescriptor(handle, nextDesc0);
    *
Parameters
handlePointer to DMA handle.
descriptordescriptor to submit.
status_t DMA_SubmitChannelTransfer ( dma_handle_t *  handle,
dma_channel_config_t *  config 
)

This function submits the DMA transfer request according to the transfer configuration structure. If the user submits the transfer request repeatedly, this function packs an unprocessed request as a TCD and enables scatter/gather feature to process it in the next time. It is used for the case:

  1. for the single transfer, application doesn't need to allocate descriptor table, the head descriptor can be used for it.
    DMA_CreateHandle(handle, base, channel)
    DMA_PrepareChannelTransfer(config,srcStartAddr,dstStartAddr,xferCfg,type,trigger,NULL);
    DMA_SubmitChannelTransfer(handle, config)
    *
  2. for the linked transfer, application should responsible for link descriptor, for example, if 4 transfer is required, then application should prepare three descriptor table with macro , the head descriptor in driver can be used for the first transfer descriptor.
    define link descriptor table in application with macro
    DMA_ALLOCATE_LINK_DESCRIPTOR(nextDesc);
    DMA_SetupDescriptor(nextDesc0, DMA_CHANNEL_XFER(reload, clrTrig, intA, intB, width, srcInc, dstInc, bytes),
    srcStartAddr, dstStartAddr, nextDesc1);
    DMA_SetupDescriptor(nextDesc1, DMA_CHANNEL_XFER(reload, clrTrig, intA, intB, width, srcInc, dstInc, bytes),
    srcStartAddr, dstStartAddr, nextDesc2);
    DMA_SetupDescriptor(nextDesc2, DMA_CHANNEL_XFER(reload, clrTrig, intA, intB, width, srcInc, dstInc, bytes),
    srcStartAddr, dstStartAddr, NULL);
    DMA_CreateHandle(handle, base, channel)
    DMA_PrepareChannelTransfer(config,srcStartAddr,dstStartAddr,xferCfg,type,trigger,nextDesc0);
    DMA_SubmitChannelTransfer(handle, config)
    *
  3. for the ping pong case, application should responsible for link descriptor, for example, application should prepare two descriptor table with macro , the head descriptor in driver can be used for the first transfer descriptor.
    define link descriptor table in application with macro
    DMA_ALLOCATE_LINK_DESCRIPTOR(nextDesc);
    DMA_SetupDescriptor(nextDesc0, DMA_CHANNEL_XFER(reload, clrTrig, intA, intB, width, srcInc, dstInc, bytes),
    srcStartAddr, dstStartAddr, nextDesc1);
    DMA_SetupDescriptor(nextDesc1, DMA_CHANNEL_XFER(reload, clrTrig, intA, intB, width, srcInc, dstInc, bytes),
    srcStartAddr, dstStartAddr, nextDesc0);
    DMA_CreateHandle(handle, base, channel)
    DMA_PrepareChannelTransfer(config,srcStartAddr,dstStartAddr,xferCfg,type,trigger,nextDesc0);
    DMA_SubmitChannelTransfer(handle, config)
    *
    Parameters
    handleDMA handle pointer.
    configPointer to DMA transfer configuration structure.
    Return values
    kStatus_DMA_SuccessIt means submit transfer request succeed.
    kStatus_DMA_QueueFullIt means TCD queue is full. Submit transfer request is not allowed.
    kStatus_DMA_BusyIt means the given channel is busy, need to submit request later.
void DMA_StartTransfer ( dma_handle_t *  handle)

This function enables the channel request. User can call this function after submitting the transfer request It will trigger transfer start with software trigger only when hardware trigger is not used.

Parameters
handleDMA handle pointer.
void DMA_IRQHandle ( DMA_Type *  base)

This function clears the channel major interrupt flag and call the callback function if it is not NULL.

Parameters
baseDMA base address.