|  | 
| enum | da7212_Input_t { kDA7212_Input_AUX = 0x0,
 kDA7212_Input_MIC1_Dig,
 kDA7212_Input_MIC1_An,
 kDA7212_Input_MIC2
 }
 | 
|  | DA7212 input source select.  More... 
 | 
|  | 
| enum | _da7212_play_channel { kDA7212_HeadphoneLeft = 1U,
 kDA7212_HeadphoneRight = 2U,
 kDA7212_Speaker = 4U
 }
 | 
|  | da7212 play channel  More... 
 | 
|  | 
| enum | da7212_Output_t { kDA7212_Output_HP = 0x0,
 kDA7212_Output_SP
 }
 | 
|  | DA7212 output device select.  More... 
 | 
|  | 
| enum | _da7212_module { kDA7212_ModuleADC,
 kDA7212_ModuleDAC,
 kDA7212_ModuleHeadphone,
 kDA7212_ModuleSpeaker
 }
 | 
|  | DA7212 module.  More... 
 | 
|  | 
| enum | da7212_dac_source_t { kDA7212_DACSourceADC = 0x0U,
 kDA7212_DACSourceInputStream = 0x3U
 }
 | 
|  | DA7212 functionality.  More... 
 | 
|  | 
| enum | da7212_volume_t { kDA7212_DACGainMute = 0x7,
 kDA7212_DACGainM72DB = 0x17,
 kDA7212_DACGainM60DB = 0x1F,
 kDA7212_DACGainM54DB = 0x27,
 kDA7212_DACGainM48DB = 0x2F,
 kDA7212_DACGainM42DB = 0x37,
 kDA7212_DACGainM36DB = 0x3F,
 kDA7212_DACGainM30DB = 0x47,
 kDA7212_DACGainM24DB = 0x4F,
 kDA7212_DACGainM18DB = 0x57,
 kDA7212_DACGainM12DB = 0x5F,
 kDA7212_DACGainM6DB = 0x67,
 kDA7212_DACGain0DB = 0x6F,
 kDA7212_DACGain6DB = 0x77,
 kDA7212_DACGain12DB = 0x7F
 }
 | 
|  | DA7212 volume.  More... 
 | 
|  | 
| enum | da7212_protocol_t { kDA7212_BusI2S = 0x0,
 kDA7212_BusLeftJustified,
 kDA7212_BusRightJustified,
 kDA7212_BusDSPMode
 }
 | 
|  | The audio data transfer protocol choice.  More... 
 | 
|  | 
| enum | da7212_sys_clk_source_t { kDA7212_SysClkSourceMCLK = 0U,
 kDA7212_SysClkSourcePLL = 1U << 14
 }
 | 
|  | da7212 system clock source  More... 
 | 
|  | 
| enum | da7212_pll_clk_source_t { kDA7212_PLLClkSourceMCLK = 0U
 } | 
|  | DA7212 pll clock source.  More... 
 | 
|  | 
| enum | da7212_pll_out_clk_t { kDA7212_PLLOutputClk11289600 = 11289600U,
 kDA7212_PLLOutputClk12288000 = 12288000U
 }
 | 
|  | DA7212 output clock frequency.  More... 
 | 
|  | 
| enum | da7212_master_bits_t { kDA7212_MasterBits32PerFrame = 0U,
 kDA7212_MasterBits64PerFrame = 1U,
 kDA7212_MasterBits128PerFrame = 2U,
 kDA7212_MasterBits256PerFrame = 3U
 }
 | 
|  | master mode bits per frame  More... 
 | 
|  | 
|  | 
| status_t | DA7212_Init (da7212_handle_t *handle, da7212_config_t *codecConfig) | 
|  | DA7212 initialize function.  More... 
 | 
|  | 
| status_t | DA7212_ConfigAudioFormat (da7212_handle_t *handle, uint32_t masterClock_Hz, uint32_t sampleRate_Hz, uint32_t dataBits) | 
|  | Set DA7212 audio format.  More... 
 | 
|  | 
| status_t | DA7212_SetPLLConfig (da7212_handle_t *handle, da7212_pll_config_t *config) | 
|  | DA7212 set PLL configuration This function will enable the GPIO1 FLL clock output function, so user can see the generated fll output clock frequency from WM8904 GPIO1.  More... 
 | 
|  | 
| void | DA7212_ChangeHPVolume (da7212_handle_t *handle, da7212_volume_t volume) | 
|  | Set DA7212 playback volume.  More... 
 | 
|  | 
| void | DA7212_Mute (da7212_handle_t *handle, bool isMuted) | 
|  | Mute or unmute DA7212.  More... 
 | 
|  | 
| void | DA7212_ChangeInput (da7212_handle_t *handle, da7212_Input_t DA7212_Input) | 
|  | Set the input data source of DA7212.  More... 
 | 
|  | 
| void | DA7212_ChangeOutput (da7212_handle_t *handle, da7212_Output_t DA7212_Output) | 
|  | Set the output device of DA7212.  More... 
 | 
|  | 
| status_t | DA7212_SetChannelVolume (da7212_handle_t *handle, uint32_t channel, uint32_t volume) | 
|  | Set module volume.  More... 
 | 
|  | 
| status_t | DA7212_SetChannelMute (da7212_handle_t *handle, uint32_t channel, bool isMute) | 
|  | Set module mute.  More... 
 | 
|  | 
| status_t | DA7212_SetProtocol (da7212_handle_t *handle, da7212_protocol_t protocol) | 
|  | Set protocol for DA7212.  More... 
 | 
|  | 
| status_t | DA7212_SetMasterModeBits (da7212_handle_t *handle, uint32_t bitWidth) | 
|  | Set master mode bits per frame for DA7212.  More... 
 | 
|  | 
| status_t | DA7212_WriteRegister (da7212_handle_t *handle, uint8_t u8Register, uint8_t u8RegisterData) | 
|  | Write a register for DA7212.  More... 
 | 
|  | 
| status_t | DA7212_ReadRegister (da7212_handle_t *handle, uint8_t u8Register, uint8_t *pu8RegisterData) | 
|  | Get a register value of DA7212.  More... 
 | 
|  | 
| status_t | DA7212_Deinit (da7212_handle_t *handle) | 
|  | Deinit DA7212.  More... 
 | 
|  |