|  | MCUXpresso SDK API Reference Manual
    Rev. 0
    NXP Semiconductors | 
| Files | |
| file | fsl_dmic.h | 
| Data Structures | |
| struct | dmic_channel_config_t | 
| DMIC Channel configuration structure.  More... | |
| Typedefs | |
| typedef void(* | dmic_callback_t )(void) | 
| DMIC Callback function.  More... | |
| typedef void(* | dmic_hwvad_callback_t )(void) | 
| HWVAD Callback function.  More... | |
| DMIC version | |
| #define | FSL_DMIC_DRIVER_VERSION (MAKE_VERSION(2, 3, 0)) | 
| DMIC driver version 2.3.0.  More... | |
| Initialization and deinitialization | |
| uint32_t | DMIC_GetInstance (DMIC_Type *base) | 
| Get the DMIC instance from peripheral base address.  More... | |
| void | DMIC_Init (DMIC_Type *base) | 
| Turns DMIC Clock on.  More... | |
| void | DMIC_DeInit (DMIC_Type *base) | 
| Turns DMIC Clock off.  More... | |
| void | DMIC_ConfigIO (DMIC_Type *base, dmic_io_t config) | 
| Configure DMIC io.  More... | |
| static void | DMIC_SetIOCFG (DMIC_Type *base, uint32_t sel) | 
| Stereo PDM select.  More... | |
| void | DMIC_SetOperationMode (DMIC_Type *base, operation_mode_t mode) | 
| Set DMIC operating mode.  More... | |
| void | DMIC_Use2fs (DMIC_Type *base, bool use2fs) | 
| Configure Clock scaling.  More... | |
| Channel configuration | |
| void | DMIC_CfgChannelDc (DMIC_Type *base, dmic_channel_t channel, dc_removal_t dc_cut_level, uint32_t post_dc_gain_reduce, bool saturate16bit) | 
| Configure DMIC channel.  More... | |
| void | DMIC_ConfigChannel (DMIC_Type *base, dmic_channel_t channel, stereo_side_t side, dmic_channel_config_t *channel_config) | 
| Configure DMIC channel.  More... | |
| void | DMIC_EnableChannnel (DMIC_Type *base, uint32_t channelmask) | 
| Enable a particualr channel.  More... | |
| void | DMIC_FifoChannel (DMIC_Type *base, uint32_t channel, uint32_t trig_level, uint32_t enable, uint32_t resetn) | 
| Configure fifo settings for DMIC channel.  More... | |
| static void | DMIC_EnableChannelInterrupt (DMIC_Type *base, dmic_channel_t channel, bool enable) | 
| Enable a particualr channel interrupt request.  More... | |
| static void | DMIC_EnableChannelDma (DMIC_Type *base, dmic_channel_t channel, bool enable) | 
| Enable a particualr channel dma request.  More... | |
| static void | DMIC_EnableChannelFifo (DMIC_Type *base, dmic_channel_t channel, bool enable) | 
| Enable a particualr channel fifo.  More... | |
| static void | DMIC_DoFifoReset (DMIC_Type *base, dmic_channel_t channel) | 
| Channel fifo reset.  More... | |
| static uint32_t | DMIC_FifoGetStatus (DMIC_Type *base, uint32_t channel) | 
| Get FIFO status.  More... | |
| static void | DMIC_FifoClearStatus (DMIC_Type *base, uint32_t channel, uint32_t mask) | 
| Clear FIFO status.  More... | |
| static uint32_t | DMIC_FifoGetData (DMIC_Type *base, uint32_t channel) | 
| Get FIFO data.  More... | |
| static uint32_t | DMIC_FifoGetAddress (DMIC_Type *base, uint32_t channel) | 
| Get FIFO address.  More... | |
| Register callback. | |
| void | DMIC_EnableIntCallback (DMIC_Type *base, dmic_callback_t cb) | 
| Enable callback.  More... | |
| void | DMIC_DisableIntCallback (DMIC_Type *base, dmic_callback_t cb) | 
| Disable callback.  More... | |
| HWVAD | |
| static void | DMIC_SetGainNoiseEstHwvad (DMIC_Type *base, uint32_t value) | 
| Sets the gain value for the noise estimator.  More... | |
| static void | DMIC_SetGainSignalEstHwvad (DMIC_Type *base, uint32_t value) | 
| Sets the gain value for the signal estimator.  More... | |
| static void | DMIC_SetFilterCtrlHwvad (DMIC_Type *base, uint32_t value) | 
| Sets the hwvad filter cutoff frequency parameter.  More... | |
| static void | DMIC_SetInputGainHwvad (DMIC_Type *base, uint32_t value) | 
| Sets the input gain of hwvad.  More... | |
| static void | DMIC_CtrlClrIntrHwvad (DMIC_Type *base, bool st10) | 
| Clears hwvad internal interrupt flag.  More... | |
| static void | DMIC_FilterResetHwvad (DMIC_Type *base, bool rstt) | 
| Resets hwvad filters.  More... | |
| static uint16_t | DMIC_GetNoiseEnvlpEst (DMIC_Type *base) | 
| Gets the value from output of the filter z7.  More... | |
| void | DMIC_HwvadEnableIntCallback (DMIC_Type *base, dmic_hwvad_callback_t vadcb) | 
| Enable hwvad callback.  More... | |
| void | DMIC_HwvadDisableIntCallback (DMIC_Type *base, dmic_hwvad_callback_t vadcb) | 
| Disable callback.  More... | |
| struct dmic_channel_config_t | 
| Data Fields | |
| pdm_div_t | divhfclk | 
| DMIC Clock pre-divider values. | |
| uint32_t | osr | 
| oversampling rate(CIC decimation rate) for PCM | |
| int32_t | gainshft | 
| 4FS PCM data gain control | |
| compensation_t | preac2coef | 
| Pre-emphasis Filter coefficient value for 2FS. | |
| compensation_t | preac4coef | 
| Pre-emphasis Filter coefficient value for 4FS. | |
| dc_removal_t | dc_cut_level | 
| DMIC DC filter control values.  More... | |
| uint32_t | post_dc_gain_reduce | 
| Fine gain adjustment in the form of a number of bits to downshift. | |
| dmic_phy_sample_rate_t | sample_rate | 
| DMIC and decimator sample rates. | |
| bool | saturate16bit | 
| Selects 16-bit saturation.  More... | |
| dc_removal_t dmic_channel_config_t::dc_cut_level | 
| bool dmic_channel_config_t::saturate16bit | 
0 means results roll over if out range and do not saturate. 1 means if the result overflows, it saturates at 0xFFFF for positive overflow and 0x8000 for negative overflow.
| #define FSL_DMIC_DRIVER_VERSION (MAKE_VERSION(2, 3, 0)) | 
| typedef void(* dmic_callback_t)(void) | 
| typedef void(* dmic_hwvad_callback_t)(void) | 
| anonymous enum | 
| enum operation_mode_t | 
| enum stereo_side_t | 
| enum pdm_div_t | 
| enum compensation_t | 
| enum dc_removal_t | 
| enum dmic_io_t | 
| enum dmic_channel_t | 
| anonymous enum | 
| uint32_t DMIC_GetInstance | ( | DMIC_Type * | base | ) | 
| base | DMIC peripheral base address. | 
| void DMIC_Init | ( | DMIC_Type * | base | ) | 
| base | : DMIC base | 
| void DMIC_DeInit | ( | DMIC_Type * | base | ) | 
| base | : DMIC base | 
| void DMIC_ConfigIO | ( | DMIC_Type * | base, | 
| dmic_io_t | config | ||
| ) | 
| base | : The base address of DMIC interface | 
| config | : DMIC io configuration | 
| 
 | inlinestatic | 
| base | : The base address of DMIC interface | 
| sel | : Reference dmic_io_t, can be a single or combination value of dmic_io_t. | 
| void DMIC_SetOperationMode | ( | DMIC_Type * | base, | 
| operation_mode_t | mode | ||
| ) | 
| base | : The base address of DMIC interface | 
| mode | : DMIC mode | 
| void DMIC_Use2fs | ( | DMIC_Type * | base, | 
| bool | use2fs | ||
| ) | 
| base | : The base address of DMIC interface | 
| use2fs | : clock scaling | 
| void DMIC_CfgChannelDc | ( | DMIC_Type * | base, | 
| dmic_channel_t | channel, | ||
| dc_removal_t | dc_cut_level, | ||
| uint32_t | post_dc_gain_reduce, | ||
| bool | saturate16bit | ||
| ) | 
| base | : The base address of DMIC interface | 
| channel | : DMIC channel | 
| dc_cut_level | : dc_removal_t, Cut off Frequency | 
| post_dc_gain_reduce | : Fine gain adjustment in the form of a number of bits to downshift. | 
| saturate16bit | : If selects 16-bit saturation. | 
| void DMIC_ConfigChannel | ( | DMIC_Type * | base, | 
| dmic_channel_t | channel, | ||
| stereo_side_t | side, | ||
| dmic_channel_config_t * | channel_config | ||
| ) | 
| base | : The base address of DMIC interface | 
| channel | : DMIC channel | 
| side | : stereo_side_t, choice of left or right | 
| channel_config | : Channel configuration | 
| void DMIC_EnableChannnel | ( | DMIC_Type * | base, | 
| uint32_t | channelmask | ||
| ) | 
| base | : The base address of DMIC interface | 
| channelmask | reference _dmic_channel_mask | 
| void DMIC_FifoChannel | ( | DMIC_Type * | base, | 
| uint32_t | channel, | ||
| uint32_t | trig_level, | ||
| uint32_t | enable, | ||
| uint32_t | resetn | ||
| ) | 
| base | : The base address of DMIC interface | 
| channel | : DMIC channel | 
| trig_level | : FIFO trigger level | 
| enable | : FIFO level | 
| resetn | : FIFO reset | 
| 
 | inlinestatic | 
| base | : The base address of DMIC interface | 
| channel | : Channel selection | 
| enable | : true is enable, false is disable | 
| 
 | inlinestatic | 
| base | : The base address of DMIC interface | 
| channel | : Channel selection | 
| enable | : true is enable, false is disable | 
| 
 | inlinestatic | 
| base | : The base address of DMIC interface | 
| channel | : Channel selection | 
| enable | : true is enable, false is disable | 
| 
 | inlinestatic | 
| base | : The base address of DMIC interface | 
| channel | : Channel selection | 
| 
 | inlinestatic | 
| base | : The base address of DMIC interface | 
| channel | : DMIC channel | 
| 
 | inlinestatic | 
| base | : The base address of DMIC interface | 
| channel | : DMIC channel | 
| mask | : Bits to be cleared | 
| 
 | inlinestatic | 
| base | : The base address of DMIC interface | 
| channel | : DMIC channel | 
| 
 | inlinestatic | 
| base | : The base address of DMIC interface | 
| channel | : DMIC channel | 
| void DMIC_EnableIntCallback | ( | DMIC_Type * | base, | 
| dmic_callback_t | cb | ||
| ) | 
This function enables the interrupt for the selected DMIC peripheral. The callback function is not enabled until this function is called.
| base | Base address of the DMIC peripheral. | 
| cb | callback Pointer to store callback function. | 
| None. | 
| void DMIC_DisableIntCallback | ( | DMIC_Type * | base, | 
| dmic_callback_t | cb | ||
| ) | 
This function disables the interrupt for the selected DMIC peripheral.
| base | Base address of the DMIC peripheral. | 
| cb | callback Pointer to store callback function.. | 
| None. | 
| 
 | inlinestatic | 
| base | DMIC base pointer | 
| value | gain value for the noise estimator. | 
| None. | 
| 
 | inlinestatic | 
| base | DMIC base pointer | 
| value | gain value for the signal estimator. | 
| None. | 
| 
 | inlinestatic | 
| base | DMIC base pointer | 
| value | cut off frequency value. | 
| None. | 
| 
 | inlinestatic | 
| base | DMIC base pointer | 
| value | input gain value for hwvad. | 
| None. | 
| 
 | inlinestatic | 
| base | DMIC base pointer | 
| st10 | bit value. | 
| None. | 
| 
 | inlinestatic | 
| base | DMIC base pointer | 
| rstt | Reset bit value. | 
| None. | 
| 
 | inlinestatic | 
| base | DMIC base pointer | 
| output | of filter z7. | 
| void DMIC_HwvadEnableIntCallback | ( | DMIC_Type * | base, | 
| dmic_hwvad_callback_t | vadcb | ||
| ) | 
This function enables the hwvad interrupt for the selected DMIC peripheral. The callback function is not enabled until this function is called.
| base | Base address of the DMIC peripheral. | 
| vadcb | callback Pointer to store callback function. | 
| None. | 
| void DMIC_HwvadDisableIntCallback | ( | DMIC_Type * | base, | 
| dmic_hwvad_callback_t | vadcb | ||
| ) | 
This function disables the hwvad interrupt for the selected DMIC peripheral.
| base | Base address of the DMIC peripheral. | 
| vadcb | callback Pointer to store callback function.. | 
| None. |