The MCUXpresso SDK provides a peripheral driver for the General Purpose I/O (GPIO) module of MCUXpresso SDK devices.
Function groups
Initialization and deinitialization
The function GPIO_PinInit() initializes the GPIO with specified configuration.
Pin manipulation
The function GPIO_PinWrite() set output state of selected GPIO pin. The function GPIO_PinRead() read input value of selected GPIO pin.
Port manipulation
The function GPIO_PortSet() sets the output level of selected GPIO pins to the logic 1. The function GPIO_PortClear() sets the output level of selected GPIO pins to the logic 0. The function GPIO_PortToggle() reverse the output level of selected GPIO pins. The function GPIO_PortRead() read input value of selected port.
Port masking
The function GPIO_PortMaskedSet() set port mask, only pins masked by 0 will be enabled in following functions. The function GPIO_PortMaskedWrite() sets the state of selected GPIO port, only pins masked by 0 will be affected. The function GPIO_PortMaskedRead() reads the state of selected GPIO port, only pins masked by 0 are enabled for read, pins masked by 1 are read as 0.
Typical use case
Example use of GPIO API. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/gpio 
|  | 
| static void | GPIO_PortSet (GPIO_Type *base, uint32_t port, uint32_t mask) | 
|  | Sets the output level of the multiple GPIO pins to the logic 1.  More... 
 | 
|  | 
| static void | GPIO_PortClear (GPIO_Type *base, uint32_t port, uint32_t mask) | 
|  | Sets the output level of the multiple GPIO pins to the logic 0.  More... 
 | 
|  | 
| static void | GPIO_PortToggle (GPIO_Type *base, uint32_t port, uint32_t mask) | 
|  | Reverses current output logic of the multiple GPIO pins.  More... 
 | 
|  | 
|  | 
| static void | GPIO_PinWrite (GPIO_Type *base, uint32_t port, uint32_t pin, uint8_t output) | 
|  | Sets the output level of the one GPIO pin to the logic 1 or 0.  More... 
 | 
|  | 
|  | 
| static uint32_t | GPIO_PinRead (GPIO_Type *base, uint32_t port, uint32_t pin) | 
|  | Reads the current input value of the GPIO PIN.  More... 
 | 
|  | 
Every pin can only be configured as either output pin or input pin at a time. If configured as a input pin, then leave the outputConfig unused. 
 
 
| Enumerator | 
|---|
| kGPIO_DigitalInput | Set current pin as digital input.  | 
| kGPIO_DigitalOutput | Set current pin as digital output.  | 
 
 
      
        
          | void GPIO_PortInit | ( | GPIO_Type * | base, | 
        
          |  |  | uint32_t | port | 
        
          |  | ) |  |  | 
      
 
This function ungates the GPIO clock.
- Parameters
- 
  
    | base | GPIO peripheral base pointer. |  | port | GPIO port number. |  
 
 
 
      
        
          | void GPIO_PinInit | ( | GPIO_Type * | base, | 
        
          |  |  | uint32_t | port, | 
        
          |  |  | uint32_t | pin, | 
        
          |  |  | const gpio_pin_config_t * | config | 
        
          |  | ) |  |  | 
      
 
To initialize the GPIO, define a pin configuration, either input or output, in the user file. Then, call the GPIO_PinInit() function.
This is an example to define an input pin or output pin configuration: 
* Define a digital input pin configuration,
* {
*   0,
* }
* Define a digital output pin configuration,
* {
*   0,
* }
* 
- Parameters
- 
  
    | base | GPIO peripheral base pointer(Typically GPIO) |  | port | GPIO port number |  | pin | GPIO pin number |  | config | GPIO pin configuration pointer |  
 
 
 
  
  | 
        
          | static void GPIO_PinWrite | ( | GPIO_Type * | base, |  
          |  |  | uint32_t | port, |  
          |  |  | uint32_t | pin, |  
          |  |  | uint8_t | output |  
          |  | ) |  |  |  | inlinestatic | 
 
- Parameters
- 
  
    | base | GPIO peripheral base pointer(Typically GPIO) |  | port | GPIO port number |  | pin | GPIO pin number |  | output | GPIO pin output logic level. 
0: corresponding pin output low-logic level.1: corresponding pin output high-logic level.  |  
 
 
 
  
  | 
        
          | static uint32_t GPIO_PinRead | ( | GPIO_Type * | base, |  
          |  |  | uint32_t | port, |  
          |  |  | uint32_t | pin |  
          |  | ) |  |  |  | inlinestatic | 
 
- Parameters
- 
  
    | base | GPIO peripheral base pointer(Typically GPIO) |  | port | GPIO port number |  | pin | GPIO pin number |  
 
- Return values
- 
  
    | GPIO | port input value 
0: corresponding pin input low-logic level.1: corresponding pin input high-logic level.  |  
 
 
 
  
  | 
        
          | static void GPIO_PortSet | ( | GPIO_Type * | base, |  
          |  |  | uint32_t | port, |  
          |  |  | uint32_t | mask |  
          |  | ) |  |  |  | inlinestatic | 
 
- Parameters
- 
  
    | base | GPIO peripheral base pointer(Typically GPIO) |  | port | GPIO port number |  | mask | GPIO pin number macro |  
 
 
 
  
  | 
        
          | static void GPIO_PortClear | ( | GPIO_Type * | base, |  
          |  |  | uint32_t | port, |  
          |  |  | uint32_t | mask |  
          |  | ) |  |  |  | inlinestatic | 
 
- Parameters
- 
  
    | base | GPIO peripheral base pointer(Typically GPIO) |  | port | GPIO port number |  | mask | GPIO pin number macro |  
 
 
 
  
  | 
        
          | static void GPIO_PortToggle | ( | GPIO_Type * | base, |  
          |  |  | uint32_t | port, |  
          |  |  | uint32_t | mask |  
          |  | ) |  |  |  | inlinestatic | 
 
- Parameters
- 
  
    | base | GPIO peripheral base pointer(Typically GPIO) |  | port | GPIO port number |  | mask | GPIO pin number macro |