![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the Reset Control Module (RCM) module of MCUXpresso SDK devices.
Data Structures | |
| struct | rcm_version_id_t |
| IP version ID definition. More... | |
| struct | rcm_reset_pin_filter_config_t |
| Reset pin filter configuration. More... | |
Enumerations | |
| enum | rcm_reset_source_t { kRCM_SourceLvd = RCM_SRS_LVD_MASK, kRCM_SourceLoc = RCM_SRS_LOC_MASK, kRCM_SourceLol = RCM_SRS_LOL_MASK, kRCM_SourceWdog = RCM_SRS_WDOG_MASK, kRCM_SourcePin = RCM_SRS_PIN_MASK, kRCM_SourcePor = RCM_SRS_POR_MASK, kRCM_SourceLockup = RCM_SRS_LOCKUP_MASK, kRCM_SourceSw = RCM_SRS_SW_MASK, kRCM_SourceMdmap = RCM_SRS_MDM_AP_MASK, kRCM_SourceSackerr = RCM_SRS_SACKERR_MASK } |
| System Reset Source Name definitions. More... | |
| enum | rcm_run_wait_filter_mode_t { kRCM_FilterDisable = 0U, kRCM_FilterBusClock = 1U, kRCM_FilterLpoClock = 2U } |
| Reset pin filter select in Run and Wait modes. More... | |
| enum | rcm_boot_rom_config_t { kRCM_BootFlash = 0U, kRCM_BootRomCfg0 = 1U, kRCM_BootRomFopt = 2U, kRCM_BootRomBoth = 3U } |
| Boot from ROM configuration. More... | |
| enum | rcm_reset_delay_t { kRCM_ResetDelay8Lpo = 0U, kRCM_ResetDelay32Lpo = 1U, kRCM_ResetDelay128Lpo = 2U, kRCM_ResetDelay512Lpo = 3U } |
| Maximum delay time from interrupt asserts to system reset. More... | |
| enum | rcm_interrupt_enable_t { kRCM_IntNone = 0U, kRCM_IntLossOfClk = RCM_SRIE_LOC_MASK, kRCM_IntLossOfLock = RCM_SRIE_LOL_MASK, kRCM_IntWatchDog = RCM_SRIE_WDOG_MASK, kRCM_IntExternalPin = RCM_SRIE_PIN_MASK, kRCM_IntGlobal = RCM_SRIE_GIE_MASK, kRCM_IntCoreLockup = RCM_SRIE_LOCKUP_MASK, kRCM_IntSoftware = RCM_SRIE_SW_MASK, kRCM_IntStopModeAckErr = RCM_SRIE_SACKERR_MASK, kRCM_IntAll } |
| System reset interrupt enable bit definitions. More... | |
Driver version | |
| #define | FSL_RCM_DRIVER_VERSION (MAKE_VERSION(2, 0, 4)) |
| RCM driver version 2.0.4. More... | |
Reset Control Module APIs | |
| static void | RCM_GetVersionId (RCM_Type *base, rcm_version_id_t *versionId) |
| Gets the RCM version ID. More... | |
| static uint32_t | RCM_GetPreviousResetSources (RCM_Type *base) |
| Gets the reset source status which caused a previous reset. More... | |
| static uint32_t | RCM_GetStickyResetSources (RCM_Type *base) |
| Gets the sticky reset source status. More... | |
| static void | RCM_ClearStickyResetSources (RCM_Type *base, uint32_t sourceMasks) |
| Clears the sticky reset source status. More... | |
| void | RCM_ConfigureResetPinFilter (RCM_Type *base, const rcm_reset_pin_filter_config_t *config) |
| Configures the reset pin filter. More... | |
| static rcm_boot_rom_config_t | RCM_GetBootRomSource (RCM_Type *base) |
| Gets the ROM boot source. More... | |
| static void | RCM_ClearBootRomSource (RCM_Type *base) |
| Clears the ROM boot source flag. More... | |
| void | RCM_SetForceBootRomSource (RCM_Type *base, rcm_boot_rom_config_t config) |
| Forces the boot from ROM. More... | |
| static void | RCM_SetSystemResetInterruptConfig (RCM_Type *base, uint32_t intMask, rcm_reset_delay_t delay) |
| Sets the system reset interrupt configuration. More... | |
| struct rcm_version_id_t |
| struct rcm_reset_pin_filter_config_t |
Data Fields | |
| bool | enableFilterInStop |
| Reset pin filter select in stop mode. More... | |
| rcm_run_wait_filter_mode_t | filterInRunWait |
| Reset pin filter in run/wait mode. More... | |
| uint8_t | busClockFilterCount |
| Reset pin bus clock filter width. More... | |
| bool rcm_reset_pin_filter_config_t::enableFilterInStop |
| rcm_run_wait_filter_mode_t rcm_reset_pin_filter_config_t::filterInRunWait |
| uint8_t rcm_reset_pin_filter_config_t::busClockFilterCount |
| #define FSL_RCM_DRIVER_VERSION (MAKE_VERSION(2, 0, 4)) |
| enum rcm_reset_source_t |
| enum rcm_reset_delay_t |
|
inlinestatic |
This function gets the RCM version ID including the major version number, the minor version number, and the feature specification number.
| base | RCM peripheral base address. |
| versionId | Pointer to the version ID structure. |
|
inlinestatic |
This function gets the current reset source status. Use source masks defined in the rcm_reset_source_t to get the desired source status.
This is an example.
| base | RCM peripheral base address. |
|
inlinestatic |
This function gets the current reset source status that has not been cleared by software for a specific source.
This is an example.
| base | RCM peripheral base address. |
|
inlinestatic |
This function clears the sticky system reset flags indicated by source masks.
This is an example.
| base | RCM peripheral base address. |
| sourceMasks | reset source status bit map |
| void RCM_ConfigureResetPinFilter | ( | RCM_Type * | base, |
| const rcm_reset_pin_filter_config_t * | config | ||
| ) |
This function sets the reset pin filter including the filter source, filter width, and so on.
| base | RCM peripheral base address. |
| config | Pointer to the configuration structure. |
|
inlinestatic |
This function gets the ROM boot source during the last chip reset.
| base | RCM peripheral base address. |
|
inlinestatic |
This function clears the ROM boot source flag.
| base | Register base address of RCM |
| void RCM_SetForceBootRomSource | ( | RCM_Type * | base, |
| rcm_boot_rom_config_t | config | ||
| ) |
This function forces booting from ROM during all subsequent system resets.
| base | RCM peripheral base address. |
| config | Boot configuration. |
|
inlinestatic |
For a graceful shut down, the RCM supports delaying the assertion of the system reset for a period of time when the reset interrupt is generated. This function can be used to enable the interrupt and the delay period. The interrupts are passed in as bit mask. See rcm_int_t for details. For example, to delay a reset for 512 LPO cycles after the WDOG timeout or loss-of-clock occurs, configure as follows: RCM_SetSystemResetInterruptConfig(kRCM_IntWatchDog | kRCM_IntLossOfClk, kRCM_ResetDelay512Lpo);
| base | RCM peripheral base address. |
| intMask | Bit mask of the system reset interrupts to enable. See rcm_interrupt_enable_t for details. |
| delay | Bit mask of the system reset interrupts to enable. |