MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Spi_dma_driver

Overview

Data Structures

struct  spi_dma_handle_t
 SPI DMA transfer handle, users should not touch the content of the handle. More...
 

Typedefs

typedef void(* spi_dma_callback_t )(SPI_Type *base, spi_dma_handle_t *handle, status_t status, void *userData)
 SPI DMA callback called at the end of transfer. More...
 

Driver version

#define FSL_SPI_DMA_DRIVER_VERSION   (MAKE_VERSION(2, 1, 1))
 SPI DMA driver version. More...
 

DMA Transactional

void SPI_MasterTransferCreateHandleDMA (SPI_Type *base, spi_dma_handle_t *handle, spi_dma_callback_t callback, void *userData, dma_handle_t *txHandle, dma_handle_t *rxHandle)
 Initialize the SPI master DMA handle. More...
 
status_t SPI_MasterTransferDMA (SPI_Type *base, spi_dma_handle_t *handle, spi_transfer_t *xfer)
 Perform a non-blocking SPI transfer using DMA. More...
 
void SPI_MasterTransferAbortDMA (SPI_Type *base, spi_dma_handle_t *handle)
 Abort a SPI transfer using DMA. More...
 
status_t SPI_MasterTransferGetCountDMA (SPI_Type *base, spi_dma_handle_t *handle, size_t *count)
 Get the transferred bytes for SPI slave DMA. More...
 
static void SPI_SlaveTransferCreateHandleDMA (SPI_Type *base, spi_dma_handle_t *handle, spi_dma_callback_t callback, void *userData, dma_handle_t *txHandle, dma_handle_t *rxHandle)
 Initialize the SPI slave DMA handle. More...
 
static status_t SPI_SlaveTransferDMA (SPI_Type *base, spi_dma_handle_t *handle, spi_transfer_t *xfer)
 Perform a non-blocking SPI transfer using DMA. More...
 
static void SPI_SlaveTransferAbortDMA (SPI_Type *base, spi_dma_handle_t *handle)
 Abort a SPI transfer using DMA. More...
 
static status_t SPI_SlaveTransferGetCountDMA (SPI_Type *base, spi_dma_handle_t *handle, size_t *count)
 Get the transferred bytes for SPI slave DMA. More...
 

Data Structure Documentation

struct _spi_dma_handle

Data Fields

bool txInProgress
 Send transfer finished.
 
bool rxInProgress
 Receive transfer finished.
 
dma_handle_t * txHandle
 DMA handler for SPI send.
 
dma_handle_t * rxHandle
 DMA handler for SPI receive.
 
uint8_t bytesPerFrame
 Bytes in a frame for SPI transfer.
 
spi_dma_callback_t callback
 Callback for SPI DMA transfer.
 
void * userData
 User Data for SPI DMA callback.
 
uint32_t state
 Internal state of SPI DMA transfer.
 
size_t transferSize
 Bytes need to be transfer.
 

Macro Definition Documentation

#define FSL_SPI_DMA_DRIVER_VERSION   (MAKE_VERSION(2, 1, 1))

Typedef Documentation

typedef void(* spi_dma_callback_t)(SPI_Type *base, spi_dma_handle_t *handle, status_t status, void *userData)

Function Documentation

void SPI_MasterTransferCreateHandleDMA ( SPI_Type *  base,
spi_dma_handle_t *  handle,
spi_dma_callback_t  callback,
void *  userData,
dma_handle_t *  txHandle,
dma_handle_t *  rxHandle 
)

This function initializes the SPI master DMA handle which can be used for other SPI master transactional APIs. Usually, for a specified SPI instance, user need only call this API once to get the initialized handle.

Parameters
baseSPI peripheral base address.
handleSPI handle pointer.
callbackUser callback function called at the end of a transfer.
userDataUser data for callback.
txHandleDMA handle pointer for SPI Tx, the handle shall be static allocated by users.
rxHandleDMA handle pointer for SPI Rx, the handle shall be static allocated by users.
status_t SPI_MasterTransferDMA ( SPI_Type *  base,
spi_dma_handle_t *  handle,
spi_transfer_t *  xfer 
)
Note
This interface returned immediately after transfer initiates, users should call SPI_GetTransferStatus to poll the transfer status to check whether SPI transfer finished.
Parameters
baseSPI peripheral base address.
handleSPI DMA handle pointer.
xferPointer to dma transfer structure.
Return values
kStatus_SuccessSuccessfully start a transfer.
kStatus_InvalidArgumentInput argument is invalid.
kStatus_SPI_BusySPI is not idle, is running another transfer.
void SPI_MasterTransferAbortDMA ( SPI_Type *  base,
spi_dma_handle_t *  handle 
)
Parameters
baseSPI peripheral base address.
handleSPI DMA handle pointer.
status_t SPI_MasterTransferGetCountDMA ( SPI_Type *  base,
spi_dma_handle_t *  handle,
size_t *  count 
)
Parameters
baseSPI peripheral base address.
handleSPI DMA handle pointer.
countTransferred bytes.
Return values
kStatus_SPI_SuccessSucceed get the transfer count.
kStatus_NoTransferInProgressThere is not a non-blocking transaction currently in progress.
static void SPI_SlaveTransferCreateHandleDMA ( SPI_Type *  base,
spi_dma_handle_t *  handle,
spi_dma_callback_t  callback,
void *  userData,
dma_handle_t *  txHandle,
dma_handle_t *  rxHandle 
)
inlinestatic

This function initializes the SPI slave DMA handle which can be used for other SPI master transactional APIs. Usually, for a specified SPI instance, user need only call this API once to get the initialized handle.

Parameters
baseSPI peripheral base address.
handleSPI handle pointer.
callbackUser callback function called at the end of a transfer.
userDataUser data for callback.
txHandleDMA handle pointer for SPI Tx, the handle shall be static allocated by users.
rxHandleDMA handle pointer for SPI Rx, the handle shall be static allocated by users.
static status_t SPI_SlaveTransferDMA ( SPI_Type *  base,
spi_dma_handle_t *  handle,
spi_transfer_t *  xfer 
)
inlinestatic
Note
This interface returned immediately after transfer initiates, users should call SPI_GetTransferStatus to poll the transfer status to check whether SPI transfer finished.
Parameters
baseSPI peripheral base address.
handleSPI DMA handle pointer.
xferPointer to dma transfer structure.
Return values
kStatus_SuccessSuccessfully start a transfer.
kStatus_InvalidArgumentInput argument is invalid.
kStatus_SPI_BusySPI is not idle, is running another transfer.
static void SPI_SlaveTransferAbortDMA ( SPI_Type *  base,
spi_dma_handle_t *  handle 
)
inlinestatic
Parameters
baseSPI peripheral base address.
handleSPI DMA handle pointer.
static status_t SPI_SlaveTransferGetCountDMA ( SPI_Type *  base,
spi_dma_handle_t *  handle,
size_t *  count 
)
inlinestatic
Parameters
baseSPI peripheral base address.
handleSPI DMA handle pointer.
countTransferred bytes.
Return values
kStatus_SPI_SuccessSucceed get the transfer count.
kStatus_NoTransferInProgressThere is not a non-blocking transaction currently in progress.