The MCUXpresso SDK provides a peripheral driver for the thermal management unit (TMU) module of MCUXpresso SDK devices.
Typical use case
Monitor and report Configuration
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/tmu
|
| enum | {
kTMU_ImmediateTemperature0InterruptEnable,
kTMU_AverageTemperature0InterruptEnable,
kTMU_AverageTemperature0CriticalInterruptEnable,
kTMU_ImmediateTemperature1Interrupt1Enable,
kTMU_AverageTemperature1Interrupt1Enable,
kTMU_AverageTemperature1CriticalInterrupt1Enable
} |
| | TMU interrupt enable, _tmu_interrupt_enable. More...
|
| |
| enum | {
kTMU_ImmediateTemperature0InterruptStausFlags,
kTMU_AverageTemperature0InterruptStausFlags,
kTMU_AverageTemperature0CriticalInterruptStausFlags,
kTMU_ImmediateTemperature1Interrupt1StausFlags,
kTMU_AverageTemperature1Interrupt1StausFlags,
kTMU_AverageTemperature1CriticalInterrupt1StausFlags
} |
| | TMU interrupt enable, _tmu_interrupt_status_flags. More...
|
| |
| enum | tmu_probe_select_t {
kTMU_ProbeSelectMainProbe = 1U << 0U,
kTMU_ProbeSelectRemoteProbe = 1U << 1U,
kTMU_ProbeSelectBothProbes = ( 1U << 0U) | (1U << 1U)
} |
| | Probe selection. More...
|
| |
| enum | tmu_average_low_pass_filter_t {
kTMU_AverageLowPassFilter1_0 = 0U,
kTMU_AverageLowPassFilter0_5 = 1U,
kTMU_AverageLowPassFilter0_25 = 2U,
kTMU_AverageLowPassFilter0_125 = 3U
} |
| | Average low pass filter setting. More...
|
| |
|
| void | TMU_Init (TMU_Type *base, const tmu_config_t *config) |
| | Enable the access to TMU registers and Initialize TMU module. More...
|
| |
| void | TMU_Deinit (TMU_Type *base) |
| | De-initialize TMU module and Disable the access to DCDC registers. More...
|
| |
| void | TMU_Enable (TMU_Type *base, bool enable) |
| | Enable/disable TMU module. More...
|
| |
| void | TMU_GetDefaultConfig (tmu_config_t *config) |
| | Gets the default configuration for TMU. More...
|
| |
| static void | TMU_EnableInterrupts (TMU_Type *base, uint32_t mask) |
| | Enable the TMU interrupts. More...
|
| |
| static void | TMU_DisableInterrupts (TMU_Type *base, uint32_t mask) |
| | Disable the TMU interrupts. More...
|
| |
| static uint32_t | TMU_GetInterruptStatusFlags (TMU_Type *base) |
| | Get interrupt status flags. More...
|
| |
| static void | TMU_ClearInterruptStatusFlags (TMU_Type *base, uint32_t mask) |
| | Clear interrupt status flags. More...
|
| |
| status_t | TMU_GetImmediateTemperature (TMU_Type *base, tmu_probe_select_t probe, int8_t *temperature) |
| | Get the last immediate temperature at site. More...
|
| |
| status_t | TMU_GetAverageTemperature (TMU_Type *base, tmu_probe_select_t probe, int8_t *temperature) |
| | Get the last average temperature at site. More...
|
| |
| void | TMU_UpdateHighTemperatureThreshold (TMU_Type *base, tmu_probe_select_t probe, const tmu_threshold_config_t *thresholdConfig) |
| | Update the high temperature threshold value. More...
|
| |
| struct tmu_threshold_config_t |
| bool tmu_threshold_config_t::immediateThresholdEnable |
| bool tmu_threshold_config_t::AverageThresholdEnable |
| bool tmu_threshold_config_t::AverageCriticalThresholdEnable |
| uint8_t tmu_threshold_config_t::immediateThresholdValueOfMainProbe |
Valid when corresponding threshold is enabled. High temperature immediate threshold value of main probe. Besides, bit-8 is sign bit: 1 means nagetive and 0 means positive.
| uint8_t tmu_threshold_config_t::averageThresholdValueOfMainProbe |
Valid when corresponding threshold is enabled. High temperature average threshold value of main probe. Besides, bit-8 is sign bit: 1 means nagetive and 0 means positive.
| uint8_t tmu_threshold_config_t::averageCriticalThresholdValueOfMainProbe |
Valid when corresponding threshold is enabled. High temperature average critical threshold value of main probe. Besides, bit-8 is sign bit: 1 means nagetive and 0 means positive.
| uint8_t tmu_threshold_config_t::immediateThresholdValueOfRemoteProbe |
Valid when corresponding threshold is enabled. High temperature immediate threshold value of remote probe. Besides, bit-8 is sign bit: 1 means nagetive and 0 means positive.
| uint8_t tmu_threshold_config_t::averageThresholdValueOfRemoteProbe |
Valid when corresponding threshold is enabled. High temperature average threshold value of remote probe. Besides, bit-8 is sign bit: 1 means nagetive and 0 means positive.
| uint8_t tmu_threshold_config_t::averageCriticalThresholdValueOfRemoteProbe |
Valid when corresponding threshold is enabled. High temperature average critical threshold value of remote probe. Besides, bit-8 is sign bit: 1 means nagetive and 0 means positive.
For proper operation, this field should only change when monitoring is disabled.
| Enumerator |
|---|
| kTMU_ImmediateTemperature0InterruptEnable |
Immediate temperature threshold exceeded interrupt enable of probe0.
|
| kTMU_AverageTemperature0InterruptEnable |
Average temperature threshold exceeded interrupt enable of probe0.
|
| kTMU_AverageTemperature0CriticalInterruptEnable |
Average temperature critical threshold exceeded interrupt enable of probe0.
|
| kTMU_ImmediateTemperature1Interrupt1Enable |
Immediate temperature threshold exceeded interrupt enable of probe1.
|
| kTMU_AverageTemperature1Interrupt1Enable |
Average temperature threshold exceeded interrupt enable of probe1.
|
| kTMU_AverageTemperature1CriticalInterrupt1Enable |
Average temperature critical threshold exceeded interrupt enable of probe1.
|
| Enumerator |
|---|
| kTMU_ImmediateTemperature0InterruptStausFlags |
Immediate temperature threshold exceeded interrupt status of probe0.
|
| kTMU_AverageTemperature0InterruptStausFlags |
Average temperature threshold exceeded interrupt status of probe0.
|
| kTMU_AverageTemperature0CriticalInterruptStausFlags |
Average temperature critical threshold exceeded interrupt status of probe0.
|
| kTMU_ImmediateTemperature1Interrupt1StausFlags |
Immediate temperature threshold exceeded interrupt status of probe1.
|
| kTMU_AverageTemperature1Interrupt1StausFlags |
Average temperature threshold exceeded interrupt status of probe1.
|
| kTMU_AverageTemperature1CriticalInterrupt1StausFlags |
Average temperature critical threshold exceeded interrupt status of probe1.
|
| Enumerator |
|---|
| kTMU_ProbeSelectMainProbe |
Select the main probe only.
|
| kTMU_ProbeSelectRemoteProbe |
Select the remote probe(near A53) only.
|
| kTMU_ProbeSelectBothProbes |
Select both 2 probes.
|
| Enumerator |
|---|
| kTMU_AverageLowPassFilter1_0 |
Average low pass filter = 1.
|
| kTMU_AverageLowPassFilter0_5 |
Average low pass filter = 0.5.
|
| kTMU_AverageLowPassFilter0_25 |
Average low pass filter = 0.25.
|
| kTMU_AverageLowPassFilter0_125 |
Average low pass filter = 0.125.
|
| void TMU_Init |
( |
TMU_Type * |
base, |
|
|
const tmu_config_t * |
config |
|
) |
| |
- Parameters
-
| base | TMU peripheral base address. |
| config | Pointer to configuration structure. Refer to "tmu_config_t" structure. |
| void TMU_Deinit |
( |
TMU_Type * |
base | ) |
|
- Parameters
-
| base | TMU peripheral base address. |
| void TMU_Enable |
( |
TMU_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
- Parameters
-
| base | TMU peripheral base address. |
| enable | enable or disable TMU. |
This function initializes the user configuration structure to default value. The default value are:
Example:
config.thresholdConfig.immediateThresholdEnable = false;
config.thresholdConfig.immediateThresholdValue = DEMO_TMU_IMMEDIATE_THRESOLD;
config.thresholdConfig.AverageThresholdEnable = true;
config.thresholdConfig.averageThresholdValue = DEMO_TMU_AVERAGE_THRESOLD;
config.thresholdConfig.AverageCriticalThresholdEnable = false;
config.thresholdConfig.averageCriticalThresholdValue = DEMO_TMU_AVERAGE_CRITICAL_THRESOLD;
- Parameters
-
| config | Pointer to TMU configuration structure. |
| static void TMU_EnableInterrupts |
( |
TMU_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | TMU peripheral base address. |
| mask | The interrupt mask. Refer to "_tmu_interrupt_enable" enumeration. |
| static void TMU_DisableInterrupts |
( |
TMU_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | TMU peripheral base address. |
| mask | The interrupt mask. Refer to "_tmu_interrupt_enable" enumeration. |
| static uint32_t TMU_GetInterruptStatusFlags |
( |
TMU_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | TMU peripheral base address. |
- Return values
-
| The | current interrupt status. |
| static void TMU_ClearInterruptStatusFlags |
( |
TMU_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | TMU peripheral base address. |
| mask | The mask of interrupt status flags. Refer to "_tmu_interrupt_status_flags" enumeration. |
- Parameters
-
| base | TMU peripheral base address. |
| probe | probe selection, if select both 2 probes, return main probe temeperature by default. Refer to "tmu_probe_select_t" structure. |
| temperature | Last immediate temperature reading at site when V=1. besides, Bit-8 is sign bit: 1 means nagetive and 0 means positive. |
- Return values
-
| get | immediate temperature status. |
- Parameters
-
| base | TMU peripheral base address. |
| probe | probe selection, if select both 2 probes, return main probe temeperature by default. Refer to "tmu_probe_select_t" structure. |
| temperature | Last average temperature reading at site; besides, Bit-8 is sign bit: 1 means nagetive and 0 means positive. |
- Return values
-
| get | average temperature status. |
- Parameters
-
| base | TMU peripheral base address. |
| probe | probe selection, if select both 2 probes, set main probe path by default. Refer to "tmu_probe_select_t" structure. |
| thresholdConfig | threshold configuration. Refer to "tmu_threshold_config_t" structure. |