![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | uart_sdma_handle_t |
| UART sDMA handle. More... | |
Typedefs | |
| typedef void(* | uart_sdma_transfer_callback_t )(UART_Type *base, uart_sdma_handle_t *handle, status_t status, void *userData) |
| UART transfer callback function. More... | |
Driver version | |
| #define | FSL_UART_SDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 1)) |
| UART SDMA driver version 2.1.1. More... | |
sDMA transactional | |
| void | UART_TransferCreateHandleSDMA (UART_Type *base, uart_sdma_handle_t *handle, uart_sdma_transfer_callback_t callback, void *userData, sdma_handle_t *txSdmaHandle, sdma_handle_t *rxSdmaHandle, uint32_t eventSourceTx, uint32_t eventSourceRx) |
| Initializes the UART handle which is used in transactional functions. More... | |
| status_t | UART_SendSDMA (UART_Type *base, uart_sdma_handle_t *handle, uart_transfer_t *xfer) |
| Sends data using sDMA. More... | |
| status_t | UART_ReceiveSDMA (UART_Type *base, uart_sdma_handle_t *handle, uart_transfer_t *xfer) |
| Receives data using sDMA. More... | |
| void | UART_TransferAbortSendSDMA (UART_Type *base, uart_sdma_handle_t *handle) |
| Aborts the sent data using sDMA. More... | |
| void | UART_TransferAbortReceiveSDMA (UART_Type *base, uart_sdma_handle_t *handle) |
| Aborts the receive data using sDMA. More... | |
| struct _uart_sdma_handle |
Data Fields | |
| uart_sdma_transfer_callback_t | callback |
| Callback function. More... | |
| void * | userData |
| UART callback function parameter. More... | |
| size_t | rxDataSizeAll |
| Size of the data to receive. More... | |
| size_t | txDataSizeAll |
| Size of the data to send out. More... | |
| sdma_handle_t * | txSdmaHandle |
| The sDMA TX channel used. More... | |
| sdma_handle_t * | rxSdmaHandle |
| The sDMA RX channel used. More... | |
| volatile uint8_t | txState |
| TX transfer state. More... | |
| volatile uint8_t | rxState |
| RX transfer state. | |
| uart_sdma_transfer_callback_t uart_sdma_handle_t::callback |
| void* uart_sdma_handle_t::userData |
| size_t uart_sdma_handle_t::rxDataSizeAll |
| size_t uart_sdma_handle_t::txDataSizeAll |
| sdma_handle_t* uart_sdma_handle_t::txSdmaHandle |
| sdma_handle_t* uart_sdma_handle_t::rxSdmaHandle |
| volatile uint8_t uart_sdma_handle_t::txState |
| #define FSL_UART_SDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 1)) |
| typedef void(* uart_sdma_transfer_callback_t)(UART_Type *base, uart_sdma_handle_t *handle, status_t status, void *userData) |
| void UART_TransferCreateHandleSDMA | ( | UART_Type * | base, |
| uart_sdma_handle_t * | handle, | ||
| uart_sdma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| sdma_handle_t * | txSdmaHandle, | ||
| sdma_handle_t * | rxSdmaHandle, | ||
| uint32_t | eventSourceTx, | ||
| uint32_t | eventSourceRx | ||
| ) |
| base | UART peripheral base address. |
| handle | Pointer to the uart_sdma_handle_t structure. |
| callback | UART callback, NULL means no callback. |
| userData | User callback function data. |
| rxSdmaHandle | User-requested DMA handle for RX DMA transfer. |
| txSdmaHandle | User-requested DMA handle for TX DMA transfer. |
| eventSourceTx | Eventsource for TX DMA transfer. |
| eventSourceRx | Eventsource for RX DMA transfer. |
| status_t UART_SendSDMA | ( | UART_Type * | base, |
| uart_sdma_handle_t * | handle, | ||
| uart_transfer_t * | xfer | ||
| ) |
This function sends data using sDMA. This is a non-blocking function, which returns right away. When all data is sent, the send callback function is called.
| base | UART peripheral base address. |
| handle | UART handle pointer. |
| xfer | UART sDMA transfer structure. See uart_transfer_t. |
| kStatus_Success | if succeeded; otherwise failed. |
| kStatus_UART_TxBusy | Previous transfer ongoing. |
| kStatus_InvalidArgument | Invalid argument. |
| status_t UART_ReceiveSDMA | ( | UART_Type * | base, |
| uart_sdma_handle_t * | handle, | ||
| uart_transfer_t * | xfer | ||
| ) |
This function receives data using sDMA. This is a non-blocking function, which returns right away. When all data is received, the receive callback function is called.
| base | UART peripheral base address. |
| handle | Pointer to the uart_sdma_handle_t structure. |
| xfer | UART sDMA transfer structure. See uart_transfer_t. |
| kStatus_Success | if succeeded; otherwise failed. |
| kStatus_UART_RxBusy | Previous transfer ongoing. |
| kStatus_InvalidArgument | Invalid argument. |
| void UART_TransferAbortSendSDMA | ( | UART_Type * | base, |
| uart_sdma_handle_t * | handle | ||
| ) |
This function aborts sent data using sDMA.
| base | UART peripheral base address. |
| handle | Pointer to the uart_sdma_handle_t structure. |
| void UART_TransferAbortReceiveSDMA | ( | UART_Type * | base, |
| uart_sdma_handle_t * | handle | ||
| ) |
This function aborts receive data using sDMA.
| base | UART peripheral base address. |
| handle | Pointer to the uart_sdma_handle_t structure. |