MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
IOMUXC: IOMUX Controller

Overview

IOMUXC driver provides APIs for pin configuration. It also supports the miscellaneous functions integrated in IOMUXC.

Files

file  fsl_iomuxc.h
 

Driver version

#define FSL_IOMUXC_DRIVER_VERSION   (MAKE_VERSION(2, 0, 4))
 IOMUXC driver version 2.0.4. More...
 

Pin function ID

The pin function ID is a tuple of <muxRegister muxMode inputRegister inputDaisy configRegister>

#define IOMUXC_BOOT_MODE0_SRC_BOOT_MODE0   0x00000000, 0x0, 0x00000000, 0x0, 0x30330250
 
#define IOMUXC_BOOT_MODE1_SRC_BOOT_MODE1   0x00000000, 0x0, 0x00000000, 0x0, 0x30330254
 
#define IOMUXC_BOOT_MODE2_SRC_BOOT_MODE2   0x00000000, 0x0, 0x00000000, 0x0, 0x30330258
 
#define IOMUXC_BOOT_MODE3_SRC_BOOT_MODE3   0x00000000, 0x0, 0x00000000, 0x0, 0x3033025C
 
#define IOMUXC_JTAG_MOD_JTAG_MODE   0x00000000, 0x0, 0x00000000, 0x0, 0x30330260
 
#define IOMUXC_JTAG_TDI_JTAG_TDI   0x00000000, 0x0, 0x00000000, 0x0, 0x30330264
 
#define IOMUXC_JTAG_TMS_JTAG_TMS   0x00000000, 0x0, 0x00000000, 0x0, 0x30330268
 
#define IOMUXC_JTAG_TCK_JTAG_TCK   0x00000000, 0x0, 0x00000000, 0x0, 0x3033026C
 
#define IOMUXC_JTAG_TDO_JTAG_TDO   0x00000000, 0x0, 0x00000000, 0x0, 0x30330270
 
#define IOMUXC_RTC_XTALI_SNVS_RTC   0x00000000, 0x0, 0x00000000, 0x0, 0x00000000
 
#define IOMUXC_PMIC_STBY_REQ_CCM_PMIC_STBY_REQ   0x00000000, 0x0, 0x00000000, 0x0, 0x00000000
 
#define IOMUXC_PMIC_ON_REQ_SNVS_PMIC_ON_REQ   0x00000000, 0x0, 0x00000000, 0x0, 0x00000000
 
#define IOMUXC_ONOFF_SNVS_ONOFF   0x00000000, 0x0, 0x00000000, 0x0, 0x00000000
 
#define IOMUXC_POR_B_SNVS_POR_B   0x00000000, 0x0, 0x00000000, 0x0, 0x00000000
 
#define IOMUXC_GPIO1_IO00_GPIO1_IO00   0x30330014, 0x0, 0x00000000, 0x0, 0x30330274
 
#define IOMUXC_GPIO1_IO00_CCM_ENET_PHY_REF_CLK_ROOT   0x30330014, 0x1, 0x00000000, 0x0, 0x30330274
 
#define IOMUXC_GPIO1_IO00_ISP_FL_TRIG_0   0x30330014, 0x3, 0x303305D4, 0x0, 0x30330274
 
#define IOMUXC_GPIO1_IO00_ANAMIX_REF_CLK_32K   0x30330014, 0x5, 0x00000000, 0x0, 0x30330274
 
#define IOMUXC_GPIO1_IO00_CCM_EXT_CLK1   0x30330014, 0x6, 0x00000000, 0x0, 0x30330274
 
#define IOMUXC_GPIO1_IO01_GPIO1_IO01   0x30330018, 0x0, 0x00000000, 0x0, 0x30330278
 
#define IOMUXC_GPIO1_IO01_PWM1_OUT   0x30330018, 0x1, 0x00000000, 0x0, 0x30330278
 
#define IOMUXC_GPIO1_IO01_ISP_SHUTTER_TRIG_0   0x30330018, 0x3, 0x303305DC, 0x0, 0x30330278
 
#define IOMUXC_GPIO1_IO01_ANAMIX_REF_CLK_24M   0x30330018, 0x5, 0x00000000, 0x0, 0x30330278
 
#define IOMUXC_GPIO1_IO01_CCM_EXT_CLK2   0x30330018, 0x6, 0x00000000, 0x0, 0x30330278
 
#define IOMUXC_GPIO1_IO02_GPIO1_IO02   0x3033001C, 0x0, 0x00000000, 0x0, 0x3033027C
 
#define IOMUXC_GPIO1_IO02_WDOG1_WDOG_B   0x3033001C, 0x1, 0x00000000, 0x0, 0x3033027C
 
#define IOMUXC_GPIO1_IO02_ISP_FLASH_TRIG_0   0x3033001C, 0x3, 0x00000000, 0x0, 0x3033027C
 
#define IOMUXC_GPIO1_IO02_WDOG1_WDOG_ANY   0x3033001C, 0x5, 0x00000000, 0x0, 0x3033027C
 
#define IOMUXC_GPIO1_IO02_SJC_DE_B   0x3033001C, 0x7, 0x00000000, 0x0, 0x3033027C
 
#define IOMUXC_GPIO1_IO03_GPIO1_IO03   0x30330020, 0x0, 0x00000000, 0x0, 0x30330280
 
#define IOMUXC_GPIO1_IO03_USDHC1_VSELECT   0x30330020, 0x1, 0x00000000, 0x0, 0x30330280
 
#define IOMUXC_GPIO1_IO03_ISP_PRELIGHT_TRIG_0   0x30330020, 0x3, 0x00000000, 0x0, 0x30330280
 
#define IOMUXC_GPIO1_IO03_SDMA1_EXT_EVENT0   0x30330020, 0x5, 0x00000000, 0x0, 0x30330280
 
#define IOMUXC_GPIO1_IO04_GPIO1_IO04   0x30330024, 0x0, 0x00000000, 0x0, 0x30330284
 
#define IOMUXC_GPIO1_IO04_USDHC2_VSELECT   0x30330024, 0x1, 0x00000000, 0x0, 0x30330284
 
#define IOMUXC_GPIO1_IO04_ISP_SHUTTER_OPEN_0   0x30330024, 0x3, 0x00000000, 0x0, 0x30330284
 
#define IOMUXC_GPIO1_IO04_SDMA1_EXT_EVENT1   0x30330024, 0x5, 0x00000000, 0x0, 0x30330284
 
#define IOMUXC_GPIO1_IO05_GPIO1_IO05   0x30330028, 0x0, 0x00000000, 0x0, 0x30330288
 
#define IOMUXC_GPIO1_IO05_M7_NMI   0x30330028, 0x1, 0x00000000, 0x0, 0x30330288
 
#define IOMUXC_GPIO1_IO05_ISP_FL_TRIG_1   0x30330028, 0x3, 0x303305D8, 0x0, 0x30330288
 
#define IOMUXC_GPIO1_IO05_CCM_PMIC_READY   0x30330028, 0x5, 0x30330554, 0x0, 0x30330288
 
#define IOMUXC_GPIO1_IO06_GPIO1_IO06   0x3033002C, 0x0, 0x00000000, 0x0, 0x3033028C
 
#define IOMUXC_GPIO1_IO06_ENET_QOS_MDC   0x3033002C, 0x1, 0x00000000, 0x0, 0x3033028C
 
#define IOMUXC_GPIO1_IO06_ISP_SHUTTER_TRIG_1   0x3033002C, 0x3, 0x303305E0, 0x0, 0x3033028C
 
#define IOMUXC_GPIO1_IO06_USDHC1_CD_B   0x3033002C, 0x5, 0x00000000, 0x0, 0x3033028C
 
#define IOMUXC_GPIO1_IO06_CCM_EXT_CLK3   0x3033002C, 0x6, 0x00000000, 0x0, 0x3033028C
 
#define IOMUXC_GPIO1_IO07_GPIO1_IO07   0x30330030, 0x0, 0x00000000, 0x0, 0x30330290
 
#define IOMUXC_GPIO1_IO07_ENET_QOS_MDIO   0x30330030, 0x1, 0x30330590, 0x0, 0x30330290
 
#define IOMUXC_GPIO1_IO07_ISP_FLASH_TRIG_1   0x30330030, 0x3, 0x00000000, 0x0, 0x30330290
 
#define IOMUXC_GPIO1_IO07_USDHC1_WP   0x30330030, 0x5, 0x00000000, 0x0, 0x30330290
 
#define IOMUXC_GPIO1_IO07_CCM_EXT_CLK4   0x30330030, 0x6, 0x00000000, 0x0, 0x30330290
 
#define IOMUXC_GPIO1_IO08_GPIO1_IO08   0x30330034, 0x0, 0x00000000, 0x0, 0x30330294
 
#define IOMUXC_GPIO1_IO08_ENET_QOS_1588_EVENT0_IN   0x30330034, 0x1, 0x00000000, 0x0, 0x30330294
 
#define IOMUXC_GPIO1_IO08_PWM1_OUT   0x30330034, 0x2, 0x00000000, 0x0, 0x30330294
 
#define IOMUXC_GPIO1_IO08_ISP_PRELIGHT_TRIG_1   0x30330034, 0x3, 0x00000000, 0x0, 0x30330294
 
#define IOMUXC_GPIO1_IO08_ENET_QOS_1588_EVENT0_AUX_IN   0x30330034, 0x4, 0x00000000, 0x0, 0x30330294
 
#define IOMUXC_GPIO1_IO08_USDHC2_RESET_B   0x30330034, 0x5, 0x00000000, 0x0, 0x30330294
 
#define IOMUXC_GPIO1_IO09_GPIO1_IO09   0x30330038, 0x0, 0x00000000, 0x0, 0x30330298
 
#define IOMUXC_GPIO1_IO09_ENET_QOS_1588_EVENT0_OUT   0x30330038, 0x1, 0x00000000, 0x0, 0x30330298
 
#define IOMUXC_GPIO1_IO09_PWM2_OUT   0x30330038, 0x2, 0x00000000, 0x0, 0x30330298
 
#define IOMUXC_GPIO1_IO09_ISP_SHUTTER_OPEN_1   0x30330038, 0x3, 0x00000000, 0x0, 0x30330298
 
#define IOMUXC_GPIO1_IO09_USDHC3_RESET_B   0x30330038, 0x4, 0x00000000, 0x0, 0x30330298
 
#define IOMUXC_GPIO1_IO09_SDMA2_EXT_EVENT0   0x30330038, 0x5, 0x00000000, 0x0, 0x30330298
 
#define IOMUXC_GPIO1_IO10_GPIO1_IO10   0x3033003C, 0x0, 0x00000000, 0x0, 0x3033029C
 
#define IOMUXC_GPIO1_IO10_USB1_ID   0x3033003C, 0x1, 0x00000000, 0x0, 0x3033029C
 
#define IOMUXC_GPIO1_IO10_PWM3_OUT   0x3033003C, 0x2, 0x00000000, 0x0, 0x3033029C
 
#define IOMUXC_GPIO1_IO11_GPIO1_IO11   0x30330040, 0x0, 0x00000000, 0x0, 0x303302A0
 
#define IOMUXC_GPIO1_IO11_USB2_ID   0x30330040, 0x1, 0x00000000, 0x0, 0x303302A0
 
#define IOMUXC_GPIO1_IO11_PWM2_OUT   0x30330040, 0x2, 0x00000000, 0x0, 0x303302A0
 
#define IOMUXC_GPIO1_IO11_USDHC3_VSELECT   0x30330040, 0x4, 0x00000000, 0x0, 0x303302A0
 
#define IOMUXC_GPIO1_IO11_CCM_PMIC_READY   0x30330040, 0x5, 0x30330554, 0x1, 0x303302A0
 
#define IOMUXC_GPIO1_IO12_GPIO1_IO12   0x30330044, 0x0, 0x00000000, 0x0, 0x303302A4
 
#define IOMUXC_GPIO1_IO12_USB1_PWR   0x30330044, 0x1, 0x00000000, 0x0, 0x303302A4
 
#define IOMUXC_GPIO1_IO12_SDMA2_EXT_EVENT1   0x30330044, 0x5, 0x00000000, 0x0, 0x303302A4
 
#define IOMUXC_GPIO1_IO13_GPIO1_IO13   0x30330048, 0x0, 0x00000000, 0x0, 0x303302A8
 
#define IOMUXC_GPIO1_IO13_USB1_OC   0x30330048, 0x1, 0x00000000, 0x0, 0x303302A8
 
#define IOMUXC_GPIO1_IO13_PWM2_OUT   0x30330048, 0x5, 0x00000000, 0x0, 0x303302A8
 
#define IOMUXC_GPIO1_IO14_GPIO1_IO14   0x3033004C, 0x0, 0x00000000, 0x0, 0x303302AC
 
#define IOMUXC_GPIO1_IO14_USB2_PWR   0x3033004C, 0x1, 0x00000000, 0x0, 0x303302AC
 
#define IOMUXC_GPIO1_IO14_USDHC3_CD_B   0x3033004C, 0x4, 0x30330608, 0x0, 0x303302AC
 
#define IOMUXC_GPIO1_IO14_PWM3_OUT   0x3033004C, 0x5, 0x00000000, 0x0, 0x303302AC
 
#define IOMUXC_GPIO1_IO14_CCM_CLKO1   0x3033004C, 0x6, 0x00000000, 0x0, 0x303302AC
 
#define IOMUXC_GPIO1_IO15_GPIO1_IO15   0x30330050, 0x0, 0x00000000, 0x0, 0x303302B0
 
#define IOMUXC_GPIO1_IO15_USB2_OC   0x30330050, 0x1, 0x00000000, 0x0, 0x303302B0
 
#define IOMUXC_GPIO1_IO15_USDHC3_WP   0x30330050, 0x4, 0x30330634, 0x0, 0x303302B0
 
#define IOMUXC_GPIO1_IO15_PWM4_OUT   0x30330050, 0x5, 0x00000000, 0x0, 0x303302B0
 
#define IOMUXC_GPIO1_IO15_CCM_CLKO2   0x30330050, 0x6, 0x00000000, 0x0, 0x303302B0
 
#define IOMUXC_ENET_MDC_ENET_QOS_MDC   0x30330054, 0x0, 0x00000000, 0x0, 0x303302B4
 
#define IOMUXC_ENET_MDC_AUDIOMIX_SAI6_TX_DATA0   0x30330054, 0x2, 0x00000000, 0x0, 0x303302B4
 
#define IOMUXC_ENET_MDC_GPIO1_IO16   0x30330054, 0x5, 0x00000000, 0x0, 0x303302B4
 
#define IOMUXC_ENET_MDC_USDHC3_STROBE   0x30330054, 0x6, 0x30330630, 0x0, 0x303302B4
 
#define IOMUXC_ENET_MDIO_ENET_QOS_MDIO   0x30330058, 0x0, 0x30330590, 0x1, 0x303302B8
 
#define IOMUXC_ENET_MDIO_AUDIOMIX_SAI6_TX_SYNC   0x30330058, 0x2, 0x30330528, 0x0, 0x303302B8
 
#define IOMUXC_ENET_MDIO_AUDIOMIX_PDM_BIT_STREAM3   0x30330058, 0x3, 0x303304CC, 0x0, 0x303302B8
 
#define IOMUXC_ENET_MDIO_GPIO1_IO17   0x30330058, 0x5, 0x00000000, 0x0, 0x303302B8
 
#define IOMUXC_ENET_MDIO_USDHC3_DATA5   0x30330058, 0x6, 0x30330624, 0x0, 0x303302B8
 
#define IOMUXC_ENET_TD3_ENET_QOS_RGMII_TD3   0x3033005C, 0x0, 0x00000000, 0x0, 0x303302BC
 
#define IOMUXC_ENET_TD3_AUDIOMIX_SAI6_TX_BCLK   0x3033005C, 0x2, 0x30330524, 0x0, 0x303302BC
 
#define IOMUXC_ENET_TD3_AUDIOMIX_PDM_BIT_STREAM2   0x3033005C, 0x3, 0x303304C8, 0x0, 0x303302BC
 
#define IOMUXC_ENET_TD3_GPIO1_IO18   0x3033005C, 0x5, 0x00000000, 0x0, 0x303302BC
 
#define IOMUXC_ENET_TD3_USDHC3_DATA6   0x3033005C, 0x6, 0x30330628, 0x0, 0x303302BC
 
#define IOMUXC_ENET_TD2_ENET_QOS_RGMII_TD2   0x30330060, 0x0, 0x00000000, 0x0, 0x303302C0
 
#define IOMUXC_ENET_TD2_CCM_ENET_QOS_CLOCK_GENERATE_REF_CLK   0x30330060, 0x1, 0x00000000, 0x0, 0x303302C0
 
#define IOMUXC_ENET_TD2_AUDIOMIX_SAI6_RX_DATA0   0x30330060, 0x2, 0x3033051C, 0x0, 0x303302C0
 
#define IOMUXC_ENET_TD2_AUDIOMIX_PDM_BIT_STREAM1   0x30330060, 0x3, 0x303304C4, 0x0, 0x303302C0
 
#define IOMUXC_ENET_TD2_GPIO1_IO19   0x30330060, 0x5, 0x00000000, 0x0, 0x303302C0
 
#define IOMUXC_ENET_TD2_USDHC3_DATA7   0x30330060, 0x6, 0x3033062C, 0x0, 0x303302C0
 
#define IOMUXC_ENET_TD1_ENET_QOS_RGMII_TD1   0x30330064, 0x0, 0x00000000, 0x0, 0x303302C4
 
#define IOMUXC_ENET_TD1_AUDIOMIX_SAI6_RX_SYNC   0x30330064, 0x2, 0x30330520, 0x0, 0x303302C4
 
#define IOMUXC_ENET_TD1_AUDIOMIX_PDM_BIT_STREAM0   0x30330064, 0x3, 0x303304C0, 0x0, 0x303302C4
 
#define IOMUXC_ENET_TD1_GPIO1_IO20   0x30330064, 0x5, 0x00000000, 0x0, 0x303302C4
 
#define IOMUXC_ENET_TD1_USDHC3_CD_B   0x30330064, 0x6, 0x30330608, 0x1, 0x303302C4
 
#define IOMUXC_ENET_TD0_ENET_QOS_RGMII_TD0   0x30330068, 0x0, 0x00000000, 0x0, 0x303302C8
 
#define IOMUXC_ENET_TD0_AUDIOMIX_SAI6_RX_BCLK   0x30330068, 0x2, 0x30330518, 0x0, 0x303302C8
 
#define IOMUXC_ENET_TD0_AUDIOMIX_PDM_CLK   0x30330068, 0x3, 0x00000000, 0x0, 0x303302C8
 
#define IOMUXC_ENET_TD0_GPIO1_IO21   0x30330068, 0x5, 0x00000000, 0x0, 0x303302C8
 
#define IOMUXC_ENET_TD0_USDHC3_WP   0x30330068, 0x6, 0x30330634, 0x1, 0x303302C8
 
#define IOMUXC_ENET_TX_CTL_ENET_QOS_RGMII_TX_CTL   0x3033006C, 0x0, 0x00000000, 0x0, 0x303302CC
 
#define IOMUXC_ENET_TX_CTL_AUDIOMIX_SAI6_MCLK   0x3033006C, 0x2, 0x30330514, 0x0, 0x303302CC
 
#define IOMUXC_ENET_TX_CTL_AUDIOMIX_SPDIF1_OUT   0x3033006C, 0x3, 0x00000000, 0x0, 0x303302CC
 
#define IOMUXC_ENET_TX_CTL_GPIO1_IO22   0x3033006C, 0x5, 0x00000000, 0x0, 0x303302CC
 
#define IOMUXC_ENET_TX_CTL_USDHC3_DATA0   0x3033006C, 0x6, 0x30330610, 0x0, 0x303302CC
 
#define IOMUXC_ENET_TXC_CCM_ENET_QOS_CLOCK_GENERATE_TX_CLK   0x30330070, 0x0, 0x00000000, 0x0, 0x303302D0
 
#define IOMUXC_ENET_TXC_ENET_QOS_TX_ER   0x30330070, 0x1, 0x00000000, 0x0, 0x303302D0
 
#define IOMUXC_ENET_TXC_AUDIOMIX_SAI7_TX_DATA0   0x30330070, 0x2, 0x00000000, 0x0, 0x303302D0
 
#define IOMUXC_ENET_TXC_GPIO1_IO23   0x30330070, 0x5, 0x00000000, 0x0, 0x303302D0
 
#define IOMUXC_ENET_TXC_USDHC3_DATA1   0x30330070, 0x6, 0x30330614, 0x0, 0x303302D0
 
#define IOMUXC_ENET_RX_CTL_ENET_QOS_RGMII_RX_CTL   0x30330074, 0x0, 0x00000000, 0x0, 0x303302D4
 
#define IOMUXC_ENET_RX_CTL_AUDIOMIX_SAI7_TX_SYNC   0x30330074, 0x2, 0x30330540, 0x0, 0x303302D4
 
#define IOMUXC_ENET_RX_CTL_AUDIOMIX_PDM_BIT_STREAM3   0x30330074, 0x3, 0x303304CC, 0x1, 0x303302D4
 
#define IOMUXC_ENET_RX_CTL_GPIO1_IO24   0x30330074, 0x5, 0x00000000, 0x0, 0x303302D4
 
#define IOMUXC_ENET_RX_CTL_USDHC3_DATA2   0x30330074, 0x6, 0x30330618, 0x0, 0x303302D4
 
#define IOMUXC_ENET_RXC_CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK   0x30330078, 0x0, 0x00000000, 0x0, 0x303302D8
 
#define IOMUXC_ENET_RXC_ENET_QOS_RX_ER   0x30330078, 0x1, 0x00000000, 0x0, 0x303302D8
 
#define IOMUXC_ENET_RXC_AUDIOMIX_SAI7_TX_BCLK   0x30330078, 0x2, 0x3033053C, 0x0, 0x303302D8
 
#define IOMUXC_ENET_RXC_AUDIOMIX_PDM_BIT_STREAM2   0x30330078, 0x3, 0x303304C8, 0x1, 0x303302D8
 
#define IOMUXC_ENET_RXC_GPIO1_IO25   0x30330078, 0x5, 0x00000000, 0x0, 0x303302D8
 
#define IOMUXC_ENET_RXC_USDHC3_DATA3   0x30330078, 0x6, 0x3033061C, 0x0, 0x303302D8
 
#define IOMUXC_ENET_RD0_ENET_QOS_RGMII_RD0   0x3033007C, 0x0, 0x00000000, 0x0, 0x303302DC
 
#define IOMUXC_ENET_RD0_AUDIOMIX_SAI7_RX_DATA0   0x3033007C, 0x2, 0x30330534, 0x0, 0x303302DC
 
#define IOMUXC_ENET_RD0_AUDIOMIX_PDM_BIT_STREAM1   0x3033007C, 0x3, 0x303304C4, 0x1, 0x303302DC
 
#define IOMUXC_ENET_RD0_GPIO1_IO26   0x3033007C, 0x5, 0x00000000, 0x0, 0x303302DC
 
#define IOMUXC_ENET_RD0_USDHC3_DATA4   0x3033007C, 0x6, 0x30330620, 0x0, 0x303302DC
 
#define IOMUXC_ENET_RD1_ENET_QOS_RGMII_RD1   0x30330080, 0x0, 0x00000000, 0x0, 0x303302E0
 
#define IOMUXC_ENET_RD1_AUDIOMIX_SAI7_RX_SYNC   0x30330080, 0x2, 0x30330538, 0x0, 0x303302E0
 
#define IOMUXC_ENET_RD1_AUDIOMIX_PDM_BIT_STREAM0   0x30330080, 0x3, 0x303304C0, 0x1, 0x303302E0
 
#define IOMUXC_ENET_RD1_GPIO1_IO27   0x30330080, 0x5, 0x00000000, 0x0, 0x303302E0
 
#define IOMUXC_ENET_RD1_USDHC3_RESET_B   0x30330080, 0x6, 0x00000000, 0x0, 0x303302E0
 
#define IOMUXC_ENET_RD2_ENET_QOS_RGMII_RD2   0x30330084, 0x0, 0x00000000, 0x0, 0x303302E4
 
#define IOMUXC_ENET_RD2_AUDIOMIX_SAI7_RX_BCLK   0x30330084, 0x2, 0x30330530, 0x0, 0x303302E4
 
#define IOMUXC_ENET_RD2_AUDIOMIX_PDM_CLK   0x30330084, 0x3, 0x00000000, 0x0, 0x303302E4
 
#define IOMUXC_ENET_RD2_GPIO1_IO28   0x30330084, 0x5, 0x00000000, 0x0, 0x303302E4
 
#define IOMUXC_ENET_RD2_USDHC3_CLK   0x30330084, 0x6, 0x30330604, 0x0, 0x303302E4
 
#define IOMUXC_ENET_RD3_ENET_QOS_RGMII_RD3   0x30330088, 0x0, 0x00000000, 0x0, 0x303302E8
 
#define IOMUXC_ENET_RD3_AUDIOMIX_SAI7_MCLK   0x30330088, 0x2, 0x3033052C, 0x0, 0x303302E8
 
#define IOMUXC_ENET_RD3_AUDIOMIX_SPDIF1_IN   0x30330088, 0x3, 0x30330544, 0x0, 0x303302E8
 
#define IOMUXC_ENET_RD3_GPIO1_IO29   0x30330088, 0x5, 0x00000000, 0x0, 0x303302E8
 
#define IOMUXC_ENET_RD3_USDHC3_CMD   0x30330088, 0x6, 0x3033060C, 0x0, 0x303302E8
 
#define IOMUXC_SD1_CLK_USDHC1_CLK   0x3033008C, 0x0, 0x00000000, 0x0, 0x303302EC
 
#define IOMUXC_SD1_CLK_ENET1_MDC   0x3033008C, 0x1, 0x00000000, 0x0, 0x303302EC
 
#define IOMUXC_SD1_CLK_I2C5_SCL   0x3033008C, 0x3, 0x303305C4, 0x0, 0x303302EC
 
#define IOMUXC_SD1_CLK_UART1_TX   0x3033008C, 0x4, 0x00000000, 0x0, 0x303302EC
 
#define IOMUXC_SD1_CLK_UART1_RX   0x3033008C, 0x4, 0x303305E8, 0x0, 0x303302EC
 
#define IOMUXC_SD1_CLK_GPIO2_IO00   0x3033008C, 0x5, 0x00000000, 0x0, 0x303302EC
 
#define IOMUXC_SD1_CMD_USDHC1_CMD   0x30330090, 0x0, 0x00000000, 0x0, 0x303302F0
 
#define IOMUXC_SD1_CMD_ENET1_MDIO   0x30330090, 0x1, 0x3033057C, 0x0, 0x303302F0
 
#define IOMUXC_SD1_CMD_I2C5_SDA   0x30330090, 0x3, 0x303305C8, 0x0, 0x303302F0
 
#define IOMUXC_SD1_CMD_UART1_RX   0x30330090, 0x4, 0x303305E8, 0x1, 0x303302F0
 
#define IOMUXC_SD1_CMD_UART1_TX   0x30330090, 0x4, 0x00000000, 0x0, 0x303302F0
 
#define IOMUXC_SD1_CMD_GPIO2_IO01   0x30330090, 0x5, 0x00000000, 0x0, 0x303302F0
 
#define IOMUXC_SD1_DATA0_USDHC1_DATA0   0x30330094, 0x0, 0x00000000, 0x0, 0x303302F4
 
#define IOMUXC_SD1_DATA0_ENET1_RGMII_TD1   0x30330094, 0x1, 0x00000000, 0x0, 0x303302F4
 
#define IOMUXC_SD1_DATA0_I2C6_SCL   0x30330094, 0x3, 0x303305CC, 0x0, 0x303302F4
 
#define IOMUXC_SD1_DATA0_UART1_RTS_B   0x30330094, 0x4, 0x303305E4, 0x0, 0x303302F4
 
#define IOMUXC_SD1_DATA0_UART1_CTS_B   0x30330094, 0x4, 0x00000000, 0x0, 0x303302F4
 
#define IOMUXC_SD1_DATA0_GPIO2_IO02   0x30330094, 0x5, 0x00000000, 0x0, 0x303302F4
 
#define IOMUXC_SD1_DATA1_USDHC1_DATA1   0x30330098, 0x0, 0x00000000, 0x0, 0x303302F8
 
#define IOMUXC_SD1_DATA1_ENET1_RGMII_TD0   0x30330098, 0x1, 0x00000000, 0x0, 0x303302F8
 
#define IOMUXC_SD1_DATA1_I2C6_SDA   0x30330098, 0x3, 0x303305D0, 0x0, 0x303302F8
 
#define IOMUXC_SD1_DATA1_UART1_CTS_B   0x30330098, 0x4, 0x00000000, 0x0, 0x303302F8
 
#define IOMUXC_SD1_DATA1_UART1_RTS_B   0x30330098, 0x4, 0x303305E4, 0x1, 0x303302F8
 
#define IOMUXC_SD1_DATA1_GPIO2_IO03   0x30330098, 0x5, 0x00000000, 0x0, 0x303302F8
 
#define IOMUXC_SD1_DATA2_USDHC1_DATA2   0x3033009C, 0x0, 0x00000000, 0x0, 0x303302FC
 
#define IOMUXC_SD1_DATA2_ENET1_RGMII_RD0   0x3033009C, 0x1, 0x30330580, 0x0, 0x303302FC
 
#define IOMUXC_SD1_DATA2_I2C4_SCL   0x3033009C, 0x3, 0x303305BC, 0x0, 0x303302FC
 
#define IOMUXC_SD1_DATA2_UART2_TX   0x3033009C, 0x4, 0x00000000, 0x0, 0x303302FC
 
#define IOMUXC_SD1_DATA2_UART2_RX   0x3033009C, 0x4, 0x303305F0, 0x0, 0x303302FC
 
#define IOMUXC_SD1_DATA2_GPIO2_IO04   0x3033009C, 0x5, 0x00000000, 0x0, 0x303302FC
 
#define IOMUXC_SD1_DATA3_USDHC1_DATA3   0x303300A0, 0x0, 0x00000000, 0x0, 0x30330300
 
#define IOMUXC_SD1_DATA3_ENET1_RGMII_RD1   0x303300A0, 0x1, 0x30330584, 0x0, 0x30330300
 
#define IOMUXC_SD1_DATA3_I2C4_SDA   0x303300A0, 0x3, 0x303305C0, 0x0, 0x30330300
 
#define IOMUXC_SD1_DATA3_UART2_RX   0x303300A0, 0x4, 0x303305F0, 0x1, 0x30330300
 
#define IOMUXC_SD1_DATA3_UART2_TX   0x303300A0, 0x4, 0x00000000, 0x0, 0x30330300
 
#define IOMUXC_SD1_DATA3_GPIO2_IO05   0x303300A0, 0x5, 0x00000000, 0x0, 0x30330300
 
#define IOMUXC_SD1_DATA4_USDHC1_DATA4   0x303300A4, 0x0, 0x00000000, 0x0, 0x30330304
 
#define IOMUXC_SD1_DATA4_ENET1_RGMII_TX_CTL   0x303300A4, 0x1, 0x00000000, 0x0, 0x30330304
 
#define IOMUXC_SD1_DATA4_I2C1_SCL   0x303300A4, 0x3, 0x303305A4, 0x0, 0x30330304
 
#define IOMUXC_SD1_DATA4_UART2_RTS_B   0x303300A4, 0x4, 0x303305EC, 0x0, 0x30330304
 
#define IOMUXC_SD1_DATA4_UART2_CTS_B   0x303300A4, 0x4, 0x00000000, 0x0, 0x30330304
 
#define IOMUXC_SD1_DATA4_GPIO2_IO06   0x303300A4, 0x5, 0x00000000, 0x0, 0x30330304
 
#define IOMUXC_SD1_DATA5_USDHC1_DATA5   0x303300A8, 0x0, 0x00000000, 0x0, 0x30330308
 
#define IOMUXC_SD1_DATA5_ENET1_TX_ER   0x303300A8, 0x1, 0x00000000, 0x0, 0x30330308
 
#define IOMUXC_SD1_DATA5_I2C1_SDA   0x303300A8, 0x3, 0x303305A8, 0x0, 0x30330308
 
#define IOMUXC_SD1_DATA5_UART2_CTS_B   0x303300A8, 0x4, 0x00000000, 0x0, 0x30330308
 
#define IOMUXC_SD1_DATA5_UART2_RTS_B   0x303300A8, 0x4, 0x303305EC, 0x1, 0x30330308
 
#define IOMUXC_SD1_DATA5_GPIO2_IO07   0x303300A8, 0x5, 0x00000000, 0x0, 0x30330308
 
#define IOMUXC_SD1_DATA6_USDHC1_DATA6   0x303300AC, 0x0, 0x00000000, 0x0, 0x3033030C
 
#define IOMUXC_SD1_DATA6_ENET1_RGMII_RX_CTL   0x303300AC, 0x1, 0x30330588, 0x0, 0x3033030C
 
#define IOMUXC_SD1_DATA6_I2C2_SCL   0x303300AC, 0x3, 0x303305AC, 0x0, 0x3033030C
 
#define IOMUXC_SD1_DATA6_UART3_TX   0x303300AC, 0x4, 0x00000000, 0x0, 0x3033030C
 
#define IOMUXC_SD1_DATA6_UART3_RX   0x303300AC, 0x4, 0x303305F8, 0x0, 0x3033030C
 
#define IOMUXC_SD1_DATA6_GPIO2_IO08   0x303300AC, 0x5, 0x00000000, 0x0, 0x3033030C
 
#define IOMUXC_SD1_DATA7_USDHC1_DATA7   0x303300B0, 0x0, 0x00000000, 0x0, 0x30330310
 
#define IOMUXC_SD1_DATA7_ENET1_RX_ER   0x303300B0, 0x1, 0x3033058C, 0x0, 0x30330310
 
#define IOMUXC_SD1_DATA7_I2C2_SDA   0x303300B0, 0x3, 0x303305B0, 0x0, 0x30330310
 
#define IOMUXC_SD1_DATA7_UART3_RX   0x303300B0, 0x4, 0x303305F8, 0x1, 0x30330310
 
#define IOMUXC_SD1_DATA7_UART3_TX   0x303300B0, 0x4, 0x00000000, 0x0, 0x30330310
 
#define IOMUXC_SD1_DATA7_GPIO2_IO09   0x303300B0, 0x5, 0x00000000, 0x0, 0x30330310
 
#define IOMUXC_SD1_RESET_B_USDHC1_RESET_B   0x303300B4, 0x0, 0x00000000, 0x0, 0x30330314
 
#define IOMUXC_SD1_RESET_B_ENET1_TX_CLK   0x303300B4, 0x1, 0x30330578, 0x0, 0x30330314
 
#define IOMUXC_SD1_RESET_B_I2C3_SCL   0x303300B4, 0x3, 0x303305B4, 0x0, 0x30330314
 
#define IOMUXC_SD1_RESET_B_UART3_RTS_B   0x303300B4, 0x4, 0x303305F4, 0x0, 0x30330314
 
#define IOMUXC_SD1_RESET_B_UART3_CTS_B   0x303300B4, 0x4, 0x00000000, 0x0, 0x30330314
 
#define IOMUXC_SD1_RESET_B_GPIO2_IO10   0x303300B4, 0x5, 0x00000000, 0x0, 0x30330314
 
#define IOMUXC_SD1_STROBE_USDHC1_STROBE   0x303300B8, 0x0, 0x00000000, 0x0, 0x30330318
 
#define IOMUXC_SD1_STROBE_I2C3_SDA   0x303300B8, 0x3, 0x303305B8, 0x0, 0x30330318
 
#define IOMUXC_SD1_STROBE_UART3_CTS_B   0x303300B8, 0x4, 0x00000000, 0x0, 0x30330318
 
#define IOMUXC_SD1_STROBE_UART3_RTS_B   0x303300B8, 0x4, 0x303305F4, 0x1, 0x30330318
 
#define IOMUXC_SD1_STROBE_GPIO2_IO11   0x303300B8, 0x5, 0x00000000, 0x0, 0x30330318
 
#define IOMUXC_SD2_CD_B_USDHC2_CD_B   0x303300BC, 0x0, 0x00000000, 0x0, 0x3033031C
 
#define IOMUXC_SD2_CD_B_GPIO2_IO12   0x303300BC, 0x5, 0x00000000, 0x0, 0x3033031C
 
#define IOMUXC_SD2_CLK_USDHC2_CLK   0x303300C0, 0x0, 0x00000000, 0x0, 0x30330320
 
#define IOMUXC_SD2_CLK_ECSPI2_SCLK   0x303300C0, 0x2, 0x30330568, 0x0, 0x30330320
 
#define IOMUXC_SD2_CLK_UART4_RX   0x303300C0, 0x3, 0x30330600, 0x0, 0x30330320
 
#define IOMUXC_SD2_CLK_UART4_TX   0x303300C0, 0x3, 0x00000000, 0x0, 0x30330320
 
#define IOMUXC_SD2_CLK_GPIO2_IO13   0x303300C0, 0x5, 0x00000000, 0x0, 0x30330320
 
#define IOMUXC_SD2_CMD_USDHC2_CMD   0x303300C4, 0x0, 0x00000000, 0x0, 0x30330324
 
#define IOMUXC_SD2_CMD_ECSPI2_MOSI   0x303300C4, 0x2, 0x30330570, 0x0, 0x30330324
 
#define IOMUXC_SD2_CMD_UART4_TX   0x303300C4, 0x3, 0x00000000, 0x0, 0x30330324
 
#define IOMUXC_SD2_CMD_UART4_RX   0x303300C4, 0x3, 0x30330600, 0x1, 0x30330324
 
#define IOMUXC_SD2_CMD_AUDIOMIX_PDM_CLK   0x303300C4, 0x4, 0x00000000, 0x0, 0x30330324
 
#define IOMUXC_SD2_CMD_GPIO2_IO14   0x303300C4, 0x5, 0x00000000, 0x0, 0x30330324
 
#define IOMUXC_SD2_DATA0_USDHC2_DATA0   0x303300C8, 0x0, 0x00000000, 0x0, 0x30330328
 
#define IOMUXC_SD2_DATA0_I2C4_SDA   0x303300C8, 0x2, 0x303305C0, 0x1, 0x30330328
 
#define IOMUXC_SD2_DATA0_UART2_RX   0x303300C8, 0x3, 0x303305F0, 0x2, 0x30330328
 
#define IOMUXC_SD2_DATA0_UART2_TX   0x303300C8, 0x3, 0x00000000, 0x0, 0x30330328
 
#define IOMUXC_SD2_DATA0_AUDIOMIX_PDM_BIT_STREAM0   0x303300C8, 0x4, 0x303304C0, 0x2, 0x30330328
 
#define IOMUXC_SD2_DATA0_GPIO2_IO15   0x303300C8, 0x5, 0x00000000, 0x0, 0x30330328
 
#define IOMUXC_SD2_DATA1_USDHC2_DATA1   0x303300CC, 0x0, 0x00000000, 0x0, 0x3033032C
 
#define IOMUXC_SD2_DATA1_I2C4_SCL   0x303300CC, 0x2, 0x303305BC, 0x1, 0x3033032C
 
#define IOMUXC_SD2_DATA1_UART2_TX   0x303300CC, 0x3, 0x00000000, 0x0, 0x3033032C
 
#define IOMUXC_SD2_DATA1_UART2_RX   0x303300CC, 0x3, 0x303305F0, 0x3, 0x3033032C
 
#define IOMUXC_SD2_DATA1_AUDIOMIX_PDM_BIT_STREAM1   0x303300CC, 0x4, 0x303304C4, 0x2, 0x3033032C
 
#define IOMUXC_SD2_DATA1_GPIO2_IO16   0x303300CC, 0x5, 0x00000000, 0x0, 0x3033032C
 
#define IOMUXC_SD2_DATA2_USDHC2_DATA2   0x303300D0, 0x0, 0x00000000, 0x0, 0x30330330
 
#define IOMUXC_SD2_DATA2_ECSPI2_SS0   0x303300D0, 0x2, 0x30330574, 0x0, 0x30330330
 
#define IOMUXC_SD2_DATA2_AUDIOMIX_SPDIF1_OUT   0x303300D0, 0x3, 0x00000000, 0x0, 0x30330330
 
#define IOMUXC_SD2_DATA2_AUDIOMIX_PDM_BIT_STREAM2   0x303300D0, 0x4, 0x303304C8, 0x2, 0x30330330
 
#define IOMUXC_SD2_DATA2_GPIO2_IO17   0x303300D0, 0x5, 0x00000000, 0x0, 0x30330330
 
#define IOMUXC_SD2_DATA3_USDHC2_DATA3   0x303300D4, 0x0, 0x00000000, 0x0, 0x30330334
 
#define IOMUXC_SD2_DATA3_ECSPI2_MISO   0x303300D4, 0x2, 0x3033056C, 0x0, 0x30330334
 
#define IOMUXC_SD2_DATA3_AUDIOMIX_SPDIF1_IN   0x303300D4, 0x3, 0x30330544, 0x1, 0x30330334
 
#define IOMUXC_SD2_DATA3_AUDIOMIX_PDM_BIT_STREAM3   0x303300D4, 0x4, 0x303304CC, 0x2, 0x30330334
 
#define IOMUXC_SD2_DATA3_GPIO2_IO18   0x303300D4, 0x5, 0x00000000, 0x0, 0x30330334
 
#define IOMUXC_SD2_RESET_B_USDHC2_RESET_B   0x303300D8, 0x0, 0x00000000, 0x0, 0x30330338
 
#define IOMUXC_SD2_RESET_B_GPIO2_IO19   0x303300D8, 0x5, 0x00000000, 0x0, 0x30330338
 
#define IOMUXC_SD2_WP_USDHC2_WP   0x303300DC, 0x0, 0x00000000, 0x0, 0x3033033C
 
#define IOMUXC_SD2_WP_GPIO2_IO20   0x303300DC, 0x5, 0x00000000, 0x0, 0x3033033C
 
#define IOMUXC_SD2_WP_CORESIGHT_EVENTI   0x303300DC, 0x6, 0x00000000, 0x0, 0x3033033C
 
#define IOMUXC_NAND_ALE_NAND_ALE   0x303300E0, 0x0, 0x00000000, 0x0, 0x30330340
 
#define IOMUXC_NAND_ALE_FLEXSPI_A_SCLK   0x303300E0, 0x1, 0x00000000, 0x0, 0x30330340
 
#define IOMUXC_NAND_ALE_AUDIOMIX_SAI3_TX_BCLK   0x303300E0, 0x2, 0x303304E8, 0x0, 0x30330340
 
#define IOMUXC_NAND_ALE_ISP_FL_TRIG_0   0x303300E0, 0x3, 0x303305D4, 0x1, 0x30330340
 
#define IOMUXC_NAND_ALE_UART3_RX   0x303300E0, 0x4, 0x303305F8, 0x2, 0x30330340
 
#define IOMUXC_NAND_ALE_UART3_TX   0x303300E0, 0x4, 0x00000000, 0x0, 0x30330340
 
#define IOMUXC_NAND_ALE_GPIO3_IO00   0x303300E0, 0x5, 0x00000000, 0x0, 0x30330340
 
#define IOMUXC_NAND_ALE_CORESIGHT_TRACE_CLK   0x303300E0, 0x6, 0x00000000, 0x0, 0x30330340
 
#define IOMUXC_NAND_CE0_B_NAND_CE0_B   0x303300E4, 0x0, 0x00000000, 0x0, 0x30330344
 
#define IOMUXC_NAND_CE0_B_FLEXSPI_A_SS0_B   0x303300E4, 0x1, 0x00000000, 0x0, 0x30330344
 
#define IOMUXC_NAND_CE0_B_AUDIOMIX_SAI3_TX_DATA0   0x303300E4, 0x2, 0x00000000, 0x0, 0x30330344
 
#define IOMUXC_NAND_CE0_B_ISP_SHUTTER_TRIG_0   0x303300E4, 0x3, 0x303305DC, 0x1, 0x30330344
 
#define IOMUXC_NAND_CE0_B_UART3_TX   0x303300E4, 0x4, 0x00000000, 0x0, 0x30330344
 
#define IOMUXC_NAND_CE0_B_UART3_RX   0x303300E4, 0x4, 0x303305F8, 0x3, 0x30330344
 
#define IOMUXC_NAND_CE0_B_GPIO3_IO01   0x303300E4, 0x5, 0x00000000, 0x0, 0x30330344
 
#define IOMUXC_NAND_CE0_B_CORESIGHT_TRACE_CTL   0x303300E4, 0x6, 0x00000000, 0x0, 0x30330344
 
#define IOMUXC_NAND_CE1_B_NAND_CE1_B   0x303300E8, 0x0, 0x00000000, 0x0, 0x30330348
 
#define IOMUXC_NAND_CE1_B_FLEXSPI_A_SS1_B   0x303300E8, 0x1, 0x00000000, 0x0, 0x30330348
 
#define IOMUXC_NAND_CE1_B_USDHC3_STROBE   0x303300E8, 0x2, 0x30330630, 0x1, 0x30330348
 
#define IOMUXC_NAND_CE1_B_I2C4_SCL   0x303300E8, 0x4, 0x303305BC, 0x2, 0x30330348
 
#define IOMUXC_NAND_CE1_B_GPIO3_IO02   0x303300E8, 0x5, 0x00000000, 0x0, 0x30330348
 
#define IOMUXC_NAND_CE1_B_CORESIGHT_TRACE00   0x303300E8, 0x6, 0x00000000, 0x0, 0x30330348
 
#define IOMUXC_NAND_CE2_B_NAND_CE2_B   0x303300EC, 0x0, 0x00000000, 0x0, 0x3033034C
 
#define IOMUXC_NAND_CE2_B_FLEXSPI_B_SS0_B   0x303300EC, 0x1, 0x00000000, 0x0, 0x3033034C
 
#define IOMUXC_NAND_CE2_B_USDHC3_DATA5   0x303300EC, 0x2, 0x30330624, 0x1, 0x3033034C
 
#define IOMUXC_NAND_CE2_B_I2C4_SDA   0x303300EC, 0x4, 0x303305C0, 0x2, 0x3033034C
 
#define IOMUXC_NAND_CE2_B_GPIO3_IO03   0x303300EC, 0x5, 0x00000000, 0x0, 0x3033034C
 
#define IOMUXC_NAND_CE2_B_CORESIGHT_TRACE01   0x303300EC, 0x6, 0x00000000, 0x0, 0x3033034C
 
#define IOMUXC_NAND_CE3_B_NAND_CE3_B   0x303300F0, 0x0, 0x00000000, 0x0, 0x30330350
 
#define IOMUXC_NAND_CE3_B_FLEXSPI_B_SS1_B   0x303300F0, 0x1, 0x00000000, 0x0, 0x30330350
 
#define IOMUXC_NAND_CE3_B_USDHC3_DATA6   0x303300F0, 0x2, 0x30330628, 0x1, 0x30330350
 
#define IOMUXC_NAND_CE3_B_I2C3_SDA   0x303300F0, 0x4, 0x303305B8, 0x1, 0x30330350
 
#define IOMUXC_NAND_CE3_B_GPIO3_IO04   0x303300F0, 0x5, 0x00000000, 0x0, 0x30330350
 
#define IOMUXC_NAND_CE3_B_CORESIGHT_TRACE02   0x303300F0, 0x6, 0x00000000, 0x0, 0x30330350
 
#define IOMUXC_NAND_CLE_NAND_CLE   0x303300F4, 0x0, 0x00000000, 0x0, 0x30330354
 
#define IOMUXC_NAND_CLE_FLEXSPI_B_SCLK   0x303300F4, 0x1, 0x00000000, 0x0, 0x30330354
 
#define IOMUXC_NAND_CLE_USDHC3_DATA7   0x303300F4, 0x2, 0x3033062C, 0x1, 0x30330354
 
#define IOMUXC_NAND_CLE_UART4_RX   0x303300F4, 0x4, 0x30330600, 0x2, 0x30330354
 
#define IOMUXC_NAND_CLE_UART4_TX   0x303300F4, 0x4, 0x00000000, 0x0, 0x30330354
 
#define IOMUXC_NAND_CLE_GPIO3_IO05   0x303300F4, 0x5, 0x00000000, 0x0, 0x30330354
 
#define IOMUXC_NAND_CLE_CORESIGHT_TRACE03   0x303300F4, 0x6, 0x00000000, 0x0, 0x30330354
 
#define IOMUXC_NAND_DATA00_NAND_DATA00   0x303300F8, 0x0, 0x00000000, 0x0, 0x30330358
 
#define IOMUXC_NAND_DATA00_FLEXSPI_A_DATA0   0x303300F8, 0x1, 0x00000000, 0x0, 0x30330358
 
#define IOMUXC_NAND_DATA00_AUDIOMIX_SAI3_RX_DATA0   0x303300F8, 0x2, 0x303304E4, 0x0, 0x30330358
 
#define IOMUXC_NAND_DATA00_ISP_FLASH_TRIG_0   0x303300F8, 0x3, 0x00000000, 0x0, 0x30330358
 
#define IOMUXC_NAND_DATA00_UART4_RX   0x303300F8, 0x4, 0x30330600, 0x3, 0x30330358
 
#define IOMUXC_NAND_DATA00_UART4_TX   0x303300F8, 0x4, 0x00000000, 0x0, 0x30330358
 
#define IOMUXC_NAND_DATA00_GPIO3_IO06   0x303300F8, 0x5, 0x00000000, 0x0, 0x30330358
 
#define IOMUXC_NAND_DATA00_CORESIGHT_TRACE04   0x303300F8, 0x6, 0x00000000, 0x0, 0x30330358
 
#define IOMUXC_NAND_DATA01_NAND_DATA01   0x303300FC, 0x0, 0x00000000, 0x0, 0x3033035C
 
#define IOMUXC_NAND_DATA01_FLEXSPI_A_DATA1   0x303300FC, 0x1, 0x00000000, 0x0, 0x3033035C
 
#define IOMUXC_NAND_DATA01_AUDIOMIX_SAI3_TX_SYNC   0x303300FC, 0x2, 0x303304EC, 0x0, 0x3033035C
 
#define IOMUXC_NAND_DATA01_ISP_PRELIGHT_TRIG_0   0x303300FC, 0x3, 0x00000000, 0x0, 0x3033035C
 
#define IOMUXC_NAND_DATA01_UART4_TX   0x303300FC, 0x4, 0x00000000, 0x0, 0x3033035C
 
#define IOMUXC_NAND_DATA01_UART4_RX   0x303300FC, 0x4, 0x30330600, 0x4, 0x3033035C
 
#define IOMUXC_NAND_DATA01_GPIO3_IO07   0x303300FC, 0x5, 0x00000000, 0x0, 0x3033035C
 
#define IOMUXC_NAND_DATA01_CORESIGHT_TRACE05   0x303300FC, 0x6, 0x00000000, 0x0, 0x3033035C
 
#define IOMUXC_NAND_DATA02_NAND_DATA02   0x30330100, 0x0, 0x00000000, 0x0, 0x30330360
 
#define IOMUXC_NAND_DATA02_FLEXSPI_A_DATA2   0x30330100, 0x1, 0x00000000, 0x0, 0x30330360
 
#define IOMUXC_NAND_DATA02_USDHC3_CD_B   0x30330100, 0x2, 0x30330608, 0x2, 0x30330360
 
#define IOMUXC_NAND_DATA02_UART4_CTS_B   0x30330100, 0x3, 0x00000000, 0x0, 0x30330360
 
#define IOMUXC_NAND_DATA02_UART4_RTS_B   0x30330100, 0x3, 0x303305FC, 0x0, 0x30330360
 
#define IOMUXC_NAND_DATA02_I2C4_SDA   0x30330100, 0x4, 0x303305C0, 0x3, 0x30330360
 
#define IOMUXC_NAND_DATA02_GPIO3_IO08   0x30330100, 0x5, 0x00000000, 0x0, 0x30330360
 
#define IOMUXC_NAND_DATA02_CORESIGHT_TRACE06   0x30330100, 0x6, 0x00000000, 0x0, 0x30330360
 
#define IOMUXC_NAND_DATA03_NAND_DATA03   0x30330104, 0x0, 0x00000000, 0x0, 0x30330364
 
#define IOMUXC_NAND_DATA03_FLEXSPI_A_DATA3   0x30330104, 0x1, 0x00000000, 0x0, 0x30330364
 
#define IOMUXC_NAND_DATA03_USDHC3_WP   0x30330104, 0x2, 0x30330634, 0x2, 0x30330364
 
#define IOMUXC_NAND_DATA03_UART4_RTS_B   0x30330104, 0x3, 0x303305FC, 0x1, 0x30330364
 
#define IOMUXC_NAND_DATA03_UART4_CTS_B   0x30330104, 0x3, 0x00000000, 0x0, 0x30330364
 
#define IOMUXC_NAND_DATA03_ISP_FL_TRIG_1   0x30330104, 0x4, 0x303305D8, 0x1, 0x30330364
 
#define IOMUXC_NAND_DATA03_GPIO3_IO09   0x30330104, 0x5, 0x00000000, 0x0, 0x30330364
 
#define IOMUXC_NAND_DATA03_CORESIGHT_TRACE07   0x30330104, 0x6, 0x00000000, 0x0, 0x30330364
 
#define IOMUXC_NAND_DATA04_NAND_DATA04   0x30330108, 0x0, 0x00000000, 0x0, 0x30330368
 
#define IOMUXC_NAND_DATA04_FLEXSPI_B_DATA0   0x30330108, 0x1, 0x00000000, 0x0, 0x30330368
 
#define IOMUXC_NAND_DATA04_USDHC3_DATA0   0x30330108, 0x2, 0x30330610, 0x1, 0x30330368
 
#define IOMUXC_NAND_DATA04_FLEXSPI_A_DATA4   0x30330108, 0x3, 0x00000000, 0x0, 0x30330368
 
#define IOMUXC_NAND_DATA04_ISP_SHUTTER_TRIG_1   0x30330108, 0x4, 0x303305E0, 0x1, 0x30330368
 
#define IOMUXC_NAND_DATA04_GPIO3_IO10   0x30330108, 0x5, 0x00000000, 0x0, 0x30330368
 
#define IOMUXC_NAND_DATA04_CORESIGHT_TRACE08   0x30330108, 0x6, 0x00000000, 0x0, 0x30330368
 
#define IOMUXC_NAND_DATA05_NAND_DATA05   0x3033010C, 0x0, 0x00000000, 0x0, 0x3033036C
 
#define IOMUXC_NAND_DATA05_FLEXSPI_B_DATA1   0x3033010C, 0x1, 0x00000000, 0x0, 0x3033036C
 
#define IOMUXC_NAND_DATA05_USDHC3_DATA1   0x3033010C, 0x2, 0x30330614, 0x1, 0x3033036C
 
#define IOMUXC_NAND_DATA05_FLEXSPI_A_DATA5   0x3033010C, 0x3, 0x00000000, 0x0, 0x3033036C
 
#define IOMUXC_NAND_DATA05_ISP_FLASH_TRIG_1   0x3033010C, 0x4, 0x00000000, 0x0, 0x3033036C
 
#define IOMUXC_NAND_DATA05_GPIO3_IO11   0x3033010C, 0x5, 0x00000000, 0x0, 0x3033036C
 
#define IOMUXC_NAND_DATA05_CORESIGHT_TRACE09   0x3033010C, 0x6, 0x00000000, 0x0, 0x3033036C
 
#define IOMUXC_NAND_DATA06_NAND_DATA06   0x30330110, 0x0, 0x00000000, 0x0, 0x30330370
 
#define IOMUXC_NAND_DATA06_FLEXSPI_B_DATA2   0x30330110, 0x1, 0x00000000, 0x0, 0x30330370
 
#define IOMUXC_NAND_DATA06_USDHC3_DATA2   0x30330110, 0x2, 0x30330618, 0x1, 0x30330370
 
#define IOMUXC_NAND_DATA06_FLEXSPI_A_DATA6   0x30330110, 0x3, 0x00000000, 0x0, 0x30330370
 
#define IOMUXC_NAND_DATA06_ISP_PRELIGHT_TRIG_1   0x30330110, 0x4, 0x00000000, 0x0, 0x30330370
 
#define IOMUXC_NAND_DATA06_GPIO3_IO12   0x30330110, 0x5, 0x00000000, 0x0, 0x30330370
 
#define IOMUXC_NAND_DATA06_CORESIGHT_TRACE10   0x30330110, 0x6, 0x00000000, 0x0, 0x30330370
 
#define IOMUXC_NAND_DATA07_NAND_DATA07   0x30330114, 0x0, 0x00000000, 0x0, 0x30330374
 
#define IOMUXC_NAND_DATA07_FLEXSPI_B_DATA3   0x30330114, 0x1, 0x00000000, 0x0, 0x30330374
 
#define IOMUXC_NAND_DATA07_USDHC3_DATA3   0x30330114, 0x2, 0x3033061C, 0x1, 0x30330374
 
#define IOMUXC_NAND_DATA07_FLEXSPI_A_DATA7   0x30330114, 0x3, 0x00000000, 0x0, 0x30330374
 
#define IOMUXC_NAND_DATA07_ISP_SHUTTER_OPEN_1   0x30330114, 0x4, 0x00000000, 0x0, 0x30330374
 
#define IOMUXC_NAND_DATA07_GPIO3_IO13   0x30330114, 0x5, 0x00000000, 0x0, 0x30330374
 
#define IOMUXC_NAND_DATA07_CORESIGHT_TRACE11   0x30330114, 0x6, 0x00000000, 0x0, 0x30330374
 
#define IOMUXC_NAND_DQS_NAND_DQS   0x30330118, 0x0, 0x00000000, 0x0, 0x30330378
 
#define IOMUXC_NAND_DQS_FLEXSPI_A_DQS   0x30330118, 0x1, 0x00000000, 0x0, 0x30330378
 
#define IOMUXC_NAND_DQS_AUDIOMIX_SAI3_MCLK   0x30330118, 0x2, 0x303304E0, 0x0, 0x30330378
 
#define IOMUXC_NAND_DQS_ISP_SHUTTER_OPEN_0   0x30330118, 0x3, 0x00000000, 0x0, 0x30330378
 
#define IOMUXC_NAND_DQS_I2C3_SCL   0x30330118, 0x4, 0x303305B4, 0x1, 0x30330378
 
#define IOMUXC_NAND_DQS_GPIO3_IO14   0x30330118, 0x5, 0x00000000, 0x0, 0x30330378
 
#define IOMUXC_NAND_DQS_CORESIGHT_TRACE12   0x30330118, 0x6, 0x00000000, 0x0, 0x30330378
 
#define IOMUXC_NAND_RE_B_NAND_RE_B   0x3033011C, 0x0, 0x00000000, 0x0, 0x3033037C
 
#define IOMUXC_NAND_RE_B_FLEXSPI_B_DQS   0x3033011C, 0x1, 0x00000000, 0x0, 0x3033037C
 
#define IOMUXC_NAND_RE_B_USDHC3_DATA4   0x3033011C, 0x2, 0x30330620, 0x1, 0x3033037C
 
#define IOMUXC_NAND_RE_B_UART4_TX   0x3033011C, 0x4, 0x00000000, 0x0, 0x3033037C
 
#define IOMUXC_NAND_RE_B_UART4_RX   0x3033011C, 0x4, 0x30330600, 0x5, 0x3033037C
 
#define IOMUXC_NAND_RE_B_GPIO3_IO15   0x3033011C, 0x5, 0x00000000, 0x0, 0x3033037C
 
#define IOMUXC_NAND_RE_B_CORESIGHT_TRACE13   0x3033011C, 0x6, 0x00000000, 0x0, 0x3033037C
 
#define IOMUXC_NAND_READY_B_NAND_READY_B   0x30330120, 0x0, 0x00000000, 0x0, 0x30330380
 
#define IOMUXC_NAND_READY_B_USDHC3_RESET_B   0x30330120, 0x2, 0x00000000, 0x0, 0x30330380
 
#define IOMUXC_NAND_READY_B_I2C3_SCL   0x30330120, 0x4, 0x303305B4, 0x2, 0x30330380
 
#define IOMUXC_NAND_READY_B_GPIO3_IO16   0x30330120, 0x5, 0x00000000, 0x0, 0x30330380
 
#define IOMUXC_NAND_READY_B_CORESIGHT_TRACE14   0x30330120, 0x6, 0x00000000, 0x0, 0x30330380
 
#define IOMUXC_NAND_WE_B_NAND_WE_B   0x30330124, 0x0, 0x00000000, 0x0, 0x30330384
 
#define IOMUXC_NAND_WE_B_USDHC3_CLK   0x30330124, 0x2, 0x30330604, 0x1, 0x30330384
 
#define IOMUXC_NAND_WE_B_I2C3_SDA   0x30330124, 0x4, 0x303305B8, 0x2, 0x30330384
 
#define IOMUXC_NAND_WE_B_GPIO3_IO17   0x30330124, 0x5, 0x00000000, 0x0, 0x30330384
 
#define IOMUXC_NAND_WE_B_CORESIGHT_TRACE15   0x30330124, 0x6, 0x00000000, 0x0, 0x30330384
 
#define IOMUXC_NAND_WP_B_NAND_WP_B   0x30330128, 0x0, 0x00000000, 0x0, 0x30330388
 
#define IOMUXC_NAND_WP_B_USDHC3_CMD   0x30330128, 0x2, 0x3033060C, 0x1, 0x30330388
 
#define IOMUXC_NAND_WP_B_I2C4_SCL   0x30330128, 0x4, 0x303305BC, 0x3, 0x30330388
 
#define IOMUXC_NAND_WP_B_GPIO3_IO18   0x30330128, 0x5, 0x00000000, 0x0, 0x30330388
 
#define IOMUXC_NAND_WP_B_CORESIGHT_EVENTO   0x30330128, 0x6, 0x00000000, 0x0, 0x30330388
 
#define IOMUXC_SAI5_RXFS_AUDIOMIX_SAI5_RX_SYNC   0x3033012C, 0x0, 0x30330508, 0x0, 0x3033038C
 
#define IOMUXC_SAI5_RXFS_AUDIOMIX_SAI1_TX_DATA0   0x3033012C, 0x1, 0x00000000, 0x0, 0x3033038C
 
#define IOMUXC_SAI5_RXFS_PWM4_OUT   0x3033012C, 0x2, 0x00000000, 0x0, 0x3033038C
 
#define IOMUXC_SAI5_RXFS_I2C6_SCL   0x3033012C, 0x3, 0x303305CC, 0x1, 0x3033038C
 
#define IOMUXC_SAI5_RXFS_GPIO3_IO19   0x3033012C, 0x5, 0x00000000, 0x0, 0x3033038C
 
#define IOMUXC_SAI5_RXC_AUDIOMIX_SAI5_RX_BCLK   0x30330130, 0x0, 0x303304F4, 0x0, 0x30330390
 
#define IOMUXC_SAI5_RXC_AUDIOMIX_SAI1_TX_DATA1   0x30330130, 0x1, 0x00000000, 0x0, 0x30330390
 
#define IOMUXC_SAI5_RXC_PWM3_OUT   0x30330130, 0x2, 0x00000000, 0x0, 0x30330390
 
#define IOMUXC_SAI5_RXC_I2C6_SDA   0x30330130, 0x3, 0x303305D0, 0x1, 0x30330390
 
#define IOMUXC_SAI5_RXC_AUDIOMIX_PDM_CLK   0x30330130, 0x4, 0x00000000, 0x0, 0x30330390
 
#define IOMUXC_SAI5_RXC_GPIO3_IO20   0x30330130, 0x5, 0x00000000, 0x0, 0x30330390
 
#define IOMUXC_SAI5_RXD0_AUDIOMIX_SAI5_RX_DATA0   0x30330134, 0x0, 0x303304F8, 0x0, 0x30330394
 
#define IOMUXC_SAI5_RXD0_AUDIOMIX_SAI1_TX_DATA2   0x30330134, 0x1, 0x00000000, 0x0, 0x30330394
 
#define IOMUXC_SAI5_RXD0_PWM2_OUT   0x30330134, 0x2, 0x00000000, 0x0, 0x30330394
 
#define IOMUXC_SAI5_RXD0_I2C5_SCL   0x30330134, 0x3, 0x303305C4, 0x1, 0x30330394
 
#define IOMUXC_SAI5_RXD0_AUDIOMIX_PDM_BIT_STREAM0   0x30330134, 0x4, 0x303304C0, 0x3, 0x30330394
 
#define IOMUXC_SAI5_RXD0_GPIO3_IO21   0x30330134, 0x5, 0x00000000, 0x0, 0x30330394
 
#define IOMUXC_SAI5_RXD1_AUDIOMIX_SAI5_RX_DATA1   0x30330138, 0x0, 0x303304FC, 0x0, 0x30330398
 
#define IOMUXC_SAI5_RXD1_AUDIOMIX_SAI1_TX_DATA3   0x30330138, 0x1, 0x00000000, 0x0, 0x30330398
 
#define IOMUXC_SAI5_RXD1_AUDIOMIX_SAI1_TX_SYNC   0x30330138, 0x2, 0x303304D8, 0x0, 0x30330398
 
#define IOMUXC_SAI5_RXD1_AUDIOMIX_SAI5_TX_SYNC   0x30330138, 0x3, 0x30330510, 0x0, 0x30330398
 
#define IOMUXC_SAI5_RXD1_AUDIOMIX_PDM_BIT_STREAM1   0x30330138, 0x4, 0x303304C4, 0x3, 0x30330398
 
#define IOMUXC_SAI5_RXD1_GPIO3_IO22   0x30330138, 0x5, 0x00000000, 0x0, 0x30330398
 
#define IOMUXC_SAI5_RXD1_CAN1_TX   0x30330138, 0x6, 0x00000000, 0x0, 0x30330398
 
#define IOMUXC_SAI5_RXD2_AUDIOMIX_SAI5_RX_DATA2   0x3033013C, 0x0, 0x30330500, 0x0, 0x3033039C
 
#define IOMUXC_SAI5_RXD2_AUDIOMIX_SAI1_TX_DATA4   0x3033013C, 0x1, 0x00000000, 0x0, 0x3033039C
 
#define IOMUXC_SAI5_RXD2_AUDIOMIX_SAI1_TX_SYNC   0x3033013C, 0x2, 0x303304D8, 0x1, 0x3033039C
 
#define IOMUXC_SAI5_RXD2_AUDIOMIX_SAI5_TX_BCLK   0x3033013C, 0x3, 0x3033050C, 0x0, 0x3033039C
 
#define IOMUXC_SAI5_RXD2_AUDIOMIX_PDM_BIT_STREAM2   0x3033013C, 0x4, 0x303304C8, 0x3, 0x3033039C
 
#define IOMUXC_SAI5_RXD2_GPIO3_IO23   0x3033013C, 0x5, 0x00000000, 0x0, 0x3033039C
 
#define IOMUXC_SAI5_RXD2_CAN1_RX   0x3033013C, 0x6, 0x3033054C, 0x0, 0x3033039C
 
#define IOMUXC_SAI5_RXD3_AUDIOMIX_SAI5_RX_DATA3   0x30330140, 0x0, 0x30330504, 0x0, 0x303303A0
 
#define IOMUXC_SAI5_RXD3_AUDIOMIX_SAI1_TX_DATA5   0x30330140, 0x1, 0x00000000, 0x0, 0x303303A0
 
#define IOMUXC_SAI5_RXD3_AUDIOMIX_SAI1_TX_SYNC   0x30330140, 0x2, 0x303304D8, 0x2, 0x303303A0
 
#define IOMUXC_SAI5_RXD3_AUDIOMIX_SAI5_TX_DATA0   0x30330140, 0x3, 0x00000000, 0x0, 0x303303A0
 
#define IOMUXC_SAI5_RXD3_AUDIOMIX_PDM_BIT_STREAM3   0x30330140, 0x4, 0x303304CC, 0x3, 0x303303A0
 
#define IOMUXC_SAI5_RXD3_GPIO3_IO24   0x30330140, 0x5, 0x00000000, 0x0, 0x303303A0
 
#define IOMUXC_SAI5_RXD3_CAN2_TX   0x30330140, 0x6, 0x00000000, 0x0, 0x303303A0
 
#define IOMUXC_SAI5_MCLK_AUDIOMIX_SAI5_MCLK   0x30330144, 0x0, 0x303304F0, 0x0, 0x303303A4
 
#define IOMUXC_SAI5_MCLK_AUDIOMIX_SAI1_TX_BCLK   0x30330144, 0x1, 0x303304D4, 0x0, 0x303303A4
 
#define IOMUXC_SAI5_MCLK_PWM1_OUT   0x30330144, 0x2, 0x00000000, 0x0, 0x303303A4
 
#define IOMUXC_SAI5_MCLK_I2C5_SDA   0x30330144, 0x3, 0x303305C8, 0x1, 0x303303A4
 
#define IOMUXC_SAI5_MCLK_GPIO3_IO25   0x30330144, 0x5, 0x00000000, 0x0, 0x303303A4
 
#define IOMUXC_SAI5_MCLK_CAN2_RX   0x30330144, 0x6, 0x30330550, 0x0, 0x303303A4
 
#define IOMUXC_SAI1_RXFS_AUDIOMIX_SAI1_RX_SYNC   0x30330148, 0x0, 0x303304D0, 0x0, 0x303303A8
 
#define IOMUXC_SAI1_RXFS_ENET1_1588_EVENT0_IN   0x30330148, 0x4, 0x00000000, 0x0, 0x303303A8
 
#define IOMUXC_SAI1_RXFS_GPIO4_IO00   0x30330148, 0x5, 0x00000000, 0x0, 0x303303A8
 
#define IOMUXC_SAI1_RXC_AUDIOMIX_SAI1_RX_BCLK   0x3033014C, 0x0, 0x00000000, 0x0, 0x303303AC
 
#define IOMUXC_SAI1_RXC_AUDIOMIX_PDM_CLK   0x3033014C, 0x3, 0x00000000, 0x0, 0x303303AC
 
#define IOMUXC_SAI1_RXC_ENET1_1588_EVENT0_OUT   0x3033014C, 0x4, 0x00000000, 0x0, 0x303303AC
 
#define IOMUXC_SAI1_RXC_GPIO4_IO01   0x3033014C, 0x5, 0x00000000, 0x0, 0x303303AC
 
#define IOMUXC_SAI1_RXD0_AUDIOMIX_SAI1_RX_DATA0   0x30330150, 0x0, 0x00000000, 0x0, 0x303303B0
 
#define IOMUXC_SAI1_RXD0_AUDIOMIX_SAI1_TX_DATA1   0x30330150, 0x2, 0x00000000, 0x0, 0x303303B0
 
#define IOMUXC_SAI1_RXD0_AUDIOMIX_PDM_BIT_STREAM0   0x30330150, 0x3, 0x303304C0, 0x4, 0x303303B0
 
#define IOMUXC_SAI1_RXD0_ENET1_1588_EVENT1_IN   0x30330150, 0x4, 0x00000000, 0x0, 0x303303B0
 
#define IOMUXC_SAI1_RXD0_GPIO4_IO02   0x30330150, 0x5, 0x00000000, 0x0, 0x303303B0
 
#define IOMUXC_SAI1_RXD1_AUDIOMIX_SAI1_RX_DATA1   0x30330154, 0x0, 0x00000000, 0x0, 0x303303B4
 
#define IOMUXC_SAI1_RXD1_AUDIOMIX_PDM_BIT_STREAM1   0x30330154, 0x3, 0x303304C4, 0x4, 0x303303B4
 
#define IOMUXC_SAI1_RXD1_ENET1_1588_EVENT1_OUT   0x30330154, 0x4, 0x00000000, 0x0, 0x303303B4
 
#define IOMUXC_SAI1_RXD1_GPIO4_IO03   0x30330154, 0x5, 0x00000000, 0x0, 0x303303B4
 
#define IOMUXC_SAI1_RXD2_AUDIOMIX_SAI1_RX_DATA2   0x30330158, 0x0, 0x00000000, 0x0, 0x303303B8
 
#define IOMUXC_SAI1_RXD2_AUDIOMIX_PDM_BIT_STREAM2   0x30330158, 0x3, 0x303304C8, 0x4, 0x303303B8
 
#define IOMUXC_SAI1_RXD2_ENET1_MDC   0x30330158, 0x4, 0x00000000, 0x0, 0x303303B8
 
#define IOMUXC_SAI1_RXD2_GPIO4_IO04   0x30330158, 0x5, 0x00000000, 0x0, 0x303303B8
 
#define IOMUXC_SAI1_RXD3_AUDIOMIX_SAI1_RX_DATA3   0x3033015C, 0x0, 0x00000000, 0x0, 0x303303BC
 
#define IOMUXC_SAI1_RXD3_AUDIOMIX_PDM_BIT_STREAM3   0x3033015C, 0x3, 0x303304CC, 0x4, 0x303303BC
 
#define IOMUXC_SAI1_RXD3_ENET1_MDIO   0x3033015C, 0x4, 0x3033057C, 0x1, 0x303303BC
 
#define IOMUXC_SAI1_RXD3_GPIO4_IO05   0x3033015C, 0x5, 0x00000000, 0x0, 0x303303BC
 
#define IOMUXC_SAI1_RXD4_AUDIOMIX_SAI1_RX_DATA4   0x30330160, 0x0, 0x00000000, 0x0, 0x303303C0
 
#define IOMUXC_SAI1_RXD4_AUDIOMIX_SAI6_TX_BCLK   0x30330160, 0x1, 0x30330524, 0x1, 0x303303C0
 
#define IOMUXC_SAI1_RXD4_AUDIOMIX_SAI6_RX_BCLK   0x30330160, 0x2, 0x30330518, 0x1, 0x303303C0
 
#define IOMUXC_SAI1_RXD4_ENET1_RGMII_RD0   0x30330160, 0x4, 0x30330580, 0x1, 0x303303C0
 
#define IOMUXC_SAI1_RXD4_GPIO4_IO06   0x30330160, 0x5, 0x00000000, 0x0, 0x303303C0
 
#define IOMUXC_SAI1_RXD5_AUDIOMIX_SAI1_RX_DATA5   0x30330164, 0x0, 0x00000000, 0x0, 0x303303C4
 
#define IOMUXC_SAI1_RXD5_AUDIOMIX_SAI6_TX_DATA0   0x30330164, 0x1, 0x00000000, 0x0, 0x303303C4
 
#define IOMUXC_SAI1_RXD5_AUDIOMIX_SAI6_RX_DATA0   0x30330164, 0x2, 0x3033051C, 0x1, 0x303303C4
 
#define IOMUXC_SAI1_RXD5_AUDIOMIX_SAI1_RX_SYNC   0x30330164, 0x3, 0x303304D0, 0x1, 0x303303C4
 
#define IOMUXC_SAI1_RXD5_ENET1_RGMII_RD1   0x30330164, 0x4, 0x30330584, 0x1, 0x303303C4
 
#define IOMUXC_SAI1_RXD5_GPIO4_IO07   0x30330164, 0x5, 0x00000000, 0x0, 0x303303C4
 
#define IOMUXC_SAI1_RXD6_AUDIOMIX_SAI1_RX_DATA6   0x30330168, 0x0, 0x00000000, 0x0, 0x303303C8
 
#define IOMUXC_SAI1_RXD6_AUDIOMIX_SAI6_TX_SYNC   0x30330168, 0x1, 0x30330528, 0x1, 0x303303C8
 
#define IOMUXC_SAI1_RXD6_AUDIOMIX_SAI6_RX_SYNC   0x30330168, 0x2, 0x30330520, 0x1, 0x303303C8
 
#define IOMUXC_SAI1_RXD6_ENET1_RGMII_RD2   0x30330168, 0x4, 0x00000000, 0x0, 0x303303C8
 
#define IOMUXC_SAI1_RXD6_GPIO4_IO08   0x30330168, 0x5, 0x00000000, 0x0, 0x303303C8
 
#define IOMUXC_SAI1_RXD7_AUDIOMIX_SAI1_RX_DATA7   0x3033016C, 0x0, 0x00000000, 0x0, 0x303303CC
 
#define IOMUXC_SAI1_RXD7_AUDIOMIX_SAI6_MCLK   0x3033016C, 0x1, 0x30330514, 0x1, 0x303303CC
 
#define IOMUXC_SAI1_RXD7_AUDIOMIX_SAI1_TX_SYNC   0x3033016C, 0x2, 0x303304D8, 0x3, 0x303303CC
 
#define IOMUXC_SAI1_RXD7_AUDIOMIX_SAI1_TX_DATA4   0x3033016C, 0x3, 0x00000000, 0x0, 0x303303CC
 
#define IOMUXC_SAI1_RXD7_ENET1_RGMII_RD3   0x3033016C, 0x4, 0x00000000, 0x0, 0x303303CC
 
#define IOMUXC_SAI1_RXD7_GPIO4_IO09   0x3033016C, 0x5, 0x00000000, 0x0, 0x303303CC
 
#define IOMUXC_SAI1_TXFS_AUDIOMIX_SAI1_TX_SYNC   0x30330170, 0x0, 0x303304D8, 0x4, 0x303303D0
 
#define IOMUXC_SAI1_TXFS_ENET1_RGMII_RX_CTL   0x30330170, 0x4, 0x30330588, 0x1, 0x303303D0
 
#define IOMUXC_SAI1_TXFS_GPIO4_IO10   0x30330170, 0x5, 0x00000000, 0x0, 0x303303D0
 
#define IOMUXC_SAI1_TXC_AUDIOMIX_SAI1_TX_BCLK   0x30330174, 0x0, 0x303304D4, 0x1, 0x303303D4
 
#define IOMUXC_SAI1_TXC_ENET1_RGMII_RXC   0x30330174, 0x4, 0x00000000, 0x0, 0x303303D4
 
#define IOMUXC_SAI1_TXC_GPIO4_IO11   0x30330174, 0x5, 0x00000000, 0x0, 0x303303D4
 
#define IOMUXC_SAI1_TXD0_AUDIOMIX_SAI1_TX_DATA0   0x30330178, 0x0, 0x00000000, 0x0, 0x303303D8
 
#define IOMUXC_SAI1_TXD0_ENET1_RGMII_TD0   0x30330178, 0x4, 0x00000000, 0x0, 0x303303D8
 
#define IOMUXC_SAI1_TXD0_GPIO4_IO12   0x30330178, 0x5, 0x00000000, 0x0, 0x303303D8
 
#define IOMUXC_SAI1_TXD1_AUDIOMIX_SAI1_TX_DATA1   0x3033017C, 0x0, 0x00000000, 0x0, 0x303303DC
 
#define IOMUXC_SAI1_TXD1_ENET1_RGMII_TD1   0x3033017C, 0x4, 0x00000000, 0x0, 0x303303DC
 
#define IOMUXC_SAI1_TXD1_GPIO4_IO13   0x3033017C, 0x5, 0x00000000, 0x0, 0x303303DC
 
#define IOMUXC_SAI1_TXD2_AUDIOMIX_SAI1_TX_DATA2   0x30330180, 0x0, 0x00000000, 0x0, 0x303303E0
 
#define IOMUXC_SAI1_TXD2_ENET1_RGMII_TD2   0x30330180, 0x4, 0x00000000, 0x0, 0x303303E0
 
#define IOMUXC_SAI1_TXD2_GPIO4_IO14   0x30330180, 0x5, 0x00000000, 0x0, 0x303303E0
 
#define IOMUXC_SAI1_TXD3_AUDIOMIX_SAI1_TX_DATA3   0x30330184, 0x0, 0x00000000, 0x0, 0x303303E4
 
#define IOMUXC_SAI1_TXD3_ENET1_RGMII_TD3   0x30330184, 0x4, 0x00000000, 0x0, 0x303303E4
 
#define IOMUXC_SAI1_TXD3_GPIO4_IO15   0x30330184, 0x5, 0x00000000, 0x0, 0x303303E4
 
#define IOMUXC_SAI1_TXD4_AUDIOMIX_SAI1_TX_DATA4   0x30330188, 0x0, 0x00000000, 0x0, 0x303303E8
 
#define IOMUXC_SAI1_TXD4_AUDIOMIX_SAI6_RX_BCLK   0x30330188, 0x1, 0x30330518, 0x2, 0x303303E8
 
#define IOMUXC_SAI1_TXD4_AUDIOMIX_SAI6_TX_BCLK   0x30330188, 0x2, 0x30330524, 0x2, 0x303303E8
 
#define IOMUXC_SAI1_TXD4_ENET1_RGMII_TX_CTL   0x30330188, 0x4, 0x00000000, 0x0, 0x303303E8
 
#define IOMUXC_SAI1_TXD4_GPIO4_IO16   0x30330188, 0x5, 0x00000000, 0x0, 0x303303E8
 
#define IOMUXC_SAI1_TXD5_AUDIOMIX_SAI1_TX_DATA5   0x3033018C, 0x0, 0x00000000, 0x0, 0x303303EC
 
#define IOMUXC_SAI1_TXD5_AUDIOMIX_SAI6_RX_DATA0   0x3033018C, 0x1, 0x3033051C, 0x2, 0x303303EC
 
#define IOMUXC_SAI1_TXD5_AUDIOMIX_SAI6_TX_DATA0   0x3033018C, 0x2, 0x00000000, 0x0, 0x303303EC
 
#define IOMUXC_SAI1_TXD5_ENET1_RGMII_TXC   0x3033018C, 0x4, 0x00000000, 0x0, 0x303303EC
 
#define IOMUXC_SAI1_TXD5_GPIO4_IO17   0x3033018C, 0x5, 0x00000000, 0x0, 0x303303EC
 
#define IOMUXC_SAI1_TXD6_AUDIOMIX_SAI1_TX_DATA6   0x30330190, 0x0, 0x00000000, 0x0, 0x303303F0
 
#define IOMUXC_SAI1_TXD6_AUDIOMIX_SAI6_RX_SYNC   0x30330190, 0x1, 0x30330520, 0x2, 0x303303F0
 
#define IOMUXC_SAI1_TXD6_AUDIOMIX_SAI6_TX_SYNC   0x30330190, 0x2, 0x30330528, 0x2, 0x303303F0
 
#define IOMUXC_SAI1_TXD6_ENET1_RX_ER   0x30330190, 0x4, 0x3033058C, 0x1, 0x303303F0
 
#define IOMUXC_SAI1_TXD6_GPIO4_IO18   0x30330190, 0x5, 0x00000000, 0x0, 0x303303F0
 
#define IOMUXC_SAI1_TXD7_AUDIOMIX_SAI1_TX_DATA7   0x30330194, 0x0, 0x00000000, 0x0, 0x303303F4
 
#define IOMUXC_SAI1_TXD7_AUDIOMIX_SAI6_MCLK   0x30330194, 0x1, 0x30330514, 0x2, 0x303303F4
 
#define IOMUXC_SAI1_TXD7_AUDIOMIX_PDM_CLK   0x30330194, 0x3, 0x00000000, 0x0, 0x303303F4
 
#define IOMUXC_SAI1_TXD7_ENET1_TX_ER   0x30330194, 0x4, 0x00000000, 0x0, 0x303303F4
 
#define IOMUXC_SAI1_TXD7_GPIO4_IO19   0x30330194, 0x5, 0x00000000, 0x0, 0x303303F4
 
#define IOMUXC_SAI1_MCLK_AUDIOMIX_SAI1_MCLK   0x30330198, 0x0, 0x00000000, 0x0, 0x303303F8
 
#define IOMUXC_SAI1_MCLK_AUDIOMIX_SAI1_TX_BCLK   0x30330198, 0x2, 0x303304D4, 0x2, 0x303303F8
 
#define IOMUXC_SAI1_MCLK_ENET1_TX_CLK   0x30330198, 0x4, 0x30330578, 0x1, 0x303303F8
 
#define IOMUXC_SAI1_MCLK_GPIO4_IO20   0x30330198, 0x5, 0x00000000, 0x0, 0x303303F8
 
#define IOMUXC_SAI2_RXFS_AUDIOMIX_SAI2_RX_SYNC   0x3033019C, 0x0, 0x00000000, 0x0, 0x303303FC
 
#define IOMUXC_SAI2_RXFS_AUDIOMIX_SAI5_TX_SYNC   0x3033019C, 0x1, 0x30330510, 0x2, 0x303303FC
 
#define IOMUXC_SAI2_RXFS_AUDIOMIX_SAI5_TX_DATA1   0x3033019C, 0x2, 0x00000000, 0x0, 0x303303FC
 
#define IOMUXC_SAI2_RXFS_AUDIOMIX_SAI2_RX_DATA1   0x3033019C, 0x3, 0x303304DC, 0x0, 0x303303FC
 
#define IOMUXC_SAI2_RXFS_UART1_TX   0x3033019C, 0x4, 0x00000000, 0x0, 0x303303FC
 
#define IOMUXC_SAI2_RXFS_UART1_RX   0x3033019C, 0x4, 0x303305E8, 0x2, 0x303303FC
 
#define IOMUXC_SAI2_RXFS_GPIO4_IO21   0x3033019C, 0x5, 0x00000000, 0x0, 0x303303FC
 
#define IOMUXC_SAI2_RXFS_AUDIOMIX_PDM_BIT_STREAM2   0x3033019C, 0x6, 0x303304C8, 0x5, 0x303303FC
 
#define IOMUXC_SAI2_RXC_AUDIOMIX_SAI2_RX_BCLK   0x303301A0, 0x0, 0x00000000, 0x0, 0x30330400
 
#define IOMUXC_SAI2_RXC_AUDIOMIX_SAI5_TX_BCLK   0x303301A0, 0x1, 0x3033050C, 0x2, 0x30330400
 
#define IOMUXC_SAI2_RXC_CAN1_TX   0x303301A0, 0x3, 0x00000000, 0x0, 0x30330400
 
#define IOMUXC_SAI2_RXC_UART1_RX   0x303301A0, 0x4, 0x303305E8, 0x3, 0x30330400
 
#define IOMUXC_SAI2_RXC_UART1_TX   0x303301A0, 0x4, 0x00000000, 0x0, 0x30330400
 
#define IOMUXC_SAI2_RXC_GPIO4_IO22   0x303301A0, 0x5, 0x00000000, 0x0, 0x30330400
 
#define IOMUXC_SAI2_RXC_AUDIOMIX_PDM_BIT_STREAM1   0x303301A0, 0x6, 0x303304C4, 0x5, 0x30330400
 
#define IOMUXC_SAI2_RXD0_AUDIOMIX_SAI2_RX_DATA0   0x303301A4, 0x0, 0x00000000, 0x0, 0x30330404
 
#define IOMUXC_SAI2_RXD0_AUDIOMIX_SAI5_TX_DATA0   0x303301A4, 0x1, 0x00000000, 0x0, 0x30330404
 
#define IOMUXC_SAI2_RXD0_ENET_QOS_1588_EVENT2_OUT   0x303301A4, 0x2, 0x00000000, 0x0, 0x30330404
 
#define IOMUXC_SAI2_RXD0_AUDIOMIX_SAI2_TX_DATA1   0x303301A4, 0x3, 0x00000000, 0x0, 0x30330404
 
#define IOMUXC_SAI2_RXD0_UART1_RTS_B   0x303301A4, 0x4, 0x303305E4, 0x2, 0x30330404
 
#define IOMUXC_SAI2_RXD0_UART1_CTS_B   0x303301A4, 0x4, 0x00000000, 0x0, 0x30330404
 
#define IOMUXC_SAI2_RXD0_GPIO4_IO23   0x303301A4, 0x5, 0x00000000, 0x0, 0x30330404
 
#define IOMUXC_SAI2_RXD0_AUDIOMIX_PDM_BIT_STREAM3   0x303301A4, 0x6, 0x303304CC, 0x5, 0x30330404
 
#define IOMUXC_SAI2_TXFS_AUDIOMIX_SAI2_TX_SYNC   0x303301A8, 0x0, 0x00000000, 0x0, 0x30330408
 
#define IOMUXC_SAI2_TXFS_AUDIOMIX_SAI5_TX_DATA1   0x303301A8, 0x1, 0x00000000, 0x0, 0x30330408
 
#define IOMUXC_SAI2_TXFS_ENET_QOS_1588_EVENT3_OUT   0x303301A8, 0x2, 0x00000000, 0x0, 0x30330408
 
#define IOMUXC_SAI2_TXFS_AUDIOMIX_SAI2_TX_DATA1   0x303301A8, 0x3, 0x00000000, 0x0, 0x30330408
 
#define IOMUXC_SAI2_TXFS_UART1_CTS_B   0x303301A8, 0x4, 0x00000000, 0x0, 0x30330408
 
#define IOMUXC_SAI2_TXFS_UART1_RTS_B   0x303301A8, 0x4, 0x303305E4, 0x3, 0x30330408
 
#define IOMUXC_SAI2_TXFS_GPIO4_IO24   0x303301A8, 0x5, 0x00000000, 0x0, 0x30330408
 
#define IOMUXC_SAI2_TXFS_AUDIOMIX_PDM_BIT_STREAM2   0x303301A8, 0x6, 0x303304C8, 0x6, 0x30330408
 
#define IOMUXC_SAI2_TXC_AUDIOMIX_SAI2_TX_BCLK   0x303301AC, 0x0, 0x00000000, 0x0, 0x3033040C
 
#define IOMUXC_SAI2_TXC_AUDIOMIX_SAI5_TX_DATA2   0x303301AC, 0x1, 0x00000000, 0x0, 0x3033040C
 
#define IOMUXC_SAI2_TXC_CAN1_RX   0x303301AC, 0x3, 0x3033054C, 0x1, 0x3033040C
 
#define IOMUXC_SAI2_TXC_GPIO4_IO25   0x303301AC, 0x5, 0x00000000, 0x0, 0x3033040C
 
#define IOMUXC_SAI2_TXC_AUDIOMIX_PDM_BIT_STREAM1   0x303301AC, 0x6, 0x303304C4, 0x6, 0x3033040C
 
#define IOMUXC_SAI2_TXD0_AUDIOMIX_SAI2_TX_DATA0   0x303301B0, 0x0, 0x00000000, 0x0, 0x30330410
 
#define IOMUXC_SAI2_TXD0_AUDIOMIX_SAI5_TX_DATA3   0x303301B0, 0x1, 0x00000000, 0x0, 0x30330410
 
#define IOMUXC_SAI2_TXD0_ENET_QOS_1588_EVENT2_IN   0x303301B0, 0x2, 0x00000000, 0x0, 0x30330410
 
#define IOMUXC_SAI2_TXD0_CAN2_TX   0x303301B0, 0x3, 0x00000000, 0x0, 0x30330410
 
#define IOMUXC_SAI2_TXD0_ENET_QOS_1588_EVENT2_AUX_IN   0x303301B0, 0x4, 0x00000000, 0x0, 0x30330410
 
#define IOMUXC_SAI2_TXD0_GPIO4_IO26   0x303301B0, 0x5, 0x00000000, 0x0, 0x30330410
 
#define IOMUXC_SAI2_MCLK_AUDIOMIX_SAI2_MCLK   0x303301B4, 0x0, 0x00000000, 0x0, 0x30330414
 
#define IOMUXC_SAI2_MCLK_AUDIOMIX_SAI5_MCLK   0x303301B4, 0x1, 0x303304F0, 0x2, 0x30330414
 
#define IOMUXC_SAI2_MCLK_ENET_QOS_1588_EVENT3_IN   0x303301B4, 0x2, 0x00000000, 0x0, 0x30330414
 
#define IOMUXC_SAI2_MCLK_CAN2_RX   0x303301B4, 0x3, 0x30330550, 0x1, 0x30330414
 
#define IOMUXC_SAI2_MCLK_ENET_QOS_1588_EVENT3_AUX_IN   0x303301B4, 0x4, 0x00000000, 0x0, 0x30330414
 
#define IOMUXC_SAI2_MCLK_GPIO4_IO27   0x303301B4, 0x5, 0x00000000, 0x0, 0x30330414
 
#define IOMUXC_SAI2_MCLK_AUDIOMIX_SAI3_MCLK   0x303301B4, 0x6, 0x303304E0, 0x1, 0x30330414
 
#define IOMUXC_SAI3_RXFS_AUDIOMIX_SAI3_RX_SYNC   0x303301B8, 0x0, 0x00000000, 0x0, 0x30330418
 
#define IOMUXC_SAI3_RXFS_AUDIOMIX_SAI2_RX_DATA1   0x303301B8, 0x1, 0x303304DC, 0x1, 0x30330418
 
#define IOMUXC_SAI3_RXFS_AUDIOMIX_SAI5_RX_SYNC   0x303301B8, 0x2, 0x30330508, 0x2, 0x30330418
 
#define IOMUXC_SAI3_RXFS_AUDIOMIX_SAI3_RX_DATA1   0x303301B8, 0x3, 0x00000000, 0x0, 0x30330418
 
#define IOMUXC_SAI3_RXFS_AUDIOMIX_SPDIF1_IN   0x303301B8, 0x4, 0x30330544, 0x2, 0x30330418
 
#define IOMUXC_SAI3_RXFS_GPIO4_IO28   0x303301B8, 0x5, 0x00000000, 0x0, 0x30330418
 
#define IOMUXC_SAI3_RXFS_AUDIOMIX_PDM_BIT_STREAM0   0x303301B8, 0x6, 0x303304C0, 0x5, 0x30330418
 
#define IOMUXC_SAI3_RXC_AUDIOMIX_SAI3_RX_BCLK   0x303301BC, 0x0, 0x00000000, 0x0, 0x3033041C
 
#define IOMUXC_SAI3_RXC_AUDIOMIX_SAI2_RX_DATA2   0x303301BC, 0x1, 0x00000000, 0x0, 0x3033041C
 
#define IOMUXC_SAI3_RXC_AUDIOMIX_SAI5_RX_BCLK   0x303301BC, 0x2, 0x303304F4, 0x2, 0x3033041C
 
#define IOMUXC_SAI3_RXC_GPT1_CLK   0x303301BC, 0x3, 0x3033059C, 0x0, 0x3033041C
 
#define IOMUXC_SAI3_RXC_UART2_CTS_B   0x303301BC, 0x4, 0x00000000, 0x0, 0x3033041C
 
#define IOMUXC_SAI3_RXC_UART2_RTS_B   0x303301BC, 0x4, 0x303305EC, 0x2, 0x3033041C
 
#define IOMUXC_SAI3_RXC_GPIO4_IO29   0x303301BC, 0x5, 0x00000000, 0x0, 0x3033041C
 
#define IOMUXC_SAI3_RXC_AUDIOMIX_PDM_CLK   0x303301BC, 0x6, 0x00000000, 0x0, 0x3033041C
 
#define IOMUXC_SAI3_RXD_AUDIOMIX_SAI3_RX_DATA0   0x303301C0, 0x0, 0x303304E4, 0x1, 0x30330420
 
#define IOMUXC_SAI3_RXD_AUDIOMIX_SAI2_RX_DATA3   0x303301C0, 0x1, 0x00000000, 0x0, 0x30330420
 
#define IOMUXC_SAI3_RXD_AUDIOMIX_SAI5_RX_DATA0   0x303301C0, 0x2, 0x303304F8, 0x2, 0x30330420
 
#define IOMUXC_SAI3_RXD_UART2_RTS_B   0x303301C0, 0x4, 0x303305EC, 0x3, 0x30330420
 
#define IOMUXC_SAI3_RXD_UART2_CTS_B   0x303301C0, 0x4, 0x00000000, 0x0, 0x30330420
 
#define IOMUXC_SAI3_RXD_GPIO4_IO30   0x303301C0, 0x5, 0x00000000, 0x0, 0x30330420
 
#define IOMUXC_SAI3_RXD_AUDIOMIX_PDM_BIT_STREAM1   0x303301C0, 0x6, 0x303304C4, 0x7, 0x30330420
 
#define IOMUXC_SAI3_TXFS_AUDIOMIX_SAI3_TX_SYNC   0x303301C4, 0x0, 0x303304EC, 0x1, 0x30330424
 
#define IOMUXC_SAI3_TXFS_AUDIOMIX_SAI2_TX_DATA1   0x303301C4, 0x1, 0x00000000, 0x0, 0x30330424
 
#define IOMUXC_SAI3_TXFS_AUDIOMIX_SAI5_RX_DATA1   0x303301C4, 0x2, 0x303304FC, 0x2, 0x30330424
 
#define IOMUXC_SAI3_TXFS_AUDIOMIX_SAI3_TX_DATA1   0x303301C4, 0x3, 0x00000000, 0x0, 0x30330424
 
#define IOMUXC_SAI3_TXFS_UART2_RX   0x303301C4, 0x4, 0x303305F0, 0x4, 0x30330424
 
#define IOMUXC_SAI3_TXFS_UART2_TX   0x303301C4, 0x4, 0x00000000, 0x0, 0x30330424
 
#define IOMUXC_SAI3_TXFS_GPIO4_IO31   0x303301C4, 0x5, 0x00000000, 0x0, 0x30330424
 
#define IOMUXC_SAI3_TXFS_AUDIOMIX_PDM_BIT_STREAM3   0x303301C4, 0x6, 0x303304CC, 0x6, 0x30330424
 
#define IOMUXC_SAI3_TXC_AUDIOMIX_SAI3_TX_BCLK   0x303301C8, 0x0, 0x303304E8, 0x1, 0x30330428
 
#define IOMUXC_SAI3_TXC_AUDIOMIX_SAI2_TX_DATA2   0x303301C8, 0x1, 0x00000000, 0x0, 0x30330428
 
#define IOMUXC_SAI3_TXC_AUDIOMIX_SAI5_RX_DATA2   0x303301C8, 0x2, 0x30330500, 0x2, 0x30330428
 
#define IOMUXC_SAI3_TXC_GPT1_CAPTURE1   0x303301C8, 0x3, 0x30330594, 0x0, 0x30330428
 
#define IOMUXC_SAI3_TXC_UART2_TX   0x303301C8, 0x4, 0x00000000, 0x0, 0x30330428
 
#define IOMUXC_SAI3_TXC_UART2_RX   0x303301C8, 0x4, 0x303305F0, 0x5, 0x30330428
 
#define IOMUXC_SAI3_TXC_GPIO5_IO00   0x303301C8, 0x5, 0x00000000, 0x0, 0x30330428
 
#define IOMUXC_SAI3_TXC_AUDIOMIX_PDM_BIT_STREAM2   0x303301C8, 0x6, 0x303304C8, 0x7, 0x30330428
 
#define IOMUXC_SAI3_TXD_AUDIOMIX_SAI3_TX_DATA0   0x303301CC, 0x0, 0x00000000, 0x0, 0x3033042C
 
#define IOMUXC_SAI3_TXD_AUDIOMIX_SAI2_TX_DATA3   0x303301CC, 0x1, 0x00000000, 0x0, 0x3033042C
 
#define IOMUXC_SAI3_TXD_AUDIOMIX_SAI5_RX_DATA3   0x303301CC, 0x2, 0x30330504, 0x2, 0x3033042C
 
#define IOMUXC_SAI3_TXD_GPT1_CAPTURE2   0x303301CC, 0x3, 0x30330598, 0x0, 0x3033042C
 
#define IOMUXC_SAI3_TXD_AUDIOMIX_SPDIF1_EXT_CLK   0x303301CC, 0x4, 0x30330548, 0x0, 0x3033042C
 
#define IOMUXC_SAI3_TXD_GPIO5_IO01   0x303301CC, 0x5, 0x00000000, 0x0, 0x3033042C
 
#define IOMUXC_SAI3_MCLK_AUDIOMIX_SAI3_MCLK   0x303301D0, 0x0, 0x303304E0, 0x2, 0x30330430
 
#define IOMUXC_SAI3_MCLK_PWM4_OUT   0x303301D0, 0x1, 0x00000000, 0x0, 0x30330430
 
#define IOMUXC_SAI3_MCLK_AUDIOMIX_SAI5_MCLK   0x303301D0, 0x2, 0x303304F0, 0x3, 0x30330430
 
#define IOMUXC_SAI3_MCLK_AUDIOMIX_SPDIF1_OUT   0x303301D0, 0x4, 0x00000000, 0x0, 0x30330430
 
#define IOMUXC_SAI3_MCLK_GPIO5_IO02   0x303301D0, 0x5, 0x00000000, 0x0, 0x30330430
 
#define IOMUXC_SAI3_MCLK_AUDIOMIX_SPDIF1_IN   0x303301D0, 0x6, 0x30330544, 0x3, 0x30330430
 
#define IOMUXC_SPDIF_TX_AUDIOMIX_SPDIF1_OUT   0x303301D4, 0x0, 0x00000000, 0x0, 0x30330434
 
#define IOMUXC_SPDIF_TX_PWM3_OUT   0x303301D4, 0x1, 0x00000000, 0x0, 0x30330434
 
#define IOMUXC_SPDIF_TX_I2C5_SCL   0x303301D4, 0x2, 0x303305C4, 0x2, 0x30330434
 
#define IOMUXC_SPDIF_TX_GPT1_COMPARE1   0x303301D4, 0x3, 0x00000000, 0x0, 0x30330434
 
#define IOMUXC_SPDIF_TX_CAN1_TX   0x303301D4, 0x4, 0x00000000, 0x0, 0x30330434
 
#define IOMUXC_SPDIF_TX_GPIO5_IO03   0x303301D4, 0x5, 0x00000000, 0x0, 0x30330434
 
#define IOMUXC_SPDIF_RX_AUDIOMIX_SPDIF1_IN   0x303301D8, 0x0, 0x30330544, 0x4, 0x30330438
 
#define IOMUXC_SPDIF_RX_PWM2_OUT   0x303301D8, 0x1, 0x00000000, 0x0, 0x30330438
 
#define IOMUXC_SPDIF_RX_I2C5_SDA   0x303301D8, 0x2, 0x303305C8, 0x2, 0x30330438
 
#define IOMUXC_SPDIF_RX_GPT1_COMPARE2   0x303301D8, 0x3, 0x00000000, 0x0, 0x30330438
 
#define IOMUXC_SPDIF_RX_CAN1_RX   0x303301D8, 0x4, 0x3033054C, 0x2, 0x30330438
 
#define IOMUXC_SPDIF_RX_GPIO5_IO04   0x303301D8, 0x5, 0x00000000, 0x0, 0x30330438
 
#define IOMUXC_SPDIF_EXT_CLK_AUDIOMIX_SPDIF1_EXT_CLK   0x303301DC, 0x0, 0x30330548, 0x1, 0x3033043C
 
#define IOMUXC_SPDIF_EXT_CLK_PWM1_OUT   0x303301DC, 0x1, 0x00000000, 0x0, 0x3033043C
 
#define IOMUXC_SPDIF_EXT_CLK_GPT1_COMPARE3   0x303301DC, 0x3, 0x00000000, 0x0, 0x3033043C
 
#define IOMUXC_SPDIF_EXT_CLK_GPIO5_IO05   0x303301DC, 0x5, 0x00000000, 0x0, 0x3033043C
 
#define IOMUXC_ECSPI1_SCLK_ECSPI1_SCLK   0x303301E0, 0x0, 0x30330558, 0x0, 0x30330440
 
#define IOMUXC_ECSPI1_SCLK_UART3_RX   0x303301E0, 0x1, 0x303305F8, 0x4, 0x30330440
 
#define IOMUXC_ECSPI1_SCLK_UART3_TX   0x303301E0, 0x1, 0x00000000, 0x0, 0x30330440
 
#define IOMUXC_ECSPI1_SCLK_I2C1_SCL   0x303301E0, 0x2, 0x303305A4, 0x1, 0x30330440
 
#define IOMUXC_ECSPI1_SCLK_AUDIOMIX_SAI7_RX_SYNC   0x303301E0, 0x3, 0x30330538, 0x1, 0x30330440
 
#define IOMUXC_ECSPI1_SCLK_GPIO5_IO06   0x303301E0, 0x5, 0x00000000, 0x0, 0x30330440
 
#define IOMUXC_ECSPI1_MOSI_ECSPI1_MOSI   0x303301E4, 0x0, 0x30330560, 0x0, 0x30330444
 
#define IOMUXC_ECSPI1_MOSI_UART3_TX   0x303301E4, 0x1, 0x00000000, 0x0, 0x30330444
 
#define IOMUXC_ECSPI1_MOSI_UART3_RX   0x303301E4, 0x1, 0x303305F8, 0x5, 0x30330444
 
#define IOMUXC_ECSPI1_MOSI_I2C1_SDA   0x303301E4, 0x2, 0x303305A8, 0x1, 0x30330444
 
#define IOMUXC_ECSPI1_MOSI_AUDIOMIX_SAI7_RX_BCLK   0x303301E4, 0x3, 0x30330530, 0x1, 0x30330444
 
#define IOMUXC_ECSPI1_MOSI_GPIO5_IO07   0x303301E4, 0x5, 0x00000000, 0x0, 0x30330444
 
#define IOMUXC_ECSPI1_MISO_ECSPI1_MISO   0x303301E8, 0x0, 0x3033055C, 0x0, 0x30330448
 
#define IOMUXC_ECSPI1_MISO_UART3_CTS_B   0x303301E8, 0x1, 0x00000000, 0x0, 0x30330448
 
#define IOMUXC_ECSPI1_MISO_UART3_RTS_B   0x303301E8, 0x1, 0x303305F4, 0x2, 0x30330448
 
#define IOMUXC_ECSPI1_MISO_I2C2_SCL   0x303301E8, 0x2, 0x303305AC, 0x1, 0x30330448
 
#define IOMUXC_ECSPI1_MISO_AUDIOMIX_SAI7_RX_DATA0   0x303301E8, 0x3, 0x30330534, 0x1, 0x30330448
 
#define IOMUXC_ECSPI1_MISO_GPIO5_IO08   0x303301E8, 0x5, 0x00000000, 0x0, 0x30330448
 
#define IOMUXC_ECSPI1_SS0_ECSPI1_SS0   0x303301EC, 0x0, 0x30330564, 0x0, 0x3033044C
 
#define IOMUXC_ECSPI1_SS0_UART3_RTS_B   0x303301EC, 0x1, 0x303305F4, 0x3, 0x3033044C
 
#define IOMUXC_ECSPI1_SS0_UART3_CTS_B   0x303301EC, 0x1, 0x00000000, 0x0, 0x3033044C
 
#define IOMUXC_ECSPI1_SS0_I2C2_SDA   0x303301EC, 0x2, 0x303305B0, 0x1, 0x3033044C
 
#define IOMUXC_ECSPI1_SS0_AUDIOMIX_SAI7_TX_SYNC   0x303301EC, 0x3, 0x30330540, 0x1, 0x3033044C
 
#define IOMUXC_ECSPI1_SS0_GPIO5_IO09   0x303301EC, 0x5, 0x00000000, 0x0, 0x3033044C
 
#define IOMUXC_ECSPI2_SCLK_ECSPI2_SCLK   0x303301F0, 0x0, 0x30330568, 0x1, 0x30330450
 
#define IOMUXC_ECSPI2_SCLK_UART4_RX   0x303301F0, 0x1, 0x30330600, 0x6, 0x30330450
 
#define IOMUXC_ECSPI2_SCLK_UART4_TX   0x303301F0, 0x1, 0x00000000, 0x0, 0x30330450
 
#define IOMUXC_ECSPI2_SCLK_I2C3_SCL   0x303301F0, 0x2, 0x303305B4, 0x3, 0x30330450
 
#define IOMUXC_ECSPI2_SCLK_AUDIOMIX_SAI7_TX_BCLK   0x303301F0, 0x3, 0x3033053C, 0x1, 0x30330450
 
#define IOMUXC_ECSPI2_SCLK_GPIO5_IO10   0x303301F0, 0x5, 0x00000000, 0x0, 0x30330450
 
#define IOMUXC_ECSPI2_MOSI_ECSPI2_MOSI   0x303301F4, 0x0, 0x30330570, 0x1, 0x30330454
 
#define IOMUXC_ECSPI2_MOSI_UART4_TX   0x303301F4, 0x1, 0x00000000, 0x0, 0x30330454
 
#define IOMUXC_ECSPI2_MOSI_UART4_RX   0x303301F4, 0x1, 0x30330600, 0x7, 0x30330454
 
#define IOMUXC_ECSPI2_MOSI_I2C3_SDA   0x303301F4, 0x2, 0x303305B8, 0x3, 0x30330454
 
#define IOMUXC_ECSPI2_MOSI_AUDIOMIX_SAI7_TX_DATA0   0x303301F4, 0x3, 0x00000000, 0x0, 0x30330454
 
#define IOMUXC_ECSPI2_MOSI_GPIO5_IO11   0x303301F4, 0x5, 0x00000000, 0x0, 0x30330454
 
#define IOMUXC_ECSPI2_MISO_ECSPI2_MISO   0x303301F8, 0x0, 0x3033056C, 0x1, 0x30330458
 
#define IOMUXC_ECSPI2_MISO_UART4_CTS_B   0x303301F8, 0x1, 0x00000000, 0x0, 0x30330458
 
#define IOMUXC_ECSPI2_MISO_UART4_RTS_B   0x303301F8, 0x1, 0x303305FC, 0x2, 0x30330458
 
#define IOMUXC_ECSPI2_MISO_I2C4_SCL   0x303301F8, 0x2, 0x303305BC, 0x4, 0x30330458
 
#define IOMUXC_ECSPI2_MISO_AUDIOMIX_SAI7_MCLK   0x303301F8, 0x3, 0x3033052C, 0x1, 0x30330458
 
#define IOMUXC_ECSPI2_MISO_CCM_CLKO1   0x303301F8, 0x4, 0x00000000, 0x0, 0x30330458
 
#define IOMUXC_ECSPI2_MISO_GPIO5_IO12   0x303301F8, 0x5, 0x00000000, 0x0, 0x30330458
 
#define IOMUXC_ECSPI2_SS0_ECSPI2_SS0   0x303301FC, 0x0, 0x30330574, 0x1, 0x3033045C
 
#define IOMUXC_ECSPI2_SS0_UART4_RTS_B   0x303301FC, 0x1, 0x303305FC, 0x3, 0x3033045C
 
#define IOMUXC_ECSPI2_SS0_UART4_CTS_B   0x303301FC, 0x1, 0x00000000, 0x0, 0x3033045C
 
#define IOMUXC_ECSPI2_SS0_I2C4_SDA   0x303301FC, 0x2, 0x303305C0, 0x4, 0x3033045C
 
#define IOMUXC_ECSPI2_SS0_CCM_CLKO2   0x303301FC, 0x4, 0x00000000, 0x0, 0x3033045C
 
#define IOMUXC_ECSPI2_SS0_GPIO5_IO13   0x303301FC, 0x5, 0x00000000, 0x0, 0x3033045C
 
#define IOMUXC_I2C1_SCL_I2C1_SCL   0x30330200, 0x0, 0x303305A4, 0x2, 0x30330460
 
#define IOMUXC_I2C1_SCL_ENET_QOS_MDC   0x30330200, 0x1, 0x00000000, 0x0, 0x30330460
 
#define IOMUXC_I2C1_SCL_ECSPI1_SCLK   0x30330200, 0x3, 0x30330558, 0x1, 0x30330460
 
#define IOMUXC_I2C1_SCL_GPIO5_IO14   0x30330200, 0x5, 0x00000000, 0x0, 0x30330460
 
#define IOMUXC_I2C1_SDA_I2C1_SDA   0x30330204, 0x0, 0x303305A8, 0x2, 0x30330464
 
#define IOMUXC_I2C1_SDA_ENET_QOS_MDIO   0x30330204, 0x1, 0x30330590, 0x2, 0x30330464
 
#define IOMUXC_I2C1_SDA_ECSPI1_MOSI   0x30330204, 0x3, 0x30330560, 0x1, 0x30330464
 
#define IOMUXC_I2C1_SDA_GPIO5_IO15   0x30330204, 0x5, 0x00000000, 0x0, 0x30330464
 
#define IOMUXC_I2C2_SCL_I2C2_SCL   0x30330208, 0x0, 0x303305AC, 0x2, 0x30330468
 
#define IOMUXC_I2C2_SCL_ENET_QOS_1588_EVENT1_IN   0x30330208, 0x1, 0x00000000, 0x0, 0x30330468
 
#define IOMUXC_I2C2_SCL_USDHC3_CD_B   0x30330208, 0x2, 0x30330608, 0x3, 0x30330468
 
#define IOMUXC_I2C2_SCL_ECSPI1_MISO   0x30330208, 0x3, 0x3033055C, 0x1, 0x30330468
 
#define IOMUXC_I2C2_SCL_ENET_QOS_1588_EVENT1_AUX_IN   0x30330208, 0x4, 0x00000000, 0x0, 0x30330468
 
#define IOMUXC_I2C2_SCL_GPIO5_IO16   0x30330208, 0x5, 0x00000000, 0x0, 0x30330468
 
#define IOMUXC_I2C2_SDA_I2C2_SDA   0x3033020C, 0x0, 0x303305B0, 0x2, 0x3033046C
 
#define IOMUXC_I2C2_SDA_ENET_QOS_1588_EVENT1_OUT   0x3033020C, 0x1, 0x00000000, 0x0, 0x3033046C
 
#define IOMUXC_I2C2_SDA_USDHC3_WP   0x3033020C, 0x2, 0x30330634, 0x3, 0x3033046C
 
#define IOMUXC_I2C2_SDA_ECSPI1_SS0   0x3033020C, 0x3, 0x30330564, 0x1, 0x3033046C
 
#define IOMUXC_I2C2_SDA_GPIO5_IO17   0x3033020C, 0x5, 0x00000000, 0x0, 0x3033046C
 
#define IOMUXC_I2C3_SCL_I2C3_SCL   0x30330210, 0x0, 0x303305B4, 0x4, 0x30330470
 
#define IOMUXC_I2C3_SCL_PWM4_OUT   0x30330210, 0x1, 0x00000000, 0x0, 0x30330470
 
#define IOMUXC_I2C3_SCL_GPT2_CLK   0x30330210, 0x2, 0x00000000, 0x0, 0x30330470
 
#define IOMUXC_I2C3_SCL_ECSPI2_SCLK   0x30330210, 0x3, 0x30330568, 0x2, 0x30330470
 
#define IOMUXC_I2C3_SCL_GPIO5_IO18   0x30330210, 0x5, 0x00000000, 0x0, 0x30330470
 
#define IOMUXC_I2C3_SDA_I2C3_SDA   0x30330214, 0x0, 0x303305B8, 0x4, 0x30330474
 
#define IOMUXC_I2C3_SDA_PWM3_OUT   0x30330214, 0x1, 0x00000000, 0x0, 0x30330474
 
#define IOMUXC_I2C3_SDA_GPT3_CLK   0x30330214, 0x2, 0x00000000, 0x0, 0x30330474
 
#define IOMUXC_I2C3_SDA_ECSPI2_MOSI   0x30330214, 0x3, 0x30330570, 0x2, 0x30330474
 
#define IOMUXC_I2C3_SDA_GPIO5_IO19   0x30330214, 0x5, 0x00000000, 0x0, 0x30330474
 
#define IOMUXC_I2C4_SCL_I2C4_SCL   0x30330218, 0x0, 0x303305BC, 0x5, 0x30330478
 
#define IOMUXC_I2C4_SCL_PWM2_OUT   0x30330218, 0x1, 0x00000000, 0x0, 0x30330478
 
#define IOMUXC_I2C4_SCL_PCIE_CLKREQ_B   0x30330218, 0x2, 0x303305A0, 0x0, 0x30330478
 
#define IOMUXC_I2C4_SCL_ECSPI2_MISO   0x30330218, 0x3, 0x3033056C, 0x2, 0x30330478
 
#define IOMUXC_I2C4_SCL_GPIO5_IO20   0x30330218, 0x5, 0x00000000, 0x0, 0x30330478
 
#define IOMUXC_I2C4_SDA_I2C4_SDA   0x3033021C, 0x0, 0x303305C0, 0x5, 0x3033047C
 
#define IOMUXC_I2C4_SDA_PWM1_OUT   0x3033021C, 0x1, 0x00000000, 0x0, 0x3033047C
 
#define IOMUXC_I2C4_SDA_ECSPI2_SS0   0x3033021C, 0x3, 0x30330574, 0x2, 0x3033047C
 
#define IOMUXC_I2C4_SDA_GPIO5_IO21   0x3033021C, 0x5, 0x00000000, 0x0, 0x3033047C
 
#define IOMUXC_UART1_RXD_UART1_RX   0x30330220, 0x0, 0x303305E8, 0x4, 0x30330480
 
#define IOMUXC_UART1_RXD_UART1_TX   0x30330220, 0x0, 0x00000000, 0x0, 0x30330480
 
#define IOMUXC_UART1_RXD_ECSPI3_SCLK   0x30330220, 0x1, 0x00000000, 0x0, 0x30330480
 
#define IOMUXC_UART1_RXD_GPIO5_IO22   0x30330220, 0x5, 0x00000000, 0x0, 0x30330480
 
#define IOMUXC_UART1_TXD_UART1_TX   0x30330224, 0x0, 0x00000000, 0x0, 0x30330484
 
#define IOMUXC_UART1_TXD_UART1_RX   0x30330224, 0x0, 0x303305E8, 0x5, 0x30330484
 
#define IOMUXC_UART1_TXD_ECSPI3_MOSI   0x30330224, 0x1, 0x00000000, 0x0, 0x30330484
 
#define IOMUXC_UART1_TXD_GPIO5_IO23   0x30330224, 0x5, 0x00000000, 0x0, 0x30330484
 
#define IOMUXC_UART2_RXD_UART2_RX   0x30330228, 0x0, 0x303305F0, 0x6, 0x30330488
 
#define IOMUXC_UART2_RXD_UART2_TX   0x30330228, 0x0, 0x00000000, 0x0, 0x30330488
 
#define IOMUXC_UART2_RXD_ECSPI3_MISO   0x30330228, 0x1, 0x00000000, 0x0, 0x30330488
 
#define IOMUXC_UART2_RXD_GPT1_COMPARE3   0x30330228, 0x3, 0x00000000, 0x0, 0x30330488
 
#define IOMUXC_UART2_RXD_GPIO5_IO24   0x30330228, 0x5, 0x00000000, 0x0, 0x30330488
 
#define IOMUXC_UART2_TXD_UART2_TX   0x3033022C, 0x0, 0x00000000, 0x0, 0x3033048C
 
#define IOMUXC_UART2_TXD_UART2_RX   0x3033022C, 0x0, 0x303305F0, 0x7, 0x3033048C
 
#define IOMUXC_UART2_TXD_ECSPI3_SS0   0x3033022C, 0x1, 0x00000000, 0x0, 0x3033048C
 
#define IOMUXC_UART2_TXD_GPT1_COMPARE2   0x3033022C, 0x3, 0x00000000, 0x0, 0x3033048C
 
#define IOMUXC_UART2_TXD_GPIO5_IO25   0x3033022C, 0x5, 0x00000000, 0x0, 0x3033048C
 
#define IOMUXC_UART3_RXD_UART3_RX   0x30330230, 0x0, 0x303305F8, 0x6, 0x30330490
 
#define IOMUXC_UART3_RXD_UART3_TX   0x30330230, 0x0, 0x00000000, 0x0, 0x30330490
 
#define IOMUXC_UART3_RXD_UART1_CTS_B   0x30330230, 0x1, 0x00000000, 0x0, 0x30330490
 
#define IOMUXC_UART3_RXD_UART1_RTS_B   0x30330230, 0x1, 0x303305E4, 0x4, 0x30330490
 
#define IOMUXC_UART3_RXD_USDHC3_RESET_B   0x30330230, 0x2, 0x00000000, 0x0, 0x30330490
 
#define IOMUXC_UART3_RXD_GPT1_CAPTURE2   0x30330230, 0x3, 0x30330598, 0x1, 0x30330490
 
#define IOMUXC_UART3_RXD_CAN2_TX   0x30330230, 0x4, 0x00000000, 0x0, 0x30330490
 
#define IOMUXC_UART3_RXD_GPIO5_IO26   0x30330230, 0x5, 0x00000000, 0x0, 0x30330490
 
#define IOMUXC_UART3_TXD_UART3_TX   0x30330234, 0x0, 0x00000000, 0x0, 0x30330494
 
#define IOMUXC_UART3_TXD_UART3_RX   0x30330234, 0x0, 0x303305F8, 0x7, 0x30330494
 
#define IOMUXC_UART3_TXD_UART1_RTS_B   0x30330234, 0x1, 0x303305E4, 0x5, 0x30330494
 
#define IOMUXC_UART3_TXD_UART1_CTS_B   0x30330234, 0x1, 0x00000000, 0x0, 0x30330494
 
#define IOMUXC_UART3_TXD_USDHC3_VSELECT   0x30330234, 0x2, 0x00000000, 0x0, 0x30330494
 
#define IOMUXC_UART3_TXD_GPT1_CLK   0x30330234, 0x3, 0x3033059C, 0x1, 0x30330494
 
#define IOMUXC_UART3_TXD_CAN2_RX   0x30330234, 0x4, 0x30330550, 0x2, 0x30330494
 
#define IOMUXC_UART3_TXD_GPIO5_IO27   0x30330234, 0x5, 0x00000000, 0x0, 0x30330494
 
#define IOMUXC_UART4_RXD_UART4_RX   0x30330238, 0x0, 0x30330600, 0x8, 0x30330498
 
#define IOMUXC_UART4_RXD_UART4_TX   0x30330238, 0x0, 0x00000000, 0x0, 0x30330498
 
#define IOMUXC_UART4_RXD_UART2_CTS_B   0x30330238, 0x1, 0x00000000, 0x0, 0x30330498
 
#define IOMUXC_UART4_RXD_UART2_RTS_B   0x30330238, 0x1, 0x303305EC, 0x4, 0x30330498
 
#define IOMUXC_UART4_RXD_PCIE_CLKREQ_B   0x30330238, 0x2, 0x303305A0, 0x1, 0x30330498
 
#define IOMUXC_UART4_RXD_GPT1_COMPARE1   0x30330238, 0x3, 0x00000000, 0x0, 0x30330498
 
#define IOMUXC_UART4_RXD_I2C6_SCL   0x30330238, 0x4, 0x303305CC, 0x2, 0x30330498
 
#define IOMUXC_UART4_RXD_GPIO5_IO28   0x30330238, 0x5, 0x00000000, 0x0, 0x30330498
 
#define IOMUXC_UART4_TXD_UART4_TX   0x3033023C, 0x0, 0x00000000, 0x0, 0x3033049C
 
#define IOMUXC_UART4_TXD_UART4_RX   0x3033023C, 0x0, 0x30330600, 0x9, 0x3033049C
 
#define IOMUXC_UART4_TXD_UART2_RTS_B   0x3033023C, 0x1, 0x303305EC, 0x5, 0x3033049C
 
#define IOMUXC_UART4_TXD_UART2_CTS_B   0x3033023C, 0x1, 0x00000000, 0x0, 0x3033049C
 
#define IOMUXC_UART4_TXD_GPT1_CAPTURE1   0x3033023C, 0x3, 0x30330594, 0x1, 0x3033049C
 
#define IOMUXC_UART4_TXD_I2C6_SDA   0x3033023C, 0x4, 0x303305D0, 0x2, 0x3033049C
 
#define IOMUXC_UART4_TXD_GPIO5_IO29   0x3033023C, 0x5, 0x00000000, 0x0, 0x3033049C
 
#define IOMUXC_HDMI_DDC_SCL_HDMIMIX_HDMI_SCL   0x30330240, 0x0, 0x00000000, 0x0, 0x303304A0
 
#define IOMUXC_HDMI_DDC_SCL_I2C5_SCL   0x30330240, 0x3, 0x303305C4, 0x3, 0x303304A0
 
#define IOMUXC_HDMI_DDC_SCL_CAN1_TX   0x30330240, 0x4, 0x00000000, 0x0, 0x303304A0
 
#define IOMUXC_HDMI_DDC_SCL_GPIO3_IO26   0x30330240, 0x5, 0x00000000, 0x0, 0x303304A0
 
#define IOMUXC_HDMI_DDC_SCL_EARC_TEST_OUT0   0x30330240, 0x6, 0x00000000, 0x0, 0x303304A0
 
#define IOMUXC_HDMI_DDC_SDA_HDMIMIX_HDMI_SDA   0x30330244, 0x0, 0x00000000, 0x0, 0x303304A4
 
#define IOMUXC_HDMI_DDC_SDA_I2C5_SDA   0x30330244, 0x3, 0x303305C8, 0x3, 0x303304A4
 
#define IOMUXC_HDMI_DDC_SDA_CAN1_RX   0x30330244, 0x4, 0x3033054C, 0x3, 0x303304A4
 
#define IOMUXC_HDMI_DDC_SDA_GPIO3_IO27   0x30330244, 0x5, 0x00000000, 0x0, 0x303304A4
 
#define IOMUXC_HDMI_DDC_SDA_EARC_TEST_OUT1   0x30330244, 0x6, 0x00000000, 0x0, 0x303304A4
 
#define IOMUXC_HDMI_CEC_HDMIMIX_HDMI_CEC   0x30330248, 0x0, 0x00000000, 0x0, 0x303304A8
 
#define IOMUXC_HDMI_CEC_I2C6_SCL   0x30330248, 0x3, 0x303305CC, 0x3, 0x303304A8
 
#define IOMUXC_HDMI_CEC_CAN2_TX   0x30330248, 0x4, 0x00000000, 0x0, 0x303304A8
 
#define IOMUXC_HDMI_CEC_GPIO3_IO28   0x30330248, 0x5, 0x00000000, 0x0, 0x303304A8
 
#define IOMUXC_HDMI_HPD_HDMIMIX_HDMI_HPD   0x3033024C, 0x0, 0x00000000, 0x0, 0x303304AC
 
#define IOMUXC_HDMI_HPD_AUDIOMIX_HDMI_HPD_O   0x3033024C, 0x1, 0x00000000, 0x0, 0x303304AC
 
#define IOMUXC_HDMI_HPD_I2C6_SDA   0x3033024C, 0x3, 0x303305D0, 0x3, 0x303304AC
 
#define IOMUXC_HDMI_HPD_CAN2_RX   0x3033024C, 0x4, 0x30330550, 0x3, 0x303304AC
 
#define IOMUXC_HDMI_HPD_GPIO3_IO29   0x3033024C, 0x5, 0x00000000, 0x0, 0x303304AC
 

Configuration

static void IOMUXC_SetPinMux (uint32_t muxRegister, uint32_t muxMode, uint32_t inputRegister, uint32_t inputDaisy, uint32_t configRegister, uint32_t inputOnfield)
 Sets the IOMUXC pin mux mode. More...
 
static void IOMUXC_SetPinConfig (uint32_t muxRegister, uint32_t muxMode, uint32_t inputRegister, uint32_t inputDaisy, uint32_t configRegister, uint32_t configValue)
 Sets the IOMUXC pin configuration. More...
 

Macro Definition Documentation

#define FSL_IOMUXC_DRIVER_VERSION   (MAKE_VERSION(2, 0, 4))

Function Documentation

static void IOMUXC_SetPinMux ( uint32_t  muxRegister,
uint32_t  muxMode,
uint32_t  inputRegister,
uint32_t  inputDaisy,
uint32_t  configRegister,
uint32_t  inputOnfield 
)
inlinestatic
Note
The first five parameters can be filled with the pin function ID macros.

This is an example to set the I2C4_SDA as the pwm1_OUT:

* IOMUXC_SetPinMux(IOMUXC_I2C4_SDA_PWM1_OUT, 0);
*
Parameters
muxRegisterThe pin mux register_
muxModeThe pin mux mode_
inputRegisterThe select input register_
inputDaisyThe input daisy_
configRegisterThe config register_
inputOnfieldThe pad->module input inversion_
static void IOMUXC_SetPinConfig ( uint32_t  muxRegister,
uint32_t  muxMode,
uint32_t  inputRegister,
uint32_t  inputDaisy,
uint32_t  configRegister,
uint32_t  configValue 
)
inlinestatic
Note
The previous five parameters can be filled with the pin function ID macros.

This is an example to set pin configuration for IOMUXC_I2C4_SDA_PWM1_OUT:

* IOMUXC_SetPinConfig(IOMUXC_I2C4_SDA_PWM1_OUT, IOMUXC_SW_PAD_CTL_PAD_ODE_MASK | IOMUXC0_SW_PAD_CTL_PAD_DSE(2U))
*
Parameters
muxRegisterThe pin mux register_
muxModeThe pin mux mode_
inputRegisterThe select input register_
inputDaisyThe input daisy_
configRegisterThe config register_
configValueThe pin config value_