The MCUXpresso SDK provides a driver for the Pulse Width Modulator (PWM) of MCUXpresso SDK devices.
PWM: Pulse Width Modulator
Initialization and deinitialization
The function PWM_Init() initializes the PWM sub module with specified configurations, the function PWM_GetDefaultConfig() could help to get the default configurations. The initialization function configures the sub module for the requested register update mode for registers with buffers. It also sets up the sub module operation in debug and wait modes.
PWM Operations
The function PWM_SetupPwm() sets up PWM channels for PWM output, the function can set up PWM signal properties for multiple channels. The PWM has 2 channels: A and B. Each channel has its own duty cycle and level-mode specified, however the same PWM period and PWM mode is applied to all channels requesting PWM output. The signal duty cycle is provided as a percentage of the PWM period, its value should be between 0 and 100; 0=inactive signal(0% duty cycle) and 100=always active signal (100% duty cycle). The function also sets up the channel dead time value which is used when the user selects complementary mode of operation.
The function PWM_UpdatePwmDutycycle() updates the PWM signal duty cycle of a particular PWM channel.
Input capture operations
The function PWM_SetupInputCapture() sets up a PWM channel for input capture. The user can specify the capture edge and the mode; one-shot capture or free-running capture.
Fault operation
The function PWM_SetupFault() sets up the properties for each fault.
PWM Start and Stop operations
The function PWM_StartTimer() can be used to start one or multiple sub modules. The function PWM_StopTimer() can be used to stop one or multiple sub modules.
Status
Provide functions to get and clear the PWM status.
Interrupt
Provide functions to enable/disable PWM interrupts and get current enabled interrupts.
Register Update
Some of the PWM registers have buffers, the driver support various methods to update these registers with the content of the register buffer. The update mechanism for register with buffers can be specified through the following fields available in the configuration structure. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/pwmThe user can select one of the reload options provided in enumeration pwm_register_reload_t. When using immediate reload, the reloadFrequency field is not used.
The driver initialization function sets up the appropriate bits in the PWM module based on the register update options selected.
The below function should be used to initiate a register reload. The example shows register reload initiated on PWM sub modules 0, 1, and 2. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/pwm
Typical use case
PWM output
Output PWM signal on 3 PWM sub module with different dutycycles. Periodically update the PWM signal duty cycle. Each sub module runs in Complementary output mode with PWM A used to generate the complementary PWM pair. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/pwm
|
| enum | pwm_submodule_t {
kPWM_Module_0 = 0U,
kPWM_Module_1,
kPWM_Module_2,
kPWM_Module_3
} |
| | List of PWM submodules. More...
|
| |
| enum | pwm_channels_t |
| | List of PWM channels in each module.
|
| |
| enum | pwm_value_register_t {
kPWM_ValueRegister_0 = 0U,
kPWM_ValueRegister_1,
kPWM_ValueRegister_2,
kPWM_ValueRegister_3,
kPWM_ValueRegister_4,
kPWM_ValueRegister_5
} |
| | List of PWM value registers. More...
|
| |
| enum | _pwm_value_register_mask {
kPWM_ValueRegisterMask_0 = (1U << 0),
kPWM_ValueRegisterMask_1 = (1U << 1),
kPWM_ValueRegisterMask_2 = (1U << 2),
kPWM_ValueRegisterMask_3 = (1U << 3),
kPWM_ValueRegisterMask_4 = (1U << 4),
kPWM_ValueRegisterMask_5 = (1U << 5)
} |
| | List of PWM value registers mask. More...
|
| |
| enum | pwm_clock_source_t {
kPWM_BusClock = 0U,
kPWM_ExternalClock,
kPWM_Submodule0Clock
} |
| | PWM clock source selection. More...
|
| |
| enum | pwm_clock_prescale_t {
kPWM_Prescale_Divide_1 = 0U,
kPWM_Prescale_Divide_2,
kPWM_Prescale_Divide_4,
kPWM_Prescale_Divide_8,
kPWM_Prescale_Divide_16,
kPWM_Prescale_Divide_32,
kPWM_Prescale_Divide_64,
kPWM_Prescale_Divide_128
} |
| | PWM prescaler factor selection for clock source. More...
|
| |
| enum | pwm_force_output_trigger_t {
kPWM_Force_Local = 0U,
kPWM_Force_Master,
kPWM_Force_LocalReload,
kPWM_Force_MasterReload,
kPWM_Force_LocalSync,
kPWM_Force_MasterSync,
kPWM_Force_External,
kPWM_Force_ExternalSync
} |
| | Options that can trigger a PWM FORCE_OUT. More...
|
| |
| enum | pwm_init_source_t {
kPWM_Initialize_LocalSync = 0U,
kPWM_Initialize_MasterReload,
kPWM_Initialize_MasterSync,
kPWM_Initialize_ExtSync
} |
| | PWM counter initialization options. More...
|
| |
| enum | pwm_load_frequency_t {
kPWM_LoadEveryOportunity = 0U,
kPWM_LoadEvery2Oportunity,
kPWM_LoadEvery3Oportunity,
kPWM_LoadEvery4Oportunity,
kPWM_LoadEvery5Oportunity,
kPWM_LoadEvery6Oportunity,
kPWM_LoadEvery7Oportunity,
kPWM_LoadEvery8Oportunity,
kPWM_LoadEvery9Oportunity,
kPWM_LoadEvery10Oportunity,
kPWM_LoadEvery11Oportunity,
kPWM_LoadEvery12Oportunity,
kPWM_LoadEvery13Oportunity,
kPWM_LoadEvery14Oportunity,
kPWM_LoadEvery15Oportunity,
kPWM_LoadEvery16Oportunity
} |
| | PWM load frequency selection. More...
|
| |
| enum | pwm_fault_input_t {
kPWM_Fault_0 = 0U,
kPWM_Fault_1,
kPWM_Fault_2,
kPWM_Fault_3
} |
| | List of PWM fault selections. More...
|
| |
| enum | pwm_fault_disable_t {
kPWM_FaultDisable_0 = (1U << 0),
kPWM_FaultDisable_1 = (1U << 1),
kPWM_FaultDisable_2 = (1U << 2),
kPWM_FaultDisable_3 = (1U << 3)
} |
| | List of PWM fault disable mapping selections. More...
|
| |
| enum | pwm_fault_channels_t |
| | List of PWM fault channels.
|
| |
| enum | pwm_input_capture_edge_t {
kPWM_Disable = 0U,
kPWM_FallingEdge,
kPWM_RisingEdge,
kPWM_RiseAndFallEdge
} |
| | PWM capture edge select. More...
|
| |
| enum | pwm_force_signal_t {
kPWM_UsePwm = 0U,
kPWM_InvertedPwm,
kPWM_SoftwareControl,
kPWM_UseExternal
} |
| | PWM output options when a FORCE_OUT signal is asserted. More...
|
| |
| enum | pwm_chnl_pair_operation_t {
kPWM_Independent = 0U,
kPWM_ComplementaryPwmA,
kPWM_ComplementaryPwmB
} |
| | Options available for the PWM A & B pair operation. More...
|
| |
| enum | pwm_register_reload_t {
kPWM_ReloadImmediate = 0U,
kPWM_ReloadPwmHalfCycle,
kPWM_ReloadPwmFullCycle,
kPWM_ReloadPwmHalfAndFullCycle
} |
| | Options available on how to load the buffered-registers with new values. More...
|
| |
| enum | pwm_fault_recovery_mode_t {
kPWM_NoRecovery = 0U,
kPWM_RecoverHalfCycle,
kPWM_RecoverFullCycle,
kPWM_RecoverHalfAndFullCycle
} |
| | Options available on how to re-enable the PWM output when recovering from a fault. More...
|
| |
| enum | pwm_interrupt_enable_t {
kPWM_CompareVal0InterruptEnable = (1U << 0),
kPWM_CompareVal1InterruptEnable = (1U << 1),
kPWM_CompareVal2InterruptEnable = (1U << 2),
kPWM_CompareVal3InterruptEnable = (1U << 3),
kPWM_CompareVal4InterruptEnable = (1U << 4),
kPWM_CompareVal5InterruptEnable = (1U << 5),
kPWM_CaptureX0InterruptEnable = (1U << 6),
kPWM_CaptureX1InterruptEnable = (1U << 7),
kPWM_CaptureB0InterruptEnable = (1U << 8),
kPWM_CaptureB1InterruptEnable = (1U << 9),
kPWM_CaptureA0InterruptEnable = (1U << 10),
kPWM_CaptureA1InterruptEnable = (1U << 11),
kPWM_ReloadInterruptEnable = (1U << 12),
kPWM_ReloadErrorInterruptEnable = (1U << 13),
kPWM_Fault0InterruptEnable = (1U << 16),
kPWM_Fault1InterruptEnable = (1U << 17),
kPWM_Fault2InterruptEnable = (1U << 18),
kPWM_Fault3InterruptEnable = (1U << 19)
} |
| | List of PWM interrupt options. More...
|
| |
| enum | pwm_status_flags_t {
kPWM_CompareVal0Flag = (1U << 0),
kPWM_CompareVal1Flag = (1U << 1),
kPWM_CompareVal2Flag = (1U << 2),
kPWM_CompareVal3Flag = (1U << 3),
kPWM_CompareVal4Flag = (1U << 4),
kPWM_CompareVal5Flag = (1U << 5),
kPWM_CaptureX0Flag = (1U << 6),
kPWM_CaptureX1Flag = (1U << 7),
kPWM_CaptureB0Flag = (1U << 8),
kPWM_CaptureB1Flag = (1U << 9),
kPWM_CaptureA0Flag = (1U << 10),
kPWM_CaptureA1Flag = (1U << 11),
kPWM_ReloadFlag = (1U << 12),
kPWM_ReloadErrorFlag = (1U << 13),
kPWM_RegUpdatedFlag = (1U << 14),
kPWM_Fault0Flag = (1U << 16),
kPWM_Fault1Flag = (1U << 17),
kPWM_Fault2Flag = (1U << 18),
kPWM_Fault3Flag = (1U << 19)
} |
| | List of PWM status flags. More...
|
| |
| enum | pwm_dma_enable_t {
kPWM_CaptureX0DMAEnable = (1U << 0),
kPWM_CaptureX1DMAEnable = (1U << 1),
kPWM_CaptureB0DMAEnable = (1U << 2),
kPWM_CaptureB1DMAEnable = (1U << 3),
kPWM_CaptureA0DMAEnable = (1U << 4),
kPWM_CaptureA1DMAEnable = (1U << 5)
} |
| | List of PWM DMA options. More...
|
| |
| enum | pwm_dma_source_select_t {
kPWM_DMARequestDisable = 0U,
kPWM_DMAWatermarksEnable,
kPWM_DMALocalSync,
kPWM_DMALocalReload
} |
| | List of PWM capture DMA enable source select. More...
|
| |
| enum | pwm_watermark_control_t {
kPWM_FIFOWatermarksOR = 0U,
kPWM_FIFOWatermarksAND
} |
| | PWM FIFO Watermark AND Control. More...
|
| |
| enum | pwm_mode_t {
kPWM_SignedCenterAligned = 0U,
kPWM_CenterAligned,
kPWM_SignedEdgeAligned,
kPWM_EdgeAligned
} |
| | PWM operation mode. More...
|
| |
| enum | pwm_level_select_t {
kPWM_HighTrue = 0U,
kPWM_LowTrue
} |
| | PWM output pulse mode, high-true or low-true. More...
|
| |
| enum | pwm_fault_state_t {
kPWM_PwmFaultState0,
kPWM_PwmFaultState1,
kPWM_PwmFaultState2,
kPWM_PwmFaultState3
} |
| | PWM output fault status. More...
|
| |
| enum | pwm_reload_source_select_t {
kPWM_LocalReload = 0U,
kPWM_MasterReload
} |
| | PWM reload source select. More...
|
| |
| enum | pwm_fault_clear_t {
kPWM_Automatic = 0U,
kPWM_ManualNormal,
kPWM_ManualSafety
} |
| | PWM fault clearing options. More...
|
| |
| enum | pwm_module_control_t {
kPWM_Control_Module_0 = (1U << 0),
kPWM_Control_Module_1 = (1U << 1),
kPWM_Control_Module_2 = (1U << 2),
kPWM_Control_Module_3 = (1U << 3)
} |
| | Options for submodule master control operation. More...
|
| |
|
| void | PWM_SetupInputCapture (PWM_Type *base, pwm_submodule_t subModule, pwm_channels_t pwmChannel, const pwm_input_capture_param_t *inputCaptureParams) |
| | Sets up the PWM input capture. More...
|
| |
| void | PWM_SetupFaultInputFilter (PWM_Type *base, const pwm_fault_input_filter_param_t *faultInputFilterParams) |
| | Sets up the PWM fault input filter. More...
|
| |
| void | PWM_SetupFaults (PWM_Type *base, pwm_fault_input_t faultNum, const pwm_fault_param_t *faultParams) |
| | Sets up the PWM fault protection. More...
|
| |
| void | PWM_FaultDefaultConfig (pwm_fault_param_t *config) |
| | Fill in the PWM fault config struct with the default settings. More...
|
| |
| void | PWM_SetupForceSignal (PWM_Type *base, pwm_submodule_t subModule, pwm_channels_t pwmChannel, pwm_force_signal_t mode) |
| | Selects the signal to output on a PWM pin when a FORCE_OUT signal is asserted. More...
|
| |
| static void | PWM_OutputTriggerEnable (PWM_Type *base, pwm_submodule_t subModule, pwm_value_register_t valueRegister, bool activate) |
| | Enables or disables the PWM output trigger. More...
|
| |
| static void | PWM_ActivateOutputTrigger (PWM_Type *base, pwm_submodule_t subModule, uint16_t valueRegisterMask) |
| | Enables the PWM output trigger. More...
|
| |
| static void | PWM_DeactivateOutputTrigger (PWM_Type *base, pwm_submodule_t subModule, uint16_t valueRegisterMask) |
| | Disables the PWM output trigger. More...
|
| |
| static void | PWM_SetupSwCtrlOut (PWM_Type *base, pwm_submodule_t subModule, pwm_channels_t pwmChannel, bool value) |
| | Sets the software control output for a pin to high or low. More...
|
| |
| static void | PWM_SetPwmLdok (PWM_Type *base, uint8_t subModulesToUpdate, bool value) |
| | Sets or clears the PWM LDOK bit on a single or multiple submodules. More...
|
| |
| static void | PWM_SetPwmFaultState (PWM_Type *base, pwm_submodule_t subModule, pwm_channels_t pwmChannel, pwm_fault_state_t faultState) |
| | Set PWM output fault status. More...
|
| |
| static void | PWM_SetupFaultDisableMap (PWM_Type *base, pwm_submodule_t subModule, pwm_channels_t pwmChannel, pwm_fault_channels_t pwm_fault_channels, uint16_t value) |
| | Set PWM fault disable mapping. More...
|
| |
|
| status_t | PWM_SetupPwm (PWM_Type *base, pwm_submodule_t subModule, const pwm_signal_param_t *chnlParams, uint8_t numOfChnls, pwm_mode_t mode, uint32_t pwmFreq_Hz, uint32_t srcClock_Hz) |
| | Sets up the PWM signals for a PWM submodule. More...
|
| |
| void | PWM_UpdatePwmDutycycle (PWM_Type *base, pwm_submodule_t subModule, pwm_channels_t pwmSignal, pwm_mode_t currPwmMode, uint8_t dutyCyclePercent) |
| | Updates the PWM signal's dutycycle. More...
|
| |
| void | PWM_UpdatePwmDutycycleHighAccuracy (PWM_Type *base, pwm_submodule_t subModule, pwm_channels_t pwmSignal, pwm_mode_t currPwmMode, uint16_t dutyCycle) |
| | Updates the PWM signal's dutycycle with 16-bit accuracy. More...
|
| |
|
| static void | PWM_StartTimer (PWM_Type *base, uint8_t subModulesToStart) |
| | Starts the PWM counter for a single or multiple submodules. More...
|
| |
| static void | PWM_StopTimer (PWM_Type *base, uint8_t subModulesToStop) |
| | Stops the PWM counter for a single or multiple submodules. More...
|
| |
| struct pwm_signal_param_t |
| uint8_t pwm_signal_param_t::dutyCyclePercent |
100=always active signal (100% duty cycle)
This structure holds the configuration settings for the PWM peripheral. To initialize this structure to reasonable defaults, call the PWM_GetDefaultConfig() function and pass a pointer to your config structure instance.
The config struct can be made const so it resides in flash
| struct pwm_fault_input_filter_param_t |
Data Fields |
|
uint8_t | faultFilterCount |
| | Fault filter count.
|
| |
|
uint8_t | faultFilterPeriod |
| | Fault filter period;value of 0 will bypass the filter.
|
| |
|
bool | faultGlitchStretch |
| | Fault Glitch Stretch Enable: A logic 1 means that input fault signals will be stretched to at least 2 IPBus clock cycles.
|
| |
| struct pwm_input_capture_param_t |
| uint8_t pwm_input_capture_param_t::fifoWatermark |
The capture flags in the status register will set if the word count in the FIFO is greater than this watermark level
| Enumerator |
|---|
| kPWM_Module_0 |
Submodule 0.
|
| kPWM_Module_1 |
Submodule 1.
|
| kPWM_Module_2 |
Submodule 2.
|
| kPWM_Module_3 |
Submodule 3.
|
| Enumerator |
|---|
| kPWM_ValueRegister_0 |
PWM Value0 register.
|
| kPWM_ValueRegister_1 |
PWM Value1 register.
|
| kPWM_ValueRegister_2 |
PWM Value2 register.
|
| kPWM_ValueRegister_3 |
PWM Value3 register.
|
| kPWM_ValueRegister_4 |
PWM Value4 register.
|
| kPWM_ValueRegister_5 |
PWM Value5 register.
|
| Enumerator |
|---|
| kPWM_ValueRegisterMask_0 |
PWM Value0 register mask.
|
| kPWM_ValueRegisterMask_1 |
PWM Value1 register mask.
|
| kPWM_ValueRegisterMask_2 |
PWM Value2 register mask.
|
| kPWM_ValueRegisterMask_3 |
PWM Value3 register mask.
|
| kPWM_ValueRegisterMask_4 |
PWM Value4 register mask.
|
| kPWM_ValueRegisterMask_5 |
PWM Value5 register mask.
|
| Enumerator |
|---|
| kPWM_BusClock |
The IPBus clock is used as the clock.
|
| kPWM_ExternalClock |
EXT_CLK is used as the clock.
|
| kPWM_Submodule0Clock |
Clock of the submodule 0 (AUX_CLK) is used as the source clock.
|
| Enumerator |
|---|
| kPWM_Prescale_Divide_1 |
PWM clock frequency = fclk/1.
|
| kPWM_Prescale_Divide_2 |
PWM clock frequency = fclk/2.
|
| kPWM_Prescale_Divide_4 |
PWM clock frequency = fclk/4.
|
| kPWM_Prescale_Divide_8 |
PWM clock frequency = fclk/8.
|
| kPWM_Prescale_Divide_16 |
PWM clock frequency = fclk/16.
|
| kPWM_Prescale_Divide_32 |
PWM clock frequency = fclk/32.
|
| kPWM_Prescale_Divide_64 |
PWM clock frequency = fclk/64.
|
| kPWM_Prescale_Divide_128 |
PWM clock frequency = fclk/128.
|
| Enumerator |
|---|
| kPWM_Force_Local |
The local force signal, CTRL2[FORCE], from the submodule is used to force updates.
|
| kPWM_Force_Master |
The master force signal from submodule 0 is used to force updates.
|
| kPWM_Force_LocalReload |
The local reload signal from this submodule is used to force updates without regard to the state of LDOK.
|
| kPWM_Force_MasterReload |
The master reload signal from submodule 0 is used to force updates if LDOK is set.
|
| kPWM_Force_LocalSync |
The local sync signal from this submodule is used to force updates.
|
| kPWM_Force_MasterSync |
The master sync signal from submodule0 is used to force updates.
|
| kPWM_Force_External |
The external force signal, EXT_FORCE, from outside the PWM module causes updates.
|
| kPWM_Force_ExternalSync |
The external sync signal, EXT_SYNC, from outside the PWM module causes updates.
|
| Enumerator |
|---|
| kPWM_Initialize_LocalSync |
Local sync causes initialization.
|
| kPWM_Initialize_MasterReload |
Master reload from submodule 0 causes initialization.
|
| kPWM_Initialize_MasterSync |
Master sync from submodule 0 causes initialization.
|
| kPWM_Initialize_ExtSync |
EXT_SYNC causes initialization.
|
| Enumerator |
|---|
| kPWM_LoadEveryOportunity |
Every PWM opportunity.
|
| kPWM_LoadEvery2Oportunity |
Every 2 PWM opportunities.
|
| kPWM_LoadEvery3Oportunity |
Every 3 PWM opportunities.
|
| kPWM_LoadEvery4Oportunity |
Every 4 PWM opportunities.
|
| kPWM_LoadEvery5Oportunity |
Every 5 PWM opportunities.
|
| kPWM_LoadEvery6Oportunity |
Every 6 PWM opportunities.
|
| kPWM_LoadEvery7Oportunity |
Every 7 PWM opportunities.
|
| kPWM_LoadEvery8Oportunity |
Every 8 PWM opportunities.
|
| kPWM_LoadEvery9Oportunity |
Every 9 PWM opportunities.
|
| kPWM_LoadEvery10Oportunity |
Every 10 PWM opportunities.
|
| kPWM_LoadEvery11Oportunity |
Every 11 PWM opportunities.
|
| kPWM_LoadEvery12Oportunity |
Every 12 PWM opportunities.
|
| kPWM_LoadEvery13Oportunity |
Every 13 PWM opportunities.
|
| kPWM_LoadEvery14Oportunity |
Every 14 PWM opportunities.
|
| kPWM_LoadEvery15Oportunity |
Every 15 PWM opportunities.
|
| kPWM_LoadEvery16Oportunity |
Every 16 PWM opportunities.
|
| Enumerator |
|---|
| kPWM_Fault_0 |
Fault 0 input pin.
|
| kPWM_Fault_1 |
Fault 1 input pin.
|
| kPWM_Fault_2 |
Fault 2 input pin.
|
| kPWM_Fault_3 |
Fault 3 input pin.
|
| Enumerator |
|---|
| kPWM_FaultDisable_0 |
Fault 0 disable mapping.
|
| kPWM_FaultDisable_1 |
Fault 1 disable mapping.
|
| kPWM_FaultDisable_2 |
Fault 2 disable mapping.
|
| kPWM_FaultDisable_3 |
Fault 3 disable mapping.
|
| Enumerator |
|---|
| kPWM_Disable |
Disabled.
|
| kPWM_FallingEdge |
Capture on falling edge only.
|
| kPWM_RisingEdge |
Capture on rising edge only.
|
| kPWM_RiseAndFallEdge |
Capture on rising or falling edge.
|
| Enumerator |
|---|
| kPWM_UsePwm |
Generated PWM signal is used by the deadtime logic.
|
| kPWM_InvertedPwm |
Inverted PWM signal is used by the deadtime logic.
|
| kPWM_SoftwareControl |
Software controlled value is used by the deadtime logic.
|
| kPWM_UseExternal |
PWM_EXTA signal is used by the deadtime logic.
|
| Enumerator |
|---|
| kPWM_Independent |
PWM A & PWM B operate as 2 independent channels.
|
| kPWM_ComplementaryPwmA |
PWM A & PWM B are complementary channels, PWM A generates the signal.
|
| kPWM_ComplementaryPwmB |
PWM A & PWM B are complementary channels, PWM B generates the signal.
|
| Enumerator |
|---|
| kPWM_ReloadImmediate |
Buffered-registers get loaded with new values as soon as LDOK bit is set.
|
| kPWM_ReloadPwmHalfCycle |
Registers loaded on a PWM half cycle.
|
| kPWM_ReloadPwmFullCycle |
Registers loaded on a PWM full cycle.
|
| kPWM_ReloadPwmHalfAndFullCycle |
Registers loaded on a PWM half & full cycle.
|
| Enumerator |
|---|
| kPWM_NoRecovery |
PWM output will stay inactive.
|
| kPWM_RecoverHalfCycle |
PWM output re-enabled at the first half cycle.
|
| kPWM_RecoverFullCycle |
PWM output re-enabled at the first full cycle.
|
| kPWM_RecoverHalfAndFullCycle |
PWM output re-enabled at the first half or full cycle.
|
| Enumerator |
|---|
| kPWM_CompareVal0InterruptEnable |
PWM VAL0 compare interrupt.
|
| kPWM_CompareVal1InterruptEnable |
PWM VAL1 compare interrupt.
|
| kPWM_CompareVal2InterruptEnable |
PWM VAL2 compare interrupt.
|
| kPWM_CompareVal3InterruptEnable |
PWM VAL3 compare interrupt.
|
| kPWM_CompareVal4InterruptEnable |
PWM VAL4 compare interrupt.
|
| kPWM_CompareVal5InterruptEnable |
PWM VAL5 compare interrupt.
|
| kPWM_CaptureX0InterruptEnable |
PWM capture X0 interrupt.
|
| kPWM_CaptureX1InterruptEnable |
PWM capture X1 interrupt.
|
| kPWM_CaptureB0InterruptEnable |
PWM capture B0 interrupt.
|
| kPWM_CaptureB1InterruptEnable |
PWM capture B1 interrupt.
|
| kPWM_CaptureA0InterruptEnable |
PWM capture A0 interrupt.
|
| kPWM_CaptureA1InterruptEnable |
PWM capture A1 interrupt.
|
| kPWM_ReloadInterruptEnable |
PWM reload interrupt.
|
| kPWM_ReloadErrorInterruptEnable |
PWM reload error interrupt.
|
| kPWM_Fault0InterruptEnable |
PWM fault 0 interrupt.
|
| kPWM_Fault1InterruptEnable |
PWM fault 1 interrupt.
|
| kPWM_Fault2InterruptEnable |
PWM fault 2 interrupt.
|
| kPWM_Fault3InterruptEnable |
PWM fault 3 interrupt.
|
| Enumerator |
|---|
| kPWM_CompareVal0Flag |
PWM VAL0 compare flag.
|
| kPWM_CompareVal1Flag |
PWM VAL1 compare flag.
|
| kPWM_CompareVal2Flag |
PWM VAL2 compare flag.
|
| kPWM_CompareVal3Flag |
PWM VAL3 compare flag.
|
| kPWM_CompareVal4Flag |
PWM VAL4 compare flag.
|
| kPWM_CompareVal5Flag |
PWM VAL5 compare flag.
|
| kPWM_CaptureX0Flag |
PWM capture X0 flag.
|
| kPWM_CaptureX1Flag |
PWM capture X1 flag.
|
| kPWM_CaptureB0Flag |
PWM capture B0 flag.
|
| kPWM_CaptureB1Flag |
PWM capture B1 flag.
|
| kPWM_CaptureA0Flag |
PWM capture A0 flag.
|
| kPWM_CaptureA1Flag |
PWM capture A1 flag.
|
| kPWM_ReloadFlag |
PWM reload flag.
|
| kPWM_ReloadErrorFlag |
PWM reload error flag.
|
| kPWM_RegUpdatedFlag |
PWM registers updated flag.
|
| kPWM_Fault0Flag |
PWM fault 0 flag.
|
| kPWM_Fault1Flag |
PWM fault 1 flag.
|
| kPWM_Fault2Flag |
PWM fault 2 flag.
|
| kPWM_Fault3Flag |
PWM fault 3 flag.
|
| Enumerator |
|---|
| kPWM_CaptureX0DMAEnable |
PWM capture X0 DMA.
|
| kPWM_CaptureX1DMAEnable |
PWM capture X1 DMA.
|
| kPWM_CaptureB0DMAEnable |
PWM capture B0 DMA.
|
| kPWM_CaptureB1DMAEnable |
PWM capture B1 DMA.
|
| kPWM_CaptureA0DMAEnable |
PWM capture A0 DMA.
|
| kPWM_CaptureA1DMAEnable |
PWM capture A1 DMA.
|
| Enumerator |
|---|
| kPWM_DMARequestDisable |
Read DMA requests disabled.
|
| kPWM_DMAWatermarksEnable |
Exceeding a FIFO watermark sets the DMA read request.
|
| kPWM_DMALocalSync |
A local sync (VAL1 matches counter) sets the read DMA request.
|
| kPWM_DMALocalReload |
A local reload (STS[RF] being set) sets the read DMA request.
|
| Enumerator |
|---|
| kPWM_FIFOWatermarksOR |
Selected FIFO watermarks are OR'ed together.
|
| kPWM_FIFOWatermarksAND |
Selected FIFO watermarks are AND'ed together.
|
| Enumerator |
|---|
| kPWM_SignedCenterAligned |
Signed center-aligned.
|
| kPWM_CenterAligned |
Unsigned cente-aligned.
|
| kPWM_SignedEdgeAligned |
Signed edge-aligned.
|
| kPWM_EdgeAligned |
Unsigned edge-aligned.
|
| Enumerator |
|---|
| kPWM_HighTrue |
High level represents "on" or "active" state.
|
| kPWM_LowTrue |
Low level represents "on" or "active" state.
|
| Enumerator |
|---|
| kPWM_PwmFaultState0 |
Output is forced to logic 0 state prior to consideration of output polarity control.
|
| kPWM_PwmFaultState1 |
Output is forced to logic 1 state prior to consideration of output polarity control.
|
| kPWM_PwmFaultState2 |
Output is tristated.
|
| kPWM_PwmFaultState3 |
Output is tristated.
|
| Enumerator |
|---|
| kPWM_LocalReload |
The local reload signal is used to reload registers.
|
| kPWM_MasterReload |
The master reload signal (from submodule 0) is used to reload.
|
| Enumerator |
|---|
| kPWM_Automatic |
Automatic fault clearing.
|
| kPWM_ManualNormal |
Manual fault clearing with no fault safety mode.
|
| kPWM_ManualSafety |
Manual fault clearing with fault safety mode.
|
| Enumerator |
|---|
| kPWM_Control_Module_0 |
Control submodule 0's start/stop,buffer reload operation.
|
| kPWM_Control_Module_1 |
Control submodule 1's start/stop,buffer reload operation.
|
| kPWM_Control_Module_2 |
Control submodule 2's start/stop,buffer reload operation.
|
| kPWM_Control_Module_3 |
Control submodule 3's start/stop,buffer reload operation.
|
- Note
- This API should be called at the beginning of the application using the PWM driver.
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| config | Pointer to user's PWM config structure. |
- Returns
- kStatus_Success means success; else failed.
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to deinitialize |
The default values are:
* config->enableDebugMode = false;
* config->enableWait = false;
*
- Parameters
-
| config | Pointer to user's PWM config structure. |
The function initializes the submodule according to the parameters passed in by the user. The function also sets up the value compare registers to match the PWM signal requirements. If the dead time insertion logic is enabled, the pulse period is reduced by the dead time period specified by the user.
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| chnlParams | Array of PWM channel parameters to configure the channel(s) |
| numOfChnls | Number of channels to configure, this should be the size of the array passed in. Array size should not be more than 2 as each submodule has 2 pins to output PWM |
| mode | PWM operation mode, options available in enumeration pwm_mode_t |
| pwmFreq_Hz | PWM signal frequency in Hz |
| srcClock_Hz | PWM main counter clock in Hz. |
- Returns
- Returns kStatusFail if there was error setting up the signal; kStatusSuccess otherwise
The function updates the PWM dutycyle to the new value that is passed in. If the dead time insertion logic is enabled then the pulse period is reduced by the dead time period specified by the user.
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| pwmSignal | Signal (PWM A or PWM B) to update |
| currPwmMode | The current PWM mode set during PWM setup |
| dutyCyclePercent | New PWM pulse width, value should be between 0 to 100 0=inactive signal(0% duty cycle)... 100=active signal (100% duty cycle) |
The function updates the PWM dutycyle to the new value that is passed in. If the dead time insertion logic is enabled then the pulse period is reduced by the dead time period specified by the user.
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| pwmSignal | Signal (PWM A or PWM B) to update |
| currPwmMode | The current PWM mode set during PWM setup |
| dutyCycle | New PWM pulse width, value should be between 0 to 65535 0=inactive signal(0% duty cycle)... 65535=active signal (100% duty cycle) |
Each PWM submodule has 3 pins that can be configured for use as input capture pins. This function sets up the capture parameters for each pin and enables the pin for input capture operation.
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| pwmChannel | Channel in the submodule to setup |
| inputCaptureParams | Parameters passed in to set up the input pin |
- Parameters
-
| base | PWM peripheral base address |
| faultInputFilterParams | Parameters passed in to set up the fault input filter. |
PWM has 4 fault inputs.
- Parameters
-
| base | PWM peripheral base address |
| faultNum | PWM fault to configure. |
| faultParams | Pointer to the PWM fault config structure |
The default values are:
* config->faultLevel = false;
* config->enableCombinationalPath = true;
*
- Parameters
-
| config | Pointer to user's PWM fault config structure. |
The user specifies which channel to configure by supplying the submodule number and whether to modify PWM A or PWM B within that submodule.
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| pwmChannel | Channel to configure |
| mode | Signal to output when a FORCE_OUT is triggered |
| void PWM_EnableInterrupts |
( |
PWM_Type * |
base, |
|
|
pwm_submodule_t |
subModule, |
|
|
uint32_t |
mask |
|
) |
| |
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| mask | The interrupts to enable. This is a logical OR of members of the enumeration pwm_interrupt_enable_t |
| void PWM_DisableInterrupts |
( |
PWM_Type * |
base, |
|
|
pwm_submodule_t |
subModule, |
|
|
uint32_t |
mask |
|
) |
| |
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| mask | The interrupts to enable. This is a logical OR of members of the enumeration pwm_interrupt_enable_t |
| uint32_t PWM_GetEnabledInterrupts |
( |
PWM_Type * |
base, |
|
|
pwm_submodule_t |
subModule |
|
) |
| |
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
- Returns
- The enabled interrupts. This is the logical OR of members of the enumeration pwm_interrupt_enable_t
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| pwm_watermark_control | PWM FIFO watermark and control |
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| pwm_dma_source_select | PWM capture DMA enable source select |
| static void PWM_EnableDMACapture |
( |
PWM_Type * |
base, |
|
|
pwm_submodule_t |
subModule, |
|
|
uint16_t |
mask, |
|
|
bool |
activate |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| mask | The DMA to enable or disable. This is a logical OR of members of the enumeration pwm_dma_enable_t |
| activate | true: Enable DMA read request; false: Disable DMA read request |
| static void PWM_EnableDMAWrite |
( |
PWM_Type * |
base, |
|
|
pwm_submodule_t |
subModule, |
|
|
bool |
activate |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| activate | true: Enable DMA write request; false: Disable DMA write request |
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
- Returns
- The status flags. This is the logical OR of members of the enumeration pwm_status_flags_t
| void PWM_ClearStatusFlags |
( |
PWM_Type * |
base, |
|
|
pwm_submodule_t |
subModule, |
|
|
uint32_t |
mask |
|
) |
| |
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| mask | The status flags to clear. This is a logical OR of members of the enumeration pwm_status_flags_t |
| static void PWM_StartTimer |
( |
PWM_Type * |
base, |
|
|
uint8_t |
subModulesToStart |
|
) |
| |
|
inlinestatic |
Sets the Run bit which enables the clocks to the PWM submodule. This function can start multiple submodules at the same time.
- Parameters
-
| base | PWM peripheral base address |
| subModulesToStart | PWM submodules to start. This is a logical OR of members of the enumeration pwm_module_control_t |
| static void PWM_StopTimer |
( |
PWM_Type * |
base, |
|
|
uint8_t |
subModulesToStop |
|
) |
| |
|
inlinestatic |
Clears the Run bit which resets the submodule's counter. This function can stop multiple submodules at the same time.
- Parameters
-
| base | PWM peripheral base address |
| subModulesToStop | PWM submodules to stop. This is a logical OR of members of the enumeration pwm_module_control_t |
This function allows the user to enable or disable the PWM trigger. The PWM has 2 triggers. Trigger 0 is activated when the counter matches VAL 0, VAL 2, or VAL 4 register. Trigger 1 is activated when the counter matches VAL 1, VAL 3, or VAL 5 register.
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| valueRegister | Value register that will activate the trigger |
| activate | true: Enable the trigger; false: Disable the trigger |
| static void PWM_ActivateOutputTrigger |
( |
PWM_Type * |
base, |
|
|
pwm_submodule_t |
subModule, |
|
|
uint16_t |
valueRegisterMask |
|
) |
| |
|
inlinestatic |
This function allows the user to enable one or more (VAL0-5) PWM trigger.
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| valueRegisterMask | Value register mask that will activate one or more (VAL0-5) trigger enumeration _pwm_value_register_mask |
| static void PWM_DeactivateOutputTrigger |
( |
PWM_Type * |
base, |
|
|
pwm_submodule_t |
subModule, |
|
|
uint16_t |
valueRegisterMask |
|
) |
| |
|
inlinestatic |
This function allows the user to disables one or more (VAL0-5) PWM trigger.
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| valueRegisterMask | Value register mask that will Deactivate one or more (VAL0-5) trigger enumeration _pwm_value_register_mask |
The user specifies which channel to modify by supplying the submodule number and whether to modify PWM A or PWM B within that submodule.
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| pwmChannel | Channel to configure |
| value | true: Supply a logic 1, false: Supply a logic 0. |
| static void PWM_SetPwmLdok |
( |
PWM_Type * |
base, |
|
|
uint8_t |
subModulesToUpdate, |
|
|
bool |
value |
|
) |
| |
|
inlinestatic |
Set LDOK bit to load buffered values into CTRL[PRSC] and the INIT, FRACVAL and VAL registers. The values are loaded immediately if kPWM_ReloadImmediate option was choosen during config. Else the values are loaded at the next PWM reload point. This function can issue the load command to multiple submodules at the same time.
- Parameters
-
| base | PWM peripheral base address |
| subModulesToUpdate | PWM submodules to update with buffered values. This is a logical OR of members of the enumeration pwm_module_control_t |
| value | true: Set LDOK bit for the submodule list; false: Clear LDOK bit |
These bits determine the fault state for the PWM_A output in fault conditions and STOP mode. It may also define the output state in WAIT and DEBUG modes depending on the settings of CTRL2[WAITEN] and CTRL2[DBGEN]. This function can update PWM output fault status.
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| pwmChannel | Channel to configure |
| faultState | PWM output fault status |
Each of the four bits of this read/write field is one-to-one associated with the four FAULTx inputs of fault channel 0/1. The PWM output will be turned off if there is a logic 1 on an FAULTx input and a 1 in the corresponding bit of this field. A reset sets all bits in this field.
- Parameters
-
| base | PWM peripheral base address |
| subModule | PWM submodule to configure |
| pwmChannel | PWM channel to configure |
| pwm_fault_channels | PWM fault channel to configure |
| value | Fault disable mapping mask value enumeration pwm_fault_disable_t |